6.15. CDD_UART

6.15.1. Types

Base type

Type Name

Brief

enum

Cdd_Uart_Instance

Uart Configuration Instance ID.

enum

Cdd_Uart_WordLength

UART Word Length.

enum

Cdd_Uart_StopBits

UART Stop Bits.

enum

Cdd_Uart_Mode

UART Mode.

enum

Cdd_Uart_FifoLevel

UART FIFO Level.

typedef void(*)(void)

Cdd_Uart_CallbackType

Cdd Uart Callback type.

typedef uint8

Cdd_Uart_DataBufferType

Typedef for the data buffer elements.

6.15.1.1. enum Cdd_Uart_Instance

Enumerator

Value

Description

CDD_UART_INSTANCE_UARTA

0U

UARTA Config Instance.

CDD_UART_INSTANCE_UARTB

1U

UARTB Config Instance.

CDD_UART_INSTANCE_UARTC

2U

UARTC Config Instance.

CDD_UART_INSTANCE_UARTD

3U

UARTD Config Instance.

CDD_UART_INSTANCE_UARTE

4U

UARTE Config Instance.

CDD_UART_INSTANCE_UARTF

5U

UARTF Config Instance.

Brief: Uart Configuration Instance ID.

6.15.1.2. enum Cdd_Uart_WordLength

Enumerator

Value

Description

CDD_UART_WORD_LENGTH_5

0U

UART Word Length 5 bits.

CDD_UART_WORD_LENGTH_6

1U

UART Word Length 6 bits.

CDD_UART_WORD_LENGTH_7

2U

UART Word Length 7 bits.

CDD_UART_WORD_LENGTH_8

3U

UART Word Length 8 bits.

Brief: UART Word Length.

6.15.1.3. enum Cdd_Uart_StopBits

Enumerator

Value

Description

CDD_UART_STOP_BITS_1

0U

UART Stop Bits 1 bit.

CDD_UART_STOP_BITS_2

1U

UART Stop Bits 2 bits.

Brief: UART Stop Bits.

6.15.1.4. enum Cdd_Uart_Mode

Enumerator

Value

Description

CDD_UART_MODE_POLLING

0U

UART Mode Polling.

CDD_UART_MODE_INTERRUPT

1U

UART Mode Interrupt.

Brief: UART Mode.

6.15.1.5. enum Cdd_Uart_FifoLevel

Enumerator

Value

Description

CDD_UART_FIFO_LEVEL_1_8

0U

UART FIFO Level 1/8.

CDD_UART_FIFO_LEVEL_1_4

1U

UART FIFO Level 1/4.

CDD_UART_FIFO_LEVEL_1_2

2U

UART FIFO Level 1/2.

CDD_UART_FIFO_LEVEL_3_4

3U

UART FIFO Level 3/4.

CDD_UART_FIFO_LEVEL_7_8

4U

UART FIFO Level 7/8.

Brief: UART FIFO Level.

6.15.1.6. typedef Cdd_Uart_CallbackType

typedef void(* Cdd_Uart_CallbackType) (void);

Brief: Cdd Uart Callback type.

6.15.1.7. typedef Cdd_Uart_DataBufferType

typedef uint8 Cdd_Uart_DataBufferType;

Brief: Typedef for the data buffer elements.

6.15.2. Structures

Name

Brief

Cdd_Uart_CfgType

UART configuration data structure for a channel.

Cdd_Uart_ConfigType

UART configuration structure for all channels in use.

Cdd_Uart_WriteStatusType

Typedef for the Write Status.

Cdd_Uart_ReadStatusType

Typedef for the Read Status.

6.15.3. Defines

Name

Brief

CDD_UART_SW_MAJOR_VERSION

Driver Implementation Major Version.

CDD_UART_SW_MINOR_VERSION

Driver Implementation Minor Version.

CDD_UART_SW_PATCH_VERSION

Driver Implementation Patch Version.

CDD_UART_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CDD_UART Driver.

CDD_UART_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CDD_UART Driver.

CDD_UART_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CDD_UART Driver.

CDD_UART_VENDOR_ID

Texas Instruments Vendor ID.

CDD_UART_MODULE_ID

CDD UART Driver Module ID.

CDD_UART_INSTANCE_ID

CDD UART Instance ID.

CDD_UART_E_UNINIT

API service used without module initialization.

CDD_UART_E_ALREADY_INITIALIZED

API Cdd_Uart_Init service called while the UART driver has already been initialized.

CDD_UART_E_PARAM_VALUE

API service called with invalid parameter value.

CDD_UART_E_PARAM_POINTER

API service called with invalid data buffer pointer.

CDD_UART_E_PARAM_HWINDEX

API service called with invalid hardware index.

CDD_UART_E_BUSY

CDD_UART_NO_ERROR

CDD_UART_SID_GET_VERSION_INFO

Cdd_Uart_GetVersionInfo API Service ID.

CDD_UART_SID_INIT

Cdd_Uart_Init() API Service ID.

CDD_UART_SID_DEINIT

Cdd_Uart_DeInit() API Service ID.

CDD_UART_SID_WRITE

Cdd_Uart_Write() API Service ID.

CDD_UART_SID_READ

Cdd_Uart_Read() API Service ID.

CDD_UART_SID_CANCEL_WRITE

Cdd_Uart_CancelWrite() API Service ID.

CDD_UART_SID_CANCEL_READ

Cdd_Uart_CancelRead() API Service ID.

CDD_UART_SID_GET_WRITE_STATUS

Cdd_Uart_GetWriteStatus() API Service ID.

CDD_UART_SID_GET_READ_STATUS

Cdd_Uart_GetReadStatus() API Service ID.

CDD_UART_SID_MAIN_FUN_WRITE

Cdd_Uart_MainFunction_Write() API Service ID.

CDD_UART_SID_POLL_READ

Cdd_Uart_Poll_Read() API Service ID.

CDD_UART_SID_ERROR_STATUS

Cdd_Uart_GetErrorStatus() API Service ID.

CDD_UART_SID_FLUSH_READ_BUFFER

Cdd_Uart_FlushReadFIFO() API Service ID.

6.15.4. Functions

Return type

Function Name

Brief

void

Cdd_Uart_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr)

Service to provide the version information of Cdd Uart module.

void

Cdd_Uart_Init(const Cdd_Uart_ConfigType * ConfigPtr)

Cdd_Uart_Init : Initializes the CDD_UART module.

void

Cdd_Uart_Deinit(void )

Cdd_Uart_Deinit : De-initializes the CDD_UART module.

Std_ReturnType

Cdd_Uart_Write(uint8 HwUnitId, const Cdd_Uart_DataBufferType * SrcBufferPtr, uint32 Count)

Service to transmit data.

Std_ReturnType

Cdd_Uart_Read(uint8 HwUnitId, Cdd_Uart_DataBufferType * DestBufferPtr, uint32 Count)

Service to reception of data.

Std_ReturnType

Cdd_Uart_CancelWrite(uint8 HwUnitId)

Service to cancel the ongoing transmission.

Std_ReturnType

Cdd_Uart_CancelRead(uint8 HwUnitId)

Service to cancel the ongoing transmission.

Std_ReturnType

Cdd_Uart_GetWriteStatus(uint8 HwUnitId, Cdd_Uart_WriteStatusType * WriteStatus)

Service to get the status of the ongoing transmission.

Std_ReturnType

Cdd_Uart_GetReadStatus(uint8 HwUnitId, Cdd_Uart_ReadStatusType * ReadStatus)

Service to get the status of the ongoing transmission.

void

Cdd_Uart_MainFunction_Write(void )

Service to auto perform the polling of configured UART Write channel.

void

Cdd_Uart_Poll_Read(void )

Service to perform the polling of confgured UART Read channel by user.

Std_ReturnType

Cdd_Uart_GetErrorStatus(uint8 HwUnitId, uint8 * ErrorStatus)

Service to get the status of the Uart error. User can use this service in the Error callback implementation to fetch the exact Uart Error.

void

Cdd_Uart_FlushReadFIFO(uint8 HwUnitId)

Service to flush the read buffer. User can use this service to flush the readbuffer incase of any unread data after any Uart Error.

6.15.4.1. function Cdd_Uart_GetVersionInfo

void Cdd_Uart_GetVersionInfo(
    Std_VersionInfoType * VersionInfoPtr
)

Brief: Service to provide the version information of Cdd Uart module.

Parameters:

  • VersionInfoPtr is the pointer to CDD UART driver version information

Returns:

  • None

Return: None

Precondition: This API is available only if CDD_UART_GET_VERSION_INFO_API is STD_ON

Postcondition: None

6.15.4.2. function Cdd_Uart_Init

void Cdd_Uart_Init(
    const Cdd_Uart_ConfigType * ConfigPtr
)

Brief: Cdd_Uart_Init : Initializes the CDD_UART module.

This service initialize the CDD_UART driver

Parameters:

  • ConfigPtr Pointer to CDD_UART driver configuration set

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.15.4.3. function Cdd_Uart_Deinit

void Cdd_Uart_Deinit(
    void 
)

Brief: Cdd_Uart_Deinit : De-initializes the CDD_UART module.

This service deinitialize the CDD_UART driver

Returns:

  • None

Return: None

Precondition: Cdd_Uart_Init should be called first, before calling this service.

Postcondition: None

6.15.4.4. function Cdd_Uart_Write

Std_ReturnType Cdd_Uart_Write(
    uint8 HwUnitId,
    const Cdd_Uart_DataBufferType * SrcBufferPtr,
    uint32 Count
)

Brief: Service to transmit data.

Parameters:

  • HwUnitId number to be used for writing data

  • SrcBufferPtr - Pointer to source data buffer

  • Count - number of data elements to be transmitted from SrcBufferPtr

Returns:

  • E_OK Write request has been accepted.

  • E_NOT_OK Write request has not been accepted.

Return: Cdd_Uart_Write request is accepted or not

Precondition: None

Postcondition: None

6.15.4.5. function Cdd_Uart_Read

Std_ReturnType Cdd_Uart_Read(
    uint8 HwUnitId,
    Cdd_Uart_DataBufferType * DestBufferPtr,
    uint32 Count
)

Brief: Service to reception of data.

Parameters:

  • HwUnitId number to be used for writing data

  • DestBufferPtr - Pointer to dest data buffer

  • Count - number of data elements to be read into DestBufferPtr

Returns:

  • E_OK Read request has been accepted.

  • E_NOT_OK Read request has not been accepted.

Return: Cdd_Uart_Read request is accepted or not

Precondition: None

Postcondition: None

6.15.4.6. function Cdd_Uart_CancelWrite

Std_ReturnType Cdd_Uart_CancelWrite(
    uint8 HwUnitId
)

Brief: Service to cancel the ongoing transmission.

Parameters:

  • HwUnitId number to be used for cancellation of Write

Returns:

  • E_OK CancelWrite request has been accepted.

  • E_NOT_OK CancelWrite request has not been accepted.

Return: Cdd_Uart_CancelWrite request is accepted or not

Precondition: None

Postcondition: None

6.15.4.7. function Cdd_Uart_CancelRead

Std_ReturnType Cdd_Uart_CancelRead(
    uint8 HwUnitId
)

Brief: Service to cancel the ongoing transmission.

Parameters:

  • HwUnitId number to be used for cancellation of Write

Returns:

  • E_OK CancelRead request has been accepted.

  • E_NOT_OK CancelRead request has not been accepted.

Return: Cdd_Uart_CancelRead request is accepted or not

Precondition: None

Postcondition: None

6.15.4.8. function Cdd_Uart_GetWriteStatus

Std_ReturnType Cdd_Uart_GetWriteStatus(
    uint8 HwUnitId,
    Cdd_Uart_WriteStatusType * WriteStatus
)

Brief: Service to get the status of the ongoing transmission.

Parameters:

  • HwUnitId hw id to be used for status of Write

  • WriteStatus pointer to Cdd_Uart_WriteStatusType

Returns:

  • E_OK GetWriteStatus request has been accepted.

  • E_NOT_OK GetWriteStatus request has not been accepted.

Return: Cdd_Uart_GetWriteStatus request is accepted or not

Precondition: None

Postcondition: None

6.15.4.9. function Cdd_Uart_GetReadStatus

Std_ReturnType Cdd_Uart_GetReadStatus(
    uint8 HwUnitId,
    Cdd_Uart_ReadStatusType * ReadStatus
)

Brief: Service to get the status of the ongoing transmission.

Parameters:

  • HwUnitId hw id to be used for status of Read

  • ReadStatus pointer to Cdd_Uart_ReadStatusType

Returns:

  • E_OK GetReadStatus request has been accepted.

  • E_NOT_OK GetReadStatus request has not been accepted.

Return: Cdd_Uart_GetReadStatus request is accepted or not

Precondition: None

Postcondition: None

6.15.4.10. function Cdd_Uart_MainFunction_Write

void Cdd_Uart_MainFunction_Write(
    void 
)

Brief: Service to auto perform the polling of configured UART Write channel.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.15.4.11. function Cdd_Uart_Poll_Read

void Cdd_Uart_Poll_Read(
    void 
)

Brief: Service to perform the polling of confgured UART Read channel by user.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.15.4.12. function Cdd_Uart_GetErrorStatus

Std_ReturnType Cdd_Uart_GetErrorStatus(
    uint8 HwUnitId,
    uint8 * ErrorStatus
)

Brief: Service to get the status of the Uart error. User can use this service in the Error callback implementation to fetch the exact Uart Error.

Parameters:

  • HwUnitId hw id to be used for status of Error

  • ErrorStatus pointer to Cdd_Uart_Error type

Returns:

  • E_OK Error status request has been accepted

  • E_NOT_OK Error status request has not been accepted

Return: Uart error : PE,OE,BE,FE

Precondition: None

Postcondition: None

6.15.4.13. function Cdd_Uart_FlushReadFIFO

void Cdd_Uart_FlushReadFIFO(
    uint8 HwUnitId
)

Brief: Service to flush the read buffer. User can use this service to flush the readbuffer incase of any unread data after any Uart Error.

Parameters:

  • HwUnitId hw id to be used to flush the read buffer

Returns:

  • None

Return: None

Precondition: None

Postcondition: None