SYSCTL Module¶
System Control (SysCtl) determines the overall operation of the device. The API provides functions to configure the clocking of the device, the set of peripherals that are enabled, the windowed watchdog, the NMI watchdog, and low-power modes. It also provides functions to handle and obtain information about resets and missing clock detection failures.
-
group
sysctl_api Defines
-
SYSCTL_CLKSRCCTL_DELAYasm(" RPT #250 || NOP \n RPT #50 || NOP")¶
-
SYSCTL_REGWRITE_DELAYasm(" RPT #45 || NOP")¶
-
SYSCTL_WD_CHKBITS0x0028U¶
-
SYSCTL_WD_ENRSTKEY0x0055U¶
-
SYSCTL_WD_RSTKEY0x00AAU¶
-
SYSCTL_PERIPH_REG_M0x001FU¶
-
SYSCTL_PERIPH_REG_S0x0000U¶
-
SYSCTL_PERIPH_BIT_M0x1F00U¶
-
SYSCTL_PERIPH_BIT_S0x0008U¶
-
SYSCTL_REG_KEY0xA5A50000U¶
-
SYSCTL_PLL_KEY0XCAFE0000U¶
-
SYSCTL_TYPE_LOCK_S0xFU¶
-
SYSCTL_LPM_IDLE0x0000U¶
-
SYSCTL_LPM_STANDBY0x0001U¶
-
SYSCTL_LPM_HALT0x0002U¶
-
SYSCTL_DEFAULT_OSC_FREQ10000000U¶
-
SYSCTL_BOOT_ROM_STATUS0x0002U¶
-
SYSCTL_BOOT_ROM_POR0x2000U¶
-
SYSCTL_BOOT_ROM_XRS0x1000U¶
-
Device_cal((void (*)(void))((uintptr_t)0x003fce6c))¶
-
SYSCTL_SYSDIV_M0x00007F00UL¶
-
SYSCTL_SYSDIV_S8U¶
-
SYSCTL_REFDIV_M0x007C0000UL¶
-
SYSCTL_REFDIV_S18U¶
-
SYSCTL_ODIV_M0x0F800000UL¶
-
SYSCTL_ODIV_S23U¶
-
SYSCTL_REFDIV(x) ((((uint32_t)(x) - 1U) << SYSCTL_REFDIV_S) & \
SYSCTL_REFDIV_M)¶ Macro to format Clock divider value. x is a number from 1 to 32.
-
SYSCTL_ODIV(x) ((((uint32_t)(x) - 1U) << SYSCTL_ODIV_S) & \
SYSCTL_ODIV_M)¶ Macro to format Clock divider value. x is a number from 1 to 32.
-
SYSCTL_SYSDIV(x) ((x << SYSCTL_SYSDIV_S) & SYSCTL_SYSDIV_M)¶ Macro to format system clock divider value. x must be values from 1 to 126.
-
SYSCTL_IMULT_M0x000000FFUL¶
-
SYSCTL_IMULT_S0U¶
-
SYSCTL_IMULT(x) (((x) << SYSCTL_IMULT_S) & SYSCTL_IMULT_M)¶ Macro to format integer multiplier value. x is a number from 1 to 127.
-
SYSCTL_DCC_BASE_M0x30000000UL¶
-
SYSCTL_DCC_BASE_S28U¶
-
SYSCTL_DCC_BASE_00x00000000UL¶ DCC0 module.
-
SYSCTL_DCC_BASE_10x10000000UL¶ DCC1 module.
-
SYSCTL_OSCSRC_M0x00030000UL¶
-
SYSCTL_OSCSRC_S16U¶
-
SYSCTL_OSCSRC_OSC20x00000000UL¶ Internal oscillator INTOSC2.
-
SYSCTL_OSCSRC_XTAL0x00010000U¶ External oscillator (XTAL) in crystal mode.
-
SYSCTL_OSCSRC_XTAL_SE0x00030000U¶ External oscillator (XTAL) in single-ended mode.
-
SYSCTL_OSCSRC_OSC10x00020000UL¶ Internal oscillator INTOSC1.
-
SYSCTL_PLL_ENABLE0x80000000U¶ Enable PLL.
-
SYSCTL_PLL_DISABLE0x00000000U¶ Disable PLL.
-
SYSCTL_PLL_BYPASS0x40000000U¶ Bypass PLL.
-
SYSCTL_PLL_CONFIG_M0xC0000000U¶
-
SYSCTL_PLL_RETRIES100U¶
-
SYSCTL_PLLLOCK_TIMEOUT2000U¶
-
SYSCTL_DCC_COUNTER0_TOLERANCE1U¶
-
SYSCTL_DCC_COUNTER0_WINDOW1000U¶
-
SYSCTL_NMI_NMIINT0x1U¶ NMI Interrupt Flag.
-
SYSCTL_NMI_CLOCKFAIL0x2U¶ Clock Fail Interrupt Flag.
-
SYSCTL_NMI_RAMUNCERR0x4U¶ RAM Uncorrectable Error NMI Flag.
-
SYSCTL_NMI_FLUNCERR0x8U¶ Flash Uncorrectable Error NMI Flag.
-
SYSCTL_NMI_CPU1HWBISTERR0x10U¶ HW BIST Error NMI Flag.
-
SYSCTL_NMI_SYSDBGNMI0x80U¶ System Debug Module NMI Flag.
-
SYSCTL_NMI_CLBNMI0x100U¶ Reconfigurable Logic NMI Flag.
-
SYSCTL_NMI_SWERR0x2000U¶ SW Error Force NMI Flag.
-
SYSCTL_NMI_CRC_FAIL0x4000U¶ BGCRC calculation failed.
-
SYSCTL_STATUS_GINT0x1U¶ Global Interrupt flag.
-
SYSCTL_STATUS_AES_BUS_ERROR0x400U¶ AES_BUS_ERROR Interrupt flag.
-
SYSCTL_STATUS_EPG1_INT0x800U¶ EPG1_INT Interrupt flag.
-
SYSCTL_CAUSE_POR0x00000001U¶ Power-on reset.
-
SYSCTL_CAUSE_XRS0x00000002U¶ External reset pin.
-
SYSCTL_CAUSE_WDRS0x00000004U¶ Watchdog reset.
-
SYSCTL_CAUSE_NMIWDRS0x00000008U¶ NMI watchdog reset.
-
SYSCTL_CAUSE_SCCRESET0x00000100U¶ SCCRESETn by DCSM.
-
SYSCTL_CAUSE_HWBISTN0x00000020U¶ HWBISTn Reset.
-
SYSCTL_CAUSE_SIMRESET_CPU1RSN0x00000400U¶ SIMRESET_CPU1RSn.
-
SYSCTL_CAUSE_SIMRESET_XRSN0x00000800U¶ SIMRESET_XRSn.
-
SYSCTL_ADCSOC_SRC_PWM1SOCA0x1U¶ ePWM1 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM2SOCA0x2U¶ ePWM2 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM3SOCA0x4U¶ ePWM3 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM4SOCA0x8U¶ ePWM4 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM5SOCA0x10U¶ ePWM5 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM6SOCA0x20U¶ ePWM6 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM7SOCA0x40U¶ ePWM7 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM8SOCA0x80U¶ ePWM8 SOCA for ADCSOCAO
-
SYSCTL_ADCSOC_SRC_PWM1SOCB0x10000U¶ ePWM1 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM2SOCB0x20000U¶ ePWM2 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM3SOCB0x40000U¶ ePWM3 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM4SOCB0x80000U¶ ePWM4 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM5SOCB0x100000U¶ ePWM5 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM6SOCB0x200000U¶ ePWM6 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM7SOCB0x400000U¶ ePWM7 SOCB for ADCSOCBO
-
SYSCTL_ADCSOC_SRC_PWM8SOCB0x800000U¶ ePWM8 SOCB for ADCSOCBO
Enums
-
enum
SysCtl_PeripheralPCLOCKCR¶ The following are values that can be passed to SysCtl_enablePeripheral() and SysCtl_disablePeripheral() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_PERIPH_CLK_CLA1= 0x0000¶ CLA1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_DMA= 0x0200¶ DMA clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER0= 0x0300¶ CPUTIMER0 clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER1= 0x0400¶ CPUTIMER1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_TIMER2= 0x0500¶ CPUTIMER2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CPUBGCRC= 0x0D00¶ CPUBGCRC clock.
-
enumerator
SYSCTL_PERIPH_CLK_CLA1BGCRC= 0x0E00¶ CLA1BGCRC clock.
-
enumerator
SYSCTL_PERIPH_CLK_HRCAL= 0x1000¶ HRCAL clock.
-
enumerator
SYSCTL_PERIPH_CLK_TBCLKSYNC= 0x1200¶ TBCLKSYNC clock.
-
enumerator
SYSCTL_PERIPH_CLK_ERAD= 0x1800¶ ERAD clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM1= 0x0002¶ EPWM1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM2= 0x0102¶ EPWM2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM3= 0x0202¶ EPWM3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM4= 0x0302¶ EPWM4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM5= 0x0402¶ EPWM5 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM6= 0x0502¶ EPWM6 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM7= 0x0602¶ EPWM7 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPWM8= 0x0702¶ EPWM8 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP1= 0x0003¶ ECAP1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP2= 0x0103¶ ECAP2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_ECAP3= 0x0203¶ ECAP3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EQEP1= 0x0004¶ EQEP1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_EQEP2= 0x0104¶ EQEP2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SD1= 0x0006¶ SD1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SD2= 0x0106¶ SD2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCIA= 0x0007¶ SCI_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_SCIB= 0x0107¶ SCI_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_SPIA= 0x0008¶ SPI_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_SPIB= 0x0108¶ SPI_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_I2CA= 0x0009¶ I2C_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_I2CB= 0x0109¶ I2C_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_CANA= 0x000A¶ CAN_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_MCANA= 0x040A¶ MCAN_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCA= 0x000D¶ ADC_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCB= 0x010D¶ ADC_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_ADCC= 0x020D¶ ADC_C clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS1= 0x000E¶ CMPSS1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS2= 0x010E¶ CMPSS2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS3= 0x020E¶ CMPSS3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CMPSS4= 0x030E¶ CMPSS4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_DACA= 0x1010¶ DAC_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_DACB= 0x1110¶ DAC_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_CLB1= 0x0011¶ CLB1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CLB2= 0x0111¶ CLB2 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CLB3= 0x0211¶ CLB3 clock.
-
enumerator
SYSCTL_PERIPH_CLK_CLB4= 0x0311¶ CLB4 clock.
-
enumerator
SYSCTL_PERIPH_CLK_FSITXA= 0x0012¶ FSITX_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_FSIRXA= 0x0112¶ FSIRX_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_LINA= 0x0013¶ LIN_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_LINB= 0x0113¶ LIN_B clock.
-
enumerator
SYSCTL_PERIPH_CLK_PMBUSA= 0x0014¶ PMBUS_A clock.
-
enumerator
SYSCTL_PERIPH_CLK_DCC0= 0x0015¶ DCC0 clock.
-
enumerator
SYSCTL_PERIPH_CLK_DCC1= 0x0115¶ DCC1 clock.
-
enumerator
SYSCTL_PERIPH_CLK_HICA= 0x0019¶ HICA clock.
-
enumerator
SYSCTL_PERIPH_CLK_AESA= 0x001A¶ AESA clock.
-
enumerator
SYSCTL_PERIPH_CLK_EPG1= 0x001B¶ EPG1 clock.
-
enumerator
-
enum
SysCtl_PeripheralSOFTPRES¶ The following are values that can be passed to SysCtl_resetPeripheral() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_PERIPH_RES_CPU1CLA1= 0x0000¶ Reset CPU1_CLA1 clock.
-
enumerator
SYSCTL_PERIPH_RES_CPU1CPUBGCRC= 0x0D00¶ Reset CPU1_CPUBGCRC clock.
-
enumerator
SYSCTL_PERIPH_RES_CPU1CLA1BGCRC= 0x0E00¶ Reset CPU1_CLA1BGCRC clock.
-
enumerator
SYSCTL_PERIPH_RES_CPU1ERAD= 0x1800¶ Reset CPU1_ERAD clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM1= 0x0002¶ Reset EPWM1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM2= 0x0102¶ Reset EPWM2 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM3= 0x0202¶ Reset EPWM3 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM4= 0x0302¶ Reset EPWM4 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM5= 0x0402¶ Reset EPWM5 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM6= 0x0502¶ Reset EPWM6 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM7= 0x0602¶ Reset EPWM7 clock.
-
enumerator
SYSCTL_PERIPH_RES_EPWM8= 0x0702¶ Reset EPWM8 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP1= 0x0003¶ Reset ECAP1 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP2= 0x0103¶ Reset ECAP2 clock.
-
enumerator
SYSCTL_PERIPH_RES_ECAP3= 0x0203¶ Reset ECAP3 clock.
-
enumerator
SYSCTL_PERIPH_RES_EQEP1= 0x0004¶ Reset EQEP1 clock.
-
enumerator
SYSCTL_PERIPH_RES_EQEP2= 0x0104¶ Reset EQEP2 clock.
-
enumerator
SYSCTL_PERIPH_RES_SD1= 0x0006¶ Reset SD1 clock.
-
enumerator
SYSCTL_PERIPH_RES_SD2= 0x0106¶ Reset SD2 clock.
-
enumerator
SYSCTL_PERIPH_RES_SCIA= 0x0007¶ Reset SCI_A clock.
-
enumerator
SYSCTL_PERIPH_RES_SCIB= 0x0107¶ Reset SCI_B clock.
-
enumerator
SYSCTL_PERIPH_RES_SPIA= 0x0008¶ Reset SPI_A clock.
-
enumerator
SYSCTL_PERIPH_RES_SPIB= 0x0108¶ Reset SPI_B clock.
-
enumerator
SYSCTL_PERIPH_RES_I2CA= 0x0009¶ Reset I2C_A clock.
-
enumerator
SYSCTL_PERIPH_RES_I2CB= 0x0109¶ Reset I2C_B clock.
-
enumerator
SYSCTL_PERIPH_RES_CANA= 0x000A¶ Reset CAN_A clock.
-
enumerator
SYSCTL_PERIPH_RES_MCANA= 0x040A¶ Reset MCAN_A clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCA= 0x000D¶ Reset ADC_A clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCB= 0x010D¶ Reset ADC_B clock.
-
enumerator
SYSCTL_PERIPH_RES_ADCC= 0x020D¶ Reset ADC_C clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS1= 0x000E¶ Reset CMPSS1 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS2= 0x010E¶ Reset CMPSS2 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS3= 0x020E¶ Reset CMPSS3 clock.
-
enumerator
SYSCTL_PERIPH_RES_CMPSS4= 0x030E¶ Reset CMPSS4 clock.
-
enumerator
SYSCTL_PERIPH_RES_DACA= 0x1010¶ Reset DAC_A clock.
-
enumerator
SYSCTL_PERIPH_RES_DACB= 0x1110¶ Reset DAC_B clock.
-
enumerator
SYSCTL_PERIPH_RES_CLB1= 0x0011¶ Reset CLB1 clock.
-
enumerator
SYSCTL_PERIPH_RES_CLB2= 0x0111¶ Reset CLB2 clock.
-
enumerator
SYSCTL_PERIPH_RES_CLB3= 0x0211¶ Reset CLB3 clock.
-
enumerator
SYSCTL_PERIPH_RES_CLB4= 0x0311¶ Reset CLB4 clock.
-
enumerator
SYSCTL_PERIPH_RES_FSITXA= 0x0012¶ Reset FSITX_A clock.
-
enumerator
SYSCTL_PERIPH_RES_FSIRXA= 0x0112¶ Reset FSIRX_A clock.
-
enumerator
SYSCTL_PERIPH_RES_LINA= 0x0013¶ Reset LIN_A clock.
-
enumerator
SYSCTL_PERIPH_RES_LINB= 0x0113¶ Reset LIN_B clock.
-
enumerator
SYSCTL_PERIPH_RES_PMBUSA= 0x0014¶ Reset PMBUS_A clock.
-
enumerator
SYSCTL_PERIPH_RES_DCC0= 0x0015¶ Reset DCC0 clock.
-
enumerator
SYSCTL_PERIPH_RES_DCC1= 0x0115¶ Reset DCC1 clock.
-
enumerator
SYSCTL_PERIPH_RES_HICA= 0x0019¶ Reset HIC_A clock.
-
enumerator
SYSCTL_PERIPH_RES_AESA= 0x001A¶ Reset AESA clock.
-
enumerator
SYSCTL_PERIPH_RES_EPG1= 0x001B¶ Reset EPG1 clock.
-
enumerator
-
enum
SysCtl_WDPredivider¶ The following are values that can be passed to SysCtl_setWatchdogPredivider() as the predivider parameter.
Values:
-
enumerator
SYSCTL_WD_PREDIV_2= 0x800¶ PREDIVCLK = INTOSC1 / 2.
-
enumerator
SYSCTL_WD_PREDIV_4= 0x900¶ PREDIVCLK = INTOSC1 / 4.
-
enumerator
SYSCTL_WD_PREDIV_8= 0xA00¶ PREDIVCLK = INTOSC1 / 8.
-
enumerator
SYSCTL_WD_PREDIV_16= 0xB00¶ PREDIVCLK = INTOSC1 / 16.
-
enumerator
SYSCTL_WD_PREDIV_32= 0xC00¶ PREDIVCLK = INTOSC1 / 32.
-
enumerator
SYSCTL_WD_PREDIV_64= 0xD00¶ PREDIVCLK = INTOSC1 / 64.
-
enumerator
SYSCTL_WD_PREDIV_128= 0xE00¶ PREDIVCLK = INTOSC1 / 128.
-
enumerator
SYSCTL_WD_PREDIV_256= 0xF00¶ PREDIVCLK = INTOSC1 / 256.
-
enumerator
SYSCTL_WD_PREDIV_512= 0x000¶ PREDIVCLK = INTOSC1 / 512.
-
enumerator
SYSCTL_WD_PREDIV_1024= 0x100¶ PREDIVCLK = INTOSC1 / 1024.
-
enumerator
SYSCTL_WD_PREDIV_2048= 0x200¶ PREDIVCLK = INTOSC1 / 2048.
-
enumerator
SYSCTL_WD_PREDIV_4096= 0x300¶ PREDIVCLK = INTOSC1 / 4096.
-
enumerator
-
enum
SysCtl_WDPrescaler¶ The following are values that can be passed to SysCtl_setWatchdogPrescaler() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_WD_PRESCALE_1= 1¶ WDCLK = PREDIVCLK / 1.
-
enumerator
SYSCTL_WD_PRESCALE_2= 2¶ WDCLK = PREDIVCLK / 2.
-
enumerator
SYSCTL_WD_PRESCALE_4= 3¶ WDCLK = PREDIVCLK / 4.
-
enumerator
SYSCTL_WD_PRESCALE_8= 4¶ WDCLK = PREDIVCLK / 8.
-
enumerator
SYSCTL_WD_PRESCALE_16= 5¶ WDCLK = PREDIVCLK / 16.
-
enumerator
SYSCTL_WD_PRESCALE_32= 6¶ WDCLK = PREDIVCLK / 32.
-
enumerator
SYSCTL_WD_PRESCALE_64= 7¶ WDCLK = PREDIVCLK / 64.
-
enumerator
-
enum
SysCtl_WDMode¶ The following are values that can be passed to SysCtl_setWatchdogMode() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_WD_MODE_RESET¶ Watchdog can generate a reset signal.
-
enumerator
SYSCTL_WD_MODE_INTERRUPT¶ Watchdog can generate an interrupt signal; reset signal is disabled.
-
enumerator
-
enum
SysCtl_LSPCLKPrescaler¶ The following are values that can be passed to SysCtl_setLowSpeedClock() as the prescaler parameter.
Values:
-
enumerator
SYSCTL_LSPCLK_PRESCALE_1= 0¶ LSPCLK = SYSCLK / 1.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_2= 1¶ LSPCLK = SYSCLK / 2.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_4= 2¶ LSPCLK = SYSCLK / 4 (default)
-
enumerator
SYSCTL_LSPCLK_PRESCALE_6= 3¶ LSPCLK = SYSCLK / 6.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_8= 4¶ LSPCLK = SYSCLK / 8.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_10= 5¶ LSPCLK = SYSCLK / 10.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_12= 6¶ LSPCLK = SYSCLK / 12.
-
enumerator
SYSCTL_LSPCLK_PRESCALE_14= 7¶ LSPCLK = SYSCLK / 14.
-
enumerator
-
enum
SysCtl_AccessPeripheral¶ The following are values that can be passed to SysCtl_setPeripheralAccessControl() and SysCtl_getPeripheralAccessControl() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_ACCESS_ADCA= 0x0¶ ADCA access.
-
enumerator
SYSCTL_ACCESS_ADCB= 0x2¶ ADCB access.
-
enumerator
SYSCTL_ACCESS_ADCC= 0x4¶ ADCC access.
-
enumerator
SYSCTL_ACCESS_CMPSS1= 0x10¶ CMPSS1 access.
-
enumerator
SYSCTL_ACCESS_CMPSS2= 0x12¶ CMPSS2 access.
-
enumerator
SYSCTL_ACCESS_CMPSS3= 0x14¶ CMPSS3 access.
-
enumerator
SYSCTL_ACCESS_CMPSS4= 0x16¶ CMPSS4 access.
-
enumerator
SYSCTL_ACCESS_DACA= 0x28¶ DACA access.
-
enumerator
SYSCTL_ACCESS_DACB= 0x2A¶ DACB access.
-
enumerator
SYSCTL_ACCESS_EPWM1= 0x48¶ EPWM1 access.
-
enumerator
SYSCTL_ACCESS_EPWM2= 0x4A¶ EPWM2 access.
-
enumerator
SYSCTL_ACCESS_EPWM3= 0x4C¶ EPWM3 access.
-
enumerator
SYSCTL_ACCESS_EPWM4= 0x4E¶ EPWM4 access.
-
enumerator
SYSCTL_ACCESS_EPWM5= 0x50¶ EPWM5 access.
-
enumerator
SYSCTL_ACCESS_EPWM6= 0x52¶ EPWM6 access.
-
enumerator
SYSCTL_ACCESS_EPWM7= 0x54¶ EPWM7 access.
-
enumerator
SYSCTL_ACCESS_EPWM8= 0x56¶ EPWM8 access.
-
enumerator
SYSCTL_ACCESS_EQEP1= 0x70¶ EQEP1 access.
-
enumerator
SYSCTL_ACCESS_EQEP2= 0x72¶ EQEP2 access.
-
enumerator
SYSCTL_ACCESS_ECAP1= 0x80¶ ECAP1 access.
-
enumerator
SYSCTL_ACCESS_ECAP2= 0x82¶ ECAP2 access.
-
enumerator
SYSCTL_ACCESS_ECAP3= 0x84¶ ECAP3 access.
-
enumerator
SYSCTL_ACCESS_SDFM1= 0xA8¶ SDFM1 access.
-
enumerator
SYSCTL_ACCESS_SDFM2= 0xAA¶ SDFM2 access.
-
enumerator
SYSCTL_ACCESS_CLB1= 0xB0¶ CLB1 access.
-
enumerator
SYSCTL_ACCESS_CLB2= 0xB2¶ CLB2 access.
-
enumerator
SYSCTL_ACCESS_CLB3= 0xB4¶ CLB3 access.
-
enumerator
SYSCTL_ACCESS_CLB4= 0xB6¶ CLB4 access.
-
enumerator
SYSCTL_ACCESS_SCIA= 0x100¶ SCIA access.
-
enumerator
SYSCTL_ACCESS_SCIB= 0x102¶ SCIB access.
-
enumerator
SYSCTL_ACCESS_SPIA= 0x110¶ SPIA access.
-
enumerator
SYSCTL_ACCESS_SPIB= 0x112¶ SPIB access.
-
enumerator
SYSCTL_ACCESS_I2CA= 0x120¶ I2CA access.
-
enumerator
SYSCTL_ACCESS_I2CB= 0x122¶ I2CB access.
-
enumerator
SYSCTL_ACCESS_PMBUSA= 0x130¶ PMBUS_A access.
-
enumerator
SYSCTL_ACCESS_LINA= 0x138¶ LIN_A access.
-
enumerator
SYSCTL_ACCESS_LINB= 0x13A¶ LIN_B access.
-
enumerator
SYSCTL_ACCESS_CANA= 0x140¶ DCANA access.
-
enumerator
SYSCTL_ACCESS_MCANA= 0x148¶ MCANA access.
-
enumerator
SYSCTL_ACCESS_FSIATX= 0x158¶ FSIATX access.
-
enumerator
SYSCTL_ACCESS_FSIARX= 0x15A¶ FSIARX access.
-
enumerator
SYSCTL_ACCESS_HRPWMA= 0x1AA¶ HRPWM_A access.
-
enumerator
SYSCTL_ACCESS_HICA= 0x1AC¶ HIC_A access.
-
enumerator
SYSCTL_ACCESS_AESA= 0x1AE¶ AESA access.
-
enumerator
-
enum
SysCtl_AccessController¶ The following are values that can be passed to SysCtl_setPeripheralAccessControl() and SysCtl_getPeripheralAccessControl() as the controller parameter.
Values:
-
enumerator
SYSCTL_ACCESS_CPU1= 0U¶ CPU access to the peripheral.
-
enumerator
SYSCTL_ACCESS_CLA1= 2U¶ CLA1 access to the peripheral.
-
enumerator
SYSCTL_ACCESS_DMA1= 4U¶ DMA access to the peripheral.
-
enumerator
SYSCTL_ACCESS_HIC= 6U¶ HICA access to the peripheral.
-
enumerator
-
enum
SysCtl_AccessPermission¶ The following are values that can be passed to SysCtl_setPeripheralAccessControl() as the permission parameter.
Values:
-
enumerator
SYSCTL_ACCESS_FULL= 3U¶ Full Access for both read and write.
-
enumerator
SYSCTL_ACCESS_PROTECTED= 2U¶ Protected RD access such that FIFOs. Clear on read, registers are not changed and no write access.
-
enumerator
SYSCTL_ACCESS_NONE= 0U¶ No read or write access.
-
enumerator
-
enum
SysCtl_ClockOut¶ The following are values that can be passed to SysCtl_selectClockOutSource() as the source parameter.
Values:
-
enumerator
SYSCTL_CLOCKOUT_PLLSYS= 0U¶ PLL System Clock post SYSCLKDIV.
-
enumerator
SYSCTL_CLOCKOUT_PLLRAW= 1U¶ PLL Raw Clock.
-
enumerator
SYSCTL_CLOCKOUT_SYSCLK= 2U¶ CPU System Clock.
-
enumerator
SYSCTL_CLOCKOUT_INTOSC1= 5U¶ Internal Oscillator 1.
-
enumerator
SYSCTL_CLOCKOUT_INTOSC2= 6U¶ Internal Oscillator 2.
-
enumerator
SYSCTL_CLOCKOUT_XTALOSC= 7U¶ External Oscillator.
-
enumerator
-
enum
SysCtl_ExternalOscMode¶ The following are values that can be passed to SysCtl_setExternalOscMode() as the mode parameter.
Values:
-
enumerator
SYSCTL_XTALMODE_CRYSTAL= 1U¶ XTAL Oscillator Crystal Mode.
-
enumerator
SYSCTL_XTALMODE_SINGLE= 2U¶ XTAL Oscillator Single-Ended Mode.
-
enumerator
-
enum
SysCtl_SyncOutputSource¶ The following values define the syncSrc parameter for SysCtl_setSyncOutputConfig().
Values:
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT= 0X0U¶ EPWM1SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM2SYNCOUT= 0X1U¶ EPWM2SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM3SYNCOUT= 0X2U¶ EPWM3SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM4SYNCOUT= 0X3U¶ EPWM4SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM5SYNCOUT= 0X4U¶ EPWM5SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM6SYNCOUT= 0X5U¶ EPWM6SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_EPWM7SYNCOUT= 0X6U¶ EPWM7SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_ECAP1SYNCOUT= 0x18¶ ECAP1SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_ECAP2SYNCOUT= 0x19¶ ECAP2SYNCOUT –> EXTSYNCOUT.
-
enumerator
SYSCTL_SYNC_OUT_SRC_ECAP3SYNCOUT= 0x20¶ ECAP3SYNCOUT –> EXTSYNCOUT.
-
enumerator
-
enum
SysCtl_DeviceParametric¶ The following values define the parametric parameter for SysCtl_getDeviceParametric().
Values:
-
enumerator
SYSCTL_DEVICE_QUAL¶ Device Qualification Status.
-
enumerator
SYSCTL_DEVICE_PINCOUNT¶ Device Pin Count.
-
enumerator
SYSCTL_DEVICE_INSTASPIN¶ Device InstaSPIN Feature Set.
-
enumerator
SYSCTL_DEVICE_FLASH¶ Device Flash size (KB)
-
enumerator
SYSCTL_DEVICE_FAMILY¶ Device Family.
-
enumerator
SYSCTL_DEVICE_PARTNO¶ Device Part Number.
-
enumerator
SYSCTL_DEVICE_CLASSID¶ Device Class ID.
-
enumerator
-
enum
SysCtl_SelType¶ The following are values that can be passed to SysCtl_configureType() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_ECAPTYPE= 0x1¶ Configure ECAP Type :
Type 0 : No EALLOW protection for ECAP registers
Type 1 : ECAP registers are EALLOW protected
-
enumerator
SYSCTL_SDFMTYPE= 0x2¶ Configure SDFM Type :
Type 0 : Data Ready conditions combined with the fault conditions on the interrupt line. Data ready interrupts from individual filters are not generated.
Type 1 : Data Ready conditions do not generate the SDFMINT. Each filter generates a separate data ready interrupts.
-
enumerator
-
enum
SysCtl_XClkDivider¶ The following are values that can be passed to SysCtl_setXClk() as divider parameter.
Values:
-
enumerator
SYSCTL_XCLKOUT_DIV_1= 0¶ XCLKOUT = XCLKOUT / 1.
-
enumerator
SYSCTL_XCLKOUT_DIV_2= 1¶ XCLKOUT = XCLKOUT / 2.
-
enumerator
SYSCTL_XCLKOUT_DIV_4= 2¶ XCLKOUT = XCLKOUT / 4.
-
enumerator
SYSCTL_XCLKOUT_DIV_8= 3¶ XCLKOUT = XCLKOUT / 8.
-
enumerator
-
enum
SysCtl_MCANClkDivider¶ The following are values that can be passed to SysCtl_setMCANClk() as divider parameter.
Values:
-
enumerator
SYSCTL_MCANCLK_DIV_1= 0x0¶ MCAN clock = MCAN clock / 1.
-
enumerator
SYSCTL_MCANCLK_DIV_2= 0x1¶ MCAN clock = MCAN clock / 2.
-
enumerator
SYSCTL_MCANCLK_DIV_3= 0x2¶ MCAN clock = MCAN clock / 3.
-
enumerator
SYSCTL_MCANCLK_DIV_4= 0x3¶ MCAN clock = MCAN clock / 4.
-
enumerator
SYSCTL_MCANCLK_DIV_5= 0x4¶ MCAN clock = MCAN clock / 5.
-
enumerator
SYSCTL_MCANCLK_DIV_6= 0x5¶ MCAN clock = MCAN clock / 6.
-
enumerator
SYSCTL_MCANCLK_DIV_7= 0x6¶ MCAN clock = MCAN clock / 7.
-
enumerator
SYSCTL_MCANCLK_DIV_8= 0x7¶ MCAN clock = MCAN clock / 8.
-
enumerator
SYSCTL_MCANCLK_DIV_9= 0x8¶ MCAN clock = MCAN clock / 9.
-
enumerator
SYSCTL_MCANCLK_DIV_10= 0x9¶ MCAN clock = MCAN clock / 10.
-
enumerator
SYSCTL_MCANCLK_DIV_11= 0xA¶ MCAN clock = MCAN clock / 11.
-
enumerator
SYSCTL_MCANCLK_DIV_12= 0xB¶ MCAN clock = MCAN clock / 12.
-
enumerator
SYSCTL_MCANCLK_DIV_13= 0xC¶ MCAN clock = MCAN clock / 13.
-
enumerator
SYSCTL_MCANCLK_DIV_14= 0xD¶ MCAN clock = MCAN clock / 14.
-
enumerator
SYSCTL_MCANCLK_DIV_15= 0xE¶ MCAN clock = MCAN clock / 15.
-
enumerator
SYSCTL_MCANCLK_DIV_16= 0xF¶ MCAN clock = MCAN clock / 16.
-
enumerator
SYSCTL_MCANCLK_DIV_17= 0x10¶ MCAN clock = MCAN clock / 17.
-
enumerator
SYSCTL_MCANCLK_DIV_18= 0x11¶ MCAN clock = MCAN clock / 18.
-
enumerator
SYSCTL_MCANCLK_DIV_19= 0x12¶ MCAN clock = MCAN clock / 19.
-
enumerator
SYSCTL_MCANCLK_DIV_20= 0x13¶ MCAN clock = MCAN clock / 20.
-
enumerator
-
enum
SysCtl_Cputimer2ClkDivider¶ The following are values that can be passed to SysCtl_setCputimer2Clk() as divider parameter.
Values:
-
enumerator
SYSCTL_TMR2CLKPRESCALE_1¶ Cputimer2 clock = Cputimer2 clock / 1.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_2¶ Cputimer2 clock = Cputimer2 clock / 2.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_4¶ Cputimer2 clock = Cputimer2 clock / 4.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_8¶ Cputimer2 clock = Cputimer2 clock / 8.
-
enumerator
SYSCTL_TMR2CLKPRESCALE_16¶ Cputimer2 clock = Cputimer2 clock / 16.
-
enumerator
-
enum
SysCtl_Cputimer2ClkSource¶ The following are values that can be passed to SysCtl_setCputimer2Clk() as source parameter.
Values:
-
enumerator
SYSCTL_TMR2CLKSRCSEL_SYSCLK= 0U¶ System Clock.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_INTOSC1= 1U¶ Internal Oscillator 1.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_INTOSC2= 2U¶ Internal Oscillator 2.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_XTAL= 3U¶ Crystal oscillator.
-
enumerator
SYSCTL_TMR2CLKSRCSEL_AUXPLLCLK= 6U¶ Aux PLL CLock.
-
enumerator
-
enum
SysCtl_ClkRegSel¶ The following are values that can be passed to SysCtl_lockClkConfig() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_REG_SEL_CLKSRCCTL1= 0x0000¶ CLKSRCCTL1 lock.
-
enumerator
SYSCTL_REG_SEL_CLKSRCCTL2= 0x0100¶ CLKSRCCTL2 lock.
-
enumerator
SYSCTL_REG_SEL_CLKSRCCTL3= 0x0200¶ CLKSRCCTL3 lock.
-
enumerator
SYSCTL_REG_SEL_SYSPLLCTL1= 0x0300¶ SYSPLLCTL1 lock.
-
enumerator
SYSCTL_REG_SEL_SYSPLLMULT= 0x0600¶ SYSPLLMULT lock.
-
enumerator
SYSCTL_REG_SEL_SYSCLKDIVSEL= 0x0B00¶ SYSCLKDIVSEL lock.
-
enumerator
SYSCTL_REG_SEL_AUXCLKDIVSEL= 0x0C00¶ AUXCLKDIVSEL lock.
-
enumerator
SYSCTL_REG_SEL_LOSPCP= 0x0F00¶ LOSPCP lock.
-
enumerator
SYSCTL_REG_SEL_XTALCR= 0x1000¶ XTALCR lock.
-
enumerator
-
enum
SysCtl_CpuRegSel¶ The following are values that can be passed to SysCtl_lockSysConfig() as the peripheral parameter.
Values:
-
enumerator
SYSCTL_REG_SEL_PIEVERRADDR= 0x0200¶ PIEVERRADDR lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR0= 0x0300¶ PCLKCR0 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR2= 0x0500¶ PCLKCR2 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR3= 0x0600¶ PCLKCR3 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR4= 0x0700¶ PCLKCR4 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR6= 0x0900¶ PCLKCR6 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR7= 0x0A00¶ PCLKCR7 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR8= 0x0B00¶ PCLKCR8 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR9= 0x0C00¶ PCLKCR9 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR10= 0x0D00¶ PCLKCR10 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR13= 0x1000¶ PCLKCR13 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR14= 0x1100¶ PCLKCR14 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR16= 0x1300¶ PCLKCR16 lock.
-
enumerator
SYSCTL_REG_SEL_LPMCR= 0x1500¶ LPMCR lock.
-
enumerator
SYSCTL_REG_SEL_GPIOLPMSEL0= 0x1600¶ GPIOLPMSEL0 lock.
-
enumerator
SYSCTL_REG_SEL_GPIOLPMSEL1= 0x1700¶ GPIOLPMSEL1 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR17= 0x1800¶ PCLKCR17 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR18= 0x1900¶ PCLKCR18 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR19= 0x1A00¶ PCLKCR19 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR20= 0x1B00¶ PCLKCR20 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR21= 0x1C00¶ PCLKCR21 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR22= 0x1D00¶ PCLKCR22 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR25= 0x0101¶ PCLKCR25 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR26= 0x0201¶ PCLKCR26 lock.
-
enumerator
SYSCTL_REG_SEL_PCLKCR27= 0x0301¶ PCLKCR27 lock.
-
enumerator
-
enum
SysCtl_LFUUserRegister¶ The following are values that can be passed to SysCtl_setLFUUserRegister() and SysCtl_getLFUUserRegister() as the reg parameter.
Values:
-
enumerator
SYSCTL_LFU_USER_REG1_SYSRSN= 0U¶ User register reset by SYSRSn.
-
enumerator
SYSCTL_LFU_USER_REG2_SYSRSN= 1U¶ User register reset by SYSRSn.
-
enumerator
SYSCTL_LFU_USER_REG1_XRSN= 2U¶ User register reset by XRSn.
-
enumerator
SYSCTL_LFU_USER_REG2_XRSN= 3U¶ User register reset by XRSn.
-
enumerator
SYSCTL_LFU_USER_REG1_PORESETN= 4U¶ User register reset by PORESETn.
-
enumerator
SYSCTL_LFU_USER_REG2_PORESETN= 5U¶ User register reset by PORESETn.
-
enumerator
Functions
-
void
SysCtl_deviceCal(void)¶ Wrapper function for Device_cal function
- Return
None.
- Parameters
None: This is a wrapper function for the Device_cal function available in the OTP memory.
-
void
SysCtl_resetPeripheral(SysCtl_PeripheralSOFTPRES peripheral)¶ Resets a peripheral
This function uses the SOFTPRESx registers to reset a specified peripheral. Module registers will be returned to their reset states.
- Parameters
peripheral: is the peripheral to reset.
- Note
This includes registers containing trim values.The peripheral software reset needed by CPU2 can be communicated to CPU1 via IPC for all shared peripherals.
- Return
None.
-
void
SysCtl_enablePeripheral(SysCtl_PeripheralPCLOCKCR peripheral)¶ Enables a peripheral.
Peripherals are enabled with this function. At power-up, all peripherals are disabled; they must be enabled in order to operate or respond to register reads/writes.
- Parameters
peripheral: is the peripheral to enable.
- Note
Note that there should be atleast 5 cycles delay between enabling the peripheral clock and accessing the peripheral registers. The delay should be added by the user if the peripheral is accessed immediately after this function call. Use asm(” RPT #5 || NOP”); to add 5 cycle delay post this function call.
- Return
None.
-
void
SysCtl_disablePeripheral(SysCtl_PeripheralPCLOCKCR peripheral)¶ Disables a peripheral.
Peripherals are disabled with this function. Once disabled, they will not operate or respond to register reads/writes.
- Parameters
peripheral: is the peripheral to disable.
- Return
None.
-
void
SysCtl_resetDevice(void)¶ Resets the device.
This function performs a watchdog reset of the device.
- Return
This function does not return.
-
uint32_t
SysCtl_getResetCause(void)¶ Gets the reason for a reset.
This function will return the reason(s) for a reset. Since the reset reasons are sticky until either cleared by software or an external reset, multiple reset reasons may be returned if multiple resets have occurred. The reset reason will be a logical OR of
SYSCTL_CAUSE_POR - Power-on reset
SYSCTL_CAUSE_XRS - External reset pin
SYSCTL_CAUSE_WDRS - Watchdog reset
SYSCTL_CAUSE_NMIWDRS - NMI watchdog reset
SYSCTL_CAUSE_SCCRESET - SCCRESETn reset from DCSM
SYSCTL_CAUSE_HWBISTN - HWBISTn Reset
SYSCTL_CAUSE_SIMRESET_CPU1RSN - SIMRESET_CPU1RSn
SYSCTL_CAUSE_SIMRESET_XRSN - SIMRESET_XRSn
- Note
If you re-purpose the reserved boot ROM RAM, the POR and XRS reset statuses won’t be accurate.
- Return
Returns the reason(s) for a reset.
-
void
SysCtl_clearResetCause(uint32_t rstCauses)¶ Clears reset reasons.
This function clears the specified sticky reset reasons. Once cleared, another reset for the same reason can be detected, and a reset for a different reason can be distinguished (instead of having two reset causes set). If the reset reason is used by an application, all reset causes should be cleared after they are retrieved with
SysCtl_getResetCause().- Parameters
rstCauses: are the reset causes to be cleared; must be a logical OR ofSYSCTL_CAUSE_POR - Power-on reset
SYSCTL_CAUSE_XRS - External reset pin
SYSCTL_CAUSE_WDRS - Watchdog reset
SYSCTL_CAUSE_NMIWDRS - NMI watchdog reset
SYSCTL_CAUSE_SCCRESET - SCCRESETn reset from DCSM
SYSCTL_CAUSE_HWBISTN - HWBISTn Reset
SYSCTL_CAUSE_SIMRESET_CPU1RSN - SIMRESET_CPU1RSn
SYSCTL_CAUSE_SIMRESET_XRSN - SIMRESET_XRSn
- Note
Some reset causes are cleared by the boot ROM.
- Return
None.
-
void
SysCtl_setLowSpeedClock(SysCtl_LSPCLKPrescaler prescaler)¶ Sets the low speed peripheral clock rate prescaler.
This function configures the clock rate of the low speed peripherals. The
prescaler parameter is the value by which the SYSCLK rate is divided to get the LSPCLK rate. For example, a prescaler of SYSCTL_LSPCLK_PRESCALE_4 will result in a LSPCLK rate that is a quarter of the SYSCLK rate.- Parameters
prescaler: is the LSPCLK rate relative to SYSCLK
- Return
None.
-
void
SysCtl_selectClockOutSource(SysCtl_ClockOut source)¶ Selects a clock source to mux to an external GPIO pin (XCLKOUT).
This function configures the specified clock source to be muxed to an external clock out (XCLKOUT) GPIO pin. The
source parameter may take a value of one of the following values:SYSCTL_CLOCKOUT_PLLSYS
SYSCTL_CLOCKOUT_PLLRAW
SYSCTL_CLOCKOUT_SYSCLK
SYSCTL_CLOCKOUT_INTOSC1
SYSCTL_CLOCKOUT_INTOSC2
SYSCTL_CLOCKOUT_XTALOSC
- Parameters
source: is the internal clock source to be configured.
- Return
None.
-
void
SysCtl_setExternalOscMode(SysCtl_ExternalOscMode mode)¶ Set the external oscillator mode.
This function sets the external oscillator mode specified by the
mode parameter which may take one of two values:SYSCTL_XTALMODE_CRYSTAL - Crystal Mode
SYSCTL_XTALMODE_SINGLE - Single-Ended Mode
- Parameters
mode: is the external oscillator mode to be configured.
- Note
The external oscillator must be powered off before this configuration can be performed.
- Return
None.
-
uint16_t
SysCtl_getExternalOscCounterValue(void)¶ Gets the external oscillator counter value.
This function returns the X1 clock counter value. When the return value reaches 0x3FF, it freezes. Before switching from INTOSC2 to an external oscillator (XTAL), an application should call this function to make sure the counter is saturated.
- Return
Returns the value of the 10-bit X1 clock counter.
-
void
SysCtl_clearExternalOscCounterValue(void)¶ Clears the external oscillator counter value.
- Return
None.
-
void
SysCtl_turnOnOsc(uint32_t oscSource)¶ Turns on the specified oscillator sources.
This function turns on the oscillator specified by the
oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.- Parameters
oscSource: is the oscillator source to be configured.
- Note
SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.
- Return
None.
-
void
SysCtl_turnOffOsc(uint32_t oscSource)¶ Turns off the specified oscillator sources.
This function turns off the oscillator specified by the
oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.- Parameters
oscSource: is the oscillator source to be configured.
- Note
SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.
- Return
None.
-
void
SysCtl_enterIdleMode(void)¶ Enters IDLE mode.
This function puts the device into IDLE mode. The CPU clock is gated while all peripheral clocks are left running. Any enabled interrupt will wake the CPU up from IDLE mode.
- Return
None.
-
void
SysCtl_enterStandbyMode(void)¶ Enters STANDBY mode.
This function puts the device into STANDBY mode. This will gate both the CPU clock and any peripheral clocks derived from SYSCLK. The watchdog is left active, and an NMI or an optional watchdog interrupt will wake the CPU subsystem from STANDBY mode.
GPIOs may be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().
The CPU will receive an interrupt (WAKEINT) on wakeup.
- Return
None.
-
void
SysCtl_enterHaltMode(void)¶ Enters HALT mode.
This function puts the device into HALT mode. This will gate almost all systems and clocks and allows for the power-down of oscillators and analog blocks. The watchdog may be left clocked to produce a reset. See SysCtl_enableWatchdogInHalt() to enable this. GPIOs should be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().
The CPU will receive an interrupt (WAKEINT) on wakeup.
- Return
None.
-
void
SysCtl_enableLPMWakeupPin(uint32_t pin)¶ Enables a pin to wake up the device from the following mode(s):
STANDBY
HALT
This function connects a pin to the LPM circuit, allowing an event on the pin to wake up the device when when it is in following mode(s):
STANDBY
HALT
- Parameters
pin: is the identifying number of the pin.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are capable of being connected to the LPM circuit.
- Return
None.
-
void
SysCtl_disableLPMWakeupPin(uint32_t pin)¶ Disables a pin to wake up the device from the following mode(s):
STANDBY
HALT
This function disconnects a pin to the LPM circuit, disallowing an event on the pin to wake up the device when when it is in following mode(s):
STANDBY
HALT
- Parameters
pin: is the identifying number of the pin.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are valid.
- Return
None.
-
void
SysCtl_setStandbyQualificationPeriod(uint16_t cycles)¶ Sets the number of cycles to qualify an input on waking from STANDBY mode.
This function sets the number of OSCCLK clock cycles used to qualify the selected inputs when waking from STANDBY mode. The
cycles parameter should be passed a cycle count between 2 and 65 cycles inclusive.- Parameters
cycles: is the number of OSCCLK cycles.
- Return
None.
-
void
SysCtl_enableWatchdogStandbyWakeup(void)¶ Enable the device to wake from STANDBY mode upon a watchdog interrupt.
- Note
In order to use this option, you must configure the watchdog to generate an interrupt using SysCtl_setWatchdogMode().
- Return
None.
-
void
SysCtl_disableWatchdogStandbyWakeup(void)¶ Disable the device from waking from STANDBY mode upon a watchdog interrupt.
- Return
None.
-
void
SysCtl_enableWatchdogInHalt(void)¶ Enable the watchdog to run while in HALT mode.
This function configures the watchdog to continue to run while in HALT mode. Additionally, INTOSC1 and INTOSC2 are not powered down when the system enters HALT mode. By default the watchdog is gated when the system enters HALT.
- Return
None.
-
void
SysCtl_disableWatchdogInHalt(void)¶ Disable the watchdog from running while in HALT mode.
This function gates the watchdog when the system enters HALT mode. INTOSC1 and INTOSC2 will be powered down. This is the default behavior of the device.
- Return
None.
-
void
SysCtl_setWatchdogMode(SysCtl_WDMode mode)¶ Configures whether the watchdog generates a reset or an interrupt signal.
This function configures the action taken when the watchdog counter reaches its maximum value. When the
mode parameter is SYSCTL_WD_MODE_INTERRUPT, the watchdog is enabled to generate a watchdog interrupt signal and disables the generation of a reset signal. This will allow the watchdog module to wake up the device from IDLE or STANDBY if desired (see SysCtl_enableWatchdogStandbyWakeup()).- Parameters
mode: is a flag to select the watchdog mode.
When the mode parameter is SYSCTL_WD_MODE_RESET, the watchdog will be put into reset mode and generation of a watchdog interrupt signal will be disabled. This is how the watchdog is configured by default.
- Note
Check the status of the watchdog interrupt using SysCtl_isWatchdogInterruptActive() before calling this function. If the interrupt is still active, switching from interrupt mode to reset mode will immediately reset the device.
- Return
None.
-
bool
SysCtl_isWatchdogInterruptActive(void)¶ Gets the status of the watchdog interrupt signal.
This function returns the status of the watchdog interrupt signal. If the interrupt is active, this function will return true. If false, the interrupt is NOT active.
- Note
Make sure to call this function to ensure that the interrupt is not active before making any changes to the configuration of the watchdog to prevent any unexpected behavior. For instance, switching from interrupt mode to reset mode while the interrupt is active will immediately reset the device.
- Return
true if the interrupt is active and false if it is not.
-
void
SysCtl_disableWatchdog(void)¶ Disables the watchdog.
This function disables the watchdog timer. Note that the watchdog timer is enabled on reset.
- Return
None.
-
void
SysCtl_enableWatchdog(void)¶ Enables the watchdog.
This function enables the watchdog timer. Note that the watchdog timer is enabled on reset.
- Return
None.
-
bool
SysCtl_isWatchdogEnabled(void)¶ Checks if the watchdog is enabled or not
This function returns the watchdog status whether it is enabled or disabled
- Return
true if the watchdog is enabled & false if the watchdog is disabled
-
void
SysCtl_serviceWatchdog(void)¶ Services the watchdog.
This function resets the watchdog.
- Return
None.
-
void
SysCtl_enableWatchdogReset(void)¶ Writes the first key to enter the watchdog reset.
This function writes the first key to enter the watchdog reset.
- Return
None.
-
void
SysCtl_resetWatchdog(void)¶ Writes the second key to reset the watchdog.
This function writes the second key to reset the watchdog.
- Return
None.
-
void
SysCtl_setWatchdogPredivider(SysCtl_WDPredivider predivider)¶ Sets up watchdog clock (WDCLK) pre-divider.
This function sets up the watchdog clock (WDCLK) pre-divider. There are two dividers that scale INTOSC1 to WDCLK. The
predivider parameter divides INTOSC1 down to PREDIVCLK and the prescaler (set by the SysCtl_setWatchdogPrescaler() function) divides PREDIVCLK down to WDCLK.- Parameters
predivider: is the value that configures the pre-divider.
- Return
None.
-
void
SysCtl_setWatchdogPrescaler(SysCtl_WDPrescaler prescaler)¶ Sets up watchdog clock (WDCLK) prescaler.
This function sets up the watchdog clock (WDCLK) prescaler. There are two dividers that scale INTOSC1 to WDCLK. The predivider (set with the
SysCtl_setWatchdogPredivider() function) divides INTOSC1 down to PREDIVCLK and the prescaler parameter divides PREDIVCLK down to WDCLK.- Parameters
prescaler: is the value that configures the watchdog clock relative to the value from the pre-divider.
- Return
None.
-
uint16_t
SysCtl_getWatchdogCounterValue(void)¶ Gets the watchdog counter value.
- Return
Returns the current value of the 8-bit watchdog counter. If this count value overflows, a watchdog output pulse is generated.
-
bool
SysCtl_getWatchdogResetStatus(void)¶ Gets the watchdog reset status.
This function returns the watchdog reset status. If this function returns true, that indicates that a watchdog reset generated the last reset condition. Otherwise, it was an external device or power-up reset condition.
- Return
Returns true if the watchdog generated the last reset condition.
-
void
SysCtl_clearWatchdogResetStatus(void)¶ Clears the watchdog reset status.
This function clears the watchdog reset status. To check if it was set first, see SysCtl_getWatchdogResetStatus().
- Return
None.
-
void
SysCtl_setWatchdogWindowValue(uint16_t value)¶ Set the minimum threshold value for windowed watchdog
This function sets the minimum threshold value used to define the lower limit of the windowed watchdog functionality.
- Parameters
value: is the value to set the window threshold
- Return
None.
-
void
SysCtl_clearWatchdogOverride(void)¶ Clears the watchdog override.
This function clears the watchdog override and locks the watchdog timer module to remain in its prior state which could be either enable /disable. The watchdog timer will remain in this state until the next system reset.
- Return
None.
-
void
SysCtl_enableNMIGlobalInterrupt(void)¶ Enable the NMI Global interrupt bit
Note: This bit should be set after the device security related initialization is complete.
- Return
None.
-
bool
SysCtl_getNMIStatus(void)¶ Read NMI interrupts.
Read the current state of NMI interrupt.
- Return
true if NMI interrupt is triggered, false if not.
-
uint16_t
SysCtl_getNMIFlagStatus(void)¶ Read NMI Flags.
Read the current state of individual NMI interrupts
- Return
Value of NMIFLG register. These defines are provided to decode the value:
SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
-
bool
SysCtl_isNMIFlagSet(uint16_t nmiFlags)¶ Check if the individual NMI interrupts are set.
Check if interrupt flags corresponding to the passed in bit mask are asserted.
- Parameters
nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
- Return
true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.
-
void
SysCtl_clearNMIStatus(uint16_t nmiFlags)¶ Function to clear individual NMI interrupts.
Clear NMI interrupt flags that correspond with the passed in bit mask.
- Parameters
nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
Note: The NMI Interrupt flag is always cleared by default and therefore doesn’t have to be included in the bit mask.
- Return
None.
-
void
SysCtl_clearAllNMIFlags(void)¶ Clear all the NMI Flags that are currently set.
- Return
None.
-
void
SysCtl_forceNMIFlags(uint16_t nmiFlags)¶ Function to force individual NMI interrupt fail flags
- Return
None.
- Parameters
nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
-
uint16_t
SysCtl_getNMIWatchdogCounter(void)¶ Gets the NMI watchdog counter value.
Note: The counter is clocked at the SYSCLKOUT rate.
- Return
Returns the NMI watchdog counter register’s current value.
-
void
SysCtl_setNMIWatchdogPeriod(uint16_t wdPeriod)¶ Sets the NMI watchdog period value.
This function writes to the NMI watchdog period register that holds the value to which the NMI watchdog counter is compared. When the two registers match, a reset is generated. By default, the period is 0xFFFF.
- Parameters
wdPeriod: is the 16-bit value at which a reset is generated.
- Note
If a value smaller than the current counter value is passed into the wdPeriod parameter, a NMIRSn will be forced.
- Return
None.
-
uint16_t
SysCtl_getNMIWatchdogPeriod(void)¶ Gets the NMI watchdog period value.
- Return
Returns the NMI watchdog period register’s current value.
-
uint32_t
SysCtl_getNMIShadowFlagStatus(void)¶ Read NMI Shadow Flags.
Read the current state of individual NMI interrupts
- Return
Value of NMISHDFLG register. These defines are provided to decode the value:
SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
-
bool
SysCtl_isNMIShadowFlagSet(uint16_t nmiFlags)¶ Check if the individual NMI shadow flags are set.
Check if interrupt flags corresponding to the passed in bit mask are asserted.
- Parameters
nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:SYSCTL_NMI_NMIINT - NMI Interrupt Flag
SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag
SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag
SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag
SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag
SYSCTL_NMI_SYSDBGNMI - System Debug Module NMI Flag
SYSCTL_NMI_CLBNMI - Reconfigurable Logic NMI Flag
SYSCTL_NMI_SWERR - SW Error Force NMI Flag
SYSCTL_NMI_CRC_FAIL - BGCRC calculation failed.
- Return
true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.
-
void
SysCtl_enableMCD(void)¶ Enable the missing clock detection (MCD) Logic
- Return
None.
-
void
SysCtl_disableMCD(void)¶ Disable the missing clock detection (MCD) Logic
- Return
None.
-
bool
SysCtl_isMCDClockFailureDetected(void)¶ Get the missing clock detection Failure Status
- Note
A failure means the oscillator clock is missing
- Return
Returns true if a failure is detected or false if a failure isn’t detected
-
void
SysCtl_resetMCD(void)¶ Reset the missing clock detection logic after clock failure
- Return
None.
-
void
SysCtl_connectMCDClockSource(void)¶ Re-connect missing clock detection clock source to stop simulating clock failure
- Return
None.
-
void
SysCtl_disconnectMCDClockSource(void)¶ Disconnect missing clock detection clock source to simulate clock failure. This is for testing the MCD functionality.
- Return
None.
-
void
SysCtl_lockAccessControlRegs(void)¶ Lock the Access Control Registers
This function locks the access control registers and puts them in a read-only state.
- Note
Only a reset can unlock the access control registers.
- Return
None.
-
void
SysCtl_setPeripheralAccessControl(SysCtl_AccessPeripheral peripheral, SysCtl_AccessController controller, SysCtl_AccessPermission permission)¶ Set the peripheral access control permissions
This function sets the specified peripheral access control permissions for the the specified controller
- Parameters
peripheral: is the selected peripheralcontroller: is the selected controllerpermission: is the selected access permissions
The peripheral parameter can have one enumerated value in the format of SYSCTL_ACCESS_X where X is the name of the peripheral instance to be configured such as SYSCTL_ACCESS_ADCA.
The controller parameter can have one the following enumerated values:
SYSCTL_ACCESS_CPU1
SYSCTL_ACCESS_CLA1
SYSCTL_ACCESS_DMA1
SYSCTL_ACCESS_HIC
The permission parameter can have one the following enumerated values:
SYSCTL_ACCESS_FULL - Full Access for both read and write
SYSCTL_ACCESS_PROTECTED - Protected read access such that FIFOs, clear on read registers are not changed, and no write access
SYSCTL_ACCESS_NONE - No read or write access
- Return
None.
-
uint16_t
SysCtl_getPeripheralAccessControl(SysCtl_AccessPeripheral peripheral, SysCtl_AccessController controller)¶ Get the peripheral access control permissions
This function gets the specified peripheral access control permissions for the the specified controller
- Parameters
peripheral: is the selected peripheralcontroller: is the selected controller
The peripheral parameter can have one enumerated value in the format of SYSCTL_ACCESS_X where X is the name of the peripheral instance to be configured such as SYSCTL_ACCESS_ADCA.
The controller parameter can have one the following enumerated values:
SYSCTL_ACCESS_CPU1
SYSCTL_ACCESS_CLA1
SYSCTL_ACCESS_DMA1
SYSCTL_ACCESS_HIC
- Return
Returns one of the following enumerated permission values:
SYSCTL_ACCESS_FULL - Full Access for both read and write
SYSCTL_ACCESS_PROTECTED - Protected read access such that FIFOs, clear on read registers are not changed, and no write access
SYSCTL_ACCESS_NONE - No read or write access
-
void
SysCtl_setSyncOutputConfig(SysCtl_SyncOutputSource syncSrc)¶ Configures the sync output source.
This function configures the sync output source from the ePWM modules. The
syncSrc parameter is a value SYSCTL_SYNC_OUT_SRC_XXXX, where XXXX is a sync signal coming from an ePWM such as SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT- Parameters
syncSrc: is sync output source selection.
- Return
None.
-
void
SysCtl_enableExtADCSOCSource(uint32_t adcsocSrc)¶ Enables ePWM SOC signals to drive an external (off-chip) ADCSOC signal.
This function configures which ePWM SOC signals are enabled as a source for either ADCSOCAO or ADCSOCBO. The
adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.- Parameters
adcsocSrc: is a bit field of the selected signals to be enabled
- Return
None.
-
void
SysCtl_disableExtADCSOCSource(uint32_t adcsocSrc)¶ Disables ePWM SOC signals from driving an external ADCSOC signal.
This function configures which ePWM SOC signals are disabled as a source for either ADCSOCAO or ADCSOCBO. The
adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.- Parameters
adcsocSrc: is a bit field of the selected signals to be disabled
- Return
None.
-
void
SysCtl_lockExtADCSOCSelect(void)¶ Locks the SOC Select of the Trig X-BAR.
This function locks the external ADC SOC select of the Trig X-BAR.
- Return
None.
-
void
SysCtl_lockSyncSelect(void)¶ Locks the Sync Select of the Trig X-BAR.
This function locks Sync Input and Output Select of the Trig X-BAR.
- Return
None.
-
uint32_t
SysCtl_getDeviceRevision(void)¶ Get the Device Silicon Revision ID
This function returns the silicon revision ID for the device.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Returns the silicon revision ID value.
-
uint16_t
SysCtl_getEfuseError(void)¶ Gets the error status of the Efuse
The function provides both the Efuse Autoload & the Efuse Self Test Error Status.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Fuse Error status.
-
void
SysCtl_setXClk(SysCtl_XClkDivider divider)¶ Sets up XCLK divider.
This function sets up the XCLK divider. There is only one divider that scales INTOSC1 to XCLK.
- Parameters
divider: is the value that configures the divider.
The divider parameter can have one enumerated value from SysCtl_XClkDivider
- Return
None.
-
void
SysCtl_setPLLSysClk(uint16_t divider)¶ Sets up PLLSYSCLK divider.
This function sets up the PLLSYSCLK divider. There is only one divider that scales PLLSYSCLK to generate the system clock.
- Parameters
divider: is the value that configures the divider.
The divider parameter can have any value (even/odd) from 1-126
- Return
None.
- Note
Please make sure to check if the PLL is locked and valid using the SysCtl_isPLLValid() before setting the divider.
-
void
SysCtl_setMCANClk(SysCtl_MCANClkDivider divider)¶ Sets up MCAN Clk divider.
This function sets up the MCANCLK divider. There is only one divider that scales MCAN clock.
- Parameters
divider: is the value that configures the divider.
The divider parameter can have one enumerated value from SysCtl_MCANClkDivider
- Return
None.
-
void
SysCtl_setCputimer2Clk(SysCtl_Cputimer2ClkDivider divider, SysCtl_Cputimer2ClkSource source)¶ Sets up CPU Timer 2 CLK source & divider.
This function sets up the CPU Timer 2 CLK divider based on the source that is selected. There is only one divider that scales the “source” to CPU Timer 2 CLK.
- Parameters
divider: is the value that configures the divider.source: is the source for the clock divider
The divider parameter can have one enumerated value from SysCtl_Cputimer2ClkDivider The source parameter can have one enumerated value from SysCtl_Cputimer2ClkSource
- Return
None.
-
uint32_t
SysCtl_getPIEVErrAddr(void)¶ Gets the PIE Vector Fetch Error Handler Routine Address.
The function indicates the address of the PIE Vector Fetch Error handler routine.
- Return
Error Handler Address.
- Note
Its the responsibility of user to initialize this register. If this register is not initialized, a default error handler at address 0x3fffbe will get executed.
-
void
SysCtl_simulateReset(uint32_t rstCauses)¶ Simulates a reset to the CPU1
The
rstCauses parameter can be one/ more of these values: SYSCTL_SIMRESET_CPU1RSN or SYSCTL_SIMRESET_XRSN- Parameters
rstCauses: is the cause for the reset.
- Return
None.
- Note
This API exists only on CPU1
-
uint32_t
SysCtl_getInterruptStatus(void)¶ Gets the status of interrupts due to multiple different errors in the system.
- Return
the Interrupt generated on the system. The values can be one/ more from:
SYSCTL_STATUS_AES_BUS_ERROR
SYSCTL_STATUS_EPG1_INT
-
void
SysCtl_clearInterruptStatus(uint32_t intFlags)¶ Clears the interrupts due to multiple different errors in the system.
The
intFlags parameter are the Interrupts generated on errors in the system that need to be cleared. The values can be one or more from:SYSCTL_STATUS_GINT
SYSCTL_STATUS_AES_BUS_ERROR
SYSCTL_STATUS_EPG1_INT
- Parameters
intFlags: is the interrupt that needs to be cleared.
- Return
None.
-
void
SysCtl_setInterruptStatus(uint32_t intFlags)¶ Sets the interrupts for the multiple different errors in the system.
The
intFlags parameter are the Interrupts that can be set for the errors in the system. The values can be one/ more from:SYSCTL_STATUS_AES_BUS_ERROR
SYSCTL_STATUS_EPG1_INT
- Parameters
intFlags: is the interrupt that needs to be set.
- Return
None.
- Note
This API is present only on CPU1.
-
uint32_t
SysCtl_getInterruptStatusMask(void)¶ Gets the masked interrupts due to multiple different errors in the system.
- Return
the Interrupt generated on the system. The values can be one/ more from:
SYSCTL_STATUS_AES_BUS_ERROR
SYSCTL_STATUS_EPG1_INT
-
void
SysCtl_setInterruptStatusMask(uint32_t intFlags)¶ Masks the interrupts for the multiple different errors in the system.
The
intFlags parameter are the Interrupts that can be masked for the errors in the system. The values can be one/ more from:SYSCTL_STATUS_AES_BUS_ERROR
SYSCTL_STATUS_EPG1_INT
- Parameters
intFlags: is the interrupt that needs to be set.
- Return
None.
- Note
This API is present only on CPU1.
-
bool
SysCtl_isErrorTriggered(void)¶ Check if One or more of the error sources triggered
Following are the events/triggers that can indicate an error:
nmi interrupt on C28x
Watchdog reset
Error on a Pie vector fetch
Efuse error
nmi interrupt on CM
- Return
true if the error is triggered false if the error is not triggered
-
bool
SysCtl_getErrorPinStatus(void)¶ Check if Error status pin is high or not
- Return
true if the error status pin is high false if the error status pin is low
-
void
SysCtl_forceError(void)¶ Forces an error flag to set to indicate an error being generated.
- Return
None.
-
void
SysCtl_clearError(void)¶ Clears any error flag set due to error generated.
- Return
None.
-
void
SysCtl_selectErrPinPolarity(uint16_t pol)¶ Selects the polarity of the error pin
The
pol parameter can take any of the below values: 0x0U: If an error is already triggered, Error pin will be driven with a value of 0, else 1. 0x1U: If an error is already triggered, Error pin will be driven with a value of 1, else 0.- Parameters
pol: is the ERROR pin polarity
- Return
None.
-
void
SysCtl_lockErrControl(void)¶ Locks the Error control registers
This function locks the Error configuration registers.
- Return
None.
- Note
The lock register is cleared only on a system reset.
-
bool
SysCtl_isMCANWakeStatusSet(void)¶ Check if the MCAN wakeup event has occured.
- Return
true if the MCAN wakeup event has occured. false if the MCAN wakeup event has not occured.
-
void
SysCtl_clearMCANWakeStatus(void)¶ Clears the MCAN wakeup event status.
This function clears the MCAN wakeup event status. To check if it was set first, see SysCtl_isMCANWakeStatusSet().
- Return
None.
-
void
SysCtl_setLFUCPU(uint16_t value)¶ Sets the LFU_CPU configuration
- Note
This bit is used by compiler/application code for implementing CPU LFU
- Return
None
- Parameters
value: is the value to be set.0 : No pending requests
1 : LFU Request in progress
-
uint16_t
SysCtl_getLFUCPU(void)¶ Gets the LFU_CPU configuration
- Note
This bit is used by compiler/application code for implementing CPU LFU
- Return
0 if No pending requests, 1 if LFU Request is in progress
-
void
SysCtl_setLFUCLA1(uint16_t value)¶ Sets the LFU_CLA configuration
- Note
This bit is used by compiler/application code for implementing CLA LFU
- Return
None
- Parameters
value: is the value to be set.0 : No pending requests
1 : LFU Request in progress
-
uint16_t
SysCtl_getLFUCLA1(void)¶ Gets the LFU_CLA configuration
- Note
This bit is used by compiler/application code for implementing CLA LFU
- Return
0 if No pending requests, 1 if LFU Request is in progress
-
void
SysCtl_swapPieVectorAndLS01(bool swap)¶ Swap PIE Vector Table to alternate location and swap LS0 and LS1
- Return
None
- Parameters
swap: Whether to enable or disable swaptrue : PIE Vector Table is swapped to alternate location. LS0 and LS1 is swapped
false : PIE vector table is mapped to the original location LS0 and LS1 is mapped to original location
-
void
SysCtl_swapPieVector(bool swap)¶ Swap PIE Vector Table to alternate location
- Return
None
- Parameters
swap: Whether to enable or disable swaptrue : PIE Vector Table is swapped to alternate location
false : PIE vector table is mapped to the original location
-
bool
SysCtl_isPieVectorSwap(void)¶ Checks if the PIE Vector Table is swapped or not
- Return
true if the PIE Vector Table is mapped to original location, false if PIE Vector Table is swapped to alternate location
- Parameters
reg: is the register to be setvalue: is the value to be set
-
void
SysCtl_swapLS01(bool swap)¶ Swap LS0 and LS1
- Return
None
- Parameters
swap: Whether to enable or disable swaptrue : LS0 and LS1 is swapped
false : LS0 and LS1 is mapped to original location
-
bool
SysCtl_isLS01Swap(void)¶ Checks if the LS0 and LS1 are swapped or not
- Return
true if the LS0 and LS1 is mapped to original location, false if LS0 and LS1 is swapped
- Parameters
reg: is the register to be setvalue: is the value to be set
-
void
SysCtl_setLFUUserRegister(SysCtl_LFUUserRegister reg, uint32_t value)¶ Sets the user register.
This function sets specified LFU user register. The
value parameter can have one enumerated value from SysCtl_LFUUserRegister.- Parameters
reg: is the register to be setvalue: is the value to be set
- Return
None.
-
uint32_t
SysCtl_getLFUUserRegister(SysCtl_LFUUserRegister reg)¶ Gets the user register.
This function sets specified LFU user register. The
value parameter can have one enumerated value from SysCtl_LFUUserRegister.- Parameters
reg: is the register to be set
- Return
value of the specified register.
-
void
SysCtl_lockLFUConfigRegister(void)¶ Locks the LFUConfig register
- Return
None.
-
void
SysCtl_lockLFUUserRegister(SysCtl_LFUUserRegister reg)¶ Locks the LFU User registers
- Return
None.
- Parameters
register: to be locked
-
void
SysCtl_unlockLFUConfigRegister(void)¶ Unlocks the LFUConfig register
- Return
None.
-
void
SysCtl_unlockLFUUserRegister(SysCtl_LFUUserRegister reg)¶ Unlocks the LFU User registers
- Return
None.
- Parameters
register: to be unlocked
-
void
SysCtl_commitLFUConfigRegister(void)¶ Commits the LFUConfig register
- Return
None.
-
void
SysCtl_commitLFUUserRegister(SysCtl_LFUUserRegister reg)¶ Commits the LFU User registers
- Return
None.
- Parameters
register: to be committed
-
uint32_t
SysCtl_getDeviceUID(void)¶ Get the device UID_UNIQUE value
This function returns the device UID_UNIQUE value
- Return
Returns the device UID_UNIQUE value
-
uint32_t
SysCtl_getTapStatus(void)¶ Get the status of JTAG State machine and debugger connect
This function returns the JTAG status
- Return
Returns the JTAG status. The bits representing will be - 0:TLR, 1:IDLE, 2:SELECTDR, 3:CAPDR, 4:SHIFTDR, 5:EXIT1DR, 6:PAUSEDR, 7:EXIT2DR, 8:UPDTDR, 9:SLECTIR, 10:CAPIR, 11:SHIFTIR, 12:EXIT1IR, 13:PAUSEIR, 14:EXIT2IR, 15:UPDTIR
-
void
SysCtl_delay(uint32_t count)¶ Delays for a fixed number of cycles.
This function generates a constant length delay using assembly code. The loop takes 5 cycles per iteration plus 9 cycles of overhead.
- Parameters
count: is the number of delay loop iterations to perform.
- Note
If count is equal to zero, the loop will underflow and run for a very long time.
- Note
Refer to the macro DEVICE_DELAY_US(x) in device.h which can be used to insert a delay in microseconds.
- Return
None.
-
uint32_t
SysCtl_getClock(uint32_t clockInHz)¶ Calculates the system clock frequency (SYSCLK).
This function determines the frequency of the system clock based on the frequency of the oscillator clock source (from
clockInHz) and the PLL and clock divider configuration registers.- Parameters
clockInHz: is the frequency of the oscillator clock source (OSCCLK).
- Return
Returns the system clock frequency. If a missing clock is detected, the function will return the INTOSC1 frequency. This needs to be corrected and cleared (see SysCtl_resetMCD()) before trying to call this function again.
-
bool
SysCtl_setClock(uint32_t config)¶ Configures the clocking of the device.
This function configures the clocking of the device. The input crystal frequency, oscillator to be used, use of the PLL, and the system clock divider are all configured with this function.
- Parameters
config: is the required configuration of the device clocking.
The config parameter is the OR of several different values, many of which are grouped into sets where only one can be chosen.
The system clock divider is chosen with the macro SYSCTL_SYSDIV(x) where x is either 1 or an even value up to 126.
The use of the PLL is chosen with ONLY one of the below modes: SYSCTL_PLL_ENABLE - This is to Enable the PLL Clock to the System or SYSCTL_PLL_BYPASS -This is to Bypass the PLLCLK from the System, this will also power up the PLL if the user desires to power up the PLL but not use it for System. or SYSCTL_PLL_DISABLE-This is to Power Down the PLL and Bypass the PLLCLK to the System.
The integer multiplier is chosen SYSCTL_IMULT(x) where x is a value from 1 to 127.
The oscillator source chosen with SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, SYSCTL_OSCSRC_XTAL_SE or SYSCTL_OSCSRC_OSC1.
This function uses the DCC to check that the PLLRAWCLK is running at the expected rate. If you are using the DCC, you must back up its configuration before calling this function and restore it afterward. Locking PLL sequence is only done if the multipliers are updated.
- Note
See your device errata for more details about locking the PLL.
- Return
Returns false if a missing clock error is detected. This needs to be cleared (see SysCtl_resetMCD()) before trying to call this function again. Also, returns false if the PLLRAWCLK is not running and its expected rate. Otherwise, returns true.
-
bool
SysCtl_isPLLValid(uint32_t base, uint32_t oscSource, uint32_t pllMultDiv)¶ Validates PLL Raw Clock Frequency (PLLRAWCLK)
This function uses DCC module to validate the PLL clock frequency. It uses oscSource as a reference clock for DCC, and PLL is used as clock under test. As long as the Counter0 (running of oscSource) & Counter1 (running of PLL) expire at the same time, DCC will not generate an Error. This function gives 100 attempts for PLL to lock and make sure frequency is as expected.
- Parameters
base: is the DCC module base addressoscSource: is the Clock Source for the PLL that is also used for DCCpllMultDiv: has the PLL Multiplier Register configuration which include integer multiplier and divider values used to configure the DCC Counter1 clock
The oscSource parameter is the oscillator source chosen with SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, SYSCTL_OSCSRC_XTAL_SE or SYSCTL_OSCSRC_OSC1.
The pllMultDiv parameter is a bitwise OR of SYSCTL_IMULT(x) where x is a value from 1 to 127 and both of the following divider values which is chosen with the macro SYSCTL_REFDIV(x) and SYSCTL_ODIV(x) where x is a value from 1 to 32 and can be different for both macros.
- Return
Returns true if the DCCSTATUS error flag is not set. Otherwise, returns false.
- Note
This function does not validate if PLL output frequency (PLLRAWCLK) is within the operating range as per the datasheet.
-
void
SysCtl_selectXTAL(void)¶ Configures the external oscillator for the clocking of the device.
This function configures the external oscillator (XTAL) to be used for the clocking of the device in crystal mode. It follows the procedure to turn on the oscillator, wait for it to power up, and select it as the source of the system clock.
Please note that this function blocks while it waits for the XTAL to power up. If the XTAL does not manage to power up properly, the function will loop for a long time. It is recommended that you modify this function to add an appropriate timeout and error-handling procedure.
- Return
None.
-
void
SysCtl_selectXTALSingleEnded(void)¶ Configures the external oscillator for the clocking of the device in single-ended mode.
This function configures the external oscillator (XTAL) to be used for the clocking of the device in single-ended mode. It follows the procedure to turn on the oscillator, wait for it to power up, and select it as the source of the system clock.
Please note that this function blocks while it waits for the XTAL to power up. If the XTAL does not manage to power up properly, the function will loop for a long time. It is recommended that you modify this function to add an appropriate timeout and error-handling procedure.
- Return
None.
-
void
SysCtl_selectOscSource(uint32_t oscSource)¶ Selects the oscillator to be used for the clocking of the device.
This function configures the oscillator to be used in the clocking of the device. The
oscSource parameter may take a value of SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, SYSCTL_OSCSRC_XTAL_SE, or SYSCTL_OSCSRC_OSC1.- Parameters
oscSource: is the oscillator source to be configured.
- See
- Return
None.
-
uint32_t
SysCtl_getLowSpeedClock(uint32_t clockInHz)¶ Calculates the low-speed peripheral clock frequency (LSPCLK).
This function determines the frequency of the low-speed peripheral clock based on the frequency of the oscillator clock source (from
clockInHz) and the PLL and clock divider configuration registers.- Parameters
clockInHz: is the frequency of the oscillator clock source (OSCCLK).
- Return
Returns the low-speed peripheral clock frequency.
-
uint16_t
SysCtl_getDeviceParametric(SysCtl_DeviceParametric parametric)¶ Get the device part parametric value
This function gets the device part parametric value.
- Parameters
parametric: is the requested device parametric value
The parametric parameter can have one the following enumerated values:
SYSCTL_DEVICE_QUAL - Device Qualification Status
SYSCTL_DEVICE_PINCOUNT - Device Pin Count
SYSCTL_DEVICE_INSTASPIN - Device InstaSPIN Feature Set
SYSCTL_DEVICE_FLASH - Device Flash size (KB)
SYSCTL_DEVICE_FAMILY - Device Family
SYSCTL_DEVICE_PARTNO - Device Part Number
SYSCTL_DEVICE_CLASSID - Device Class ID
- Note
This API is applicable only for the CPU1 subsystem.
- Return
Returns the specified parametric value.
-
void
SysCtl_configureType(SysCtl_SelType type, uint16_t config, uint16_t lock)¶ Configures & locks/unlocks the peripheral type
The
type parameter can be a value from the enumeration SysCtl_SelType The config parameter can be a value from the ones below: 0x0U : disables the feature for the type. 0x1U : enables the feature for the type.- Parameters
type: is the peripheral type that needs to be configured.config: is the configuration done to the peripheral which is dependent on the peripheral type.lock: is to decide if writes for any further configuration is to be allowed or not.
For ECAP: ECAP registers are EALLOW protected or not. For SDFM: Data Ready conditions do not generate the SDFMINT. & Each filter generates a separate data ready interrupts.
The lock parameter can be a value from the ones below: 0x1U : Write for any further configuration is not allowed. 0x0U : Write for any further configuration is allowed.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
None.
-
bool
SysCtl_isConfigTypeLocked(SysCtl_SelType type)¶ Check if writes for any further configuration of peripheral types is to be allowed or not.
- Note
This API is applicable only for the CPU1 subsystem.
- Return
true if Write for any further configuration is not allowed. false if Write for any further configuration is allowed.
- Parameters
type: is the peripheral type for which permissions are being checked
-
void
SysCtl_lockClkConfig(SysCtl_ClkRegSel registerName)¶ Locks the Clock configuration registers
The
registerName parameter can be a value from the enumeration SysCtl_ClkRegSel- Parameters
registerName: is clock configuration register which needs to be locked.
- Return
None.
- Note
The register is unlocked only on a system reset.
-
void
SysCtl_lockSysConfig(SysCtl_CpuRegSel registerName)¶ Locks the CPU system configuration registers
The
registerName parameter can be a value from the enumeration SysCtl_CpuRegSel- Parameters
registerName: is CPU system configuration register which needs to be locked.
- Return
None.
- Note
The register is unlocked only on a system reset.
-
Many of the functions provided by the SysCtl API are related to device clocking. The most important of these functions is SysCtl_setClock() which will configure which oscillator is to be used, configure the PLL, and configure the system clock divider. SysCtl_getClock() is a complementary function to this one that will, given the frequency of the oscillator source used, read back the configuration of the PLL and clock divider and calculate the system clock frequency. A similar pair of functions is provided for the low-speed peripheral clock, SysCtl_setLowSpeedClock() and SysCtl_getLowSpeedClock().
The ability to enable (turn on the module clock), disable (gate off the module clock), and perform a software reset on most of the peripherals on a device is provided by SysCtl_enablePeripheral(), SysCtl_disablePeripheral(), and SysCtl_resetPeripheral() respectively.
The device’s windowed watchdog is enabled and disabled by SysCtl_enableWatchdog() and SysCtl_disableWatchdog() respectively. The watchdog can be serviced by SysCtl_serviceWatchdog(). Several functions are also provided to configure the watchdog’s clock and windowed functionality.
This section will give further details of these functions and each of the others used for the configuration of SysCtl.
The code for this module is contained in driverlib/sysctl.c, with driverlib/sysctl.h containing the API declarations for use by applications.