CLB Module¶
The Configurable Logic Block (CLB) API provides a set of functions to configure the CLB. The CLB is a collection of configurable blocks that can be interconnected using software to implement custom digital logic functions.
The CLB is able to enhance existing peripherals through a set of crossbar interconnections, which provides a high level of connectivity to existing control peripherals such as enhanced pulse width modulators (ePWM), enhanced capture modules (eCAP), and enhanced quadrature encoder pulse modules (eQEP). The crossbars also allow the CLB to be connected to external GPIO pins.
In this way, the CLB can be configured to interact with device peripherals to perform small logical functions such as simple PWM generators, or to implement custom serial data exchange protocols.
-
group
clb_api Defines
-
CLB_LOGICCTL0x0100U¶
-
CLB_DATAEXCH0x0180U¶
-
CLB_ADDR_COUNTER_0_LOAD0x0U¶
-
CLB_ADDR_COUNTER_1_LOAD0x1U¶
-
CLB_ADDR_COUNTER_2_LOAD0x2U¶
-
CLB_ADDR_COUNTER_0_MATCH10x4U¶
-
CLB_ADDR_COUNTER_1_MATCH10x5U¶
-
CLB_ADDR_COUNTER_2_MATCH10x6U¶
-
CLB_ADDR_COUNTER_0_MATCH20x8U¶
-
CLB_ADDR_COUNTER_1_MATCH20x9U¶
-
CLB_ADDR_COUNTER_2_MATCH20xAU¶
-
CLB_ADDR_HLC_R00xCU¶
-
CLB_ADDR_HLC_R10xDU¶
-
CLB_ADDR_HLC_R20xEU¶
-
CLB_ADDR_HLC_R30xFU¶
-
CLB_ADDR_HLC_BASE0x20U¶
-
CLB_NUM_HLC_INSTR31U¶
-
CLB_FIFO_SIZE4U¶
-
CLB_LOCK_KEY0x5A5AU¶
-
CLB_LCL_MUX_SEL_MISC_INPUT_SEL_M0x20U¶
-
CLB_LCL_MUX_SEL_MISC_INPUT_SEL_S28U¶
-
CLB_LCL_MUX_SEL_MISC_INPUT_SEL_BITM(uint32_t)1U¶
-
CLB_OUTPUT_000x00000001U¶ Mask for CLB OUTPUT ENABLE/DISABLE 0.
Values that can be passed to control the CLB output enable signal. It can be passed to CLB_setOutputMask() as the outputMask parameter.
-
CLB_OUTPUT_010x00000002U¶ Mask for CLB OUTPUT ENABLE/DISABLE 1.
-
CLB_OUTPUT_020x00000004U¶ Mask for CLB OUTPUT ENABLE/DISABLE 2.
-
CLB_OUTPUT_030x00000008U¶ Mask for CLB OUTPUT ENABLE/DISABLE 3.
-
CLB_OUTPUT_040x00000010U¶ Mask for CLB OUTPUT ENABLE/DISABLE 4.
-
CLB_OUTPUT_050x00000020U¶ Mask for CLB OUTPUT ENABLE/DISABLE 5.
-
CLB_OUTPUT_060x00000040U¶ Mask for CLB OUTPUT ENABLE/DISABLE 6.
-
CLB_OUTPUT_070x00000080U¶ Mask for CLB OUTPUT ENABLE/DISABLE 7.
-
CLB_OUTPUT_080x00000100U¶ Mask for CLB OUTPUT ENABLE/DISABLE 8.
-
CLB_OUTPUT_090x00000200U¶ Mask for CLB OUTPUT ENABLE/DISABLE 9.
-
CLB_OUTPUT_100x00000400U¶ Mask for CLB OUTPUT ENABLE/DISABLE 10.
-
CLB_OUTPUT_110x00000800U¶ Mask for CLB OUTPUT ENABLE/DISABLE 11.
-
CLB_OUTPUT_120x00001000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 12.
-
CLB_OUTPUT_130x00002000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 13.
-
CLB_OUTPUT_140x00004000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 14.
-
CLB_OUTPUT_150x00008000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 15.
-
CLB_OUTPUT_160x00010000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 16.
-
CLB_OUTPUT_170x00020000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 17.
-
CLB_OUTPUT_180x00040000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 18.
-
CLB_OUTPUT_190x00080000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 19.
-
CLB_OUTPUT_200x00100000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 20.
-
CLB_OUTPUT_210x00200000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 21.
-
CLB_OUTPUT_220x00400000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 22.
-
CLB_OUTPUT_230x00800000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 23.
-
CLB_OUTPUT_240x01000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 24.
-
CLB_OUTPUT_250x02000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 25.
-
CLB_OUTPUT_260x04000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 26.
-
CLB_OUTPUT_270x08000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 27.
-
CLB_OUTPUT_280x10000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 28.
-
CLB_OUTPUT_290x20000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 29.
-
CLB_OUTPUT_300x40000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 30.
-
CLB_OUTPUT_310x80000000U¶ Mask for CLB OUTPUT ENABLE/DISABLE 31.
Enums
-
enum
CLB_Inputs¶ Values that can be passed to select CLB input signal.
Values:
-
enumerator
CLB_IN0= 0¶ Input 0.
-
enumerator
CLB_IN1= 1¶ Input 1.
-
enumerator
CLB_IN2= 2¶ Input 2.
-
enumerator
CLB_IN3= 3¶ Input 3.
-
enumerator
CLB_IN4= 4¶ Input 4.
-
enumerator
CLB_IN5= 5¶ Input 5.
-
enumerator
CLB_IN6= 6¶ Input 6.
-
enumerator
CLB_IN7= 7¶ Input 7.
-
enumerator
-
enum
CLB_Outputs¶ Values that can be passed to select CLB output signal. It can be passed to CLB_configOutputLUT() as the outID parameter.
Values:
-
enumerator
CLB_OUT0= 0¶ Output 0.
-
enumerator
CLB_OUT1= 1¶ Output 1.
-
enumerator
CLB_OUT2= 2¶ Output 2.
-
enumerator
CLB_OUT3= 3¶ Output 3.
-
enumerator
CLB_OUT4= 4¶ Output 4.
-
enumerator
CLB_OUT5= 5¶ Output 5.
-
enumerator
CLB_OUT6= 6¶ Output 6.
-
enumerator
CLB_OUT7= 7¶ Output 7.
-
enumerator
-
enum
CLB_AOCs¶ Values that can be passed to select CLB AOC signal. It can be passed to CLB_configAOC() as the aocID parameter. AOC is the Asynchronous Output Conditioning block.
Values:
-
enumerator
CLB_AOC0= 0¶ AOC 0.
-
enumerator
CLB_AOC1= 1¶ AOC 1.
-
enumerator
CLB_AOC2= 2¶ AOC 2.
-
enumerator
CLB_AOC3= 3¶ AOC 3.
-
enumerator
CLB_AOC4= 4¶ AOC 4.
-
enumerator
CLB_AOC5= 5¶ AOC 5.
-
enumerator
CLB_AOC6= 6¶ AOC 6.
-
enumerator
CLB_AOC7= 7¶ AOC 7.
-
enumerator
-
enum
CLB_SWReleaseCtrl¶ Values that can be passed to set/clear CLB SW release signals. It can be passed to CLB_writeSWReleaseControl() as the inID parameter.
Values:
-
enumerator
CLB_SW_RLS_CTRL0= 0¶ SW RLS CTRL 0.
-
enumerator
CLB_SW_RLS_CTRL1= 1¶ SW RLS CTRL 1.
-
enumerator
CLB_SW_RLS_CTRL2= 2¶ SW RLS CTRL 2.
-
enumerator
CLB_SW_RLS_CTRL3= 3¶ SW RLS CTRL 3.
-
enumerator
CLB_SW_RLS_CTRL4= 4¶ SW RLS CTRL 4.
-
enumerator
CLB_SW_RLS_CTRL5= 5¶ SW RLS CTRL 5.
-
enumerator
CLB_SW_RLS_CTRL6= 6¶ SW RLS CTRL 6.
-
enumerator
CLB_SW_RLS_CTRL7= 7¶ SW RLS CTRL 7.
-
enumerator
-
enum
CLB_SWGateCtrl¶ Values that can be passed to set/clear CLB SW release signals. It can be passed to CLB_writeSWGateControl() as the inID parameter.
Values:
-
enumerator
CLB_SW_GATE_CTRL0= 0¶ SW GATE CTRL 0.
-
enumerator
CLB_SW_GATE_CTRL1= 1¶ SW GATE CTRL 1.
-
enumerator
CLB_SW_GATE_CTRL2= 2¶ SW GATE CTRL 2.
-
enumerator
CLB_SW_GATE_CTRL3= 3¶ SW GATE CTRL 3.
-
enumerator
CLB_SW_GATE_CTRL4= 4¶ SW GATE CTRL 4.
-
enumerator
CLB_SW_GATE_CTRL5= 5¶ SW GATE CTRL 5.
-
enumerator
CLB_SW_GATE_CTRL6= 6¶ SW GATE CTRL 6.
-
enumerator
CLB_SW_GATE_CTRL7= 7¶ SW GATE CTRL 7.
-
enumerator
-
enum
CLB_Counters¶ Values that can be passed to select CLB counter. It can be passed to CLB_configCounterLoadMatch() as the counterID parameter.
Values:
-
enumerator
CLB_CTR0= 0¶ Counter 0.
-
enumerator
CLB_CTR1= 1¶ Counter 1.
-
enumerator
CLB_CTR2= 2¶ Counter 2.
-
enumerator
-
enum
CLB_Register¶ Values that can be passed to CLB_getRegister() as the registerID parameter.
Values:
-
enumerator
CLB_REG_HLC_R0= 0x30U¶ HLC R0 register.
-
enumerator
CLB_REG_HLC_R1= 0x32U¶ HLC R1 register.
-
enumerator
CLB_REG_HLC_R2= 0x34U¶ HLC R2 register.
-
enumerator
CLB_REG_HLC_R3= 0x36U¶ HLC R3 register.
-
enumerator
CLB_REG_CTR_C0= 0x38U¶ Counter 0 register.
-
enumerator
CLB_REG_CTR_C1= 0x3AU¶ Counter 1 register.
-
enumerator
CLB_REG_CTR_C2= 0x3CU¶ Counter 2 register.
-
enumerator
-
enum
CLB_FilterType¶ Values that can be passed to CLB_selectInputFilter() as the filterType parameter.
Values:
-
enumerator
CLB_FILTER_NONE= 0¶ No filtering.
-
enumerator
CLB_FILTER_RISING_EDGE= 1¶ Rising edge detect.
-
enumerator
CLB_FILTER_FALLING_EDGE= 2¶ Falling edge detect.
-
enumerator
CLB_FILTER_ANY_EDGE= 3¶ Any edge detect.
-
enumerator
-
enum
CLB_GPInputMux¶ Values that can be passed to CLB_configGPInputMux() as the gpMuxCfg parameter.
Values:
-
enumerator
CLB_GP_IN_MUX_EXTERNAL= 0¶ Use external input path.
-
enumerator
CLB_GP_IN_MUX_GP_REG= 1¶ Use CLB_GP_REG bit value as input.
-
enumerator
-
enum
CLB_LocalInputMux¶ Values that can be passed to CLB_configLocalInputMux() as the localMuxCfg parameter.
Values:
-
enumerator
CLB_LOCAL_IN_MUX_GLOBAL_IN= 0¶ Global input mux selection.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCAEVT1= 1¶ EPWMx DCAEVT1.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCAEVT2= 2¶ EPWMx DCAEVT2.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCBEVT1= 3¶ EPWMx DCBEVT1.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCBEVT2= 4¶ EPWMx DCBEVT2.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCAH= 5¶ EPWMx DCAH.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCAL= 6¶ EPWMx DCAL.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCBH= 7¶ EPWMx DCBH.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_DCBL= 8¶ EPWMx DCBL.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_OST= 9¶ EPWMx OST.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM_CBC= 10¶ EPWMx CBC.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_ECAPIN= 11¶ ECAPx ECAPIN.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_ECAP_OUT= 12¶ ECAPx ECAP_OUT.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_ECAP_OUT_EN= 13¶ ECAPx ECAP_OUT_EN.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_CEVT1= 14¶ ECAPx CEVT1.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_CEVT2= 15¶ ECAPx CEVT2.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_CEVT3= 16¶ ECAPx CEVT3.
-
enumerator
CLB_LOCAL_IN_MUX_ECAP_CEVT4= 17¶ ECAPx CEVT4.
-
enumerator
CLB_LOCAL_IN_MUX_EQEP_EQEPA= 18¶ EQEPx EQEPA.
-
enumerator
CLB_LOCAL_IN_MUX_EQEP_EQEPB= 19¶ EQEPx EQEPB.
-
enumerator
CLB_LOCAL_IN_MUX_EQEP_EQEPI= 20¶ EQEPx EQEPI.
-
enumerator
CLB_LOCAL_IN_MUX_EQEP_EQEPS= 21¶ EQEPx EQEPS.
-
enumerator
CLB_LOCAL_IN_MUX_CPU1_TBCLKSYNC= 22¶ CPU1.TBCLKSYNC.
-
enumerator
CLB_LOCAL_IN_MUX_CPU1_HALT= 24¶ CPU1.HALT.
-
enumerator
CLB_LOCAL_IN_MUX_SPIPICO_CONTROLLER= 25¶ SPIPICO Controller Output.
-
enumerator
CLB_LOCAL_IN_MUX_SPICLK= 26¶ SPI Clock.
-
enumerator
CLB_LOCAL_IN_MUX_SPIPICO_PERIPHERAL= 27¶ SPIPICO Peripheral Input.
-
enumerator
CLB_LOCAL_IN_MUX_SPIPTE= 28¶ SPI PTE.
-
enumerator
CLB_LOCAL_IN_MUX_SCI_TX= 29¶ SCI TX.
-
enumerator
CLB_LOCAL_IN_MUX_SPIPOCI_OUT= 30¶ SPIPOCI(OUT)
-
enumerator
CLB_LOCAL_IN_MUX_CLB_PSCLK= 31¶ CLB prescaled clock.
-
enumerator
CLB_LOCAL_IN_MUX_EPWM5A= 32¶ EPWM5A (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM5A_OE= 33¶ EPWM5A trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM5B= 34¶ EPWM5B (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM5B_OE= 35¶ EPWM5B trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM6A= 36¶ EPWM6A (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM6A_OE= 37¶ EPWM6A trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM6B= 38¶ EPWM6B (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM6B_OE= 39¶ EPWM6B trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM7A= 40¶ EPWM7A (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM7A_OE= 41¶ EPWM7A trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM7B= 42¶ EPWM7B (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM7B_OE= 43¶ EPWM7B trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM8A= 44¶ EPWM8A (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM8A_OE= 45¶ EPWM8A trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM8B= 46¶ EPWM8B (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_EPWM8B_OE= 47¶ EPWM8B trip output (CLB 1-4)
-
enumerator
CLB_LOCAL_IN_MUX_INPUT1= 48¶ CLBINPUTXBAR INPUT1.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT2= 49¶ CLBINPUTXBAR INPUT2.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT3= 50¶ CLBINPUTXBAR INPUT3.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT4= 51¶ CLBINPUTXBAR INPUT4.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT5= 52¶ CLBINPUTXBAR INPUT5.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT6= 53¶ CLBINPUTXBAR INPUT6.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT7= 54¶ CLBINPUTXBAR INPUT7.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT8= 55¶ CLBINPUTXBAR INPUT8.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT9= 56¶ CLBINPUTXBAR INPUT9.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT10= 57¶ CLBINPUTXBAR INPUT10.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT11= 58¶ CLBINPUTXBAR INPUT11.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT12= 59¶ CLBINPUTXBAR INPUT12.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT13= 60¶ CLBINPUTXBAR INPUT13.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT14= 61¶ CLBINPUTXBAR INPUT14.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT15= 62¶ CLBINPUTXBAR INPUT15.
-
enumerator
CLB_LOCAL_IN_MUX_INPUT16= 63¶ CLBINPUTXBAR INPUT16.
-
enumerator
-
enum
CLB_GlobalInputMux¶ Values that can be passed to CLB_configGlobalInputMux() as the globalMuxCfg parameter.
Values:
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1A= 0¶ EPWM1A.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1A_OE= 1¶ EPWM1A trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1B= 2¶ EPWM1B.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1B_OE= 3¶ EPWM1B trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_ZERO= 4¶ EPWM1 TBCTR = Zero.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_PRD= 5¶ EPWM1 TBCTR = TBPRD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTRDIR= 6¶ EPWM1 CTRDIR.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_TBCLK= 7¶ EPWM1 TBCLK.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_CMPA= 8¶ EPWM1 TBCTR = CMPA.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_CMPB= 9¶ EPWM1 TBCTR = CMPB.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_CMPC= 10¶ EPWM1 TBCTR = CMPC.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1_CTR_CMPD= 11¶ EPWM1 TBCTR = CMPD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1A_AQ= 12¶ EPWM1A AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1B_AQ= 13¶ EPWM1B AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1A_DB= 14¶ EPWM1A DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM1B_DB= 15¶ EPWM1B DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2A= 16¶ EPWM2A.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2A_OE= 17¶ EPWM2A trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2B= 18¶ EPWM2B.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2B_OE= 19¶ EPWM2B trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_ZERO= 20¶ EPWM2 TBCTR = Zero.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_PRD= 21¶ EPWM2 TBCTR = TBPRD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTRDIR= 22¶ EPWM2 CTRDIR.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_TBCLK= 23¶ EPWM2 TBCLK.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_CMPA= 24¶ EPWM2 TBCTR = CMPA.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_CMPB= 25¶ EPWM2 TBCTR = CMPB.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_CMPC= 26¶ EPWM2 TBCTR = CMPC.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2_CTR_CMPD= 27¶ EPWM2 TBCTR = CMPD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2A_AQ= 28¶ EPWM2A AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2B_AQ= 29¶ EPWM2B AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2A_DB= 30¶ EPWM2A DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM2B_DB= 31¶ EPWM2B DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3A= 32¶ EPWM3A.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3A_OE= 33¶ EPWM3A trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3B= 34¶ EPWM3B.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3B_OE= 35¶ EPWM3B trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_ZERO= 36¶ EPWM3 TBCTR = Zero.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_PRD= 37¶ EPWM3 TBCTR = TBPRD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTRDIR= 38¶ EPWM3 CTRDIR.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_TBCLK= 39¶ EPWM3 TBCLK.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_CMPA= 40¶ EPWM3 TBCTR = CMPA.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_CMPB= 41¶ EPWM3 TBCTR = CMPB.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_CMPC= 42¶ EPWM3 TBCTR = CMPC.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3_CTR_CMPD= 43¶ EPWM3 TBCTR = CMPD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3A_AQ= 44¶ EPWM3A AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3B_AQ= 45¶ EPWM3B AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3A_DB= 46¶ EPWM3A DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM3B_DB= 47¶ EPWM3B DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4A= 48¶ EPWM4A.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4A_OE= 49¶ EPWM4A trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4B= 50¶ EPWM4B.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4B_OE= 51¶ EPWM4B trip output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_ZERO= 52¶ EPWM4 TBCTR = Zero.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_PRD= 53¶ EPWM4 TBCTR = TBPRD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTRDIR= 54¶ EPWM4 CTRDIR.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_TBCLK= 55¶ EPWM4 TBCLK.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_CMPA= 56¶ EPWM4 TBCTR = CMPA.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_CMPB= 57¶ EPWM4 TBCTR = CMPB.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_CMPC= 58¶ EPWM4 TBCTR = CMPC.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4_CTR_CMPD= 59¶ EPWM4 TBCTR = CMPD.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4A_AQ= 60¶ EPWM4A AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4B_AQ= 61¶ EPWM4B AQ submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4A_DB= 62¶ EPWM4A DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_EPWM4B_DB= 63¶ EPWM4B DB submodule output.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG0= 64¶ CLB X-BAR AUXSIG0.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG1= 65¶ CLB X-BAR AUXSIG1.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG2= 66¶ CLB X-BAR AUXSIG2.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG3= 67¶ CLB X-BAR AUXSIG3.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG4= 68¶ CLB X-BAR AUXSIG4.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG5= 69¶ CLB X-BAR AUXSIG5.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG6= 70¶ CLB X-BAR AUXSIG6.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB_AUXSIG7= 71¶ CLB X-BAR AUXSIG7.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT16= 72¶ CLB1 OUT16.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT17= 73¶ CLB1 OUT17.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT18= 74¶ CLB1 OUT18.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT19= 75¶ CLB1 OUT19.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT20= 76¶ CLB1 OUT20.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT21= 77¶ CLB1 OUT21.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT22= 78¶ CLB1 OUT22.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB1_OUT23= 79¶ CLB1 OUT23.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT16= 80¶ CLB2 OUT16.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT17= 81¶ CLB2 OUT17.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT18= 82¶ CLB2 OUT18.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT19= 83¶ CLB2 OUT19.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT20= 84¶ CLB2 OUT20.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT21= 85¶ CLB2 OUT21.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT22= 86¶ CLB2 OUT22.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB2_OUT23= 87¶ CLB2 OUT23.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT16= 88¶ CLB3 OUT16.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT17= 89¶ CLB3 OUT17.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT18= 90¶ CLB3 OUT18.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT19= 91¶ CLB3 OUT19.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT20= 92¶ CLB3 OUT20.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT21= 93¶ CLB3 OUT21.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT22= 94¶ CLB3 OUT22.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB3_OUT23= 95¶ CLB3 OUT23.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT16= 96¶ CLB4 OUT16.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT17= 97¶ CLB4 OUT17.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT18= 98¶ CLB4 OUT18.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT19= 99¶ CLB4 OUT19.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT20= 100¶ CLB4 OUT20.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT21= 101¶ CLB4 OUT21.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT22= 102¶ CLB4 OUT22.
-
enumerator
CLB_GLOBAL_IN_MUX_CLB4_OUT23= 103¶ CLB4 OUT23.
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT0= 104¶ ERAD Event 0 (BUSCOMP1)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT1= 105¶ ERAD Event 1 (BUSCOMP2)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT2= 106¶ ERAD Event 2 (BUSCOMP3)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT3= 107¶ ERAD Event 3 (BUSCOMP4)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT4= 108¶ ERAD Event 4 (BUSCOMP5)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT5= 109¶ ERAD Event 5 (BUSCOMP6)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT6= 110¶ ERAD Event 6 (BUSCOMP7)
-
enumerator
CLB_GLOBAL_IN_MUX_ERAD_EVENT7= 111¶ ERAD Event 7 (BUSCOMP8)
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_DATA_PACKET_RCVD= 112¶ FSIRXA Data Packet Received.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_ERROR_PACKET_RCVD= 113¶ FSIRXA Error Packet Received.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_PING_PACKET_RCVD= 114¶ FSIRXA PING Packet Received.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_OUTPUT_FRAME_DONE= 115¶ FSIRXA Output Frame Done.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_PING_TAG_MATCH= 116¶ FSIRXA PING TAG Match.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_DATA_TAG_MATCH= 117¶ FSIRXA DATA TAG Match.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_ERROR_TAG_MATCH= 118¶ FSIRXA ERROR TAG Match.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_RX_TRIG2= 119¶ FSIRXA RX Trig 2.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI1_SPICLK= 120¶ SPI1 SPICLK OUT.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI1_SPIPOCI_CONTROLLER= 121¶ SPI1 SPIPOCI Controller IN.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI1_SPIPTE= 122¶ SPI1 SPIPTE OUT.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI2_SPICLK= 123¶ SPI2 SPICLK OUT.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI2_SPIPOCI_CONTROLLER= 124¶ SPI2 SPIPOCI Controller IN.
-
enumerator
CLB_GLOBAL_IN_MUX_SPI2_SPIPTE= 125¶ SPI2 SPIPTE OUT.
-
enumerator
CLB_GLOBAL_IN_MUX_FSIRXA_RX_TRIG3= 127¶ FSIRXA RX Trig 3.
-
enumerator
Functions
-
void
CLB_enableCLB(uint32_t base)¶ Checks the CLB base address.
This function determines if a CLB base address is valid.
- Parameters
base: is the base address of a CLB tile’s logic config register.
This function enables the CLB via global enable register.
- Return
Returns true if the base address is valid and false otherwise. Set global enable.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disableCLB(uint32_t base)¶ Clear global enable.
This function disables the CLB via global enable register.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_enableNMI(uint32_t base)¶ Enable HLC NMI.
This function enables the CLB HLC NMI.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disableNMI(uint32_t base)¶ Disable HLC NMI.
This function disables the CLB HLC NMI.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_configureClockPrescalar(uint32_t base, uint16_t prescl)¶ Configure Clock Prescalar.
This function enables and configures the CLB Clock Precalar.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_configureStrobeMode(uint32_t base, uint16_t strb)¶ Configures Clock Precalar Strobe Mode.
This function enables and configures the CLB Clock Precalar Strobe Mode.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_writeSWReleaseControl(uint32_t base, CLB_SWReleaseCtrl inID, bool val)¶ Configures the general purpose SW release control value.
This function configures the general purpose SW release control value. The
inID parameter can have one enumeration value from CLB_SWReleaseCtrl.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB SW Release input signal.val: is the value of the SW RLS control.
- Return
None.
-
void
CLB_writeSWGateControl(uint32_t base, CLB_SWGateCtrl inID, bool val)¶ Configures the general purpose SW gate control value.
This function configures the general purpose SW release control value. The
inID parameter can have one enumeration value from CLB_SWGateCtrl.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB SW Release input signal.val: is the value of the SW GATE control.
- Return
None.
-
void
CLB_configCounterTapSelects(uint32_t base, uint32_t tapSel)¶ Configures Counter TAP Selects.
This function configures the counter tap selects.
- Parameters
base: is the base address of a CLB tile’s logic config register.miscCtrl: is the value to represent counter tap selects. Generated by tool as TILEx_CFG_TAP_SELL.
- Return
None.
-
void
CLB_configAOC(uint32_t base, CLB_AOCs aocID, uint32_t aocCfg)¶ Configures AOC (Asynchronous Output Conditioning) functions.
This function configures the input signals and equations of the aoc LUT corresponding to the /e aocID parameter.
- Parameters
base: is the base address of a CLB tile’s logic config register.aocID: is the specified CLB tile AOC signal.aocCfg: is the value for the AOC signal function and input signal selections. Generated by tool as TILEx_OUTPUT_COND_CTR_n where n is the output number.
- Return
None.
-
void
CLB_enableLock(uint32_t base)¶ Enable CLB lock.
This function enables the lock bit of the lock register. The lock can only be set once and can only be cleared by a device reset.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_writeInterface(uint32_t base, uint32_t address, uint32_t value)¶ Write value to address.
This function writes the specified value to CLB internal memory.
- Parameters
base: is the base address of a CLB tile’s logic config register.address: is the address of CLB internal memory.value: is the value to write to specified address.
- Return
None.
-
void
CLB_selectInputFilter(uint32_t base, CLB_Inputs inID, CLB_FilterType filterType)¶ Select input filter type.
This function configures the filter selection for the specified input. The
inID parameter can have one enumeration value from CLB_Inputs. The filterType parameter can have one enumeration value from CLB_FilterType.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.filterType: is the selected type of filter applied to the input.
- Return
None.
-
void
CLB_enableSynchronization(uint32_t base, CLB_Inputs inID)¶ Enables synchronization of an input signal.
This function enables synchronization on the specified input signal. The
inID parameter can have one enumeration value from CLB_Inputs.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.
- Return
None.
-
void
CLB_disableSynchronization(uint32_t base, CLB_Inputs inID)¶ Disables synchronization of an input signal.
This function disables synchronization on the specified input signal. The
inID parameter can have one enumeration value from CLB_Inputs.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.
- Return
None.
-
void
CLB_configGPInputMux(uint32_t base, CLB_Inputs inID, CLB_GPInputMux gpMuxCfg)¶ Configures the general purpose input mux.
This function configures the general purpose input mux. The
gpMuxCfg parameter can select either the use of an external input signal (CLB_GP_IN_MUX_EXTERNAL) or the use of the corresponding CLB_GP_REG bit as an input (CLB_GP_IN_MUX_GP_REG). The inID parameter can have one enumeration value from CLB_Inputs.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.gpMuxCfg: is the mux selection for the general purpose input mux.
- See
CLB_setGPREG() to write to the CLB_GP_REG.
- Return
None.
-
void
CLB_setGPREG(uint32_t base, uint32_t gpRegVal)¶ Sets the CLB_GP_REG register value.
This function writes to the CLB_GP_REG register. When the general purpose input mux is configured to use CLB_GP_REG, each bit in
gpRegVal corresponds to an input signal (bit 0 to Input 0, bit 1 to Input 1, and so on).- Parameters
base: is the base address of a CLB tile’s logic config register.gpRegVal: is the value to be written to CLB_GP_REG.
- See
CLB_configGPInputMux() to select the CLB_GP_REG as the source for an input signal.
- Return
None.
-
uint32_t
CLB_getGPREG(uint32_t base)¶ Gets the CLB_GP_REG register value.
This function writes to the CLB_GP_REG register. When the general purpose input mux is configured to use CLB_GP_REG, each bit in
gpRegVal corresponds to an input signal (bit 0 to Input 0, bit 1 to Input 1, and so on).- Parameters
base: is the base address of a CLB tile’s logic config register.
- See
CLB_configGPInputMux() to select the CLB_GP_REG as the source for an input signal.
- Return
CLB_GP_REG value.
-
void
CLB_configLocalInputMux(uint32_t base, CLB_Inputs inID, CLB_LocalInputMux localMuxCfg)¶ Configures the local input mux.
This function configures the local input mux for the specified input signal.
- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.localMuxCfg: is the mux selection for the local input mux.
The inID parameter can have one enumeration value from CLB_Inputs. The localMuxCfg parameter can have one enumeration value from CLB_LocalInputMux.
- Note
The local input mux options’ peripheral sources depend on which instance of the CLB (base) you are using. For example, for CLB1 the EPWM signal selections come from EPWM1 but for CLB2 they come from EPWM2. See your technical reference manual for details.
- Return
None.
-
void
CLB_configGlobalInputMux(uint32_t base, CLB_Inputs inID, CLB_GlobalInputMux globalMuxCfg)¶ Configures the global input mux.
This function configures the global input mux for the specified input signal. The
inID parameter can have one enumeration value from CLB_Inputs. The globalMuxCfg parameter can have one enumeration value from CLB_GlobalInputMux.- Parameters
base: is the base address of a CLB tile’s logic config register.inID: is the specified CLB tile input signal.globalMuxCfg: is the mux selection for the global input mux.
- Note
The global input mux options’ peripheral sources depend on which instance of the CLB (base) you are using. For example, for CLB1 the EPWM signal selections come from EPWM1 but for CLB2 they come from EPWM2. See your technical reference manual for details.
- Return
None.
-
void
CLB_setOutputMask(uint32_t base, uint32_t outputMask, bool enable)¶ Controls the output enable.
This function is used to enable and disable CLB outputs by writing a mask to CLB_OUT_EN. Each bit corresponds to a CLB output. When a bit is 1, the corresponding output is enabled; when a bit is 0, the output is disabled.
- Parameters
base: is the base address of a CLB tile’s logic config register.outputMask: is a mask of the outputs to be enabled.enable: is a switch to decide if the CLB outputs need to be enabled or not.
The outputMask parameter takes a logical OR of any of the CLB_OUTPUT_0x values that correspond to the CLB OUTPUT ENABLE for the respective outputs. The enable parameter can have one of the values from: false: Disable the respective CLB outputs true: Enable the respective CLB outputs
- Note
Note that the 8 CLB outputs are replicated to create more output paths. See your technical reference manual for more details. If no further modifications are expected, then it is advised to set the block writes bit of the MISC_ACCESS_CTRL Register. This will prevent accidental writes.
- Return
None.
-
uint16_t
CLB_getInterruptTag(uint32_t base)¶ Reads the interrupt tag register.
- Return
Returns the value in the interrupt tag register which is a 6-bit constant set by the HLC.
- Parameters
base: is the base address of a CLB tile’s logic config register.
-
void
CLB_clearInterruptTag(uint32_t base)¶ Clears the interrupt tag register.
This function clears the interrupt tag register, setting it to 0.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_selectLUT4Inputs(uint32_t base, uint32_t lut4In0, uint32_t lut4In1, uint32_t lut4In2, uint32_t lut4In3)¶ Selects LUT4 inputs.
This function configures the LUT4 block’s input signals.
- Parameters
base: is the base address of a CLB tile’s logic config register.lut4In0: is the value for LUT4 input signal 0. Generated by tool as TILEx_CFG_LUT4_IN0.lut4In1: is the value for LUT4 input signal 1. Generated by tool as TILEx_CFG_LUT4_IN1.lut4In2: is the value for LUT4 input signal 2. Generated by tool as TILEx_CFG_LUT4_IN2.lut4In3: is the value for LUT4 input signal 3. Generated by tool as TILEx_CFG_LUT4_IN3.
- Return
None.
-
void
CLB_configLUT4Function(uint32_t base, uint32_t lut4Fn10, uint32_t lut4Fn2)¶ Configures LUT4 functions.
This function configures the LUT4 block’s equations.
- Parameters
base: is the base address of a CLB tile’s logic config register.lut4Fn10: is the equation value for LUT4 blocks 0 and 1. Generated by tool as TILEx_CFG_LUT4_FN10.lut4Fn2: is the equation value for LUT4 block2. Generated by tool as TILEx_CFG_LUT4_FN2.
- Return
None.
-
void
CLB_selectFSMInputs(uint32_t base, uint32_t external0, uint32_t external1, uint32_t extra0, uint32_t extra1)¶ Selects FSM inputs.
This function configures the FSM block’s external inputs and extra external inputs.
- Parameters
base: is the base address of a CLB tile’s logic config register.external0: is the value for FSM external 0 input. Generated by tool as TILEx_CFG_FSM_EXT_IN0.external1: is the value for FSM external 1 input. Generated by tool as TILEx_CFG_FSM_EXT_IN1.extra0: is the value for FSM extra 0 input. Generated by tool as TILEx_CFG_FSM_EXTRA_IN0.extra1: is the value for FSM extra 1 input. Generated by tool as TILEx_CFG_FSM_EXTRA_IN1.
- Return
None.
-
void
CLB_configFSMLUTFunction(uint32_t base, uint32_t fsmLutFn10, uint32_t fsmLutFn2)¶ Configures FSM LUT function.
This function configures the FSM block’s LUT equations.
- Parameters
base: is the base address of a CLB tile’s logic config register.fsmLutFn10: is the value for FSM 0 & FSM 1 LUT function. Generated by tool as TILEx_CFG_FSM_LUT_FN10.fsmLutFn2: is the value for FSM 2 LUT function. Generated by tool as TILEx_CFG_FSM_LUT_FN2.
- Return
None.
-
void
CLB_configFSMNextState(uint32_t base, uint32_t nextState0, uint32_t nextState1, uint32_t nextState2)¶ Configures FSM next state.
This function configures the FSM’s next state equation.
- Parameters
base: is the base address of a CLB tile’s logic config register.nextState0: is the value for FSM 0’s next state. Generated by tool as TILEx_CFG_FSM_NEXT_STATE_0.nextState1: is the value for FSM 1’s next state. Generated by tool as TILEx_CFG_FSM_NEXT_STATE_1.nextState2: is the value for FSM 2’s next state. Generated by tool as TILEx_CFG_FSM_NEXT_STATE_2.
- Return
None.
-
void
CLB_selectCounterInputs(uint32_t base, uint32_t reset, uint32_t event, uint32_t mode0, uint32_t mode1)¶ Selects Counter inputs.
This function selects the input signals to the counter block.
- Parameters
base: is the base address of a CLB tile’s logic config register.reset: is the value for counter’s reset inputs. Generated by tool as TILEx_CFG_COUNTER_RESET.event: is the value for counter’s event inputs. Generated by tool as TILEx_CFG_COUNTER_EVENT.mode0: is the value for counter’s mode 0 inputs. Generated by tool as TILEx_CFG_COUNTER_MODE_0.mode1: is the value for counter’s mode 1 inputs. Generated by tool as TILEx_CFG_COUNTER_MODE_1.
- Return
None.
-
void
CLB_configMiscCtrlModes(uint32_t base, uint32_t miscCtrl)¶ Configures Counter and FSM modes.
This function configures the counter mode, particularly add/shift, load modes. The function also configures whether the FSM should use state inputs or an extra external input.
- Parameters
base: is the base address of a CLB tile’s logic config register.miscCtrl: is the value to represent counter and FSM modes. Generated by tool as TILEx_CFG_MISC_CONTROL.
- Return
None.
-
void
CLB_configOutputLUT(uint32_t base, CLB_Outputs outID, uint32_t outputCfg)¶ Configures Output LUT functions.
This function configures the input signals and equations of the output LUT corresponding to the /e outID parameter.
- Parameters
base: is the base address of a CLB tile’s logic config register.outID: is the specified CLB tile output signal.outputCfg: is the value for the output LUT signal function and input signal selections. Generated by tool as TILEx_CFG_OUTLUT_n where n is the output number.
- Return
None.
-
void
CLB_configHLCEventSelect(uint32_t base, uint32_t eventSel)¶ Configures HLC event selection.
This function configures the event selection for the High Level Controller.
- Parameters
base: is the base address of a CLB tile’s logic config register.eventSel: is the value for HLC event selection. Generated by tool as TILEx_HLC_EVENT_SEL.
- Return
None.
-
void
CLB_programHLCInstruction(uint32_t base, uint32_t instructionNum, uint32_t instruction)¶ Program HLC instruction.
This function configures the CLB internal memory corresponding to the specified HLC instruction number with the given instruction.
- Parameters
base: is the base address of a CLB tile’s logic config register.instructionNum: is the index into the HLC instruction memory. For example, a value of 0 corresponds to instruction 0 of event 0, a value of 1 corresponds to instruction 1 of event 0, and so on up to a value of 31 which corresponds to instruction 7 of event 3.instruction: is the instruction to be programmed. Generated by tool as TILEx_HLCINSTR_n where n is the instruction number.
- Return
None.
-
void
CLB_setHLCRegisters(uint32_t base, uint32_t r0Init, uint32_t r1Init, uint32_t r2Init, uint32_t r3Init)¶ Set HLC registers.
This function configures the CLB internal memory corresponding to the HLC registers R0-R3 with the specified values.
- Parameters
base: is the base address of a CLB tile’s logic config register.r0Init: is the value to write to HLC register R0. Generated by tool as TILEx_HLC_R0_INIT.r1Init: is the value to write to HLC register R1. Generated by tool as TILEx_HLC_R1_INIT.r2Init: is the value to write to HLC register R2. Generated by tool as TILEx_HLC_R2_INIT.r3Init: is the value to write to HLC register R3. Generated by tool as TILEx_HLC_R3_INIT.
- Return
None.
-
uint32_t
CLB_getRegister(uint32_t base, CLB_Register registerID)¶ Get HLC or counter register values.
- Return
Returns the value in the specified HLC register or counter.
- Parameters
base: is the base address of a CLB tile’s logic config register.registerID: is the internal register from which to read. Can be either an HLC register (CLB_REG_HLC_Rn) or a counter value (CLB_REG_CTR_Cn).
-
uint32_t
CLB_getOutputStatus(uint32_t base)¶ Get output status.
- Return
Returns the output status of various components within the CLB tile such as a counter match or LUT output. Use the CLB_DBG_OUT_* masks from
hw_clb.hto decode the bits.- Parameters
base: is the base address of a CLB tile’s logic config register.
-
void
CLB_enablePipelineMode(uint32_t base)¶ Enable CLB Pipeline Mode.
This function enables the CLB Pipeline Mode
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disablePipelineMode(uint32_t base)¶ Disable CLB Pipeline Mode.
This function disables the CLB Pipeline Mode.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disableOutputMaskUpdates(uint32_t base)¶ Disable CLB Output Mask Updates.
This function disables the CLB Output Mask updates
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_enableOutputMaskUpdates(uint32_t base)¶ Enable CLB Output Mask Updates.
This function enables the CLB Output Mask updates
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_enableInputPipelineMode(uint32_t base, CLB_Inputs inID)¶ Enable Input Pipeline Mode.
This function enables the CLB Input Pipeline mode
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disableInputPipelineMode(uint32_t base, CLB_Inputs inID)¶ Disable Input Pipeline Mode.
This function disables the CLB Input Pipeline mode
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_disableSPIBufferAccess(uint32_t base)¶ Disable SPI RX Buffer Access.
This function disables the CLB SPI RX Buffer access
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_enableSPIBufferAccess(uint32_t base)¶ Enable SPI RX Buffer Access.
This function enables the CLB SPI RX Buffer access
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_configSPIBufferLoadSignal(uint32_t base, uint16_t eventSel)¶ Configures SPI RX Buffer Load Signal event selection.
This function configures the event selection for the SPI RX Buffer.
- Parameters
base: is the base address of a CLB tile’s logic config register.eventSel: is the value for HLC event selection. Generated by tool as TILEx_SPI_BUF_EVENT_SEL.
- Return
None.
-
void
CLB_configSPIBufferShift(uint32_t base, uint16_t shiftVal)¶ Configures SPI Export HLC R0 Shift value.
This function configures the SPI Export HLC R0 Shift value.
- Parameters
base: is the base address of a CLB tile’s logic config register.shiftVal: is the value for SPI export HLC R0 bit range selection.
- Return
None.
-
void
CLB_configCounterLoadMatch(uint32_t base, CLB_Counters counterID, uint32_t load, uint32_t match1, uint32_t match2)¶ Configures Counter load and match.
This function configures the CLB internal memory corresponding to the counter block’s load and match values.
- Parameters
base: is the base address of a CLB tile’s logic config register.counterID: is the specified counter unit.load: is the value for counter’s load mode. Generated by tool as TILEx_COUNTER_n_LOAD_VAL where n is the counter number.match1: is the value for counter’s match 1. Generated by tool as TILEx_COUNTER_n_MATCH1_VAL where n is the counter number.match2: is the value for counter’s match 2. Generated by tool as TILEx_COUNTER_n_MATCH2_VAL where n is the counter number.
- Return
None.
-
void
CLB_clearFIFOs(uint32_t base)¶ Clear FIFO registers.
This function clears the PUSH/PULL FIFOs as well as its pointers.
- Parameters
base: is the base address of a CLB tile’s logic config register.
- Return
None.
-
void
CLB_writeFIFOs(uint32_t base, const uint32_t pullData[])¶ Configure the FIFO registers.
This function writes to the PULL FIFO. This also clears the FIFOs and its pointer using the
CLB_clearFIFOs() API prior to writing to the FIFO.- Parameters
base: is the base address of a CLB tile’s logic config register.pullData[]: is a pointer to an array of bytes which needs to be written into the FIFO. The 0th FIFO data is in the 0th index.
- Return
None.
-
void
CLB_readFIFOs(uint32_t base, uint32_t pushData[])¶ Read FIFO registers.
This function reads from the PUSH FIFO. The 0th FIFO data would be in the 0th index.
- Parameters
base: is the base address of a CLB tile’s logic config register.pushData[]: is a pointer to an array of bytes which needs to be read from the FIFO.
- Return
None.
-
The code for this module is contained in driverlib/clb.c, with driverlib/clb.h containing the API declarations for use by applications.