ASysCtl Module¶
The ASysCtl or Analog System Control driver provides functions to enable, disable and lock the temperature sensor on the device. It will also provide additional functionality if available for that device.
-
group
asysctl_api Defines
-
ASYSCTL_VREFHI0x1U¶ VREFHI.
-
ASYSCTL_CMPHNMUX_SELECT_10x1U¶ CMPHNMUX select 1.
-
ASYSCTL_CMPHNMUX_SELECT_20x2U¶ CMPHNMUX select 2.
-
ASYSCTL_CMPHNMUX_SELECT_30x4U¶ CMPHNMUX select 3.
-
ASYSCTL_CMPHNMUX_SELECT_40x8U¶ CMPHNMUX select 4.
-
ASYSCTL_CMPLNMUX_SELECT_10x1U¶ CMPLNMUX select 1.
-
ASYSCTL_CMPLNMUX_SELECT_20x2U¶ CMPLNMUX select 2.
-
ASYSCTL_CMPLNMUX_SELECT_30x4U¶ CMPLNMUX select 3.
-
ASYSCTL_CMPLNMUX_SELECT_40x8U¶ CMPLNMUX select 4.
Enums
-
enum
ASysCtl_CMPHPMuxSelect¶ ASysCtl_CMPHPMuxSelect used for function ASysCtl_selectCMPHPMux().
Values:
-
enumerator
ASYSCTL_CMPHPMUX_SELECT_1= 0U¶ CMPHPMUX select 1.
-
enumerator
ASYSCTL_CMPHPMUX_SELECT_2= 3U¶ CMPHPMUX select 2.
-
enumerator
ASYSCTL_CMPHPMUX_SELECT_3= 6U¶ CMPHPMUX select 3.
-
enumerator
ASYSCTL_CMPHPMUX_SELECT_4= 9U¶ CMPHPMUX select 4.
-
enumerator
-
enum
ASysCtl_CMPLPMuxSelect¶ ASysCtl_CMPLPMuxSelect used for function ASysCtl_selectCMPLPMux().
Values:
-
enumerator
ASYSCTL_CMPLPMUX_SELECT_1= 0U¶ CMPLPMUX select 1.
-
enumerator
ASYSCTL_CMPLPMUX_SELECT_2= 3U¶ CMPLPMUX select 2.
-
enumerator
ASYSCTL_CMPLPMUX_SELECT_3= 6U¶ CMPLPMUX select 3.
-
enumerator
ASYSCTL_CMPLPMUX_SELECT_4= 9U¶ CMPLPMUX select 4.
-
enumerator
Functions
-
void
ASysCtl_enableTemperatureSensor(void)¶ Enable temperature sensor.
This function enables the temperature sensor output to the ADC.
- Return
None.
-
void
ASysCtl_disableTemperatureSensor(void)¶ Disable temperature sensor.
This function disables the temperature sensor output to the ADC.
- Return
None.
-
void
ASysCtl_setAnalogReferenceInternal(uint16_t reference)¶ Set the analog voltage reference selection to internal.
The parameter
reference can be a combination of the following values:- Parameters
reference: is the analog reference.
ASYSCTL_VREFHI
- Return
None.
-
void
ASysCtl_setAnalogReferenceExternal(uint16_t reference)¶ Set the analog voltage reference selection to external.
The parameter
reference can be a combination of the following values:- Parameters
reference: is the analog reference.
ASYSCTL_VREFHI
- Return
None.
-
void
ASysCtl_setAnalogReference2P5(uint16_t reference)¶ Set the internal analog voltage reference selection to 2.5V.
The parameter
reference can be a combination of the following values:- Parameters
reference: is the analog reference.
ASYSCTL_VREFHI
- Return
None.
-
void
ASysCtl_setAnalogReference1P65(uint16_t reference)¶ Set the internal analog voltage reference selection to 1.65V.
The parameter
reference can be a combination of the following values:- Parameters
reference: is the analog reference.
ASYSCTL_VREFHI
- Return
None.
-
void
ASysCtl_selectCMPHNMux(uint16_t select)¶ Select the value for CMPHNMXSEL.
The parameter
select can be a bitwise OR of the below values:- Parameters
select: is a combination of CMPHNMXSEL values.
ASYSCTL_CMPHNMUX_SELECT_1
ASYSCTL_CMPHNMUX_SELECT_2
ASYSCTL_CMPHNMUX_SELECT_3
ASYSCTL_CMPHNMUX_SELECT_4
- Return
None.
-
void
ASysCtl_selectCMPHNMuxValue(uint16_t select, uint16_t value)¶ Select the value for individual CMPxHNMXSEL.
The parameter
select can be one of the below values:- Parameters
select: is the CMPxHNMXSEL to be set.value: is 0 or 1.
ASYSCTL_CMPHNMUX_SELECT_1
ASYSCTL_CMPHNMUX_SELECT_2
ASYSCTL_CMPHNMUX_SELECT_3
ASYSCTL_CMPHNMUX_SELECT_4
- Return
None.
-
void
ASysCtl_selectCMPLNMux(uint16_t select)¶ Select the value for individual CMPxLNMXSEL.
The parameter
select can be the bitwise OR of the below values:- Parameters
select: is a combination of CMPLNMXSEL values.
ASYSCTL_CMPLNMUX_SELECT_1
ASYSCTL_CMPLNMUX_SELECT_2
ASYSCTL_CMPLNMUX_SELECT_3
ASYSCTL_CMPLNMUX_SELECT_4
- Return
None.
-
void
ASysCtl_selectCMPLNMuxValue(uint16_t select, uint16_t value)¶ Select the value for CMPLNMXSEL.
The parameter
select can be one of the below values:- Parameters
select: is the CMPxHNMXSEL to be set.value: is 0 or 1.
ASYSCTL_CMPLNMUX_SELECT_1
ASYSCTL_CMPLNMUX_SELECT_2
ASYSCTL_CMPLNMUX_SELECT_3
ASYSCTL_CMPLNMUX_SELECT_4
- Return
None.
-
void
ASysCtl_selectCMPHPMux(ASysCtl_CMPHPMuxSelect select, uint32_t value)¶ Select the value for CMPHPMXSEL.
This function is used to write a value to one mux select at a time. The parameter
select can be one of the following values:- Parameters
select: is of type ASysCtl_CMPHPMuxSelect.value: is 0, 1, 2, 3, 4 or 5.
ASYSCTL_CMPHPMUX_SELECT_1
ASYSCTL_CMPHPMUX_SELECT_2
ASYSCTL_CMPHPMUX_SELECT_3
ASYSCTL_CMPHPMUX_SELECT_4
- Return
None.
-
void
ASysCtl_selectCMPLPMux(ASysCtl_CMPLPMuxSelect select, uint32_t value)¶ Select the value for CMPLPMXSEL.
This function is used to write a value to one mux select at a time. The parameter
select can be one of the following values:- Parameters
select: is of type ASysCtl_CMPLPMuxSelect.value: is 0, 1, 2, 3, 4 or 5.
ASYSCTL_CMPLPMUX_SELECT_1
ASYSCTL_CMPLPMUX_SELECT_2
ASYSCTL_CMPLPMUX_SELECT_3
ASYSCTL_CMPLPMUX_SELECT_4
- Return
None.
-
void
ASysCtl_lockTemperatureSensor(void)¶ Locks the temperature sensor control register.
- Return
None.
-
void
ASysCtl_lockANAREF(void)¶ Locks the analog reference control register.
- Return
None.
-
void
ASysCtl_lockVMON(void)¶ Locks the voltage monitor control register.
- Return
None.
-
void
ASysCtl_lockCMPHPMux(void)¶ Locks the CMPHPMXSEL control register.
- Return
None.
-
void
ASysCtl_lockCMPLPMux(void)¶ Locks the CMPLPMXSEL control register.
- Return
None.
-
void
ASysCtl_lockCMPHNMux(void)¶ Locks the CMPHNMXSEL control register.
- Return
None.
-
void
ASysCtl_lockCMPLNMux(void)¶ Locks the CMPLNMXSEL control register.
- Return
None.
-
void
ASysCtl_lockVREG(void)¶ Locks the VREG control register.
- Return
None.
-
void
ASysCtl_enableADCDACLoopback(uint32_t config)¶ Enable loopback from DAC to ADCs.
- Return
None
- Parameters
config: can be bitwise OR of the following values:ASYSCTL_ADCDACLOOPBACK_ENLB2ADCA
ASYSCTL_ADCDACLOOPBACK_ENLB2ADCB
ASYSCTL_ADCDACLOOPBACK_ENLB2ADCC
-
void
ASysCtl_disableADCDACLoopback(uint32_t config)¶ Disable loopback from DAC to ADCs.
- Return
None
- Parameters
config: can be bitwise OR of the following values:ASYSCTL_ADCDACLOOPBACK_ENLB2ADCA
ASYSCTL_ADCDACLOOPBACK_ENLB2ADCB
ASYSCTL_ADCDACLOOPBACK_ENLB2ADCC
-
The code for this module is contained in driverlib/asysctl.c, with driverlib/asysctl.h containing the API declarations for use by applications.