ERAD Module¶
C2000 MCU’s have an IP called Embedded Real Time Analysis And Diagnostics (ERAD) that provides unique hardware capabilities for real time analysis, monitoring and diagnostics of the systems. The ERAD module is accessible both by the debugger and the application software, which significantly increases the debug capabilities of many real-time systems, especially in situations where the debugger is not connected The ERAD driver includes high level APIs for various use cases like profiling functions, detecting stack overflow, counting memory accesses etc.
-
group
erad_api Defines
-
ERAD_HWBP_CNTL_STOP_S0x05U¶
-
ERAD_HWBP_CNTL_RTOSINT_S0x06U¶
-
ERAD_CTM_CNTL_EVENT_MODE_S0x03U¶
-
ERAD_CTM_CNTL_RST_ON_MATCH_S0x04U¶
-
ERAD_CTM_CNTL_STOP_S0x06U¶
-
ERAD_CTM_CNTL_RTOSINT_S0x07U¶
-
ERAD_getBusCompInstance(base) (1UL << ((base >> 3U) & 0x7U))¶
-
ERAD_getCounterInstance(base) ((1UL << ((base >> 4U) & 0x3U)) << 8U)¶
-
ERAD_getCRCInstance(base) (1U << (((base >> 4U) & 0xFU) - 1U))¶
-
ERAD_BUSCOMP_BASE_TO_EVENT(base) ((base >> 3U) & 0x07U)¶
-
ERAD_INST_BUSCOMP10x00000001UL¶ Instance for bus comparator 1.
Values that can be passed to ERAD_enableModules() or ERAD_disableModules() as instances parameter.
-
ERAD_INST_BUSCOMP20x00000002UL¶ Instance for bus comparator 2.
-
ERAD_INST_BUSCOMP30x00000004UL¶ Instance for bus comparator 3.
-
ERAD_INST_BUSCOMP40x00000008UL¶ Instance for bus comparator 4.
-
ERAD_INST_BUSCOMP50x00000010UL¶ Instance for bus comparator 5.
-
ERAD_INST_BUSCOMP60x00000020UL¶ Instance for bus comparator 6.
-
ERAD_INST_BUSCOMP70x00000040UL¶ Instance for bus comparator 7.
-
ERAD_INST_BUSCOMP80x00000080UL¶ Instance for bus comparator 8.
-
ERAD_INST_COUNTER10x00000100UL¶ Instance for counter 1.
-
ERAD_INST_COUNTER20x00000200UL¶ Instance for counter 2.
-
ERAD_INST_COUNTER30x00000400UL¶ Instance for counter 3.
-
ERAD_INST_COUNTER40x00000800UL¶ Instance for counter 4.
-
ERAD_INST_CRC10x00000001UL¶ Instance for CRC unit 1.
-
ERAD_INST_CRC20x00000002UL¶ Instance for CRC unit 2.
-
ERAD_INST_CRC30x00000004UL¶ Instance for CRC unit 3.
-
ERAD_INST_CRC40x00000008UL¶ Instance for CRC unit 4.
-
ERAD_INST_CRC50x00000010UL¶ Instance for CRC unit 5.
-
ERAD_INST_CRC60x00000020UL¶ Instance for CRC unit 6.
-
ERAD_INST_CRC70x00000040UL¶ Instance for CRC unit 7.
-
ERAD_INST_CRC80x00000080UL¶ Instance for CRC unit 8.
-
ERAD_INPUT_INVERT_DISABLE0x00U¶ Do not invert the input.
Values that can be passed to ERAD_setCounterInputConditioning() as options parameter.
-
ERAD_INPUT_INVERT_ENABLE0x01U¶ Invert the input.
-
ERAD_INPUT_SYNC_DISABLE0x00U¶ Disable 2-stage synchronizer.
-
ERAD_INPUT_SYNC_ENABLE0x02U¶ Enable 2-stage synchronizer.
Enums
-
enum
ERAD_Owner¶ Values that can be passed to ERAD_initModule() as owner parameter to set owner of ERAD.
Values:
-
enumerator
ERAD_OWNER_NOOWNER= 0¶ No owner.
-
enumerator
ERAD_OWNER_APPLICATION= 1¶ Application owned.
-
enumerator
ERAD_OWNER_DEBUGGER= 2¶ Debugger owned.
-
enumerator
-
enum
ERAD_Status¶ Values that can are returned by ERAD_getBusCompStatus() and ERAD_getCounterStatus() to indicate the state of the respective module.
Values:
-
enumerator
ERAD_STATE_IDLE= 0¶ Module is idle.
-
enumerator
ERAD_STATE_ENABLED= 2¶ Module is enabled.
-
enumerator
ERAD_STATE_COMPLETED= 3¶ Module was enabled and an event occurred.
-
enumerator
-
enum
ERAD_BusComp_Bus_Select¶ Values that can be passed to ERAD_configBusComp() and ERAD_profile() as config_params.bus_sel parameter to choose which CPU bus to monitor.
Values:
-
enumerator
ERAD_BUSCOMP_BUS_PAB= 0¶ Use the Program Address Bus.
-
enumerator
ERAD_BUSCOMP_BUS_VPC= 1¶ Use the Virtual Program Counter.
-
enumerator
ERAD_BUSCOMP_BUS_DWAB= 2¶ Use the Data Write Address Bus.
-
enumerator
ERAD_BUSCOMP_BUS_DRAB= 3¶ Use the Data Read Address Bus.
-
enumerator
ERAD_BUSCOMP_BUS_DWDB= 4¶ Use the Data Write Data Bus.
-
enumerator
ERAD_BUSCOMP_BUS_DRDB= 5¶ Use the Data Read Data Bus.
-
enumerator
ERAD_BUSCOMP_BUS_VPC_I_ALIGNED= 6¶ Use VPC Instruction aligned match.
-
enumerator
ERAD_BUSCOMP_BUS_VPC_R1_ALIGNED= 7¶ Use VPC R1 aligned match.
-
enumerator
ERAD_BUSCOMP_BUS_VPC_R2_ALIGNED= 8¶ Use VPC R2 aligned match.
-
enumerator
ERAD_BUSCOMP_BUS_VPC_W_ALIGNED= 9¶ Use VPC Word aligned match.
-
enumerator
-
enum
ERAD_BusComp_Comp_Mode¶ Values that can be passed to ERAD_configBusComp() and ERAD_profile() as config_params.comp_mode to indicate what kind of comparison to use for the bus comparators.
Values:
-
enumerator
ERAD_BUSCOMP_COMPMODE_GT= 4¶ Check for greater than.
-
enumerator
ERAD_BUSCOMP_COMPMODE_GE= 5¶ Check for greater than equal to.
-
enumerator
ERAD_BUSCOMP_COMPMODE_LT= 6¶ Check for lesser than.
-
enumerator
ERAD_BUSCOMP_COMPMODE_LE= 7¶ Check for lesser than equal to.
-
enumerator
ERAD_BUSCOMP_COMPMODE_EQ= 0¶ Check for only equality.
-
enumerator
-
enum
ERAD_Counter_Event_Mode¶ Values that can be passed to ERAD_configCounterInStartStopMode() and ERAD_configCounterInCountingMode() as config_params.event_mode to indicate whether to count rising edges or the number of CPU clock cycles an is active.
Values:
-
enumerator
ERAD_COUNTER_MODE_ACTIVE= 0¶ Count number of CPU Cycles event is active for
-
enumerator
ERAD_COUNTER_MODE_RISING_EDGE= 1¶ Count number of Rising Edges of event
-
enumerator
-
enum
ERAD_Counter_Input_Event¶ Values that can be passed to ERAD_configCounterInStartStopMode() and ERAD_configCounterInCountingMode() as config_params.event to indicate what event to consider as input. Also may be passed to ERAD_configCounterInStartStopMode() as start_event and stop_event to indicate start and stop events for the counter.
Values:
-
enumerator
ERAD_EVENT_HWBP1= 0¶
-
enumerator
ERAD_EVENT_HWBP2= 1¶
-
enumerator
ERAD_EVENT_HWBP3= 2¶
-
enumerator
ERAD_EVENT_HWBP4= 3¶
-
enumerator
ERAD_EVENT_HWBP5= 4¶
-
enumerator
ERAD_EVENT_HWBP6= 5¶
-
enumerator
ERAD_EVENT_HWBP7= 6¶
-
enumerator
ERAD_EVENT_HWBP8= 7¶
-
enumerator
ERAD_EVENT_COUNTER1_EVENT= 8¶
-
enumerator
ERAD_EVENT_COUNTER2_EVENT= 9¶
-
enumerator
ERAD_EVENT_COUNTER3_EVENT= 10¶
-
enumerator
ERAD_EVENT_COUNTER4_EVENT= 11¶
-
enumerator
ERAD_EVENT_ERAD_OR_MASK0= 12¶
-
enumerator
ERAD_EVENT_ERAD_OR_MASK1= 13¶
-
enumerator
ERAD_EVENT_ERAD_OR_MASK2= 14¶
-
enumerator
ERAD_EVENT_ERAD_OR_MASK3= 15¶
-
enumerator
ERAD_EVENT_ERAD_AND_MASK0= 16¶
-
enumerator
ERAD_EVENT_ERAD_AND_MASK1= 17¶
-
enumerator
ERAD_EVENT_ERAD_AND_MASK2= 18¶
-
enumerator
ERAD_EVENT_ERAD_AND_MASK3= 19¶
-
enumerator
ERAD_EVENT_PIE_INT1= 20¶
-
enumerator
ERAD_EVENT_PIE_INT2= 21¶
-
enumerator
ERAD_EVENT_PIE_INT3= 22¶
-
enumerator
ERAD_EVENT_PIE_INT4= 23¶
-
enumerator
ERAD_EVENT_PIE_INT5= 24¶
-
enumerator
ERAD_EVENT_PIE_INT6= 25¶
-
enumerator
ERAD_EVENT_PIE_INT7= 26¶
-
enumerator
ERAD_EVENT_PIE_INT8= 27¶
-
enumerator
ERAD_EVENT_PIE_INT9= 28¶
-
enumerator
ERAD_EVENT_PIE_INT10= 29¶
-
enumerator
ERAD_EVENT_PIE_INT11= 30¶
-
enumerator
ERAD_EVENT_PIE_INT12= 31¶
-
enumerator
ERAD_EVENT_TIMER0_TINT0= 32¶
-
enumerator
ERAD_EVENT_TIMER1_TINT1= 33¶
-
enumerator
ERAD_EVENT_TIMER2_TINT2= 34¶
-
enumerator
ERAD_EVENT_DMACH1INT= 35¶
-
enumerator
ERAD_EVENT_DMACH2INT= 36¶
-
enumerator
ERAD_EVENT_DMACH3INT= 37¶
-
enumerator
ERAD_EVENT_DMACH4INT= 38¶
-
enumerator
ERAD_EVENT_DMACH5INT= 39¶
-
enumerator
ERAD_EVENT_DMACH6INT= 40¶
-
enumerator
ERAD_EVENT_FSI_DATA_PKT_RCVD= 41¶
-
enumerator
ERAD_EVENT_FSI_ERROR_PKT_RCVD= 42¶
-
enumerator
ERAD_EVENT_FSI_PING_PKT_RCVD= 43¶
-
enumerator
ERAD_EVENT_FSI_PING_FRAME_TAG_MATCH= 44¶
-
enumerator
ERAD_EVENT_FSI_DATA_FRAME_TAG_MATCH= 45¶
-
enumerator
ERAD_EVENT_FSI_ERROR_FRAME_TAG_MATCH= 46¶
-
enumerator
ERAD_EVENT_FSI_FRAME_DONE= 47¶
-
enumerator
ERAD_EVENT_ADCAEVTINT= 48¶
-
enumerator
ERAD_EVENT_ADCCEVTINT= 49¶
-
enumerator
ERAD_EVENT_MCANA_EVT0= 50¶
-
enumerator
ERAD_EVENT_MCANA_EVT1= 51¶
-
enumerator
ERAD_EVENT_MCANA_EVT2= 52¶
-
enumerator
ERAD_EVENT_ADCSOCA= 53¶
-
enumerator
ERAD_EVENT_ADCSOCB= 54¶
-
enumerator
ERAD_EVENT_CLATASKRUN1= 55¶
-
enumerator
ERAD_EVENT_CLATASKRUN2= 56¶
-
enumerator
ERAD_EVENT_CLATASKRUN3= 57¶
-
enumerator
ERAD_EVENT_CLATASKRUN4= 58¶
-
enumerator
ERAD_EVENT_CLATASKRUN5= 59¶
-
enumerator
ERAD_EVENT_CLATASKRUN6= 60¶
-
enumerator
ERAD_EVENT_CLATASKRUN7= 61¶
-
enumerator
ERAD_EVENT_CLATASKRUN8= 62¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT1= 63¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT2= 64¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT3= 65¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT4= 66¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT5= 67¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT6= 68¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT7= 69¶
-
enumerator
ERAD_EVENT_EPWMXBAR_OUT8= 70¶
-
enumerator
ERAD_EVENT_INPUTXBAR0= 71¶
-
enumerator
ERAD_EVENT_INPUTXBAR1= 72¶
-
enumerator
ERAD_EVENT_INPUTXBAR2= 73¶
-
enumerator
ERAD_EVENT_INPUTXBAR3= 74¶
-
enumerator
ERAD_EVENT_INPUTXBAR4= 75¶
-
enumerator
ERAD_EVENT_INPUTXBAR5= 76¶
-
enumerator
ERAD_EVENT_INPUTXBAR6= 77¶
-
enumerator
ERAD_EVENT_INPUTXBAR7= 78¶
-
enumerator
ERAD_EVENT_INPUTXBAR8= 79¶
-
enumerator
ERAD_EVENT_INPUTXBAR9= 80¶
-
enumerator
ERAD_EVENT_INPUTXBAR10= 81¶
-
enumerator
ERAD_EVENT_INPUTXBAR11= 82¶
-
enumerator
ERAD_EVENT_INPUTXBAR12= 83¶
-
enumerator
ERAD_EVENT_INPUTXBAR13= 84¶
-
enumerator
ERAD_EVENT_INPUTXBAR14= 85¶
-
enumerator
ERAD_EVENT_INPUTXBAR15= 86¶
-
enumerator
ERAD_EVENT_CPUx_CPUSTAT= 87¶
-
enumerator
ERAD_EVENT_CPUx_DBGACK= 88¶
-
enumerator
ERAD_EVENT_CPUx_NMI= 89¶
-
enumerator
ERAD_EVENT_CMPSS1_CTRIPH_OR_CTRIPL= 90¶
-
enumerator
ERAD_EVENT_CMPSS2_CTRIPH_OR_CTRIPL= 91¶
-
enumerator
ERAD_EVENT_CMPSS3_CTRIPH_OR_CTRIPL= 92¶
-
enumerator
ERAD_EVENT_CMPSS4_CTRIPH_OR_CTRIPL= 93¶
-
enumerator
ERAD_EVENT_SD1FLT1_COMPH_OR_COMPL= 98¶
-
enumerator
ERAD_EVENT_SD1FLT2_COMPH_OR_COMPL= 99¶
-
enumerator
ERAD_EVENT_SD1FLT3_COMPH_OR_COMPL= 100¶
-
enumerator
ERAD_EVENT_SD1FLT4_COMPH_OR_COMPL= 101¶
-
enumerator
ERAD_EVENT_SD2FLT1_COMPH_OR_COMPL= 102¶
-
enumerator
ERAD_EVENT_SD2FLT2_COMPH_OR_COMPL= 103¶
-
enumerator
ERAD_EVENT_SD2FLT3_COMPH_OR_COMPL= 104¶
-
enumerator
ERAD_EVENT_SD2FLT4_COMPH_OR_COMPL= 105¶
-
enumerator
ERAD_EVENT_ADCAINT1= 106¶
-
enumerator
ERAD_EVENT_ADCAINT2= 107¶
-
enumerator
ERAD_EVENT_ADCAINT3= 108¶
-
enumerator
ERAD_EVENT_ADCAINT4= 109¶
-
enumerator
ERAD_EVENT_ADCBINT1= 110¶
-
enumerator
ERAD_EVENT_ADCBINT2= 111¶
-
enumerator
ERAD_EVENT_ADCBINT3= 112¶
-
enumerator
ERAD_EVENT_ADCBINT4= 113¶
-
enumerator
ERAD_EVENT_ADCCINT1= 114¶
-
enumerator
ERAD_EVENT_ADCCINT2= 115¶
-
enumerator
ERAD_EVENT_ADCCINT3= 116¶
-
enumerator
ERAD_EVENT_ADCCINT4= 117¶
-
enumerator
ERAD_EVENT_HIC_nOE= 122¶
-
enumerator
ERAD_EVENT_HIC_nWE= 123¶
-
enumerator
ERAD_EVENT_HIC_nRDY= 124¶
-
enumerator
ERAD_EVENT_ADCBEVTINT= 125¶
-
enumerator
ERAD_EVENT_NO_EVENT= 256¶
-
enumerator
-
enum
ERAD_Mask¶ Values:
-
enumerator
ERAD_AND_MASK1= 0¶
-
enumerator
ERAD_AND_MASK2= 1¶
-
enumerator
ERAD_AND_MASK3= 2¶
-
enumerator
ERAD_AND_MASK4= 3¶
-
enumerator
ERAD_OR_MASK1= 4¶
-
enumerator
ERAD_OR_MASK2= 5¶
-
enumerator
ERAD_OR_MASK3= 6¶
-
enumerator
ERAD_OR_MASK4= 7¶
-
enumerator
-
enum
ERAD_CRC_Qualifiers¶ Values that can be passed to ERAD_setCRCQualifier() as the qualifier paramter to specify which events to set as the qualifier for the CRC unit.
Values:
-
enumerator
ERAD_CRC_QUAL_NONE= 0¶ Use every valid event as qualifier for CRC computation
-
enumerator
ERAD_CRC_QUAL_HWBP1= 1¶ CRC Compute Qualified by HWBP_EVENT1.
-
enumerator
ERAD_CRC_QUAL_HWBP2= 2¶ CRC Compute Qualified by HWBP_EVENT2.
-
enumerator
ERAD_CRC_QUAL_HWBP3= 3¶ CRC Compute Qualified by HWBP_EVENT3.
-
enumerator
ERAD_CRC_QUAL_HWBP4= 4¶ CRC Compute Qualified by HWBP_EVENT4.
-
enumerator
ERAD_CRC_QUAL_HWBP5= 5¶ CRC Compute Qualified by HWBP_EVENT5.
-
enumerator
ERAD_CRC_QUAL_HWBP6= 6¶ CRC Compute Qualified by HWBP_EVENT6.
-
enumerator
ERAD_CRC_QUAL_HWBP7= 7¶ CRC Compute Qualified by HWBP_EVENT7.
-
enumerator
ERAD_CRC_QUAL_HWBP8= 8¶ CRC Compute Qualified by HWBP_EVENT8.
-
enumerator
ERAD_CRC_QUAL_HWBP_OR1= 9¶ CRC Compute Qualified by HWBP_EVENT_OR1.
-
enumerator
ERAD_CRC_QUAL_HWBP_OR2= 10¶ CRC Compute Qualified by HWBP_EVENT_OR1.
-
enumerator
ERAD_CRC_QUAL_HWBP_OR3= 11¶ CRC Compute Qualified by HWBP_EVENT_OR1.
-
enumerator
ERAD_CRC_QUAL_HWBP_OR4= 12¶ CRC Compute Qualified by HWBP_EVENT_OR1.
-
enumerator
ERAD_CRC_QUAL_HWBP_AND1= 13¶ CRC Compute Qualified by HWBP_EVENT_AND2.
-
enumerator
ERAD_CRC_QUAL_HWBP_AND2= 14¶ CRC Compute Qualified by HWBP_EVENT_AND2.
-
enumerator
ERAD_CRC_QUAL_HWBP_AND3= 15¶ CRC Compute Qualified by HWBP_EVENT_AND2.
-
enumerator
ERAD_CRC_QUAL_HWBP_AND4= 16¶ CRC Compute Qualified by HWBP_EVENT_AND2.
-
enumerator
-
enum
ERAD_Counter_Input_Type¶ Values that can be passed to ERAD_setCounterInputConditioning() as input_type parameter. To specify which input to condition.
Values:
-
enumerator
ERAD_COUNTER_COUNT_INPUT= 0¶
-
enumerator
ERAD_COUNTER_START_INPUT= 1¶
-
enumerator
ERAD_COUNTER_STOP_INPUT= 2¶
-
enumerator
ERAD_COUNTER_RESET_INPUT= 3¶
-
enumerator
Functions
-
ERAD_Owner
ERAD_getOwnership(void)¶ Gets the current owner of ERAD.
- Return
Owner of ERAD.
- Parameters
None.: This function returns the current owner of ERAD.
-
void
ERAD_setOwnership(ERAD_Owner owner)¶ Sets the current owner of ERAD.
This function sets the current owner of ERAD.
- Parameters
owner: is the Owner of ERAD that is to be set
- Return
None.
-
void
ERAD_resetCounter(uint16_t instances)¶ Resets the counter using the global registers.
This function resets the selected counters using the global registers.
- Parameters
instances: is the OR’d value of counter instances to be reset. Following macros can be used:ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
- Return
None.
-
void
ERAD_enableModules(uint16_t instances)¶ Enables counters and bus comparators.
This function enables bus comparators and counters whose instances are passed.
- Parameters
instances: is the OR’d value of instances of the counters and bus comparators. Following macros can be used:ERAD_INST_BUSCOMP1
ERAD_INST_BUSCOMP2
ERAD_INST_BUSCOMP3
ERAD_INST_BUSCOMP4
ERAD_INST_BUSCOMP5
ERAD_INST_BUSCOMP6
ERAD_INST_BUSCOMP7
ERAD_INST_BUSCOMP8
ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
- Return
None.
-
void
ERAD_disableModules(uint16_t instances)¶ Disables counters and bus comparators.
This function disables bus comparators and counters whose instances are passed.
- Parameters
instances: is the OR’d value of instances of the counters and bus comparators. Following macros can be used:ERAD_INST_BUSCOMP1
ERAD_INST_BUSCOMP2
ERAD_INST_BUSCOMP3
ERAD_INST_BUSCOMP4
ERAD_INST_BUSCOMP5
ERAD_INST_BUSCOMP6
ERAD_INST_BUSCOMP7
ERAD_INST_BUSCOMP8
ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
- Return
None.
-
void
ERAD_initModule(ERAD_Owner owner)¶ Initialises ERAD.
This function resets all the counters and disables all bus comparators and counters. Also sets the owner of the ERAD to the required owner.
- Parameters
owner: is the owner of ERAD that is to be set.
- Return
None.
-
uint16_t
ERAD_getHaltStatus(void)¶ Returns the completed status of any of the modules.
- Return
Completed status of all the modules as stored in the global register.
- Parameters
None.: This function returns the completed status of the counters and bus comparators as stored in the global registers. This allows us to read just one register and see if any of the modules are in a completed state.
-
uint16_t
ERAD_getEventStatus(void)¶ Returns the event fired status of any of the modules.
- Return
Event fired status of all the modules as stored in the global register.
- Parameters
None.: This function returns the event fired status of the counters and bus comparators as stored in the global registers. This allows us to read just one register and see if any of the modules have fired.
-
void
ERAD_enableNMI(uint16_t instances)¶ Enables an NMI for the specified modules.
This function enables an NMI to be generated whenever any of the specified counters or bus comparator units generate and event.
- Parameters
instances: is the OR’d value of the instances of the counters and bus comparator units that need to have an NMI enabled. Following macros can be used:ERAD_INST_BUSCOMP1
ERAD_INST_BUSCOMP2
ERAD_INST_BUSCOMP3
ERAD_INST_BUSCOMP4
ERAD_INST_BUSCOMP5
ERAD_INST_BUSCOMP6
ERAD_INST_BUSCOMP7
ERAD_INST_BUSCOMP8
ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
- Return
None.
-
void
ERAD_disableNMI(uint16_t instances)¶ Disables an NMI for the specified modules.
This function disables the NMI for the specified counters and bus comparator units.
- Parameters
instances: is the OR’d value of the instances of the counters and bus comparator units that need to have an NMI disabled. Following macros can be used:ERAD_INST_BUSCOMP1
ERAD_INST_BUSCOMP2
ERAD_INST_BUSCOMP3
ERAD_INST_BUSCOMP4
ERAD_INST_BUSCOMP5
ERAD_INST_BUSCOMP6
ERAD_INST_BUSCOMP7
ERAD_INST_BUSCOMP8
ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
- Return
None.
-
ERAD_Status
ERAD_getBusCompStatus(uint32_t base)¶ Returns the status of a bus comparator.
This function returns the status of the bus comparator whose base was passed. It may be either
ERAD_STATE_IDLE, ERAD_STATE_ENABLED or ERAD_STATE_COMPLETED.- Parameters
base: is the base of the bus comparator.
- Return
Status of bus comparator.
-
void
ERAD_clearBusCompEvent(uint32_t base)¶ Clears the event fired status of any of the modules.
This function clears the event fired status of the bus comparator and brings the module and brings the module back to
ERAD_STATE_IDLE .- Parameters
base: is the base of the bus comparator.
- Return
None
-
ERAD_Status
ERAD_getCounterStatus(uint32_t base)¶ Returns the status of a counter.
This function returns the status of the counter whose base was passed. It may be either
ERAD_STATE_IDLE, ERAD_STATE_ENABLED or ERAD_STATE_COMPLETED.- Parameters
base: is the base of the counter.
- Return
Status of counter.
-
void
ERAD_configBusComp(uint32_t base, ERAD_BusComp_Config config_params)¶ Configures the bus comparators.
This function configures the bus comparator with the given parameters.
- Parameters
base: is the base of the bus comparator to be configured.config_params: are the configuration parameters to be used to configure the bus comparator.
- Return
None.
-
void
ERAD_configCounterInCountingMode(uint32_t base, ERAD_Counter_Config config_params)¶ Configures the counter in Counting mode.
This function configures the counter with the given parameters. The counter is setup in Counting mode, which means counting begins as soon as the counter is enabled. NOTE: This function does not enable the counter. The counter must be enabled using the
ERAD_enableModules method to begin counting.- Parameters
base: is the base of the counter to be configured.config_params: are the configuration parameters to be used to configure the counter.
- Return
None.
-
void
ERAD_configCounterInStartStopMode(uint32_t base, ERAD_Counter_Config config_params, ERAD_Counter_Input_Event start_event, ERAD_Counter_Input_Event stop_event)¶ Configures the counter in Start-Stop mode.
This function configures the counter with the given parameters. The counter is setup in Start-Stop mode, which means counting will happen only between two specified events. The event that will be counted can be any of the
ERAD_Counter_Input_Event and not only CPU cycles. NOTE: ERAD_EVENT_NO_EVENT causes the counter to use the CPU cycles. NOTE: This function does not enable the counter. The counter must be enabled using the ERAD_enableModules method to begin counting.- Parameters
base: is the base of the counter to be configured.config_params: are the configuration parameters to be used to configure the counter.start_event: is the event that starts the counterstop_event: is the event which stops that counter
- Return
None.
-
void
ERAD_configCounterInCumulativeMode(uint32_t base, ERAD_Counter_Config config_params, ERAD_Counter_Input_Event start_event, ERAD_Counter_Input_Event stop_event)¶ Configures the counter in Start-Stop Cumulative mode.
This function configures the counter with the given parameters. The counter is setup in Cumulative mode, which means counting will happen only between two specified events and the counter will not reset on
stop_event. The event that will be counted can be any of the ERAD_Counter_Input_Event and not only CPU cycles. NOTE: ERAD_EVENT_NO_EVENT causes the counter to use the CPU cycles. NOTE: This function does not enable the counter. The counter must be enabled using the ERAD_enableModules method to begin counting.- Parameters
base: is the base of the counter to be configured.config_params: are the configuration parameters to be used to configure the counter.start_event: is the event that starts the counterstop_event: is the event which stops that counter
- Return
None.
-
void
ERAD_configMask(ERAD_Mask mask, uint32_t instances, bool enable_int)¶ Configures the AND and OR masks
This function enables the event generated from the specified bus comparator units to be used for the specified Mask. It also configures the interrupt generation when the mask event occurs.
- Parameters
mask: is the Mask to be used.instances: is the OR’d value of the instances of the bus comparator units whose events need to be used for the mask. Following macros can be used:ERAD_INST_BUSCOMP1
ERAD_INST_BUSCOMP2
ERAD_INST_BUSCOMP3
ERAD_INST_BUSCOMP4
ERAD_INST_BUSCOMP5
ERAD_INST_BUSCOMP6
ERAD_INST_BUSCOMP7
ERAD_INST_BUSCOMP8
ERAD_INST_COUNTER1
ERAD_INST_COUNTER2
ERAD_INST_COUNTER3
ERAD_INST_COUNTER4
enable_int: True if interrupt needs to be enabled, False if not
- Return
None.
-
void
ERAD_enableCounterResetInput(uint32_t base, ERAD_Counter_Input_Event reset_event)¶ Configures the reset event of the counter.
This function sets the event upon which the counter must reset and enables reset upon such an event.
- Parameters
base: is the base of the counter to be configured.reset_event: is the event upon which the counter must be reset.
- Return
None.
-
void
ERAD_disableCounterResetInput(uint32_t base)¶ Disables the reset event of the counter.
This function disables the reset event that may have been set earlier
- Parameters
base: is the base of the counter.
- Return
None.
-
void
ERAD_clearCounterEvent(uint32_t base)¶ Clears an event that may have fired in the counter upon match.
This function clears a counter event that may have fired when the counter hit a match.
- Parameters
base: is the base of the counter.
- Return
None.
-
void
ERAD_clearCounterOverflow(uint32_t base)¶ Clears an overflow that may have occured in the counter.
This function clears the overflow bit that may have got set when the counter may have crossed 0xFFFFFFFF.
- Parameters
base: is the base of the counter.
- Return
None.
-
uint32_t
ERAD_getCurrentCount(uint32_t base)¶ Gets the current count of a counter.
This function returns the current count of the counter which was configured earlier.
- Parameters
base: is the base of the counter.
- Return
Returns the value of the current count of the counter.
-
void
ERAD_setCurrentCount(uint32_t base, uint32_t value)¶ Sets the current count of a counter.
This function sets the current count of the counter which was configured earlier. This can be used to reset the counter or start at a value other than 0.
- Parameters
base: is the base of the counter.value: is the value to be written as the current count.
- Return
None.
-
uint32_t
ERAD_getMaxCount(uint32_t base)¶ Gets the maximum count of a counter.
This function returns the current maximum count of the counter which was configured earlier.
- Parameters
base: is the base of the counter.
- Return
Returns the value of the current maximum count of the counter.
-
void
ERAD_setMaxCount(uint32_t base, uint32_t value)¶ Sets the maximum count of a counter.
This function sets the current maximum count of the counter which was configured earlier.
- Parameters
base: is the base of the counter.value: is the value to be written as the maximum count.
- Return
None.
-
void
ERAD_setCounterInputConditioning(uint32_t base, ERAD_Counter_Input_Type input_type, uint16_t options)¶ Sets conditioning on the inputs to the counter.
This function conditions the inputs to the counter specified. This includes inverting the input and enabling a 2-stage synchronizer for any 4 of the inputs:
reset, stop, start, count_input.- Parameters
base: is the base value of the counter to be configuredinput_type: defines which input needs to be conditionedoptions: is the kind of conditioning that needs to applied. This will be an OR’d value of ERAD_INVERT_ENABLE, ERAD_INVERT_DISABLE, ERAD_SYNC_ENABLE or ERAD_SYNC_DISABLE.
- Return
None.
-
void
ERAD_initCRC(uint16_t instances)¶ Initialises the CRC unit.
This function initialises the specified CRC units.
- Parameters
instances: is the OR’d value of CRC instances. Following macros can be used:ERAD_INST_CRC1
ERAD_INST_CRC2
ERAD_INST_CRC3
ERAD_INST_CRC4
ERAD_INST_CRC5
ERAD_INST_CRC6
ERAD_INST_CRC7
ERAD_INST_CRC8
- Return
None.
-
void
ERAD_enableCRC(uint16_t instances)¶ Enables the CRC unit.
This function enables the specified CRC units.
- Parameters
instances: is the OR’d value of CRC instances. Following macros can be used:ERAD_INST_CRC1
ERAD_INST_CRC2
ERAD_INST_CRC3
ERAD_INST_CRC4
ERAD_INST_CRC5
ERAD_INST_CRC6
ERAD_INST_CRC7
ERAD_INST_CRC8
- Return
None.
-
void
ERAD_disableCRC(uint16_t instances)¶ Disables the CRC unit.
This function disables the specified CRC units.
- Parameters
instances: is the OR’d value of CRC instances. Following macros can be used:ERAD_INST_CRC1
ERAD_INST_CRC2
ERAD_INST_CRC3
ERAD_INST_CRC4
ERAD_INST_CRC5
ERAD_INST_CRC6
ERAD_INST_CRC7
ERAD_INST_CRC8
- Return
None.
-
uint32_t
ERAD_getCurrentCRC(uint32_t base)¶ Gets the current value of the CRC unit.
This function returns the current value of te specified CRC unit.
- Parameters
base: is the base value of CRC unit
- Return
Current CRC value.
-
void
ERAD_setSeed(uint32_t base, uint32_t seed)¶ Sets the seed value of the CRC unit
This function sets a seed value of the CRC unit. Note: The corresponding CRC unit must be disabled before setting the seed value.
- Parameters
base: is the base value of the CRC unitseed: is the value of seed to be set
- Return
None.
-
void
ERAD_setCRCQualifier(uint32_t base, ERAD_CRC_Qualifiers qualifier)¶ Sets the qualifier event of the CRC unit
This function sets a qualifier to decide which events require a CRC computation. Note: The corresponding CRC unit must be disabled before setting the qualifier.
- Parameters
base: is the base value of the CRC unitqualifier: is the type of qualifier to be set
- Return
None.
-
void
ERAD_profile(ERAD_Profile_Params config_params)¶ Configures the ERAD to profile a certain piece of code
This function configures 2 bus comparators and 1 counter to profile a certain piece of code. The base address of the bus comparators and the counter to be used are specified in
config_params. Note: Use ERAD_getMaxCount to get the latest profiled value. The maximum count of the counter being used must be reset to 0x0 to get the correct value everytime.- Parameters
config_params: are the parameters that will be used to configure ERAD
- Return
None.
-
void
ERAD_enableInterruptOnAddressHit(ERAD_AddressHit_Params config_params, uint32_t busComp_base)¶ Enables an RTOS interrupt at a specified address.
This function enables an RTOS interrupt to be generated when an address in memory or instruction is hit.
- Parameters
config_params: contrains the bus to be monitored and the addressbusComp_base: is the base of the bus compoarator to be used
If the selected bus is ERAD_BUSCOMP_BUS_PAB, then the ERAD will be configured to trigger an interrupt when there is instruction fetch happening at the specified address. Similary, if ERAD_BUSCOMP_BUS_DWAB is selected, the ERAD will be configured to trigger an interrupt when there write access to the specified address, and so on.
Use
- Return
None.
-
void
ERAD_countAddressHits(ERAD_AddressHit_Params config_params, uint32_t busComp_base, uint32_t counter_base)¶ Configures the ERAD to count the number of times a the specified address is hit
This function configures 1 bus comparator and 1 counter to count how many times a the specified address is hit.
- Parameters
config_params: are the parameters that will be used to configure ERADbusComp_base: is the base of the bus compoarator to be usedcounter_base: is the base of the counter to be used
If the selected bus is ERAD_BUSCOMP_BUS_PAB, then the ERAD will be configured to count the number of times an instruction fetch happens at the specified address. Similary, if ERAD_BUSCOMP_BUS_DWAB is selected, the ERAD will be configured to count the number of times there is a write access to the specified address, and so on.
- Return
None.
-
struct
ERAD_BusComp_Config¶ - #include <erad.h>
Structure that is passed to ERAD_configBusComp() as config_params to configure a bus comparator.
-
struct
ERAD_Profile_Params¶ - #include <erad.h>
Structure that is passed to ERAD_profile() as config_params to setup the required modules appropriately for each use case.
-
struct
ERAD_Counter_Config¶ - #include <erad.h>
Structure that is passed to ERAD_configCounterInStartStopMode() and ERA_configCounterInCountingMode() as config_params to setup a counter appropriately.
-
struct
ERAD_AddressHit_Params¶ - #include <erad.h>
Structure that is passed to ERAD_enableInterruptOnAddressHit() and ERAD_countAddressHits() as config_params to select the bus and the address to compare. bus_Sel can be one of the following: ERAD_BUSCOMP_BUS_PAB : for instruction fetch at the address ERAD_BUSCOMP_BUS_DWAB : for data write access to the address ERAD_BUSCOMP_BUS_DRAB : for data read access to the address
-
The code for this module is contained in driverlib/erad.c, with driverlib/erad.h containing the API declarations for use by applications.