MEMCFG Module¶
The MemCfg module provides an API to configure the device’s Memory Control Module. The functions that are provided fall into three main categories: RAM section configuration, access violation status and interrupts, and memory error status an interrupts. The RAM section configuration functions can initialize RAM, configure access protection settings, and configure section ownership. The access violation and memory error categories contain functions that can return violation and error status and address information as well as configure interrupts that can be generated as a result of these issues.
-
group
memcfg_api Defines
-
MEMCFG_SECT_TYPE_MASK0xFF000000U¶
-
MEMCFG_SECT_TYPE_D0x00000000U¶
-
MEMCFG_SECT_TYPE_LS0x01000000U¶
-
MEMCFG_SECT_TYPE_GS0x02000000U¶
-
MEMCFG_SECT_TYPE_MSG0x03000000U¶
-
MEMCFG_SECT_TYPE_ROM0x04000000U¶
-
MEMCFG_SECT_NUM_MASK0x00FFFFFFU¶
-
MEMCFG_XACCPROTX_M((uint32_t)MEMCFG_GSXACCPROT0_FETCHPROT_GS0| \
(uint32_t)
MEMCFG_GSXACCPROT0_CPUWRPROT_GS0| \
(uint32_t)
MEMCFG_GSXACCPROT0_HICWRPROT_GS0| \
(uint32_t)
MEMCFG_GSXACCPROT0_DMAWRPROT_GS0)¶
-
MEMCFG_XTEST_MMEMCFG_DXTEST_TEST_M0_M¶
-
MEMCFG_NMVIOL_MASK0x0000FFFFU¶
-
MEMCFG_MVIOL_MASK0x000F0000U¶
-
MEMCFG_MVIOL_SHIFT16U¶
-
MEMCFG_TESTLOCK_KEY0xA5A50000U¶
-
MEMCFG_SECT_M00x00000001U¶ M0 RAM.
-
MEMCFG_SECT_M10x00000002U¶ M1 RAM.
-
MEMCFG_SECT_DX_ALL0x00000003U¶ All M and D RAM.
-
MEMCFG_SECT_LS00x01000001U¶ LS0 RAM.
-
MEMCFG_SECT_LS10x01000002U¶ LS1 RAM.
-
MEMCFG_SECT_LS20x01000004U¶ LS2 RAM.
-
MEMCFG_SECT_LS30x01000008U¶ LS3 RAM.
-
MEMCFG_SECT_LS40x01000010U¶ LS4 RAM.
-
MEMCFG_SECT_LS50x01000020U¶ LS5 RAM.
-
MEMCFG_SECT_LS60x01000040U¶ LS6 RAM.
-
MEMCFG_SECT_LS70x01000080U¶ LS7 RAM.
-
MEMCFG_SECT_LSX_ALL0x010000FFU¶ All LS RAM.
-
MEMCFG_SECT_GS00x02000001U¶ GS0 RAM.
-
MEMCFG_SECT_GS10x02000002U¶ GS1 RAM.
-
MEMCFG_SECT_GS20x02000004U¶ GS2 RAM.
-
MEMCFG_SECT_GS30x02000008U¶ GS3 RAM.
-
MEMCFG_SECT_GSX_ALL0x0200000FU¶ All GS RAM.
-
MEMCFG_SECT_MSGCPUTOCLA10x03000002U¶ CPU-to-CLA1 message RAM.
-
MEMCFG_SECT_MSGCLA1TOCPU0x03000004U¶ CLA1-to-CPU message RAM.
-
MEMCFG_SECT_MSGCLA1TODMA0x03000020U¶ CLA1-to-DMA message RAM.
-
MEMCFG_SECT_MSGDMATOCLA10x03000040U¶ DMA-to-CLA1 message RAM.
-
MEMCFG_SECT_MSGX_ALL0x03000006U¶ All message RAM.
-
MEMCFG_SECT_ROMBOOT0x04000001U¶ BOOT ROM.
-
MEMCFG_SECT_ROMSECURE0x04000002U¶ Secure ROM.
-
MEMCFG_SECT_ROMCLADATA0x04000004U¶ CLA Data ROM.
-
MEMCFG_SECT_ROM_ALL0x04000007U¶ All ROMs.
-
MEMCFG_SECT_ALL0xFFFFFFFFU¶ All configurable RAM.
-
MEMCFG_PROT_ALLOWCPUFETCH0x00000000U¶ CPU fetch allowed.
-
MEMCFG_PROT_BLOCKCPUFETCH0x00000001U¶ CPU fetch blocked.
-
MEMCFG_PROT_ALLOWCPUWRITE0x00000000U¶ CPU write allowed.
-
MEMCFG_PROT_BLOCKCPUWRITE0x00000002U¶ CPU write blocked.
-
MEMCFG_PROT_ALLOWDMAWRITE0x00000000U¶ DMA write allowed (GSxRAM)
-
MEMCFG_PROT_BLOCKDMAWRITE0x00000004U¶ DMA write blocked (GSxRAM)
-
MEMCFG_PROT_ALLOWHICWRITE0x00000000U¶ HIC write allowed (GSxRAM)
-
MEMCFG_PROT_BLOCKHICWRITE0x00000008U¶ HIC write blocked (GSxRAM)
-
MEMCFG_NMVIOL_CPUREAD0x00000001U¶ Non-controller CPU read access.
-
MEMCFG_NMVIOL_CPUWRITE0x00000002U¶ Non-controller CPU write access.
-
MEMCFG_NMVIOL_CPUFETCH0x00000004U¶ Non-controller CPU fetch access.
-
MEMCFG_NMVIOL_DMAWRITE0x00000008U¶ Non-controller DMA write access.
-
MEMCFG_NMVIOL_CLA1READ0x00000010U¶ Non-controller CLA1 read access.
-
MEMCFG_NMVIOL_CLA1WRITE0x00000020U¶ Non-controller CLA1 write access.
-
MEMCFG_NMVIOL_CLA1FETCH0x00000040U¶ Non-controller CLA1 fetch access.
-
MEMCFG_NMVIOL_DMAREAD0x00000400U¶ Non-controller DMA read access.
-
MEMCFG_NMVIOL_HICREAD0x00000800U¶ Non-controller HIC read access.
-
MEMCFG_NMVIOL_HICWRITE0x00001000U¶ Non-controller HIC write access.
-
MEMCFG_MVIOL_CPUFETCH0x00010000U¶ Controller CPU fetch access.
-
MEMCFG_MVIOL_CPUWRITE0x00020000U¶ Controller CPU write access.
-
MEMCFG_MVIOL_DMAWRITE0x00040000U¶ Controller DMA write access.
-
MEMCFG_MVIOL_HICWRITE0x00080000U¶ Controller HIC write access.
-
MEMCFG_CERR_CPUREAD0x0001U¶ Correctable CPU read error.
-
MEMCFG_CERR_DMAREAD0x0002U¶ Correctable DMA read error.
-
MEMCFG_CERR_CLA1READ0x0004U¶ Correctable CLA1 read error.
-
MEMCFG_CERR_HICREAD0x0020U¶ Correctable DMA read error.
-
MEMCFG_UCERR_CPUREAD0x0001U¶ Uncorrectable CPU read error.
-
MEMCFG_UCERR_DMAREAD0x0002U¶ Uncorrectable DMA read error.
-
MEMCFG_UCERR_CLA1READ0x0004U¶ Uncorrectable CLA1 read error.
-
MEMCFG_UCERR_HICREAD0x0020U¶ Uncorrectable HIC read error.
-
MEMCFG_DIAGERR_UNCORR0x00000002U¶ Uncorr error in diag/test mode.
-
MEMCFG_DIAGERR_CORR0x00000001U¶ Corr error in diag/test mode.
Enums
-
enum
MemCfg_CLAMemoryType¶ Values that can be passed to MemCfg_setCLAMemType() as the claMemType parameter.
Values:
-
enumerator
MEMCFG_CLA_MEM_DATA¶ Section is CLA data memory.
-
enumerator
MEMCFG_CLA_MEM_PROGRAM¶ Section is CLA program memory.
-
enumerator
-
enum
MemCfg_LSRAMControllerSel¶ Values that can be passed to MemCfg_setLSRAMControllerSel() as the controllerSel parameter.
Values:
-
enumerator
MEMCFG_LSRAMCONTROLLER_CPU_ONLY¶ CPU is the owner of the section.
-
enumerator
MEMCFG_LSRAMCONTROLLER_CPU_CLA1¶ CPU and CLA1 share this section.
-
enumerator
-
enum
MemCfg_TestMode¶ Values that can be passed to MemCfg_setTestMode() as the testMode parameter.
Values:
-
enumerator
MEMCFG_TEST_FUNCTIONAL= 0¶ Functional mode. Test mode is disabled.
-
enumerator
MEMCFG_TEST_WRITE_DATA= 1¶ Writes allowed to data only.
-
enumerator
MEMCFG_TEST_WRITE_ECC= 2¶ Writes allowed to ECC only (for DxRAM/MxRAM)
-
enumerator
MEMCFG_TEST_WRITE_PARITY= 2¶ Writes allowed to parity only (for LSxRAM, GSxRAM, and MSGxRAM)
-
enumerator
MEMCFG_TEST_FUNC_DIAG= 3¶ Diagnostic mode, similar to functional mode but NMI is not generated.
-
enumerator
Functions
-
void
MemCfg_setCLAMemType(uint32_t ramSections, MemCfg_CLAMemoryType claMemType)¶ Sets the CLA memory type of the specified RAM section.
This function sets the CLA memory type configuration of the RAM section. If the
claMemType parameter is MEMCFG_CLA_MEM_DATA, the RAM section will be configured as CLA data memory. If MEMCFG_CLA_MEM_PROGRAM, the RAM section will be configured as CLA program memory.- Parameters
ramSections: is the logical OR of the sections to be configured.claMemType: indicates data memory or program memory.
The ramSections parameter is an OR of the following indicators: MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.
- Note
This API only applies to LSx RAM and has no effect if the CLA isn’t controller of the memory section.
- See
MemCfg_setLSRAControllerSel()
- Return
None.
-
void
MemCfg_enableViolationInterrupt(uint32_t intFlags)¶ Enables individual RAM access violation interrupt sources.
- Return
None.
- Parameters
intFlags: is a bit mask of the interrupt sources to be enabled. Can be a logical OR any of the following values:MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access This function enables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
-
void
MemCfg_disableViolationInterrupt(uint32_t intFlags)¶ Disables individual RAM access violation interrupt sources.
This function disables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Parameters
intFlags: is a bit mask of the interrupt sources to be disabled. Can be a logical OR any of the following values:MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access
- Note
Note that only non-controller violations may generate interrupts.
- Return
None.
-
uint32_t
MemCfg_getViolationInterruptStatus(void)¶ Gets the current RAM access violation status.
This function returns the RAM access violation status. This function will return flags for both controller and non-controller access violations although only the non-controller flags have the ability to cause the generation of an interrupt.
- Return
Returns the current violation status, enumerated as a bit field of the values:
MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access
-
void
MemCfg_forceViolationInterrupt(uint32_t intFlags)¶ Sets the RAM access violation status.
This function sets the RAM access violation status. This function will set flags for both controller and non-controller access violations, and an interrupt will be generated if it is enabled.
- Parameters
intFlags: is a bit mask of the access violation flags to be set. Can be a logical OR any of the following values:MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access
- Return
None.
-
void
MemCfg_clearViolationInterruptStatus(uint32_t intFlags)¶ Clears RAM access violation flags.
- Return
None.
- Parameters
intFlags: is a bit mask of the access violation flags to be cleared. Can be a logical OR any of the following values:MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access
-
void
MemCfg_setCorrErrorThreshold(uint32_t threshold)¶ Sets the correctable error threshold value.
This value sets the error-count threshold at which a correctable error interrupt is generated. That is when the error count register reaches the value specified by the
threshold parameter, an interrupt is generated if it is enabled.- Parameters
threshold: is the correctable error threshold.
- Return
None.
-
uint32_t
MemCfg_getCorrErrorCount(void)¶ Gets the correctable error count.
- Return
Returns the number of correctable error have occurred.
-
void
MemCfg_enableCorrErrorInterrupt(uint32_t intFlags)¶ Enables individual RAM correctable error interrupt sources.
This function enables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Parameters
intFlags: is a bit mask of the interrupt sources to be enabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.
- Note
Note that only correctable errors may generate interrupts.
- Return
None.
-
void
MemCfg_disableCorrErrorInterrupt(uint32_t intFlags)¶ Disables individual RAM correctable error interrupt sources.
This function disables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Parameters
intFlags: is a bit mask of the interrupt sources to be disabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.
- Note
Note that only correctable errors may generate interrupts.
- Return
None.
-
uint32_t
MemCfg_getCorrErrorInterruptStatus(void)¶ Gets the current RAM correctable error interrupt status.
- Return
Returns the current error interrupt status. Will return a value of MEMCFG_CERR_CPUREAD if an interrupt has been generated. If not, the function will return 0.
-
void
MemCfg_forceCorrErrorInterrupt(uint32_t intFlags)¶ Sets the RAM correctable error interrupt status.
This function sets the correctable error interrupt flag.
- Parameters
intFlags: is a bit mask of the interrupt sources to be set. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.
- Note
Note that only correctable errors may generate interrupts.
- Return
None.
-
void
MemCfg_clearCorrErrorInterruptStatus(uint32_t intFlags)¶ Clears the RAM correctable error interrupt status.
This function clears the correctable error interrupt flag.
- Parameters
intFlags: is a bit mask of the interrupt sources to be cleared. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.
- Note
Note that only correctable errors may generate interrupts.
- Return
None.
-
uint32_t
MemCfg_getCorrErrorStatus(void)¶ Gets the current correctable RAM error status.
- Return
Returns the current error status, enumerated as a bit field of MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ
-
uint32_t
MemCfg_getUncorrErrorStatus(void)¶ Gets the current uncorrectable RAM error status.
- Return
Returns the current error status, enumerated as a bit field of MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ or MEMCFG_UCERR_HICREAD.
-
void
MemCfg_forceCorrErrorStatus(uint32_t stsFlags)¶ Sets the specified correctable RAM error status flag.
This function sets the specified correctable RAM error status flag.
- Parameters
stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ
- Return
None.
-
void
MemCfg_forceUncorrErrorStatus(uint32_t stsFlags)¶ Sets the specified uncorrectable RAM error status flag.
This function sets the specified uncorrectable RAM error status flag.
- Parameters
stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ or MEMCFG_UCERR_HICREAD.
- Return
None.
-
void
MemCfg_clearCorrErrorStatus(uint32_t stsFlags)¶ Clears correctable RAM error flags.
This function clears the specified correctable RAM error flags.
- Parameters
stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ
- Return
None.
-
void
MemCfg_clearUncorrErrorStatus(uint32_t stsFlags)¶ Clears uncorrectable RAM error flags.
This function clears the specified uncorrectable RAM error flags.
- Parameters
stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ or MEMCFG_UCERR_HICREAD.
- Return
None.
-
uint32_t
MemCfg_getDiagErrorStatus(void)¶ Gets the diagnostics corr/uncorr memory error status in test mode.
- Return
Returns the diagnostics error status in test mode. It can return following values: MEMCFG_DIAGERR_UNCORR, and/or MEMCFG_DIAGERR_CORR.
-
void
MemCfg_clearDiagErrorStatus(uint32_t stsFlags)¶ Clears the diagnostics corr/uncorr memory error status.
This function clears the specified diagnostics corr/uncorr RAM/ROM memory error flags in test mode. The param
stsFlags can be any of the following values: MEMCFG_DIAGERR_UNCORR, and/or MEMCFG_DIAGERR_CORR.- Parameters
stsFlags: is a bit mask of the status flags to be cleared.
- Return
None.
-
uint32_t
MemCfg_getDiagErrorAddress(void)¶ Gets address location of diagnostics corr/uncorr memory read/write error.
- Return
Return address location of diagnostics corr/uncorr memory error error in test mode.
-
void
MemCfg_lockConfig(uint32_t memSections)¶ Locks the writes to the configuration of specified memory sections.
This function locks writes to the access protection and controller select configuration of a memory section.That means calling
MemCfg_setProtection() or MemCfg_setLSRAMControllerSel() for a locked memory section will have no effect until MemCfg_unlockConfig() is called.- Parameters
memSections: is the logical OR of the sections to be configured.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL
MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCPUTOCLA1 MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or use MEMCFG_SECT_MSGX_ALL to configure all message RAM sections.
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
void
MemCfg_unlockConfig(uint32_t memSections)¶ Unlocks the writes to the configuration of a memory section.
This function unlocks writes to the access protection and controller select configuration of a memory section that has been locked using
MemCfg_lockConfig().- Parameters
memSections: is the logical OR of the sections to be configured.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL
MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCPUTOCLA1 MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or use MEMCFG_SECT_MSGX_ALL to configure all message RAM sections.
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
void
MemCfg_commitConfig(uint32_t memSections)¶ Permanently locks writes to the configuration of a memory section.
This function permanently locks writes to the access protection and controller select configuration of a memory section. That means calling
MemCfg_setProtection() or MemCfg_setLSRAMControllerSel() for a locked memory section will have no effect. To lock the configuration in a nonpermanent way, use MemCfg_lockConfig().- Parameters
memSections: is the logical OR of the sections to be configured.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL
MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCPUTOCLA1 MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or use MEMCFG_SECT_MSGX_ALL to configure all message RAM sections.
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
void
MemCfg_setProtection(uint32_t memSection, uint32_t protectMode)¶ Sets the access protection mode of a single memory section.
This function sets the access protection mode of a specified memory section. The mode is passed into the
protectMode parameter as the logical OR of the following values:MEMCFG_PROT_ALLOWCPUFETCH or MEMCFG_PROT_BLOCKCPUFETCH - CPU fetch
MEMCFG_PROT_ALLOWCPUWRITE or MEMCFG_PROT_BLOCKCPUWRITE - CPU write
MEMCFG_PROT_ALLOWDMAWRITE or MEMCFG_PROT_BLOCKDMAWRITE - DMA write
MEMCFG_PROT_ALLOWHICWRITE or MEMCFG_PROT_BLOCKHICWRITE - HIC write
- Parameters
memSection: is the memory section to be configured.protectMode: is the logical OR of the settings to be applied.
The memSection parameter is one of the following indicators:
MEMCFG_SECT_M0 or MEMCFG_SECT_M1
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx
This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig() or if the memory is configured as CLA program memory.
- Return
None.
-
void
MemCfg_setLSRAMControllerSel(uint32_t ramSection, MemCfg_LSRAMControllerSel controllerSel)¶ Sets the controller of the specified LSxRAM section.
This function sets the controller select configuration of the LSxRAM section. If the
controllerSel parameter is MEMCFG_LSRAMCONTROLLER_CPU_ONLY, the LSxRAM section passed into the ramSection parameter will be dedicated to the CPU. If MEMCFG_LSRAMCONTROLLER_CPU_CLA1, the memory section will be shared between the CPU and the CLA.- Parameters
ramSection: is the LSxRAM section to be configured.controllerSel: is the sharing selection.
The ramSection parameter should be a value from MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.
This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig().
- Note
This API only applies to LSxRAM.
- Return
None.
-
void
MemCfg_lockTestConfig(uint32_t memSections)¶ Locks the writes to the test mode configuration of specified memory sections.
This function locks writes to the test mode configuration of a RAM section. That means calling
MemCfg_setTestMode() for a locked RAM section will have no effect until MemCfg_unlockTestConfig() is called.- Parameters
memSections: is the logical OR of the sections to be configured.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0, MEMCFG_SECT_M1, or use MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or use MEMCFG_SECT_LSX_ALL to configure all possible LSRAM sections.
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or use MEMCFG_SECT_GSX_ALL to configure all possible GSRAM sections.
MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or use MEMCFG_SECT_MSGX_ALL to configure all possible message RAM sections.
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
void
MemCfg_unlockTestConfig(uint32_t memSections)¶ Unlocks the writes to the test mode configuration of specified memory sections.
This function unlocks writes to the test mode configuration of a RAM section that has been locked using
MemCfg_lockTestConfig().- Parameters
memSections: is the logical OR of the sections to be configured.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0, MEMCFG_SECT_M1, or use MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or use MEMCFG_SECT_LSX_ALL to configure all possible LSRAM sections.
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or use MEMCFG_SECT_GSX_ALL to configure all possible GSRAM sections.
MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or use MEMCFG_SECT_MSGX_ALL to configure all possible message RAM sections.
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
void
MemCfg_setTestMode(uint32_t memSection, MemCfg_TestMode testMode)¶ Sets the test mode of the specified memory section.
This function sets the test mode configuration of the RAM section. The
testMode parameter can take one of the following values:MEMCFG_TEST_FUNCTIONAL
MEMCFG_TEST_WRITE_DATA
MEMCFG_TEST_WRITE_ECC
MEMCFG_TEST_WRITE_PARITY
MEMCFG_TEST_FUNC_DIAG
- Parameters
memSection: is the memory section to be configured.testMode: is the test mode selected.
The memSection parameter is one of the following indicators:
MEMCFG_SECT_M0, MEMCFG_SECT_M1
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx
MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1
- Return
None.
-
void
MemCfg_initSections(uint32_t ramSections)¶ Starts the initialization the specified RAM sections.
This function starts the initialization of the specified RAM sections. Use
MemCfg_getInitStatus() to check if the initialization is done.- Parameters
ramSections: is the logical OR of the sections to be initialized.
The ramSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0, MEMCFG_SECT_M1, or MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL
MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or MEMCFG_SECT_MSGX_ALL
OR use MEMCFG_SECT_ALL to configure all possible sections.
- Return
None.
-
bool
MemCfg_getInitStatus(uint32_t ramSections)¶ Get the status of initialized RAM sections.
This function gets the initialization status of the RAM sections specified by the
ramSections parameter.- Parameters
ramSections: is the logical OR of the sections to be checked.
The ramSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_M0, MEMCFG_SECT_M1, or MEMCFG_SECT_DX_ALL
MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL
MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL
MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, or MEMCFG_SECT_MSGX_ALL
OR use MEMCFG_SECT_ALL to get status of all possible sections.
- Note
Use MemCfg_initSections() to start the initialization.
- Return
Returns true if all the sections specified by ramSections have been initialized and false if not.
-
uint32_t
MemCfg_getViolationAddress(uint32_t intFlag)¶ Get the violation address associated with a intFlag.
- Return
Returns the violation address associated with the intFlag.
- Parameters
intFlag: is the type of access violation as indicated by ONE of these values:MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access
MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access
MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access
MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access
MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access
MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access
MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access
MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access
MEMCFG_NMVIOL_HICREAD - Non-controller HIC read access
MEMCFG_NMVIOL_HICWRITE - Non-controller HIC write access
MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access
MEMCFG_MVIOL_CPUWRITE - Controller CPU write access
MEMCFG_MVIOL_DMAWRITE - Controller DMA write access
MEMCFG_MVIOL_HICWRITE - Controller HIC write access
-
uint32_t
MemCfg_getCorrErrorAddress(uint32_t stsFlag)¶ Get the correctable error address associated with a stsFlag.
- Return
Returns the error address associated with the stsFlag.
- Parameters
stsFlag: is the type of error to which the returned address will correspond. It can take following values: MEMCFG_CERR_CPUREAD, MEMCFG_CERR_CLA1READ, MEMCFG_CERR_DMAREAD.
-
uint32_t
MemCfg_getUncorrErrorAddress(uint32_t stsFlag)¶ Get the uncorrectable error address associated with a stsFlag.
- Return
Returns the error address associated with the stsFlag.
- Parameters
stsFlag: is the type of error to which the returned address will correspond. It may be passed one of these values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, or MEMCFG_UCERR_CLA1READ values
-
void
MemCfg_forceMemError(uint32_t memSections)¶ Forces parity error in the selected memory.
This function forces the parity error in the memories specified by the
memSections parameter.- Parameters
memSections: is the logical OR of the sections to be tested.
The memSections parameter is an OR of one of the following sets of indicators:
MEMCFG_SECT_ROMBOOT, MEMCFG_SECT_ROMSECURE , MEMCFG_SECT_ROMCLADATA, MEMCFG_SECT_ROM_ALL.
OR use MEMCFG_SECT_ALL to force parity error in all possible memory sections.
- Return
None.
-
Many of the functions provided by this API to configure RAM sections’ settings will take a RAM section identifier or an OR of several identifiers as a parameter. These are #defines with names in the format MEMCFG_SECT_X. Take care to read the function description to learn which functions can operate on multiple sections of the same type at a time and which ones can only configure one section at a time. A quick way to check this is to see if the parameter says e ramSection or the plural e ramSections. Some functions may also be able to take a MEMCFG_SECT_ALL value to indicate that all RAM sections should be operated on at the same time. Again, read the function’s detailed description to be sure.
The code for this module is contained in driverlib/memcfg.c, with driverlib/memcfg.h containing the API declarations for use by applications.