HIC Module¶
The Host Interface Controller (HIC) API provides a set of functions for configuring and using the Host Interface Controller module. The functions provided helps in the setup and configuration of the Host Interface Controller.
-
group
hic_api
This module is used for Host Interface Controller(HIC) configuration.
Defines
-
HIC_NUM_BASE_ADDRESS
8U¶ Number of Base Regions.
-
HIC_NUM_BUFFER_REGS
16U¶ Number of D2H,H2D Buffers.
-
HIC_HOST_INTERFACE_ENABLE
0x0AU¶ Host Interface Enable.
-
HIC_LOCK_WRITE_ENABLE_KEY
0x5A5AU¶ Write Enable Key.
-
HIC_HOSTCR_WRITE_ENABLE_KEY
0xA5U¶ Host CR Reg Write Enable Key.
-
HIC_LOCK_UNLOCK
0x0U¶ Lock is Unlocked.
-
HIC_MODE_DW_8BIT
0U¶ 8 Bit Mode
Values that can be passed to HIC_setConfig() as flags or used with HIC_getConfig() API return value parsing
-
HIC_MODE_DW_16BIT
1U¶ 16 Bit Mode
-
HIC_MODE_DW_32BIT
2U¶ 32 Bit Mode
-
HIC_MODE_RW_PIN_SEPARATE
0U¶ RW Control Pins are separate.
-
HIC_MODE_RW_PIN_SINGLE
0x10U¶ Single RnW Control Pin.
-
HIC_MODE_BEN_PRESENT
0x20U¶ Byte Enable Present.
-
HIC_MODE_BEN_ABSENT
0U¶ Byte Enable not Present.
-
HIC_MODE_RDY_PRESENT
0x40U¶ nRDY Pin Present
-
HIC_MODE_RDY_ABSENT
0U¶ nRDY Pin not Present
-
HIC_MODE_H2DBUF_DEVWREN
0x100U¶ H2D Buf Device Write Enable.
-
HIC_MODE_D2HBUF_HOST_WR_ENABLE
0x200U¶ D2H Buf Host Write Enable.
-
HIC_MODE_DEVICE_HOST_ACCESS_ENABLE
0x400U¶ Host Access Enable.
-
HIC_MODE_HOST_WREALLOW_ENABLE
0x800U¶ Host EALLOW Write Enable.
-
HIC_PIN_POLARITY_CS_HIGH
0x1U¶ Active High Chip Select.
Values that can be passed to HIC_setPinPolarity() API as flags or used with HIC_getPinPolarity() API return value parsing
-
HIC_PIN_POLARITY_CS_LOW
0x0U¶ Active Low Chip Select.
-
HIC_PIN_POLARITY_BEN_HIGH
0x2U¶ Active High Byte Enable.
-
HIC_PIN_POLARITY_BEN_LOW
0x0U¶ Active Low Byte Enable.
-
HIC_PIN_POLARITY_OE_HIGH
0x4U¶ Active High Output Enable.
-
HIC_PIN_POLARITY_OE_LOW
0x0U¶ Active Low Output Enable.
-
HIC_PIN_POLARITY_WE_HIGH
0x8U¶ Active High Write Enable.
-
HIC_PIN_POLARITY_WE_LOW
0x0U¶ Active Low Write Enable.
-
HIC_PIN_POLARITY_RDY_HIGH
0x10U¶ Active High Ready Pin.
-
HIC_PIN_POLARITY_RDY_LOW
0x0U¶ Active Low Ready Pin.
-
HIC_HOST_CONTROL_EALLOW_EN
1U¶ Host EALLOW Enable.
Values that can be passed to HIC_configureHostAccessMode() API as config or used with HIC_getHostAccessMode() API return value parsing
-
HIC_HOST_CONTROL_EALLOW_DIS
0U¶ Host EALLOW Disable.
-
HIC_HOST_CONTROL_ACCSIZE_16BIT
0U¶ Device MMR Access size 16 bit.
-
HIC_HOST_CONTROL_ACCSIZE_32BIT
2U¶ Device MMR Access size 32 bit.
-
HIC_HOST_CONTROL_PAGESEL_REG
0U¶ Page selected via Register.
-
HIC_HOST_CONTROL_PAGESEL_PIN
4U¶ Page selected via Pin.
-
HIC_EVTTRIG_EVENT_0
0x010000U¶ EVTTRIG0.
Values that can be passed to HIC_enableD2HInterrupt() API or or used with HIC_disableD2HInterrupt() API to enable/disable interrupt or with HIC_clearD2HInterrupt() API to clear interrupt
-
HIC_EVTTRIG_EVENT_1
0x020000U¶ EVTTRIG1.
-
HIC_EVTTRIG_EVENT_2
0x040000U¶ EVTTRIG2.
-
HIC_EVTTRIG_EVENT_3
0x080000U¶ EVTTRIG3.
-
HIC_EVTTRIG_EVENT_4
0x100000U¶ EVTTRIG4.
-
HIC_EVTTRIG_EVENT_5
0x200000U¶ EVTTRIG5.
-
HIC_EVTTRIG_EVENT_6
0x400000U¶ EVTTRIG6.
-
HIC_EVTTRIG_EVENT_7
0x800000U¶ EVTTRIG7.
Functions
-
uint32_t
HIC_getRevision
(void)¶ Returns the Revision of HIC Controller interface.
This function returns the hardware revision of the Host Interface controller module
- Return
The Hardware Version number returns the content of HICREV register. Please refer to device TRM for field wise details.
-
void
HIC_enableHostInterface
(void)¶ Enables the Host Access to the Device region and to the Mailbox
The Host interface Controller module provides two mechanisms of access
Using Device Memory access, the host can access the memory directly read/write/poll for registers
Using the Mailbox mechanism which can be used when the Host can write the parameters to the mailbox Host-to-Device buffer region and then trigger an interrupt to the Device. The HIC module with the other application running on device side can then be used to signal to the host, using the Device-to-Host buffer region in response. This API enables the access to the Device region and Mailbox. This should be used as the first API in sequence of configuring the HIC module.
- Return
none
-
void
HIC_enableLock
(void)¶ Enables the Lock for the HIC module registers protected by Writes
This API enables the lock, which protects the writes to registers protected by Lock. Calling this API prevents writes to the write protected registers.
- Return
none
-
void
HIC_disableLock
(void)¶ Disables the Lock for the HIC module registers protected by Writes
This API disables the lock(unlocks), which enables the writes to registers protected by Lock. Calling this API enables writes to the write protected registers. This API must be called one time before calling any of these APIs
- Return
None
-
void
HIC_setConfig
(uint32_t flags)¶ Sets the Host Interface Controller Configurations
This API configures the HICMODECR register for the selected configuration
HIC_disableLock() API should have been called prior to this API.Any one of following values for Data Width
HIC_MODE_DW_8BIT -for 8bit Data
HIC_MODE_DW_16BIT -for 16bit Data
HIC_MODE_DW_32BIT -for 32bit Data
- Parameters
flags
: specifies the ORed values of any of following flags.
Any one of following values for Read Write Pin
HIC_MODE_RW_PIN_SEPARATE - for Separate Read and Write Pin
HIC_MODE_RW_PIN_SINGLE - for Same Read and Write Pin
Any one of following values for Byte Enable Pin configuration
HIC_MODE_BEN_PRESENT - for using Byte Enable Pin
HIC_MODE_BEN_ABSENT - for not using Byte Enable Pin
Any one of following values for Ready Pin
HIC_MODE_RDY_PRESENT - for using Ready Pin for extended wait
HIC_MODE_RDY_ABSENT - for not using Extended Wait pin
Other configurations:
HIC_MODE_H2DBUF_DEVWREN - for enabling Device access to host to Device Buffers. If this is not enabled the device cannot write to Host to Device buffers
HIC_MODE_D2HBUF_HOST_WR_ENABLE - for enabling host access to device to host buffers. If this is not enabled the host cannot write to device to host buffers.
HIC_MODE_DEVICE_HOST_ACCESS_ENABLE - for enabling access to the device region. Only if this is enabled the regions selected by Base select registers using the HIC_selectBaseAddress() API shall be accessible. Without this only the HIC registers and Mailbox registers will be accessible for the host.
HIC_MODE_HOST_WREALLOW_ENABLE - for enabling host access to write to EALLOW bitfield using HIC_configureHostAccessMode() API. Without enabling this HIC_configureHostAccessMode(HIC_HOSTCR_EALLOW_EN) will not work.
- Return
None
-
uint32_t
HIC_getConfig
(void)¶ Returns the Host Interface Controller Configurations
Following values for Other Configurations
HIC_MODE_RW_PIN_SEPARATE/ HIC_MODE_RW_PIN_SINGLE - for Read/Write Pin
HIC_MODE_BEN_PRESENT/HIC_MODE_BEN_ABSENT - for Byte Enable Pin Usage
HIC_MODE_RDY_PRESENT/HIC_MODE_RDY_ABSENT - for using Ready Pin for extended wait
HIC_MODE_H2DBUF_DEVWREN- Device access to Host to Device Buffer Enabled
HIC_MODE_D2HBUF_HOST_WR_ENABLE - Host access to Device to Host Buffer enabled
HIC_MODE_DEVICE_HOST_ACCESS_ENABLE - for enabling access to the device
HIC_MODE_HOST_WREALLOW_ENABLE - for host access to write to EALLOW
- Return
32-bit integer specifies the ORed values of following flags Any one of following values for Data Width
HIC_MODE_DW_8BIT -for 8bit Data
HIC_MODE_DW_16BIT -for 16bit Data
HIC_MODE_DW_32BIT -for 32bit Data
This API returns the current configuration of HIC module. It can be used along with macros defined in hw_hic.h as below. For querying the Data width use like in below examples HIC_getConfig() & HIC_MODECR_DW_MODE_M == HIC_MODE_DW_8BIT for Data width HIC_getConfig() & HIC_MODECR_RW_MODE == HIC_MODE_RW_PIN_SINGLE for RW Pin HIC_getConfig() & HIC_MODECR_BEN_PRESENT == HIC_MODE_BEN_PRESENT for BE Pin
-
void
HIC_setPinPolarity
(uint16_t flags)¶ Sets the Host Interface Controller Pin Polarity. This API configures the HICPINPOLCR register for the selected configuration. HIC_disableLock() API should have been called prior to this API.
Any one of following values for Chip Select Pin
HIC_PIN_POLARITY_CS_HIGH - for Active High Chip Select Pin
HIC_PIN_POLARITY_CS_LOW - for Active Low Chip Select Pin
- Parameters
flags
: specifies the ORed values of any of following flags
Any one of following values for Byte Enable Pin configuration
HIC_PIN_POLARITY_BEN_HIGH - for Active High Byte Enable
HIC_PIN_POLARITY_BEN_LOW - for Active Low Byte Enable
Any one of following values for Output Enable Pin
HIC_PIN_POLARITY_OE_HIGH - for Active High Output Enable
HIC_PIN_POLARITY_OE_LOW - for Active Low Output Enable
Any one of following values for Write Enable Pin
HIC_PIN_POLARITY_WE_HIGH - for Active High Write Enable
HIC_PIN_POLARITY_WE_LOW - for Active Low Write Enable
Any one of following values for Ready Pin
HIC_PIN_POLARITY_RDY_HIGH - for Active High Write Enable
HIC_PIN_POLARITY_RDY_LOW - for Active Low Write Enable
- Return
None
-
uint32_t
HIC_getPinPolarity
(void)¶ Returns the Host Interface Controller Pin Polarity Configurations
This API returns the HICPINPOLCR register for the selected configuration
This API returns the Pin Polarity.This can be used with the macros defined in
hw_hic.h as shown below HIC_getPinPolarity & HIC_PINPOLCR_BEN_POL == HIC_PIN_POLARITY_BEN_HIGH for checking the status of Byte Enable Pin Polarity- Return
32-bit integer specifies the ORed values of any of following flags Following values for corresponding Pin Configuration
HIC_PIN_POLARITY_CS_HIGH/ HIC_PIN_POLARITY_CS_HIGH - for CS Pin
HIC_PIN_POLARITY_BEN_HIGH/HIC_PIN_POLARITY_BEN_HIGH- for Byte Enable pin
HIC_PIN_POLARITY_OE_HIGH/HIC_PIN_POLARITY_OE_LOW - for OE Pin
HIC_PIN_POLARITY_WE_HIGH/HIC_PIN_POLARITY_WE_LOW- for WE Pin
HIC_PIN_POLARITY_RDY_HIGH/HIC_PIN_POLARITY_RDY_LOW - for RDY Pin
-
void
HIC_selectBaseAddress
(uint16_t selectIndex)¶ Selects the Base Address for the device memory access
The Device memory region will be accessible by the region selected in this API. Also look at HIC_configureHostAccessMode(HIC_HOSTCR_PAGESEL)
- Parameters
selectIndex
: specifies the index of Base address in the Base Address regions can vary from 0 to HIC_NUM_BASE_ADDRESS-1
- Return
None
-
uint16_t
HIC_getSelectedBaseAddressIndex
(void)¶ Returns the Selected Base address index for the device memory access
The Device memory region will be accessible by the region selected in this API. Also look at HIC_configureHostAccessMode(HIC_HOSTCR_PAGESEL)
- Return
selected index of Base address in the Base Address regions. can vary from 0 to HIC_NUM_BASE_ADDRESS-1
-
void
HIC_configureHostAccessMode
(uint16_t config)¶ Configures the Host Access modes to the device region
- Return
None
- Parameters
config
: logical OR of the following valuesHIC_HOSTCR_EALLOW_EN for enabling module writes to EALLOW Protected registers
either of HIC_HOST_CONTROL_ACCSIZE_16BIT/HIC_HOST_CONTROL_ACCSIZE_32BIT to select 16 bit or 32 bit device side master port accesses
either of HIC_HOST_CONTROL_PAGESEL_REG/HIC_HOST_CONTROL_PAGESEL_PIN to select Page/Region selection based on PAGESEL register programmed using HIC_selectBaseAddress()API or the PAGESEL Pin
-
uint32_t
HIC_getHostAccessMode
(void)¶ Provides the Host Access modes configured currently
This API can be used with few Macros defined in
hw_hic.h as below (HIC_getAccessMode() & HIC_HOSTCR_ACCSIZE) == HIC_HOST_CONTROL_ACCSIZE_32BIT for Access size checking. Similarly it can be used for other bit fields.- Return
Host Access mode value as configured HIC_configureHostAccessMode() API which is a logical OR of
HIC_HOSTCR_EALLOW_EN for enabling module writes to EALLOW Protected registers
either of HIC_HOST_CONTROL_ACCSIZE_16BIT/HIC_HOST_CONTROL_ACCSIZE_32BIT for selected 16 bit or 32 bit device side master port accesses
either of HIC_HOST_CONTROL_PAGESEL_REG/HIC_HOST_CONTROL_PAGESEL_PIN for selected Page/Region selection based on PAGESEL register programmed using HIC_selectBaseAddress()API or the PAGESEL Pin
-
uint32_t
HIC_getErrorAddress
(void)¶ Returns the Host and Device side Status when an Error happened on interface
- Return
returns the logical OR of the following
8 bit Host to Device Error Address when Host to Device Error happens
3 bit Base select value when Host to Device Error happens
8 bit Device to Host Error Address when Device to Host Error happens
3 bit Base select value when Device to Host Error Happens.
Please refer to TRM HICERRADDR register for more details on this.
-
uint32_t
HIC_getH2DToken
(void)¶ Returns the token written by the token written onto the Host to Device Token
This API can be used while using the Mailbox mechanism.
- Return
the 32 bit Token value written into the register
-
void
HIC_setD2HToken
(uint32_t token)¶ Writes the Token to the Host from Device
This API can be used while using the Mailbox mechanism. Writing to this register could be used to trigger an interrupt to the Host using the Device to Host interrupt line(D2HINT) of the module. It can be used to interrupt the external host.
- Return
None
- Parameters
token
: is the 32 bit token value to be written. It could be used to denote the number of bytes written on to the Device-to-Host buffer
-
uint32_t
HIC_getD2HToken
(void)¶ Returns the token written by the token written onto the Device to Host Token
This API can be used while using the Mailbox mechanism.
- Return
the 32 bit Token value written into the register
-
void
HIC_setBaseAddress
(uint16_t index, uint32_t baseAddress)¶ Configures the Base Address of the region
The device memory which HIC module can access can be divided into multiple 256 byte regions. For Example: GSRAM in Region 0, ADC registers in Region 1 FSI registers in Region 2,etc This API helps to configure the base address for each region The HIC address Pin can then be used to offset into the specific region by the host
- Parameters
index
: specifies the index of the Device Region to be configured can be from 0 to HIC_NUM_BASE_ADDRESS-1baseAddress
: the 32 bit base address of the device region being configured
- Return
None
-
uint32_t
HIC_getBaseAddress
(uint16_t index)¶ Returns the Base Address configured for the region
Returns the configured base address for the Region index provided
- Parameters
index
: specifies the index of the Device Region to be configured can be from 0 to HIC_NUM_BASE_ADDRESS-1
- Return
32 bit base address configured for the region
-
void
HIC_enableH2DInterrupt
(uint32_t flags)¶ Enables the Interrupts from Host to Device
Enables the specified interrupts. This will result in a HIC interrupt generated to the C28x core.
- Parameters
flags
: specifies the logical ORed values belowHIC_H2DINTEN_H2D_INTEN - Data Ready interrupt Enable
HIC_H2DINTEN_BUSERR_INTEN - Bus error Interrupt Enable
HIC_H2DINTEN_ILLWR_INTEN - Illegal Write Interrupt Enable
HIC_H2DINTEN_ILLRD_INTEN - Illegal Read Interrupt Enable
- Return
None
-
void
HIC_disableH2DInterrupt
(uint32_t flags)¶ Disables the Interrupts from Host to Device
Disables the interrupt flags specified
- Parameters
flags
: specifies the logical ORed values belowHIC_H2DINTEN_H2D_INTEN - Data Ready interrupt Enable
HIC_H2DINTEN_BUSERR_INTEN - Bus error Interrupt Enable
HIC_H2DINTEN_ILLWR_INTEN - Illegal Write Interrupt Enable
HIC_H2DINTEN_ILLRD_INTEN - Illegal Read Interrupt Enable
- Return
None
-
uint32_t
HIC_getH2DInterruptStatus
(void)¶ Gives the status of Host to Device interrupts
The Flag if Set indicates that the corresponding Interrupt is active (has occured)
- Return
32bit flag with the logical ORed values below
HIC_H2DINTFLG_H2D_FLG - Data Ready interrupt Status
HIC_H2DINTFLG_BUSERR_FLG - Bus error Interrupt Status
HIC_H2DINTFLG_ILLWR_FLG - Illegal Write Interrupt Status
HIC_H2DINTFLG_ILLRD_FLG - Illegal Read Interrupt Status.
-
void
HIC_clearH2DInterrupt
(uint32_t flags)¶ Clears the Interrupts from Host to Device
Clears the interrupt flags specified
- Parameters
flags
: specifies the logical ORed values below to be clearedHIC_H2DINTCLR_H2D_CLR - Data Ready interrupt Clear
HIC_H2DINTCLR_BUSERR_CLR - Bus error Interrupt Clear
HIC_H2DINTCLR_ILLWR_CLR - Illegal Write Interrupt Clear
HIC_H2DINTCLR_ILLRD_CLR - Illegal Read Interrupt Clear
- Return
None
-
void
HIC_forceH2DInterrupt
(uint32_t flags)¶ Forces the Interrupts from Host to Device
Forces the interrupt flags specified. Can be used for Debug purpose.
- Parameters
flags
: specifies the logical ORed values below to be ForcedHIC_H2DINTFRC_H2D_INTFRC - Data Ready interrupt Force
HIC_H2DINTFRC_BUSERR_INTFRC - Bus error Interrupt Force
HIC_H2DINTFRC_ILLWR_INTFRC - Illegal Write Interrupt Force
HIC_H2DINTFRC_ILLRD_INTFRC - Illegal Read Interrupt Force
- Return
None
-
void
HIC_enableD2HInterrupt
(uint32_t flags)¶ Enables the Interrupts from Device to Host
Enables the specified interrupts. This will result in a HIC interrupt generated to the Host(D2HINT).
- Parameters
flags
: specifies the logical ORed values belowHIC_D2HINTEN_D2H_INTEN - Data Ready interrupt Enable
HIC_D2HINTEN_BUSERR_INTEN - Bus error Interrupt Enable
HIC_D2HINTEN_ILLWR_INTEN - Illegal Write Interrupt Enable
HIC_D2HINTEN_ILLRD_INTEN - Illegal Read Interrupt Enable
HIC_D2HINTEN_ACCVIO_INTEN - Access Violation Interrupt Enable
Event Trigger interrupt flags - The higher 16 bits when Set will enable corresponding D2H interrupts. Refer TRM for details.
- Return
None
-
void
HIC_disableD2HInterrupt
(uint32_t flags)¶ Disables the Interrupts from Device to Host
Disables the interrupt flags specified
- Parameters
flags
: specifies the logical ORed values belowHIC_D2HINTEN_D2H_INTEN - Data Ready interrupt Enable
HIC_D2HINTEN_BUSERR_INTEN - Bus error Interrupt Enable
HIC_D2HINTEN_ILLWR_INTEN - Illegal Write Interrupt Enable
HIC_D2HINTEN_ILLRD_INTEN - Illegal Read Interrupt Enable
HIC_D2HINTEN_ACCVIO_INTEN - Access Violation Interrupt Enable
Event Trigger interrupt flags - The higher 16 bits when set will disable corresponding D2H interrupts. Refer TRM for details.
- Return
None
-
uint32_t
HIC_getD2HInterruptStatus
(void)¶ Gives the status of Device to Host interrupts
- Return
32bit flag with the logical ORed values below
HIC_D2HINTFLG_D2H_FLG - Data Ready interrupt Status
HIC_D2HINTFLG_BUSERR_FLG - Bus error Interrupt Status
HIC_D2HINTFLG_ILLWR_FLG - Illegal Write Interrupt Status
HIC_D2HINTFLG_ILLRD_FLG - Illegal Read Interrupt Status
HIC_D2HINTFLG_ACCVIO_FLG - Access Violation Interrupt Status
Event Trigger Interrupt Flags - The higher 16 bits give the status of event Trigger Interrupt flags. Refer TRM for the sources of these interrupts.
The Flag if Set indicates that the corresponding Interrupt is active (has occurred)
-
void
HIC_clearD2HInterrupt
(uint32_t flags)¶ Clears the Interrupts from Host to Device
Clears the interrupt flags specified
- Parameters
flags
: specifies the logical ORed values below to be clearedHIC_D2HINTCLR_D2H_CLR - Data Ready interrupt Clear
HIC_D2HINTCLR_BUSERR_CLR - Bus error Interrupt Clear
HIC_D2HINTCLR_ILLWR_CLR - Illegal Write Interrupt Clear
HIC_D2HINTCLR_ILLRD_CLR - Illegal Read Interrupt Clear
HIC_D2HINTCLR_ACCVIO_CLR - Access Violation Interrupt Clear
Event Trigger Interrupt Clear Flags - The higher 16 bits indicates event trigger flags to be cleared. Refer TRM for the sources of these interrupts.
- Return
None
-
void
HIC_forceD2HInterrupt
(uint32_t flags)¶ Forces the Interrupts from Host to Device
Forces the interrupt flags specified. Can be used for Debug purposes.
- Parameters
flags
: specifies the logical ORed values below to be ForcedHIC_D2HINTFRC_D2H_INTFRC - Data Ready interrupt Force
HIC_D2HINTFRC_BUSERR_INTFRC - Bus error Interrupt Force
HIC_D2HINTFRC_ILLWR_INTFRC - Illegal Write Interrupt Force
HIC_D2HINTFRC_ILLRD_INTFRC - Illegal Read Interrupt Force
HIC_D2HINTFRC_ACCVIO_INTFRC - Access violation Interrupt Force
Event Trigger Interrupt Force Flags - The higher 16 bits indicates event trigger flags to be cleared. Refer TRM for the sources of these interrupts.
- Return
None
-
uint32_t
HIC_getAccessViolationAddress
(void)¶ Returns the Address when Access violation happened
While the HIC module internal access port accesses a memory, if there is an access violation, the module updates the address in this register.
- Return
returns the 32 bit address when the Access violation happened
-
uint32_t
HIC_readH2DBuffer
(uint16_t offset)¶ Returns the Host to Device Buffer for the offset specified
The Host to Device buffer can be used to implement a communication scheme on which the Host writes the data to sent to the Control peripherals. The MCU can pick it up and stream it over control peripherals. The Device to Host Buffer can be used to write the response back. The External host need not continuously wait for the data/response.
- Return
returns the 32 bit content of the Host to Device buffer.
- Parameters
offset
: specifies the offset of the H2D buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1
-
void
HIC_writeH2DBuffer
(uint16_t offset, uint32_t data)¶ Writes to the Host to Device buffer
This API should be used only when the Device write to Host buffer is enabled, using HIC_setConfig(HIC_MODECR_H2DBUF_DEVWREN) API.
- Return
none
- Parameters
offset
: specifies the offset of the H2D buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1data
: the 32bit data to be written onto the buffer
-
void
HIC_clearH2DBuffer
(uint16_t offset)¶ Clears the Host to Device buffer (by making it Zero)
This API should be used only when the Device write to Host buffer is enabled, using HIC_setConfig(HIC_MODECR_H2DBUF_DEVWREN) API. This API can be used to clear the content of H2D Buffer
- Return
none
- Parameters
offset
: specifies the offset of the H2D buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1
-
uint32_t
HIC_readD2HBuffer
(uint16_t offset)¶ Returns the Device to Host Buffer for the offset specified
The Device to Host Buffer can be used to write the response back to host The External host need not continuously wait for the data/response.
- Return
returns the 32 bit content of the Device to Host buffer
- Parameters
offset
: specifies the offset of the D2H buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1
-
void
HIC_writeD2HBuffer
(uint16_t offset, uint32_t data)¶ Writes to the Device to Host buffer
- Return
none
- Parameters
offset
: specifies the offset of the D2H buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1data
: the 32bit data to be written onto the buffer
-
void
HIC_clearD2HBuffer
(uint16_t offset)¶ Clears the Device to Host buffer (by making it Zero)
This API can be used to clear the content of D2H Buffer
- Return
none
- Parameters
offset
: specifies the offset of the D2H buffer can vary from 0 to HIC_NUM_BUFFER_REGS-1
-
The code for this module is contained in driverlib/hic.h containing the API declarations for use by applications.