DCSM Module¶
The DCSM driver accesses the DCSM COMMON registers. In order to configure the Dual Code Security Module, the user must program the Linkpointer in DCSM OTP as well as the security configuration registers of the Zone Select Blocks in DCSM OTP. The DCSM driver provides functions which secure and unsecure each zone and return the ownership, security status, EXEONLY status of specific RAM modules or Flash sectors. Included are two functions which can claim and release the Flash pump to operate on a specific zone.
-
group
dcsm_api
Defines
-
DCSM_O_Z1_CSMPSWD0
0x08U¶ Z1 CSMPSWD0 offset.
-
DCSM_O_Z1_CSMPSWD1
0x0AU¶ Z1 CSMPSWD1 offset.
-
DCSM_O_Z1_CSMPSWD2
0x0CU¶ Z1 CSMPSWD2 offset.
-
DCSM_O_Z1_CSMPSWD3
0x0EU¶ Z1 CSMPSWD3 offset.
-
DCSM_O_Z2_CSMPSWD0
0x08U¶ Z2 CSMPSWD0 offset.
-
DCSM_O_Z2_CSMPSWD1
0x0AU¶ Z2 CSMPSWD1 offset.
-
DCSM_O_Z2_CSMPSWD2
0x0CU¶ Z2 CSMPSWD2 offset.
-
DCSM_O_Z2_CSMPSWD3
0x0EU¶ Z2 CSMPSWD3 offset.
-
FLSEM_KEY
0xA5U¶ Zone semaphore key.
-
DCSM_ALLZERO
0x08U¶ CSM Passwords all zeros.
-
DCSM_ALLONE
0x10U¶ CSM Passwords all ones.
-
DCSM_UNSECURE
0x20U¶ Zone is secure/unsecure.
-
DCSM_ARMED
0x40U¶ CSM is armed.
Enums
-
enum
DCSM_MemoryStatus
¶ Values to distinguish the status of RAM or FLASH sectors. These values describe which zone the memory location belongs too. These values can be returned from DCSM_getRAMZone(), DCSM_getFlashSectorZone().
Values:
-
enumerator
DCSM_MEMORY_INACCESSIBLE
¶ Inaccessible.
-
enumerator
DCSM_MEMORY_ZONE1
¶ Zone 1.
-
enumerator
DCSM_MEMORY_ZONE2
¶ Zone 2.
-
enumerator
DCSM_MEMORY_FULL_ACCESS
¶ Full access.
-
enumerator
-
enum
DCSM_SemaphoreZone
¶ Values to pass to DCSM_claimZoneSemaphore(). These values are used to describe the zone that can write to Flash Wrapper registers.
Values:
-
enumerator
DCSM_FLSEM_ZONE1
= 0x01U¶ Flash semaphore Zone 1.
-
enumerator
DCSM_FLSEM_ZONE2
= 0x02U¶ Flash semaphore Zone 2.
-
enumerator
-
enum
DCSM_SecurityStatus
¶ Values to distinguish the security status of the zones. These values can be returned from DCSM_getZone1CSMSecurityStatus(), DCSM_getZone2CSMSecurityStatus().
Values:
-
enumerator
DCSM_STATUS_SECURE
¶ Secure.
-
enumerator
DCSM_STATUS_UNSECURE
¶ Unsecure.
-
enumerator
DCSM_STATUS_LOCKED
¶ Locked.
-
enumerator
DCSM_STATUS_BLOCKED
¶ Blocked.
-
enumerator
-
enum
DCSM_EXEOnlyStatus
¶ Values to decribe the EXEONLY Status. These values are returned from to DCSM_getZone1RAMEXEStatus(), DCSM_getZone2RAMEXEStatus(), DCSM_getZone1FlashEXEStatus(), DCSM_getZone2FlashEXEStatus().
Values:
-
enumerator
DCSM_PROTECTED
¶ Protected.
-
enumerator
DCSM_UNPROTECTED
¶ Unprotected.
-
enumerator
DCSM_INCORRECT_ZONE
¶ Incorrect Zone.
-
enumerator
-
enum
DCSM_RAMModule
¶ Values to distinguish RAM Module. These values can be passed to DCSM_getZone1RAMEXEStatus() DCSM_getZone2RAMEXEStatus(), DCSM_getRAMZone().
Values:
-
enumerator
DCSM_RAMLS4
= 4¶ RAMLS4.
-
enumerator
DCSM_RAMLS5
= 5¶ RAMLS5.
-
enumerator
DCSM_RAMLS6
= 6¶ RAMLS6.
-
enumerator
DCSM_RAMLS7
= 7¶ RAMLS7.
-
enumerator
-
enum
DCSM_Sector
¶ Values to distinguish Flash Sector. These values can be passed to DCSM_getZone1FlashEXEStatus() DCSM_getZone2FlashEXEStatus(), DCSM_getFlashSectorZone().
Values:
-
enumerator
DCSM_BANK0_SECTOR0
¶ Bank 0 - Sector 0.
-
enumerator
DCSM_BANK0_SECTOR1
¶ Bank 0 - Sector 1.
-
enumerator
DCSM_BANK0_SECTOR2
¶ Bank 0 - Sector 2.
-
enumerator
DCSM_BANK0_SECTOR3
¶ Bank 0 - Sector 3.
-
enumerator
DCSM_BANK0_SECTOR4
¶ Bank 0 - Sector 4.
-
enumerator
DCSM_BANK0_SECTOR5
¶ Bank 0 - Sector 5.
-
enumerator
DCSM_BANK0_SECTOR6
¶ Bank 0 - Sector 6.
-
enumerator
DCSM_BANK0_SECTOR7
¶ Bank 0 - Sector 7.
-
enumerator
DCSM_BANK0_SECTOR8
¶ Bank 0 - Sector 8.
-
enumerator
DCSM_BANK0_SECTOR9
¶ Bank 0 - Sector 9.
-
enumerator
DCSM_BANK0_SECTOR10
¶ Bank 0 - Sector 10.
-
enumerator
DCSM_BANK0_SECTOR11
¶ Bank 0 - Sector 11.
-
enumerator
DCSM_BANK0_SECTOR12
¶ Bank 0 - Sector 12.
-
enumerator
DCSM_BANK0_SECTOR13
¶ Bank 0 - Sector 13.
-
enumerator
DCSM_BANK0_SECTOR14
¶ Bank 0 - Sector 14.
-
enumerator
DCSM_BANK0_SECTOR15
¶ Bank 0 - Sector 15.
-
enumerator
Functions
-
void
DCSM_secureZone1
(void)¶ Secures zone 1 by setting the FORCESEC bit of Z1_CR register
This function resets the state of the zone. If the zone is unlocked, it will lock (secure) the zone and also reset all the bits in the Control Register.
- Return
None.
-
void
DCSM_secureZone2
(void)¶ Secures zone 2 by setting the FORCESEC bit of Z2_CR register
This function resets the state of the zone. If the zone is unlocked, it will lock (secure) the zone and also reset all the bits in the Control Register.
- Return
None.
-
DCSM_SecurityStatus
DCSM_getZone1CSMSecurityStatus
(void)¶ Returns the CSM security status of zone 1
This function returns the security status of zone 1 CSM
- Return
Returns security status as an enumerated type DCSM_SecurityStatus.
-
DCSM_SecurityStatus
DCSM_getZone2CSMSecurityStatus
(void)¶ Returns the CSM security status of zone 2
This function returns the security status of zone 2 CSM
- Return
Returns security status as an enumerated type DCSM_SecurityStatus.
-
uint16_t
DCSM_getZone1ControlStatus
(void)¶ Returns the Control Status of zone 1
This function returns the Control Status of zone 1 CSM
- Return
Returns the contents of the Control Register which can be used with provided defines.
-
uint16_t
DCSM_getZone2ControlStatus
(void)¶ Returns the Control Status of zone 2
This function returns the Control Status of zone 2 CSM
- Return
Returns the contents of the Control Register which can be used with the provided defines.
-
DCSM_MemoryStatus
DCSM_getRAMZone
(DCSM_RAMModule module)¶ Returns the security zone a RAM section belongs to
This function returns the security zone a RAM section belongs to.
- Parameters
module
: is the RAM module value. Valid values are type DCSM_RAMModuleDCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMLS6
DCSM_RAMLS7
- Return
Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible, DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure).
-
DCSM_MemoryStatus
DCSM_getFlashSectorZone
(DCSM_Sector sector)¶ Returns the security zone a flash sector belongs to
This function returns the security zone a flash sector belongs to.
- Parameters
sector
: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible , DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure)..
-
uint32_t
DCSM_getZone1LinkPointerError
(void)¶ Read Zone 1 Link Pointer Error
A non-zero value indicates an error on the bit position that is set to 1.
- Return
Returns the value of the Zone 1 Link Pointer error.
-
uint32_t
DCSM_getZone2LinkPointerError
(void)¶ Read Zone 2 Link Pointer Error
A non-zero value indicates an error on the bit position that is set to 1.
- Return
Returns the value of the Zone 2 Link Pointer error.
-
bool
DCSM_getFlashErrorStatus
(void)¶ Get the status of the security configuration load from USER-OTP or sector error status
- Return
Returns 0 if no error in loading security information from USER-OTP, 1 if an error has occurred in the load from USER-OTP.
-
void
DCSM_clearFlashErrorStatus
(void)¶ Clear the Flash Error Status bit
Write a ‘1’ to the clear bit to clear the sector error status bit.
- Return
None.
-
void
DCSM_forceFlashErrorStatus
(void)¶ Set the force Flash Error Status bit
Write a ‘1’ to force bit to set the sector error status bit.
- Return
None.
-
void
DCSM_unlockZone1CSM
(const DCSM_CSMPasswordKey *const psCMDKey)¶ Unlocks Zone 1 CSM.
This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers
- Parameters
psCMDKey
: is a pointer to the DCSM_CSMPasswordKey struct that has the CSM password for zone 1.
- Return
None.
-
void
DCSM_unlockZone2CSM
(const DCSM_CSMPasswordKey *const psCMDKey)¶ Unlocks Zone 2 CSM.
This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers
- Parameters
psCMDKey
: is a pointer to the CSMPSWDKEY that has the CSM password for zone 2.
- Return
None.
-
DCSM_EXEOnlyStatus
DCSM_getZone1FlashEXEStatus
(DCSM_Sector sector)¶ Returns the EXE-ONLY status of zone 1 for a flash sector
This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.
- Parameters
sector
: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone1RAMEXEStatus
(DCSM_RAMModule module)¶ Returns the EXE-ONLY status of zone 1 for a RAM module
This function takes in a valid module value and returns the status of EXE ONLY security protection for that module.
- Parameters
module
: is the RAM module value. Valid values are type DCSM_RAMModuleDCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMLS6
DCSM_RAMLS7
- Return
Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone2FlashEXEStatus
(DCSM_Sector sector)¶ Returns the EXE-ONLY status of zone 2 for a flash sector
This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.
- Parameters
sector
: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone2RAMEXEStatus
(DCSM_RAMModule module)¶ Returns the EXE-ONLY status of zone 2 for a RAM module
This function takes in a valid module value and returns the status of EXE ONLY security protection for that module.
- Parameters
module
: is the RAM module value. Valid values are type DCSM_RAMModuleDCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMLS6
DCSM_RAMLS7
- Return
Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.
-
bool
DCSM_claimZoneSemaphore
(DCSM_SemaphoreZone zone)¶ Claims the zone semaphore which allows access to the Flash Wrapper register for that zone.
- Return
Returns true for a successful semaphore capture, false if it was unable to capture the semaphore.
- Parameters
zone
: is the zone which is trying to claim the semaphore which allows access to the Flash Wrapper registers.
-
bool
DCSM_releaseZoneSemaphore
(void)¶ Releases the zone semaphore.
- Return
Returns true if was successful in releasing the zone semaphore and false if it was unsuccessful in releasing the zone semaphore.
- Note
If the calling function is not in the right zone to be able to access this register, it will return a false.
-
struct
DCSM_CSMPasswordKey
¶ - #include <dcsm.h>
Data structures to hold password keys.
-
The code for this module is contained in driverlib/dcsm.c, with driverlib/dcsm.h containing the API declarations for use by applications.