SimpleLink MCU SDK Driver APIs
tidrivers_msp43x_3_01_01_03
|
SDSPIMSP432 Hardware attributes. More...
#include <SDSPIMSP432.h>
SDSPIMSP432 Hardware attributes.
The SDSPIMSP432 HWAttrs configuration structure contains SPI peripheral and GPIO Pin details required by the SDSPIMSP432 driver implementation.
The SDSPIMSP432 driver uses this information to:
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in:
An example configuration structure could look as the following: