Build date: 07152016
Release Information
Click on the links in the table below to download.
TI has partnered with SOMNIUM Technologies to bring you a new and fully supported open source compiler. This free MSP430 GCC compiler has no code size limit.
This compiler can be used as a standalone or can be integrated in Code Composer Studio.
The MSP430-GCC 4.1.0.0 standalone package based on GCC compiler to 5.3.0 (msp430-gcc 5.3.0.219) is the first release as maintained by SOMNIUM Technologies.
Changes in This Release
- Updated GCC compiler to 5.3.0.219 (SOMNIUM)
- First release as maintained by SOMNIUM Technologies
- Update MSP430 support files to 1.191
- Components version
- GCC 5.3.0.219
- GDB 7.7
- binutils 2.25
- Newlib 2.2.0
- MSPDebugStack 3.8.0.2
- MSP430 GDB Agent 6.0.228.0
- Updated GCC compiler to 5.3.0 (buildid 219)
- 5.3.0 patches applied
- The toolchain has been built from the upstream release branches, with several patches backported from upstream mainline branches.
- Newlib has been configured to use nano-formatted-io (refer to newlib/README for more details).
- GCC and binutils MSP430 device information has been updated to reflect the latest version of devices.csv.
- Fixed bug: DWARF error with -mhwmult=f5series
- Updated support files
- Added device support:
MSP430FR2111 and MSP430FR2110
- Added missing register definition macros to iomacros.h for GCC
- Added missing __MSP430_HAS_P*SEL__ definitions in F1xx/F2xx/F4xx headers
- Fixed typo in GCC linker files
- Fixed debug_line option in GCC linker files for smaller memory devices
- Added SIGNATURE sections in GCC linker command files
- Removed invalid code from generic GCC symbol files
- Added silicon errata switches to GCC compiler options in CCS device XMLs
- Added missing register separator comments in header files for newer MSP430s
- Added missing alternate register definitions (RTCCNT) for devices with RTC_C
- Corrected TLV address offsets in header files for G2xx/F2xx devices
Known Issues
- The MSP430FR4133 is currently not fully supported by GDB + GDB Agent.
- When running the GNU debugger on Microsoft Windows, pressing Ctrl-C may terminate the debugger.
- The GDB Agent is not able to connect to MSP430L092 target devices.
- The GDB Agent is not able to connect to RF430FRL15xH target devices.
Older Releases
Releases maintained by Red Hat
- 4_00_01_00 MSP430 Debug Stack, compiler, support files
- 4_00_00_900 Initial release (GCC 5.2.1 build 50, beta)
- 3_05_00_00 MSP430 Debug Stack, compiler, support files
- 3_04_05_01 MSP430 Debug Stack, compiler, support files
- 3_04_05_00 MSP430 Debug Stack, compiler, support files
- 3_03_04_00 MSP430 Debug Stack, compiler, support files
- 3_02_03_00 MSP430 Debug Stack, compiler, support files
- 3_02_02_00 MSP430 Debug Stack, compiler, support files
- 2_01_01_00 MSP430 Debug Stack update and compiler
- 2_00_00_00 Version 14r1-10, first official production release
- 1_01_00_00 Version 371, beta
- 1_00_01_00 Minor update - source code only (version 317, beta)
- 1_00_00_00 Initial release (version 271, beta)
Get started today in Windows, Linux or Mac OS X environments!
MSP430-GCC Product downloads
Legend
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.
For more information