Release Information
Click on the links in the table below to download.
z:\gcc.html
TI has partnered with Red Hat to bring you a new and fully supported open
source compiler. This free GCC compiler has no code size limit. In
addition, this compiler can be used standalone or selected within Code Composer 6.0 (beta).
Date
2014-11-20
Key Changes in This Release
- Fixed loading of program into GDB with function in high memory.
- Fixed BISX.A opcode syntax error
- Includes MSPDebugStack v3.4.3.4:
- New device support:
RF430FRL152H, RF430FRL153H, RF430FRL154H
MSP430FR6972, MSP430FR6970, MSP430FR6922, MSP430FR6920, MSP430FR6872, MSP430FR6870, MSP430FR6822, MSP430FR6820, MSP430FR5972, MSP430FR5970, MSP430FR5872, MSP430FR5870
- Changes:
Advanced hardware cycle counter support
Hardware cycle counters can be freely configured
Support both cycle counters where available
Software breakpoints support when MPU is enabled
- Bug Fixes:
Fixed eZ-FET LED signaling - not according to specification for over-current detection
Fixed secure device message - Report "Security Fuse has been blown" instead of "Unknown device"
Fixed endianness in IntelHex offset record
Fixed clock control module names for MSP430FR413x
Fixed accidentally changing WDT interval on sync
Fixed secure device for MSP430FR413x
Fixed SendJtag mailbox function - Send pattern while Reset line is low
Fixed ResetXv2 function - Send pattern while Reset line is low
Fixed Erase for password protected FRAM devices - do segment erase from 0xFF80 to 0x10000 on all FRAM devices to erase the password and the Reset vector to prevent code execution and to disable the password protection
Fixed possible deadlock in MSP430_Close function
Fixed Reset function for MSP430F5438 non A devices. Mailbox is not functional in Reset state on this device
- Header & Support File Changes:
Remove legacy NACCESSx definitions from Havok/Wolverine header files
New command files place .text into FLASH2 first, breaking small code model apps
Support for TinyRAM
MSP430F5217 Port 7 defines added
Added .infomem sections in GCC linker files
Improved support for large memory devices
Known Issues
- The MSP430FR4133 (Gradon) is currently not fully supported by GDB + GDB Agent.
- When running the GNU debugger on Microsoft Windows, pressing Ctrl-C may terminate the debugger.
- The GDB Agent is not able to connect to MSP430L092 target devices.
- The GDB Agent is not able to connect to RF430FRL15xH target devices.
Older Releases
1_00_00_00 Initial release (version 271, beta)
1_00_01_00 Minor update - source code only (version 317, beta)
1_01_00_00 Version 371, beta
2_00_00_00 Version 14r1-10, first official production release
2_01_01_00 MSP430 Debug Stack update and compiler
Get started today in Windows or Linux environments!
Legend
 |
Fill in Form. Approved users receive download URL in 1 minute. |
|
 |
Fill in Form. TI will contact you in 1-2+ business days. |
|