TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_16_00_08
Data Structures
Here are the data structures with brief descriptions:
 CCamera_ConfigCamera Global configuration
 CCamera_FxnTableThe definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation
 CCamera_ParamsCamera Parameters
 CClockP_FreqHzFrequency-in-hertz struct
 CClockP_ParamsBasic ClockP Parameters
 CCryptoCC26XX_AESCCM_TransactionCryptoCC26XX AES-CCM Transaction
 CCryptoCC26XX_AESECB_TransactionCryptoCC26XX AES-ECB Transaction
 CCryptoCC26XX_ConfigCryptoCC26XX Global Configuration
 CCryptoCC26XX_HWAttrsCryptoCC26XX Hardware Attributes
 CCryptoCC26XX_ObjectCryptoCC26XX Object
 CCryptoCC26XX_ParamsCryptoCC26XX Parameters
 CCryptoCC26XX_TransactionCryptoCC26XX Transaction
 CDIR
 Cdiskio_fxns
 CDisplay_ConfigDisplay Global configuration
 CDisplay_FxnTableThe definition of a Display function table that contains the required set of functions to control a specific Display driver implementation
 CDisplay_ParamsDisplay Parameters
 CDisplayDogm1286_HWAttrs
 CDisplayDogm1286_Object
 CDisplayGrLib_Object
 CDisplayLog_Object
 CDisplaySharp_HWAttrs
 CDisplaySharp_Object
 CDisplaySharpColor_tForeground and background color struct, compatible with GrLib
 CDisplayUart_HWAttrs
 CDisplayUart_Object
 CEMAC_ConfigEMAC Global configuration
 CEMAC_FxnTableEMAC Function table structure
 CExtFlashInfo_t
 CFATFS
 CFIL
 CFILINFO
 CGPIOCC26XX_ConfigGPIO device specific driver configuration structure
 CHwiP_ParamsBasic HwiP Parameters
 CI2C_ConfigI2C Global configuration
 CI2C_FxnTableThe definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation
 CI2C_ParamsI2C Parameters
 CI2C_TransactionI2C transaction
 CI2CCC26XX_HWAttrsV1I2CCC26XX Hardware attributes
 CI2CCC26XX_I2CPinCfgI2CCC26XX Pin Configuration
 CI2CCC26XX_ObjectI2CCC26XX Object
 CI2S_BufDescI2S buffer descriptor for issue/reclaim mode
 CI2S_ConfigI2S Global configuration
 CI2S_FxnTableThe definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation
 CI2S_ParamsBasic I2S Parameters
 CLCD_BufferLCD_Buffer used to store data to be printed on the LCD display
 CLCD_CommandFormat of LCD commands used by the LCD controller
 CLCD_ConfigThe LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation
 CLCD_HWAttrsLCD Hardware attributes
 CLCD_ObjectLCD Object
 CLCD_ParamsLCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init()
 CList_Elem
 CList_List
 CMutexP_ParamsBasic MutexP Parameters
 CNVS_AttrsNVS attributes
 CNVS_ConfigNVS Global configuration
 CNVS_FxnTableThe definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation
 CNVS_ParamsNVS Parameters
 CNVSCC26XX_CmdSetCopyBlockArgsNVSCC26XX command structure for setting copy block
 CNVSCC26XX_HWAttrsNVSCC26XX attributes
 CNVSCC26XX_Object
 CPDMCC26XX_BufferRequestA PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer()
 CPDMCC26XX_ConfigThe PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation
 CPDMCC26XX_HWAttrsPDMCC26XX Hardware attributes
 CPDMCC26XX_I2S_AudioClockConfigPDMCC26XX_I2S Audio Clock configuration
 CPDMCC26XX_I2S_AudioFormatConfigPDMCC26XX_I2S Hardware configuration
 CPDMCC26XX_I2S_AudioPinConfigPDMCC26XX_I2S Audio Pin configuration
 CPDMCC26XX_I2S_BufferReleaseA PDMCC26XX_I2S_BufferRelease data structure is used with PDMCC26XX_I2S_releaseBuffer()
 CPDMCC26XX_I2S_BufferRequestA PDMCC26XX_I2S_BufferRequest data structure is used with PDMCC26XX_I2S_requestBuffer()
 CPDMCC26XX_I2S_ConfigThe PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation
 CPDMCC26XX_I2S_HWAttrsPDMCC26XX_I2S Hardware attributes
 CPDMCC26XX_I2S_ObjectPDMCC26XX_I2S Object
 CPDMCC26XX_I2S_ParamsPDMCC26XX I2S Parameters are used when calling PDMCC26XX_I2S_open()
 CPDMCC26XX_I2S_StreamNotificationA PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors
 CPDMCC26XX_metaDataMetadata associated with an array of PCM data
 CPDMCC26XX_ObjectPDMCC26XX Object
 CPDMCC26XX_ParamsPDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init()
 CPDMCC26XX_pcmBufferPCM buffer pointed to in a PDMCC26XX_BufferRequest
 CPDMCC26XX_StreamNotificationA PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors
 CPIN_State_sUnderlying data structure for type PIN_State
 CPINCC26XX_HWAttrsPINCC26XX Hardware attributes
 CPower_NotifyObjPower notify object structure
 CPowerCC26XX_ConfigGlobal configuration structure
 CPowerCC26XX_ModuleStateInternal module state
 CPowerCC26XX_ResourceRecordPower resource database record format
 CPWM_ConfigPWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMTimerCC26XX_HWAttrsPWMTimerCC26XX Hardware attributes
 CPWMTimerCC26XX_ObjectPWMTimerCC26XX Object
 CPWMTimerCC26XX_PWMPinCfgPWMTimerCC26XX PWM Pin Configuration
 CRF_InfoValRF_getParamsVal used to input and return RF driver paramters with RF_getParams()
 CRF_ModeStruct defining operating mode of RF driver
 CRF_ObjectStruct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver
 CRF_ParamsRF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call
 CRF_RadioSetupUnion of the different flavors of RADIO_SETUP commands
 CRFCC26XX_HWAttrsRF Hardware attributes
 CRingBuf_Object
 CSDSPI_ConfigSDSPI Global configuration
 CSDSPI_FxnTableThe definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation
 CSDSPI_ParamsSDSPI Parameters
 CSemaphoreP_ParamsBasic SemaphoreP Parameters
 CSPI_ConfigSPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 CSPICC26XXDMA_HWAttrsV1SPICC26XXDMA Hardware attributes
 CSPICC26XXDMA_ObjectSPICC26XXDMA Object
 CtContext
 CtDisplayThis structure defines the characteristics of a display driver
 CtDisplayFxnsThis structure defines the implementation of a display driver
 CtFontThis structure describes a font used for drawing text onto the screen
 CtFontEx
 CtImageThis structure defines the characteristics of a Bitmap Image
 CtRectangle
 CUART_ConfigUART Global configuration
 CUART_FxnTableThe definition of a UART function table that contains the required set of functions to control a specific UART driver implementation
 CUART_ParamsUART Parameters
 CUARTCC26XX_HWAttrsV1UARTCC26XX Hardware attributes
 CUARTCC26XX_ObjectUARTCC26XX Object
 CUDMACC26XX_ConfigUDMACC26XX Global configuration
 CUDMACC26XX_HWAttrsUDMACC26XX hardware attributes
 CUDMACC26XX_ObjectUDMACC26XX object
 CUSBMSCHFatFs_ConfigUSBMSCHFatFs Global configuration
 CUSBMSCHFatFs_FxnTableThe definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation
 CUSBMSCHFatFs_ParamsUSBMSCHFatFs Parameters
 CWatchdog_ConfigWatchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWiFi_ConfigWiFi Global configuration
 CWiFi_FxnTableThe definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation
 CWiFi_ParamsWiFi Parameters
Copyright 2016, Texas Instruments Incorporated