CaptureMSP432 Hardware Attributes. More...
#include <CaptureMSP432.h>
Data Fields | |
uint32_t | timerBaseAddress |
uint32_t | clockSource |
uint32_t | clockDivider |
uint32_t | capturePort |
uint32_t | intPriority |
CaptureMSP432 Hardware Attributes.
Capture hardware attributes that tell the CaptureMSP432 driver specific hardware configurations and interrupt/priority settings.
A sample structure is shown below:
uint32_t CaptureMSP432_HWAttrs::timerBaseAddress |
Specifies the base address of the Timer_A peripheral.
uint32_t CaptureMSP432_HWAttrs::clockSource |
Specifies the clock source for the Timer_A peripheral.
uint32_t CaptureMSP432_HWAttrs::clockDivider |
Specifies the divider applied to the clockSource.
uint32_t CaptureMSP432_HWAttrs::capturePort |
Predefined capture port and pin. The Timer_A peripheral used by this define should match that of timerBaseAddress.
uint32_t CaptureMSP432_HWAttrs::intPriority |
The interrupt priority.