![]() |
![]() |
Go to the source code of this file.
#define ROM_APITABLE ((unsigned long *)0x02000800) |
#define ROM_VERSION (ROM_APITABLE[0]) |
#define ROM_ADC14TABLE ((unsigned long *)(ROM_APITABLE[1])) |
#define ROM_AES256TABLE ((unsigned long *)(ROM_APITABLE[2])) |
#define ROM_COMPTABLE ((unsigned long *)(ROM_APITABLE[3])) |
#define ROM_CRC32TABLE ((unsigned long *)(ROM_APITABLE[4])) |
#define ROM_CSTABLE ((unsigned long *)(ROM_APITABLE[5])) |
#define ROM_DMATABLE ((unsigned long *)(ROM_APITABLE[6])) |
#define ROM_FLASHCTLTABLE ((unsigned long *)(ROM_APITABLE[7])) |
#define ROM_FPUTABLE ((unsigned long *)(ROM_APITABLE[8])) |
#define ROM_GPIOTABLE ((unsigned long *)(ROM_APITABLE[9])) |
#define ROM_I2CTABLE ((unsigned long *)(ROM_APITABLE[10])) |
#define ROM_INTTABLE ((unsigned long *)(ROM_APITABLE[11])) |
#define ROM_MPUTABLE ((unsigned long *)(ROM_APITABLE[12])) |
#define ROM_PCMTABLE ((unsigned long *)(ROM_APITABLE[13])) |
#define ROM_PMAPTABLE ((unsigned long *)(ROM_APITABLE[14])) |
#define ROM_PSSTABLE ((unsigned long *)(ROM_APITABLE[15])) |
#define ROM_REFTABLE ((unsigned long *)(ROM_APITABLE[16])) |
#define ROM_RESETCTLTABLE ((unsigned long *)(ROM_APITABLE[17])) |
#define ROM_RTCTABLE ((unsigned long *)(ROM_APITABLE[18])) |
#define ROM_SPITABLE ((unsigned long *)(ROM_APITABLE[19])) |
#define ROM_SYSCTLTABLE ((unsigned long *)(ROM_APITABLE[20])) |
#define ROM_SYSTICKTABLE ((unsigned long *)(ROM_APITABLE[21])) |
#define ROM_TIMER_ATABLE ((unsigned long *)(ROM_APITABLE[22])) |
#define ROM_TIMER32TABLE ((unsigned long *)(ROM_APITABLE[23])) |
#define ROM_UARTTABLE ((unsigned long *)(ROM_APITABLE[24])) |
#define ROM_WDTTABLE ((unsigned long *)(ROM_APITABLE[25])) |
#define ROM_SYSCTLATABLE ((unsigned long *)(ROM_APITABLE[26])) |
#define ROM_FLASHCTLATABLE ((unsigned long *)(ROM_APITABLE[27])) |
#define ROM_LCDFTABLE ((unsigned long *)(ROM_APITABLE[28])) |
#define TARGET_IS_MSP432P4XX_NEXT |
#define ROM_ADC14_enableModule ((void (*)(void))ROM_ADC14TABLE[0]) |
#define ROM_ADC14_disableModule ((bool (*)(void))ROM_ADC14TABLE[1]) |
#define ROM_ADC14_initModule |
#define ROM_ADC14_setResolution ((void (*)(uint32_t resolution))ROM_ADC14TABLE[3]) |
#define ROM_ADC14_getResolution ((uint_fast32_t (*)(void))ROM_ADC14TABLE[4]) |
#define ROM_ADC14_setSampleHoldTrigger |
#define ROM_ADC14_setSampleHoldTime |
#define ROM_ADC14_configureMultiSequenceMode |
#define ROM_ADC14_configureSingleSampleMode |
#define ROM_ADC14_enableConversion ((bool (*)(void))ROM_ADC14TABLE[9]) |
#define ROM_ADC14_disableConversion ((void (*)(void))ROM_ADC14TABLE[10]) |
#define ROM_ADC14_isBusy ((bool (*)(void))ROM_ADC14TABLE[11]) |
#define ROM_ADC14_configureConversionMemory |
#define ROM_ADC14_enableComparatorWindow |
#define ROM_ADC14_disableComparatorWindow ((bool (*)(uint32_t memorySelect))ROM_ADC14TABLE[14]) |
#define ROM_ADC14_setComparatorWindowValue |
#define ROM_ADC14_setResultFormat ((bool (*)(uint32_t resultFormat))ROM_ADC14TABLE[16]) |
#define ROM_ADC14_getResult ((uint_fast16_t (*)(uint32_t memorySelect))ROM_ADC14TABLE[17]) |
#define ROM_ADC14_getMultiSequenceResult ((void (*)(uint16_t* res))ROM_ADC14TABLE[18]) |
#define ROM_ADC14_getResultArray |
#define ROM_ADC14_enableReferenceBurst ((bool (*)(void))ROM_ADC14TABLE[20]) |
#define ROM_ADC14_disableReferenceBurst ((bool (*)(void))ROM_ADC14TABLE[21]) |
#define ROM_ADC14_setPowerMode ((bool (*)(uint32_t powerMode))ROM_ADC14TABLE[22]) |
#define ROM_ADC14_enableInterrupt ((void (*)(uint_fast64_t mask))ROM_ADC14TABLE[23]) |
#define ROM_ADC14_disableInterrupt ((void (*)(uint_fast64_t mask))ROM_ADC14TABLE[24]) |
#define ROM_ADC14_getInterruptStatus ((uint_fast64_t (*)(void))ROM_ADC14TABLE[25]) |
#define ROM_ADC14_getEnabledInterruptStatus ((uint_fast64_t (*)(void))ROM_ADC14TABLE[26]) |
#define ROM_ADC14_clearInterruptFlag ((void (*)(uint_fast64_t mask))ROM_ADC14TABLE[27]) |
#define ROM_ADC14_toggleConversionTrigger ((bool (*)(void))ROM_ADC14TABLE[28]) |
#define ROM_ADC14_enableSampleTimer ((bool (*)(uint32_t multiSampleConvert))ROM_ADC14TABLE[29]) |
#define ROM_ADC14_disableSampleTimer ((bool (*)(void))ROM_ADC14TABLE[30]) |
#define ROM_AES256_setCipherKey |
#define ROM_AES256_encryptData |
#define ROM_AES256_decryptData |
#define ROM_AES256_setDecipherKey |
#define ROM_AES256_reset ((void (*)(uint32_t moduleInstance))ROM_AES256TABLE[4]) |
#define ROM_AES256_startEncryptData |
#define ROM_AES256_startDecryptData |
#define ROM_AES256_startSetDecipherKey |
#define ROM_AES256_getDataOut |
#define ROM_AES256_isBusy ((bool (*)(uint32_t moduleInstance))ROM_AES256TABLE[9]) |
#define ROM_AES256_clearErrorFlag ((void (*)(uint32_t moduleInstance))ROM_AES256TABLE[10]) |
#define ROM_AES256_getErrorFlagStatus ((uint32_t (*)(uint32_t moduleInstance))ROM_AES256TABLE[11]) |
#define ROM_AES256_clearInterruptFlag ((void (*)(uint32_t moduleInstance))ROM_AES256TABLE[12]) |
#define ROM_AES256_getInterruptStatus ((uint32_t (*)(uint32_t moduleInstance))ROM_AES256TABLE[13]) |
#define ROM_AES256_enableInterrupt ((void (*)(uint32_t moduleInstance))ROM_AES256TABLE[14]) |
#define ROM_AES256_disableInterrupt ((void (*)(uint32_t moduleInstance))ROM_AES256TABLE[15]) |
#define ROM_AES256_getInterruptFlagStatus ((uint32_t (*)(uint32_t moduleInstance))ROM_AES256TABLE[18]) |
#define ROM_COMP_E_initModule |
#define ROM_COMP_E_setReferenceVoltage |
#define ROM_COMP_E_setReferenceAccuracy |
#define ROM_COMP_E_setPowerMode |
#define ROM_COMP_E_enableModule ((void (*)(uint32_t comparator))ROM_COMPTABLE[4]) |
#define ROM_COMP_E_disableModule ((void (*)(uint32_t comparator))ROM_COMPTABLE[5]) |
#define ROM_COMP_E_shortInputs ((void (*)(uint32_t comparator))ROM_COMPTABLE[6]) |
#define ROM_COMP_E_unshortInputs ((void (*)(uint32_t comparator))ROM_COMPTABLE[7]) |
#define ROM_COMP_E_disableInputBuffer |
#define ROM_COMP_E_enableInputBuffer |
#define ROM_COMP_E_swapIO ((void (*)(uint32_t comparator))ROM_COMPTABLE[10]) |
#define ROM_COMP_E_outputValue ((uint8_t (*)(uint32_t comparator))ROM_COMPTABLE[11]) |
#define ROM_COMP_E_enableInterrupt |
#define ROM_COMP_E_disableInterrupt |
#define ROM_COMP_E_clearInterruptFlag |
#define ROM_COMP_E_getInterruptStatus ((uint_fast16_t (*)(uint32_t comparator))ROM_COMPTABLE[15]) |
#define ROM_COMP_E_getEnabledInterruptStatus ((uint_fast16_t (*)(uint32_t comparator))ROM_COMPTABLE[16]) |
#define ROM_COMP_E_setInterruptEdgeDirection |
#define ROM_COMP_E_toggleInterruptEdgeDirection ((void (*)(uint32_t comparator))ROM_COMPTABLE[18]) |
#define ROM_CRC32_setSeed |
#define ROM_CRC32_set8BitData |
#define ROM_CRC32_set16BitData |
#define ROM_CRC32_set32BitData ((void (*)(uint32_t dataIn))ROM_CRC32TABLE[3]) |
#define ROM_CRC32_set8BitDataReversed |
#define ROM_CRC32_set16BitDataReversed |
#define ROM_CRC32_set32BitDataReversed ((void (*)(uint32_t dataIn))ROM_CRC32TABLE[6]) |
#define ROM_CRC32_getResult ((uint32_t (*)(uint_fast8_t crcType))ROM_CRC32TABLE[7]) |
#define ROM_CRC32_getResultReversed ((uint32_t (*)(uint_fast8_t crcType))ROM_CRC32TABLE[8]) |
#define ROM_CS_initClockSignal |
#define ROM_CS_setReferenceOscillatorFrequency ((void (*)(uint8_t referenceFrequency))ROM_CSTABLE[1]) |
#define ROM_CS_enableClockRequest ((void (*)(uint32_t selectClock))ROM_CSTABLE[2]) |
#define ROM_CS_disableClockRequest ((void (*)(uint32_t selectClock))ROM_CSTABLE[3]) |
#define ROM_CS_setDCOCenteredFrequency ((void (*)(uint32_t dcoFreq))ROM_CSTABLE[4]) |
#define ROM_CS_tuneDCOFrequency ((void (*)(int16_t tuneParameter))ROM_CSTABLE[5]) |
#define ROM_CS_enableDCOExternalResistor ((void (*)(void))ROM_CSTABLE[6]) |
#define ROM_CS_disableDCOExternalResistor ((void (*)(void))ROM_CSTABLE[7]) |
#define ROM_CS_enableInterrupt ((void (*)(uint32_t flags))ROM_CSTABLE[8]) |
#define ROM_CS_disableInterrupt ((void (*)(uint32_t flags))ROM_CSTABLE[9]) |
#define ROM_CS_getEnabledInterruptStatus ((uint32_t (*)(void))ROM_CSTABLE[10]) |
#define ROM_CS_getInterruptStatus ((uint32_t (*)(void))ROM_CSTABLE[11]) |
#define ROM_CS_setDCOFrequency ((void (*)(uint32_t dcoFrequency))ROM_CSTABLE[12]) |
#define ROM_CS_getDCOFrequency ((uint32_t (*)(void))ROM_CSTABLE[13]) |
#define ROM_CS_enableFaultCounter ((void (*)(uint_fast8_t counterSelect))ROM_CSTABLE[14]) |
#define ROM_CS_disableFaultCounter ((void (*)(uint_fast8_t counterSelect))ROM_CSTABLE[15]) |
#define ROM_CS_resetFaultCounter ((void (*)(uint_fast8_t counterSelect))ROM_CSTABLE[16]) |
#define ROM_CS_startFaultCounter |
#define ROM_CS_clearInterruptFlag ((void (*)(uint32_t flags))ROM_CSTABLE[20]) |
#define ROM_CS_setDCOExternalResistorCalibration |
#define ROM_DMA_enableModule ((void (*)(void))ROM_DMATABLE[0]) |
#define ROM_DMA_disableModule ((void (*)(void))ROM_DMATABLE[1]) |
#define ROM_DMA_getErrorStatus ((uint32_t (*)(void))ROM_DMATABLE[2]) |
#define ROM_DMA_clearErrorStatus ((void (*)(void))ROM_DMATABLE[3]) |
#define ROM_DMA_enableChannel ((void (*)(uint32_t channelNum))ROM_DMATABLE[4]) |
#define ROM_DMA_disableChannel ((void (*)(uint32_t channelNum))ROM_DMATABLE[5]) |
#define ROM_DMA_isChannelEnabled ((bool (*)(uint32_t channelNum))ROM_DMATABLE[6]) |
#define ROM_DMA_setControlBase ((void (*)(void *controlTable))ROM_DMATABLE[7]) |
#define ROM_DMA_getControlBase ((void* (*)(void))ROM_DMATABLE[8]) |
#define ROM_DMA_getControlAlternateBase ((void* (*)(void))ROM_DMATABLE[9]) |
#define ROM_DMA_requestChannel ((void (*)(uint32_t channelNum))ROM_DMATABLE[10]) |
#define ROM_DMA_enableChannelAttribute |
#define ROM_DMA_disableChannelAttribute |
#define ROM_DMA_getChannelAttribute ((uint32_t (*)(uint32_t channelNum))ROM_DMATABLE[13]) |
#define ROM_DMA_setChannelControl |
#define ROM_DMA_setChannelTransfer |
#define ROM_DMA_setChannelScatterGather |
#define ROM_DMA_getChannelSize ((uint32_t (*)(uint32_t channelStructIndex))ROM_DMATABLE[17]) |
#define ROM_DMA_getChannelMode ((uint32_t (*)(uint32_t channelStructIndex))ROM_DMATABLE[18]) |
#define ROM_DMA_assignChannel ((void (*)(uint32_t mapping))ROM_DMATABLE[19]) |
#define ROM_DMA_requestSoftwareTransfer ((void (*)(uint32_t channel))ROM_DMATABLE[20]) |
#define ROM_DMA_assignInterrupt |
#define ROM_DMA_enableInterrupt ((void (*)(uint32_t interruptNumber))ROM_DMATABLE[22]) |
#define ROM_DMA_disableInterrupt ((void (*)(uint32_t interruptNumber))ROM_DMATABLE[23]) |
#define ROM_DMA_getInterruptStatus ((uint32_t (*)(void))ROM_DMATABLE[24]) |
#define ROM_DMA_clearInterruptFlag ((void (*)(uint32_t intChannel))ROM_DMATABLE[25]) |
#define ROM_FPU_enableModule ((void (*)(void))ROM_FPUTABLE[0]) |
#define ROM_FPU_disableModule ((void (*)(void))ROM_FPUTABLE[1]) |
#define ROM_FPU_enableStacking ((void (*)(void))ROM_FPUTABLE[2]) |
#define ROM_FPU_enableLazyStacking ((void (*)(void))ROM_FPUTABLE[3]) |
#define ROM_FPU_disableStacking ((void (*)(void))ROM_FPUTABLE[4]) |
#define ROM_FPU_setHalfPrecisionMode ((void (*)(uint32_t mode))ROM_FPUTABLE[5]) |
#define ROM_FPU_setNaNMode ((void (*)(uint32_t mode))ROM_FPUTABLE[6]) |
#define ROM_FPU_setFlushToZeroMode ((void (*)(uint32_t mode))ROM_FPUTABLE[7]) |
#define ROM_FPU_setRoundingMode ((void (*)(uint32_t mode))ROM_FPUTABLE[8]) |
#define ROM_GPIO_setAsOutputPin |
#define ROM_GPIO_setOutputHighOnPin |
#define ROM_GPIO_setOutputLowOnPin |
#define ROM_GPIO_toggleOutputOnPin |
#define ROM_GPIO_setAsInputPinWithPullDownResistor |
#define ROM_GPIO_setAsInputPinWithPullUpResistor |
#define ROM_GPIO_setAsPeripheralModuleFunctionOutputPin |
#define ROM_GPIO_setAsPeripheralModuleFunctionInputPin |
#define ROM_GPIO_getInputPinValue |
#define ROM_GPIO_interruptEdgeSelect |
#define ROM_GPIO_enableInterrupt |
#define ROM_GPIO_disableInterrupt |
#define ROM_GPIO_getInterruptStatus |
#define ROM_GPIO_clearInterruptFlag |
#define ROM_GPIO_setAsInputPin |
#define ROM_GPIO_getEnabledInterruptStatus ((uint_fast16_t (*)(uint_fast8_t selectedPort))ROM_GPIOTABLE[15]) |
#define ROM_GPIO_setDriveStrengthHigh |
#define ROM_GPIO_setDriveStrengthLow |
#define ROM_I2C_initMaster |
#define ROM_I2C_initSlave |
#define ROM_I2C_enableModule ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[2]) |
#define ROM_I2C_disableModule ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[3]) |
#define ROM_I2C_setSlaveAddress |
#define ROM_I2C_setMode |
#define ROM_I2C_slavePutData |
#define ROM_I2C_slaveGetData ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[7]) |
#define ROM_I2C_isBusBusy ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[8]) |
#define ROM_I2C_masterSendSingleByte |
#define ROM_I2C_masterSendMultiByteNext |
#define ROM_I2C_masterSendMultiByteNextWithTimeout |
#define ROM_I2C_masterSendMultiByteStop ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[17]) |
#define ROM_I2C_masterSendMultiByteStopWithTimeout |
#define ROM_I2C_masterReceiveStart ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[19]) |
#define ROM_I2C_masterReceiveMultiByteNext ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[20]) |
#define ROM_I2C_masterReceiveMultiByteFinish ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[21]) |
#define ROM_I2C_masterReceiveMultiByteFinishWithTimeout |
#define ROM_I2C_masterReceiveMultiByteStop ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[23]) |
#define ROM_I2C_masterReceiveSingleByte ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[24]) |
#define ROM_I2C_masterReceiveSingle ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[25]) |
#define ROM_I2C_getReceiveBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[26]) |
#define ROM_I2C_getTransmitBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[27]) |
#define ROM_I2C_masterIsStopSent ((uint8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[28]) |
#define ROM_I2C_masterIsStartSent ((bool (*)(uint32_t moduleInstance))ROM_I2CTABLE[29]) |
#define ROM_I2C_masterSendStart ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[30]) |
#define ROM_I2C_enableMultiMasterMode ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[31]) |
#define ROM_I2C_disableMultiMasterMode ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[32]) |
#define ROM_I2C_enableInterrupt |
#define ROM_I2C_disableInterrupt |
#define ROM_I2C_clearInterruptFlag |
#define ROM_I2C_getInterruptStatus |
#define ROM_I2C_getEnabledInterruptStatus ((uint_fast16_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[37]) |
#define ROM_I2C_getMode ((uint_fast8_t (*)(uint32_t moduleInstance))ROM_I2CTABLE[38]) |
#define ROM_I2C_slaveSendNAK ((void (*)(uint32_t moduleInstance))ROM_I2CTABLE[41]) |
#define ROM_Interrupt_enableMaster ((bool (*)(void))ROM_INTTABLE[0]) |
#define ROM_Interrupt_disableMaster ((bool (*)(void))ROM_INTTABLE[1]) |
#define ROM_Interrupt_setPriorityGrouping ((void (*)(uint32_t bits))ROM_INTTABLE[2]) |
#define ROM_Interrupt_getPriorityGrouping ((uint32_t (*)(void))ROM_INTTABLE[3]) |
#define ROM_Interrupt_setPriority |
#define ROM_Interrupt_getPriority ((uint8_t (*)(uint32_t interruptNumber))ROM_INTTABLE[5]) |
#define ROM_Interrupt_enableInterrupt ((void (*)(uint32_t interruptNumber))ROM_INTTABLE[6]) |
#define ROM_Interrupt_disableInterrupt ((void (*)(uint32_t interruptNumber))ROM_INTTABLE[7]) |
#define ROM_Interrupt_isEnabled ((bool (*)(uint32_t interruptNumber))ROM_INTTABLE[8]) |
#define ROM_Interrupt_pendInterrupt ((void (*)(uint32_t interruptNumber))ROM_INTTABLE[9]) |
#define ROM_Interrupt_setPriorityMask ((void (*)(uint8_t priorityMask))ROM_INTTABLE[10]) |
#define ROM_Interrupt_getPriorityMask ((uint8_t (*)(void))ROM_INTTABLE[11]) |
#define ROM_Interrupt_setVectorTableAddress ((void (*)(uint32_t addr))ROM_INTTABLE[12]) |
#define ROM_Interrupt_getVectorTableAddress ((uint32_t (*)(void))ROM_INTTABLE[13]) |
#define ROM_Interrupt_enableSleepOnIsrExit ((void (*)(void))ROM_INTTABLE[14]) |
#define ROM_Interrupt_disableSleepOnIsrExit ((void (*)(void))ROM_INTTABLE[15]) |
#define ROM_Interrupt_unpendInterrupt ((void (*)(uint32_t interruptNumber))ROM_INTTABLE[18]) |
#define ROM_MPU_enableModule ((void (*)(uint32_t mpuConfig))ROM_MPUTABLE[0]) |
#define ROM_MPU_disableModule ((void (*)(void))ROM_MPUTABLE[1]) |
#define ROM_MPU_getRegionCount ((uint32_t (*)(void))ROM_MPUTABLE[2]) |
#define ROM_MPU_enableRegion ((void (*)(uint32_t region))ROM_MPUTABLE[3]) |
#define ROM_MPU_disableRegion ((void (*)(uint32_t region))ROM_MPUTABLE[4]) |
#define ROM_MPU_setRegion |
#define ROM_MPU_getRegion |
#define ROM_MPU_enableInterrupt ((void (*)(void))ROM_MPUTABLE[7]) |
#define ROM_MPU_disableInterrupt ((void (*)(void))ROM_MPUTABLE[8]) |
#define ROM_PCM_shutdownDevice ((bool (*)(uint32_t shutdownMode))ROM_PCMTABLE[9]) |
#define ROM_PCM_gotoLPM0 ((bool (*)(void))ROM_PCMTABLE[10]) |
#define ROM_PCM_enableInterrupt ((void (*)(uint32_t flags))ROM_PCMTABLE[12]) |
#define ROM_PCM_disableInterrupt ((void (*)(uint32_t flags))ROM_PCMTABLE[13]) |
#define ROM_PCM_getInterruptStatus ((uint32_t (*)(void))ROM_PCMTABLE[14]) |
#define ROM_PCM_getEnabledInterruptStatus ((uint32_t (*)(void))ROM_PCMTABLE[15]) |
#define ROM_PCM_clearInterruptFlag ((void (*)(uint32_t flags))ROM_PCMTABLE[16]) |
#define ROM_PCM_enableRudeMode ((void (*)(void))ROM_PCMTABLE[17]) |
#define ROM_PCM_disableRudeMode ((void (*)(void))ROM_PCMTABLE[18]) |
#define ROM_PCM_gotoLPM0InterruptSafe ((bool (*)(void))ROM_PCMTABLE[19]) |
#define ROM_PMAP_configurePorts |
#define ROM_PSS_enableHighSidePinToggle ((void (*)(bool activeLow))ROM_PSSTABLE[0]) |
#define ROM_PSS_disableHighSidePinToggle ((void (*)(void))ROM_PSSTABLE[1]) |
#define ROM_PSS_enableHighSide ((void (*)(void))ROM_PSSTABLE[2]) |
#define ROM_PSS_disableHighSide ((void (*)(void))ROM_PSSTABLE[3]) |
#define ROM_PSS_setHighSidePerformanceMode ((void (*)(uint_fast8_t powerMode))ROM_PSSTABLE[6]) |
#define ROM_PSS_getHighSidePerformanceMode ((uint_fast8_t (*)(void))ROM_PSSTABLE[7]) |
#define ROM_PSS_enableHighSideMonitor ((void (*)(void))ROM_PSSTABLE[10]) |
#define ROM_PSS_disableHighSideMonitor ((void (*)(void))ROM_PSSTABLE[11]) |
#define ROM_PSS_setHighSideVoltageTrigger ((void (*)(uint_fast8_t triggerVoltage))ROM_PSSTABLE[12]) |
#define ROM_PSS_getHighSideVoltageTrigger ((uint_fast8_t (*)(void))ROM_PSSTABLE[13]) |
#define ROM_PSS_enableInterrupt ((void (*)(void))ROM_PSSTABLE[14]) |
#define ROM_PSS_disableInterrupt ((void (*)(void))ROM_PSSTABLE[15]) |
#define ROM_PSS_getInterruptStatus ((uint32_t (*)(void))ROM_PSSTABLE[16]) |
#define ROM_PSS_clearInterruptFlag ((void (*)(void))ROM_PSSTABLE[17]) |
#define ROM_PSS_enableForcedDCDCOperation ((void (*)(void))ROM_PSSTABLE[20]) |
#define ROM_PSS_disableForcedDCDCOperation ((void (*)(void))ROM_PSSTABLE[21]) |
#define ROM_REF_A_setReferenceVoltage ((void (*)(uint_fast8_t referenceVoltageSelect))ROM_REFTABLE[0]) |
#define ROM_REF_A_disableTempSensor ((void (*)(void))ROM_REFTABLE[1]) |
#define ROM_REF_A_enableTempSensor ((void (*)(void))ROM_REFTABLE[2]) |
#define ROM_REF_A_enableReferenceVoltageOutput ((void (*)(void))ROM_REFTABLE[3]) |
#define ROM_REF_A_disableReferenceVoltageOutput ((void (*)(void))ROM_REFTABLE[4]) |
#define ROM_REF_A_enableReferenceVoltage ((void (*)(void))ROM_REFTABLE[5]) |
#define ROM_REF_A_disableReferenceVoltage ((void (*)(void))ROM_REFTABLE[6]) |
#define ROM_REF_A_getBandgapMode ((uint_fast8_t (*)(void))ROM_REFTABLE[7]) |
#define ROM_REF_A_isBandgapActive ((bool (*)(void))ROM_REFTABLE[8]) |
#define ROM_REF_A_isRefGenBusy ((bool (*)(void))ROM_REFTABLE[9]) |
#define ROM_REF_A_isRefGenActive ((bool (*)(void))ROM_REFTABLE[10]) |
#define ROM_REF_A_getBufferedBandgapVoltageStatus ((bool (*)(void))ROM_REFTABLE[11]) |
#define ROM_REF_A_getVariableReferenceVoltageStatus ((bool (*)(void))ROM_REFTABLE[12]) |
#define ROM_REF_A_setReferenceVoltageOneTimeTrigger ((void (*)(void))ROM_REFTABLE[13]) |
#define ROM_REF_A_setBufferedBandgapVoltageOneTimeTrigger ((void (*)(void))ROM_REFTABLE[14]) |
#define ROM_ResetCtl_initiateSoftReset ((void (*)(void))ROM_RESETCTLTABLE[0]) |
#define ROM_ResetCtl_initiateSoftResetWithSource ((void (*)(uint32_t source))ROM_RESETCTLTABLE[1]) |
#define ROM_ResetCtl_getSoftResetSource ((uint32_t (*)(void))ROM_RESETCTLTABLE[2]) |
#define ROM_ResetCtl_clearSoftResetSource ((void (*)(uint32_t mask))ROM_RESETCTLTABLE[3]) |
#define ROM_ResetCtl_initiateHardReset ((void (*)(void))ROM_RESETCTLTABLE[4]) |
#define ROM_ResetCtl_initiateHardResetWithSource ((void (*)(uint32_t source))ROM_RESETCTLTABLE[5]) |
#define ROM_ResetCtl_getHardResetSource ((uint32_t (*)(void))ROM_RESETCTLTABLE[6]) |
#define ROM_ResetCtl_clearHardResetSource ((void (*)(uint32_t mask))ROM_RESETCTLTABLE[7]) |
#define ROM_ResetCtl_getPSSSource ((uint32_t (*)(void))ROM_RESETCTLTABLE[8]) |
#define ROM_ResetCtl_clearPSSFlags ((void (*)(void))ROM_RESETCTLTABLE[9]) |
#define ROM_ResetCtl_getPCMSource ((uint32_t (*)(void))ROM_RESETCTLTABLE[10]) |
#define ROM_ResetCtl_clearPCMFlags ((void (*)(void))ROM_RESETCTLTABLE[11]) |
#define ROM_RTC_C_startClock ((void (*)(void))ROM_RTCTABLE[0]) |
#define ROM_RTC_C_holdClock ((void (*)(void))ROM_RTCTABLE[1]) |
#define ROM_RTC_C_setCalibrationFrequency ((void (*)(uint_fast16_t frequencySelect))ROM_RTCTABLE[2]) |
#define ROM_RTC_C_setCalibrationData |
#define ROM_RTC_C_setTemperatureCompensation |
#define ROM_RTC_C_initCalendar |
#define ROM_RTC_C_setCalendarAlarm |
#define ROM_RTC_C_setCalendarEvent ((void (*)(uint_fast16_t eventSelect))ROM_RTCTABLE[8]) |
#define ROM_RTC_C_getPrescaleValue ((uint_fast8_t (*)(uint_fast8_t prescaleSelect))ROM_RTCTABLE[10]) |
#define ROM_RTC_C_setPrescaleValue |
#define ROM_RTC_C_convertBCDToBinary ((uint16_t (*)(uint16_t valueToConvert))ROM_RTCTABLE[12]) |
#define ROM_RTC_C_convertBinaryToBCD ((uint16_t (*)(uint16_t valueToConvert))ROM_RTCTABLE[13]) |
#define ROM_RTC_C_getInterruptStatus ((uint_fast8_t (*)(void))ROM_RTCTABLE[16]) |
#define ROM_RTC_C_getEnabledInterruptStatus ((uint_fast8_t (*)(void))ROM_RTCTABLE[17]) |
#define ROM_RTC_C_clearInterruptFlag ((void (*)(uint_fast8_t interruptFlagMask))ROM_RTCTABLE[18]) |
#define ROM_SPI_selectFourPinFunctionality |
#define ROM_SPI_changeMasterClock |
#define ROM_SPI_initSlave |
#define ROM_SPI_changeClockPhasePolarity |
#define ROM_SPI_transmitData |
#define ROM_SPI_receiveData ((uint8_t (*)(uint32_t moduleInstance))ROM_SPITABLE[6]) |
#define ROM_SPI_enableModule ((void (*)(uint32_t moduleInstance))ROM_SPITABLE[7]) |
#define ROM_SPI_disableModule ((void (*)(uint32_t moduleInstance))ROM_SPITABLE[8]) |
#define ROM_SPI_getReceiveBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_SPITABLE[9]) |
#define ROM_SPI_getTransmitBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_SPITABLE[10]) |
#define ROM_SPI_isBusy ((uint_fast8_t (*)(uint32_t moduleInstance))ROM_SPITABLE[11]) |
#define ROM_SPI_enableInterrupt |
#define ROM_SPI_disableInterrupt |
#define ROM_SPI_getInterruptStatus |
#define ROM_SPI_getEnabledInterruptStatus ((uint_fast8_t (*)(uint32_t moduleInstance))ROM_SPITABLE[15]) |
#define ROM_SPI_clearInterruptFlag |
#define ROM_SysTick_enableModule ((void (*)(void))ROM_SYSTICKTABLE[0]) |
#define ROM_SysTick_disableModule ((void (*)(void))ROM_SYSTICKTABLE[1]) |
#define ROM_SysTick_enableInterrupt ((void (*)(void))ROM_SYSTICKTABLE[2]) |
#define ROM_SysTick_disableInterrupt ((void (*)(void))ROM_SYSTICKTABLE[3]) |
#define ROM_SysTick_setPeriod ((void (*)(uint32_t period))ROM_SYSTICKTABLE[4]) |
#define ROM_SysTick_getPeriod ((uint32_t (*)(void))ROM_SYSTICKTABLE[5]) |
#define ROM_SysTick_getValue ((uint32_t (*)(void))ROM_SYSTICKTABLE[6]) |
#define ROM_Timer_A_startCounter |
#define ROM_Timer_A_configureContinuousMode |
#define ROM_Timer_A_configureUpMode |
#define ROM_Timer_A_configureUpDownMode |
#define ROM_Timer_A_initCapture |
#define ROM_Timer_A_initCompare |
#define ROM_Timer_A_clearTimer ((void (*)(uint32_t timer))ROM_TIMER_ATABLE[6]) |
#define ROM_Timer_A_getSynchronizedCaptureCompareInput |
#define ROM_Timer_A_getOutputForOutputModeOutBitValue |
#define ROM_Timer_A_getCaptureCompareCount |
#define ROM_Timer_A_setOutputForOutputModeOutBitValue |
#define ROM_Timer_A_generatePWM |
#define ROM_Timer_A_stopTimer ((void (*)(uint32_t timer))ROM_TIMER_ATABLE[12]) |
#define ROM_Timer_A_setCompareValue |
#define ROM_Timer_A_clearInterruptFlag ((void (*)(uint32_t timer))ROM_TIMER_ATABLE[14]) |
#define ROM_Timer_A_clearCaptureCompareInterrupt |
#define ROM_Timer_A_enableInterrupt ((void (*)(uint32_t timer))ROM_TIMER_ATABLE[16]) |
#define ROM_Timer_A_disableInterrupt ((void (*)(uint32_t timer))ROM_TIMER_ATABLE[17]) |
#define ROM_Timer_A_getInterruptStatus ((uint32_t (*)(uint32_t timer))ROM_TIMER_ATABLE[18]) |
#define ROM_Timer_A_getEnabledInterruptStatus ((uint32_t (*)(uint32_t timer))ROM_TIMER_ATABLE[19]) |
#define ROM_Timer_A_enableCaptureCompareInterrupt |
#define ROM_Timer_A_disableCaptureCompareInterrupt |
#define ROM_Timer_A_getCaptureCompareInterruptStatus |
#define ROM_Timer_A_getCaptureCompareEnabledInterruptStatus |
#define ROM_Timer_A_getCounterValue ((uint16_t (*)(uint32_t timer))ROM_TIMER_ATABLE[26]) |
#define ROM_Timer32_initModule |
#define ROM_Timer32_setCount |
#define ROM_Timer32_setCountInBackground |
#define ROM_Timer32_getValue ((uint32_t (*)(uint32_t timer))ROM_TIMER32TABLE[3]) |
#define ROM_Timer32_startTimer |
#define ROM_Timer32_haltTimer ((void (*)(uint32_t timer))ROM_TIMER32TABLE[5]) |
#define ROM_Timer32_enableInterrupt ((void (*)(uint32_t timer))ROM_TIMER32TABLE[6]) |
#define ROM_Timer32_disableInterrupt ((void (*)(uint32_t timer))ROM_TIMER32TABLE[7]) |
#define ROM_Timer32_clearInterruptFlag ((void (*)(uint32_t timer))ROM_TIMER32TABLE[8]) |
#define ROM_Timer32_getInterruptStatus ((uint32_t (*)(uint32_t timer))ROM_TIMER32TABLE[9]) |
#define ROM_UART_initModule |
#define ROM_UART_transmitData |
#define ROM_UART_enableModule ((void (*)(uint32_t moduleInstance))ROM_UARTTABLE[2]) |
#define ROM_UART_disableModule ((void (*)(uint32_t moduleInstance))ROM_UARTTABLE[3]) |
#define ROM_UART_queryStatusFlags |
#define ROM_UART_setDormant ((void (*)(uint32_t moduleInstance))ROM_UARTTABLE[5]) |
#define ROM_UART_resetDormant ((void (*)(uint32_t moduleInstance))ROM_UARTTABLE[6]) |
#define ROM_UART_transmitAddress |
#define ROM_UART_transmitBreak ((void (*)(uint32_t moduleInstance))ROM_UARTTABLE[8]) |
#define ROM_UART_getReceiveBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_UARTTABLE[9]) |
#define ROM_UART_getTransmitBufferAddressForDMA ((uint32_t (*)(uint32_t moduleInstance))ROM_UARTTABLE[10]) |
#define ROM_UART_selectDeglitchTime |
#define ROM_UART_enableInterrupt |
#define ROM_UART_disableInterrupt |
#define ROM_UART_getInterruptStatus |
#define ROM_UART_clearInterruptFlag |
#define ROM_UART_receiveData ((uint8_t (*)(uint32_t moduleInstance))ROM_UARTTABLE[16]) |
#define ROM_UART_getEnabledInterruptStatus ((uint_fast8_t (*)(uint32_t moduleInstance))ROM_UARTTABLE[17]) |
#define ROM_WDT_A_holdTimer ((void (*)(void))ROM_WDTTABLE[0]) |
#define ROM_WDT_A_startTimer ((void (*)(void))ROM_WDTTABLE[1]) |
#define ROM_WDT_A_clearTimer ((void (*)(void))ROM_WDTTABLE[2]) |
#define ROM_WDT_A_initWatchdogTimer |
#define ROM_WDT_A_initIntervalTimer |
#define ROM_WDT_A_setPasswordViolationReset ((void (*)(uint_fast8_t resetType))ROM_WDTTABLE[7]) |
#define ROM_WDT_A_setTimeoutReset ((void (*)(uint_fast8_t resetType))ROM_WDTTABLE[8]) |
#define ROM_SysCtl_A_getSRAMSize ((uint_least32_t (*)(void))ROM_SYSCTLATABLE[0]) |
#define ROM_SysCtl_A_getFlashSize ((uint_least32_t (*)(void))ROM_SYSCTLATABLE[1]) |
#define ROM_SysCtl_A_rebootDevice ((void (*)(void))ROM_SYSCTLATABLE[2]) |
#define ROM_SysCtl_A_enableSRAM ((bool (*)(uint32_t addr))ROM_SYSCTLATABLE[3]) |
#define ROM_SysCtl_A_disableSRAM ((bool (*)(uint32_t addr))ROM_SYSCTLATABLE[4]) |
#define ROM_SysCtl_A_enableSRAMRetention |
#define ROM_SysCtl_A_disableSRAMRetention |
#define ROM_SysCtl_A_enablePeripheralAtCPUHalt ((void (*)(uint_fast16_t devices))ROM_SYSCTLATABLE[7]) |
#define ROM_SysCtl_A_disablePeripheralAtCPUHalt ((void (*)(uint_fast16_t devices))ROM_SYSCTLATABLE[8]) |
#define ROM_SysCtl_A_setWDTTimeoutResetType ((void (*)(uint_fast8_t resetType))ROM_SYSCTLATABLE[9]) |
#define ROM_SysCtl_A_setWDTPasswordViolationResetType ((void (*)(uint_fast8_t resetType))ROM_SYSCTLATABLE[10]) |
#define ROM_SysCtl_A_disableNMISource ((void (*)(uint_fast8_t flags))ROM_SYSCTLATABLE[11]) |
#define ROM_SysCtl_A_enableNMISource ((void (*)(uint_fast8_t flags))ROM_SYSCTLATABLE[12]) |
#define ROM_SysCtl_A_getTempCalibrationConstant |
#define ROM_SysCtl_A_enableGlitchFilter ((void (*)(void))ROM_SYSCTLATABLE[15]) |
#define ROM_SysCtl_A_disableGlitchFilter ((void (*)(void))ROM_SYSCTLATABLE[16]) |
#define ROM_SysCtl_A_getTLVInfo |
#define ROM_SysCtl_A_getInfoFlashSize ((uint_least32_t (*)(void))ROM_SYSCTLATABLE[18]) |
#define ROM_FlashCtl_A_enableReadBuffering |
#define ROM_FlashCtl_A_disableReadBuffering |
#define ROM_FlashCtl_A_unprotectMemory |
#define ROM_FlashCtl_A_protectMemory |
#define ROM_FlashCtl_A_isMemoryRangeProtected |
#define ROM_FlashCtl_A_verifyMemory |
#define ROM_FlashCtl_A_performMassErase ((bool (*)(void))ROM_FLASHCTLATABLE[8]) |
#define ROM_FlashCtl_A_eraseSector ((bool (*)(uint32_t addr))ROM_FLASHCTLATABLE[9]) |
#define ROM_FlashCtl_A_programMemory |
#define ROM_FlashCtl_A_setProgramVerification ((void (*)(uint32_t verificationSetting))ROM_FLASHCTLATABLE[11]) |
#define ROM_FlashCtl_A_clearProgramVerification ((void (*)( uint32_t verificationSetting))ROM_FLASHCTLATABLE[12]) |
#define ROM_FlashCtl_A_enableWordProgramming ((void (*)(uint32_t mode))ROM_FLASHCTLATABLE[13]) |
#define ROM_FlashCtl_A_disableWordProgramming ((void (*)(void))ROM_FLASHCTLATABLE[14]) |
#define ROM_FlashCtl_A_isWordProgrammingEnabled ((uint32_t (*)(void))ROM_FLASHCTLATABLE[15]) |
#define ROM_FlashCtl_A_enableInterrupt ((void (*)(uint32_t flags))ROM_FLASHCTLATABLE[16]) |
#define ROM_FlashCtl_A_disableInterrupt ((void (*)(uint32_t flags))ROM_FLASHCTLATABLE[17]) |
#define ROM_FlashCtl_A_getEnabledInterruptStatus ((uint32_t (*)(void))ROM_FLASHCTLATABLE[18]) |
#define ROM_FlashCtl_A_getInterruptStatus ((uint32_t (*)(void))ROM_FLASHCTLATABLE[19]) |
#define ROM_FlashCtl_A_clearInterruptFlag ((void (*)(uint32_t flags))ROM_FLASHCTLATABLE[20]) |
#define ROM_FlashCtl_A_setWaitState |
#define ROM_FlashCtl_A_getWaitState ((uint32_t (*)(uint32_t bank))ROM_FLASHCTLATABLE[22]) |
#define ROM_FlashCtl_A_setReadMode |
#define ROM_FlashCtl_A_getReadMode ((uint32_t (*)(uint32_t flashBank))ROM_FLASHCTLATABLE[24]) |
#define ROM___FlashCtl_A_remaskData8Post |
#define ROM___FlashCtl_A_remaskData8Pre |
#define ROM___FlashCtl_A_remaskData32Pre |
#define ROM___FlashCtl_A_remaskData32Post |
#define ROM___FlashCtl_A_remaskBurstDataPre |
#define ROM___FlashCtl_A_remaskBurstDataPost |
#define ROM_FlashCtl_A_initiateSectorErase ((void (*)(uint32_t addr))ROM_FLASHCTLATABLE[33]) |
#define ROM_FlashCtl_A_initiateMassErase ((void (*)(void))ROM_FLASHCTLATABLE[34]) |
#define ROM_FlashCtl_A_isMemoryProtected ((bool (*)(uint32_t addr))ROM_FLASHCTLATABLE[35]) |
#define ROM_LCD_F_turnOff ((void (*)(void))ROM_LCDFTABLE[2]) |
#define ROM_LCD_F_clearAllMemory ((void (*)(void))ROM_LCDFTABLE[3]) |
#define ROM_LCD_F_clearAllBlinkingMemory ((void (*)(void))ROM_LCDFTABLE[4]) |
#define ROM_LCD_F_selectDisplayMemory ((void (*)(uint_fast16_t displayMemory))ROM_LCDFTABLE[5]) |
#define ROM_LCD_F_setBlinkingControl |
#define ROM_LCD_F_setAnimationControl |
#define ROM_LCD_F_clearAllAnimationMemory ((void (*)(void))ROM_LCDFTABLE[8]) |
#define ROM_LCD_F_setPinAsLCDFunction ((void (*)(uint_fast8_t pin))ROM_LCDFTABLE[9]) |
#define ROM_LCD_F_setPinAsPortFunction ((void (*)(uint_fast8_t pin))ROM_LCDFTABLE[10]) |
#define ROM_LCD_F_setPinAsSEG ((void (*)(uint_fast8_t pin))ROM_LCDFTABLE[13]) |
#define ROM_LCD_F_selectBias ((void (*)(uint_fast16_t bias))ROM_LCDFTABLE[14]) |
#define ROM_LCD_F_setVLCDSource |
#define ROM_LCD_F_clearInterrupt ((void (*)(uint32_t mask))ROM_LCDFTABLE[16]) |
#define ROM_LCD_F_getInterruptStatus ((uint32_t (*)(void))ROM_LCDFTABLE[17]) |
#define ROM_LCD_F_getEnabledInterruptStatus ((uint32_t (*)(void))ROM_LCDFTABLE[18]) |
#define ROM_LCD_F_enableInterrupt ((void (*)(uint32_t mask))ROM_LCDFTABLE[19]) |
#define ROM_LCD_F_disableInterrupt ((void (*)(uint32_t mask))ROM_LCDFTABLE[20]) |