Data Fields
_Timer_A_UpModeConfig Struct Reference

Type definition for _Timer_A_UpModeConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t clockSource
 
uint_fast16_t clockSourceDivider
 
uint_fast16_t timerPeriod
 
uint_fast16_t timerInterruptEnable_TAIE
 
uint_fast16_t captureCompareInterruptEnable_CCR0_CCIE
 
uint_fast16_t timerClear
 

Detailed Description

Type definition for _Timer_A_UpModeConfig structure.

ypedef Timer_A_UpModeConfig

Configuration structure for Up mode in the Timer_A module. See Timer_A_configureUpMode for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_UpModeConfig::clockSource

Referenced by Timer_A_configureUpMode().

uint_fast16_t _Timer_A_UpModeConfig::clockSourceDivider

Referenced by Timer_A_configureUpMode().

uint_fast16_t _Timer_A_UpModeConfig::timerPeriod

Referenced by Timer_A_configureUpMode().

uint_fast16_t _Timer_A_UpModeConfig::timerInterruptEnable_TAIE

Referenced by Timer_A_configureUpMode().

uint_fast16_t _Timer_A_UpModeConfig::captureCompareInterruptEnable_CCR0_CCIE

Referenced by Timer_A_configureUpMode().

uint_fast16_t _Timer_A_UpModeConfig::timerClear

Referenced by Timer_A_configureUpMode().


The documentation for this struct was generated from the following file:

Copyright 2017, Texas Instruments Incorporated