Data Fields
_eUSCI_SPI_SlaveConfig Struct Reference

Type definition for _eUSCI_SPI_SlaveConfig structure. More...

#include <spi.h>

Data Fields

uint_fast16_t msbFirst
 
uint_fast16_t clockPhase
 
uint_fast16_t clockPolarity
 
uint_fast16_t spiMode
 

Detailed Description

Type definition for _eUSCI_SPI_SlaveConfig structure.

ypedef eUSCI_SPI_SlaveConfig

Configuration structure for slave mode in the SPI module. See SPI_initSlave for parameter documentation.

Field Documentation

uint_fast16_t _eUSCI_SPI_SlaveConfig::msbFirst

Referenced by SPI_initSlave().

uint_fast16_t _eUSCI_SPI_SlaveConfig::clockPhase

Referenced by SPI_initSlave().

uint_fast16_t _eUSCI_SPI_SlaveConfig::clockPolarity

Referenced by SPI_initSlave().

uint_fast16_t _eUSCI_SPI_SlaveConfig::spiMode

Referenced by SPI_initSlave().


The documentation for this struct was generated from the following file:

Copyright 2017, Texas Instruments Incorporated