MSP Graphics Library
|
Functions | |
void | Graphics_drawCheckBox (const Graphics_Context *context, const Graphics_CheckBox *checkBox) |
bool | Graphics_isCheckBoxSelected (const Graphics_CheckBox *checkBox, uint16_t x, uint16_t y) |
void | Graphics_drawSelectedCheckBox (const Graphics_Context *context, const Graphics_CheckBox *checkBox) |
void | Graphics_drawReleasedCheckBox (const Graphics_Context *context, const Graphics_CheckBox *checkBox) |
void Graphics_drawCheckBox | ( | const Graphics_Context * | context, |
const Graphics_CheckBox * | checkBox | ||
) |
Draws a checkbox.
context | is a pointer to the drawing context to use. |
checkBox | is a pointer to the structure containing the extents of the checkbox. |
This function draws a checkbox. The checkbox will be created based on the parameters passed in the checkbox struct.
void Graphics_drawReleasedCheckBox | ( | const Graphics_Context * | context, |
const Graphics_CheckBox * | checkBox | ||
) |
Draws a released Checkbox.
context | is a pointer to the drawing context to use. |
checkBox | is a pointer to the structure containing the extents of the checkBox. |
This function draws a released checkbox using the selected parameters.
void Graphics_drawSelectedCheckBox | ( | const Graphics_Context * | context, |
const Graphics_CheckBox * | checkBox | ||
) |
Draws a selected Checkbox.
context | is a pointer to the drawing context to use. |
checkBox | is a pointer to the structure containing the extents of the checkBox. |
This function draws a selected checkbox using the selected parameters.
bool Graphics_isCheckBoxSelected | ( | const Graphics_CheckBox * | checkBox, |
uint16_t | x, | ||
uint16_t | y | ||
) |
Determines if x and y coordinates are contained in the checkbox.
checkBox | is a pointer to the structure containing the extents of the checkbox. |
x | x-coordinate to be determined if is inside button |
y | y-coordinate to be determined if is inside button . |
This function determines if x and y coordinates are contains inside checkbox struct.