MSP Graphics Library
|
#include <grlib.h>
Data Fields | |
int32_t | size |
The size of this structure. | |
const Graphics_Display * | display |
The screen onto which drawing operations are performed. | |
Graphics_Rectangle | clipRegion |
The clipping region to be used when drawing onto the screen. | |
uint32_t | foreground |
The color used to draw primitives onto the screen. | |
uint32_t | background |
The background color used to draw primitives onto the screen. | |
const Graphics_Font * | font |
The font used to render text onto the screen. | |
This structure defines a drawing context to be used to draw onto the screen. Multiple drawing contexts may exist at any time.