MSP Graphics Library
|
This structure defines the characteristics of a Checkbox. More...
#include <checkbox.h>
Data Fields | |
uint16_t | xPosition |
uint16_t | yPosition |
bool | selected |
uint8_t | gap |
uint32_t | textColor |
uint32_t | backgroundColor |
uint32_t | selectedColor |
uint8_t | numbOfChar |
const Graphics_Font * | font |
int8_t * | text |
This structure defines the characteristics of a Checkbox.
uint32_t Graphics_CheckBox::backgroundColor |
Color for background of checbox
const Graphics_Font* Graphics_CheckBox::font |
Font for text to be displayed in button
uint8_t Graphics_CheckBox::gap |
draws checbox with checkbox selected in pixels
uint8_t Graphics_CheckBox::numbOfChar |
Number of characters in checkbox message
bool Graphics_CheckBox::selected |
draws checbox with checkbox selected
uint32_t Graphics_CheckBox::selectedColor |
Selected check color
int8_t* Graphics_CheckBox::text |
Text to be displayed in button
uint32_t Graphics_CheckBox::textColor |
Text color
uint16_t Graphics_CheckBox::xPosition |
x coordinate for upper left corner of button
uint16_t Graphics_CheckBox::yPosition |
y coordinate for upper left corner of button