uint32_t backgroundColor
Definition: checkbox.h:18
uint8_t gap
Definition: checkbox.h:16
void Graphics_drawSelectedCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:126
uint8_t numbOfChar
Definition: checkbox.h:20
uint16_t xPosition
Definition: checkbox.h:13
This structure defines the characteristics of a Checkbox.
Definition: checkbox.h:11
uint32_t selectedColor
Definition: checkbox.h:19
bool Graphics_isCheckBoxSelected(const Graphics_CheckBox *checkBox, uint16_t x, uint16_t y)
Definition: checkbox.c:99
const Graphics_Font * font
Definition: checkbox.h:21
bool selected
Definition: checkbox.h:15
uint32_t textColor
Definition: checkbox.h:17
int8_t * text
Definition: checkbox.h:22
uint16_t yPosition
Definition: checkbox.h:14
This structure describes a font used for drawing text onto the screen.
Definition: grlib.h:154
void Graphics_drawCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:27
void Graphics_drawReleasedCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:165