![]() |
![]() |
TI BLE5-Stack API Documentation
1.00.01.04
|
Files | |
file | simple_np_dev.h |
SNP Device API. | |
Functions | |
uint8_t | SNP_executeHCIcmd (snpHciCmdReq_t *pReq, uint16_t dataLen) |
SNP Execute HCI Command (0x04) More... | |
void | SNP_executeTestCmd (snpTestCmdRsp_t *pRsp) |
SNP Execute Memory Test. More... | |
void | SNP_getRand (snpGetRandRsp_t *pRsp) |
SNP Get Random Number. More... | |
void | SNP_getRev (snpGetRevisionRsp_t *Msg) |
SNP Get Revision. More... | |
void | SNP_getStatus (snpGetStatusCmdRsp_t *pRsp) |
SNP Get Status. More... | |
void | SNP_maskEvt (snpMaskEventReq_t *pReq, snpMaskEventRsp_t *pRsp) |
SNP Mask Event (0x02) More... | |
uint8_t SNP_executeHCIcmd | ( | snpHciCmdReq_t * | pReq, |
uint16_t | dataLen | ||
) |
SNP Execute HCI Command (0x04)
AP -> NP (SNP_executeTestCmd)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x04 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_HCI_CMD_REQ |
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x55 | 0x04 |
SNP_NPI_ASYNC_CMD_TYPE | SNP_HCI_CMD_RSP |
The SNP Encapsulated HCI Command is used to encapsulate and send an HCI command to the SNP. Only the HCI commands listed in the parameter section below are supported.
The functionality of the HCI extension commands can be found in the HCI Vendor Specific Guide. The format of these commands can also be found in the Vendor Specific guide. Note that some HCI commands are defined in the Bluetooth Specification
The list of supported HCI commands are list of all HCI commands allowed by the SNP.
AP -> NP
snpHciCmdReq_t
Size | Description |
---|---|
2 Byte | HCI Command Opcode to Execute list of all HCI commands allowed by the SNP. |
X Byte | Parameters, if required by HCI Command |
NP -> AP
snpHciCmdRsp_t
Size | Description |
---|---|
1 Byte | Command Status list of status generated by the SNP. |
2 Byte | HCI Command Opcode Executed list of all HCI commands allowed by the SNP. |
X Byte | Return Values if HCI Command has any |
[in] | pReq | :HCI Request Structure, snpHciCmdReq_t |
[in] | dataLen | :Length in Bytes of snpHciCmdReq_t::pData |
void SNP_executeTestCmd | ( | snpTestCmdRsp_t * | pRsp | ) |
SNP Execute Memory Test.
AP -> NP (SNP_executeTestCmd)
CMD 0 | CMD 1 |
---|---|
0x35 | 0x10 |
SNP_NPI_SYNC_REQ_TYPE | SNP_GET_STATUS_REQ |
NP -> AP (N/A)
CMD 0 | CMD 1 |
---|---|
0x75 | 0x10 |
SNP_NPI_SYNC_RSP_TYPE | SNP_GET_STATUS_RSP |
This SNP Test command is used to profile the heap usage of the SNP.
AP -> NP
No Parameter Structure
NP -> AP
snpTestCmdRsp_t
Size | Description |
---|---|
2 Byte | HEAP allocated in bytes |
2 Byte | Peak HEAP Allocated since startup |
2 Byte | Total HEAP Size |
[out] | pRsp | : Heap Test Command Response Structure, snpTestCmdRsp_t |
void SNP_getRand | ( | snpGetRandRsp_t * | pRsp | ) |
SNP Get Random Number.
AP -> NP (SNP_getRand)
CMD 0 | CMD 1 |
---|---|
0x35 | 0x08 |
SNP_NPI_SYNC_REQ_TYPE | SNP_GET_RAND_REQ |
NP -> AP (SNP_getRand)
CMD 0 | CMD 1 |
---|---|
0x75 | 0x08 |
SNP_NPI_SYNC_RSP_TYPE | SNP_GET_RAND_RSP |
This SNP Test command is used to access the true random number generator on the SNP and return a random number to the AP.
AP -> NP
No Parameter Payload
NP -> AP
snpGetRandRsp_t
Size | Description |
---|---|
4 Byte | 32-bit Random Number from TRNG |
[out] | pRsp | : Get Random Number Response Structure snpGetRandRsp_t |
void SNP_getRev | ( | snpGetRevisionRsp_t * | Msg | ) |
SNP Get Revision.
AP -> NP (SNP_getRev)
CMD 0 | CMD 1 |
---|---|
0x35 | 0x03 |
SNP_NPI_SYNC_REQ_TYPE | SNP_GET_REVISION_REQ |
NP -> AP (SNP_getRev)
CMD 0 | CMD 1 |
---|---|
0x75 | 0x03 |
SNP_NPI_SYNC_RSP_TYPE | SNP_GET_REVISION_RSP |
The SNP Get Revision command is used to get the current revision of the SNP API as well as the full stack revision number as defined in the HCI vendor guide.
AP -> NP
No Parameter Payload
NP -> AP
snpGetRevisionRsp_t
Size | Description |
---|---|
1 Byte | Command Status list of status generated by the SNP. |
2 Byte | Version of SNP [Major, Minor] |
10 Byte | See TI Vendor Specific HCI Guide |
[out] | Msg | : Get Revision Response Structure, snpGetRevisionRsp_t |
void SNP_getStatus | ( | snpGetStatusCmdRsp_t * | pRsp | ) |
SNP Get Status.
AP -> NP (SNP_getStatus)
CMD 0 | CMD 1 |
---|---|
0x35 | 0x06 |
SNP_NPI_SYNC_REQ_TYPE | SNP_GET_STATUS_REQ |
NP -> AP (SNP_getStatus)
CMD 0 | CMD 1 |
---|---|
0x75 | 0x06 |
SNP_NPI_SYNC_RSP_TYPE | SNP_GET_STATUS_RSP |
The SNP Get Status command is used to get the current status of the SNP
AP -> NP
No Parameter Structure
NP -> AP
snpGetStatusCmdRsp_t
Size | Description |
---|---|
1 Byte | Current State of the GAP Role gaprole_States_t |
1 Byte | Current State of Advertising (TRUE | FALSE) 1 Byte | Current State of the GATT server (TRUE | FALSE) 1 Byte | Current GATT Methods (only if previous byte is TRUE)
[out] | pRsp | : Get Status Response Structure, snpGetStatusCmdRsp_t |
void SNP_maskEvt | ( | snpMaskEventReq_t * | pReq, |
snpMaskEventRsp_t * | pRsp | ||
) |
SNP Mask Event (0x02)
AP -> NP (SNP_maskEvt)
CMD 0 | CMD 1 |
---|---|
0x35 | 0x02 |
SNP_NPI_SYNC_REQ_TYPE | SNP_MASK_EVENT_RSP |
NP -> AP (SNP_maskEvt)
CMD 0 | CMD 1 |
---|---|
0x75 | 0x02 |
SNP_NPI_SYNC_RSP_TYPE | SNP_MASK_EVENT_RSP |
The SNP Mask Event command enables the AP to mask some events returned from the SNP if they are not needed by the AP.
Masking events may be useful in order to limit the possible wake up conditions of the AP, thus reducing power consumption.
All of the events that can be masked by this command are triggered asynchronously due to an action from the AP, an action of the remote peer, or timer expiration.
By default, ALL events are enabled and will be returned to the AP.
For a list of events, see list of asynchronous events generated by the SNP..
AP -> NP
snpMaskEventReq_t
Size | Description |
---|---|
2 Byte | Events Requested to be Masked list of asynchronous events generated by the SNP. |
NP -> AP
snpMaskEventRsp_t
Size | Description |
---|---|
2 Byte | Events that have been Masked list of asynchronous events generated by the SNP. |
[in] | pReq | : Mask Event Request Structure, snpMaskEventReq_t |
[out] | pRsp | : Mask Event Request Response, snpMaskEventRsp_t |