TI BLE5-Stack API Documentation
1.00.01.04
|
Parameter Structure for SNP_getRev. More...
Data Fields | |
uint16_t | snpVer |
2 Byte Version of the SNP (major, minor) | |
uint8_t | stackBuildVer [10] |
10 Byte Stack Revision see TI HCI vendor guide. | |
uint8_t | status |
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.) | |
Parameter Structure for SNP_getRev.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.