![]() |
![]() |
rflib
|
Radio Frequency (RF) Core Driver for the CC13X2 and CC26X2 device family.
To use the RF driver, ensure that the correct driver library for your device is linked in and include the top-level header file as follows:
The RF driver provides access to the radio core on the CC13x2/CC26x2 device family. It offers a high-level interface for command execution and to the radio timer (RAT). The RF driver ensures the lowest possible power consumption by providing automatic power management that is fully transparent for the application.
Key features are:
The RF driver can be configured at 4 different places:
The RF driver comes in two versions: single-client and multi-client. The single-client version allows only one driver instance to access the RF core at a time. The multi-client driver version allows concurrent access to the RF core with different RF settings. The multi-client driver has a slightly larger footprint and is not needed for many proprietary applications. The driver version can be selected in the build configuration by linking against a RFCC26X2_multiMode pre-built library. The multi-client driver is the default configuration in the SimpleLink SDKs.
The RF driver handles RF core hardware interrupts and uses software interrupts for its internal state machine. For managing the interrupt priorities, it expects the existence of a global RFCC26XX_HWAttrsV2 object. This object is configured in SysConfig and defined in the generated file ti_drivers_config.c
. By default, the priorities are set to the lowest possible value:
When initiating an RF driver instance, the function RF_open() accepts a pointer to a RF_Params object which might set several driver parameters. In addition, it expects an RF_Mode object and a setup command which is usually generated by SmartRF Studio:
The function RF_open() returns a driver handle that is used for accessing the correct driver instance. Please note that the first RF operation command before an RX or TX operation command must be a CMD_FS
to set the synthesizer frequency. The RF driver caches both, the pointer to the setup command and the physical CMD_FS
for automatic power management.
While a driver instance is opened, it can be re-configured with the function RF_control(). Various configuration parameters RF_CTRL are available. Example:
The RF core supports 3 different kinds of commands:
Direct and immediate commands are dispatched via RF_runDirectCmd() and RF_runImmediateCmd() respectively. These functions block until the command has completed and return a status code of the type RF_Stat when done.
Radio operation commands are potentially long-running commands and support different triggers as well as conditional execution. Only one command can be executed at a time, but the RF driver provides an internal queue that stores commands until the RF core is free. Two interfaces are provided for radio operation commands:
The asynchronous function RF_postCmd() posts a radio operation into the driver's internal command queue and returns a command handle of the type RF_CmdHandle which is an index in the command queue. The command is dispatched as soon as the RF core has completed any previous radio operation command.
Command execution happens in background. The calling task may proceed with other work or execute direct and immediate commands to interact with the posted radio operation. But beware that the posted command might not have started, yet. By calling the function RF_pendCmd() and subscribing events of the type RF_EventMask, it is possible to re-synchronize to a posted command:
The function RF_runCmd() is a combination of both, RF_postCmd() and RF_pendCmd() and allows synchronous execution.
A pending or already running command might be aborted at any time by calling the function RF_cancelCmd() or RF_flushCmd(). These functions take command handles as parameters, but can also just abort anything in the RF driver's queue:
When aborting a command, the return value of RF_runCmd() or RF_pendCmd() will contain the termination reason in form of event flags. If the command is in the RF driver queue, but has not yet start, the RF_EventCmdCancelled event is raised.
The RF core generates multiple interrupts during command execution. The RF driver maps these interrupts 1:1 to callback events of the type RF_EventMask. Hence, it is unnecessary to implement own interrupt handlers. Callback events are divided into 3 groups:
CMD_PROP_RX
.How callback events are subscribed was shown in the previous section. The following snippet shows a typical event handler callback for a proprietary RX operation:
In addition, the RF driver can generate error and power-up events that do not relate directly to the execution of a radio command. Such events can be subscribed by specifying the callback function pointers RF_Params::pErrCb and RF_Params::pPowerCb.
All callback functions run in software interrupt (SWI) context. Therefore, only a minimum amount of code should be executed. When using absolute timed commands with tight timing constraints, then it is recommended to set the RF driver SWIs to a high priority. See Setup and configuration for more details.
The RF core is a hardware peripheral and can be switched on and off. The RF driver handles that automatically and provides the following power optimization features:
The RF core optimizes the power consumption by enabling the RF core as late as possible. For instance does RF_open() not power up the RF core immediately. Instead, it waits until the first radio operation command is dispatched by RF_postCmd() or RF_runCmd().
The function RF_open() takes a radio setup command as parameter and expects a CMD_FS
command to follow. The pointer to the radio setup command and the whole CMD_FS
command are cached internally in the RF driver. They will be used for every proceeding power-up procedure. Whenever the client re-runs a setup command, the driver updates its internal cache with the new settings. RF driver also caches the first CMD_FS from the list of done commands. Please refer RF_postCmd() for limitations of command chains.
By default, the RF driver measures the time that it needs for the power-up procedure and uses that as an estimate for the next power cycle. On the CC13x0/CC26x0 devices, power-up takes usually 1.6 ms. Automatic measurement can be suppressed by specifying a custom power-up time with RF_Params::nPowerUpDuration. In addition, the client might set RF_Params::nPowerUpDurationMargin to cover any uncertainty when doing automatic measurements. This is necessary in applications with a high hardware interrupt load which can delay the RF driver's internal state machine execution.
Whenever a radio operation completes and there is no other radio operation in the queue, the RF core might be powered down. There are two options in the RF driver:
During the power-down procedure the RF driver stops the radio timer and saves a synchronization timestamp for the next power-up. This keeps the radio timer virtually in sync with the RTC even though it is not running all the time. The synchronization is done in hardware.
When dispatching a radio operation command with an absolute start trigger that is ahead in the future, the RF driver defers the execution and powers the RF core down until the command is due. It does that only, when:
cmd.startTrigger.triggerType
is set to TRIG_ABSTIME
cmd.startTime
is at not more than 3/4 of a full RAT cycle. Otherwise the driver assumes that cmd.startTime
is in the past.cmd.startTime
is due. That includes:If one of the conditions are not fulfilled, the RF core is kept up and running and the command is dispatched immediately. This ensures, that the command will execute on-time and not miss the configured start trigger.
Schedule BLE and proprietary radio commands.
The Radio Timer on the RF core is an independent 32 bit timer running at a tick rate of 4 ticks per microsecond. It is only physically active while the RF core is on. But because the RF driver resynchronizes the RAT to the RTC on every power-up, it appears to the application as the timer is always running. The RAT accuracy depends on the system HF clock while the RF core is active and on the LF clock while the RF core is powered down.
The current RAT time stamp can be obtained by RF_getCurrentTime():
The RAT has 8 independent channels that can be set up in capture and compare mode by RF_ratCapture() and RF_ratCompare() respectively. Three of these channels are accessible by the RF driver. Each channel may be connected to physical hardware signals for input and output or may trigger a callback function.
In order to allocate a RAT channel and trigger a callback function at a certain time stamp, use RF_ratCompare():
The RAT may be used to capture a time stamp on an edge of a physical pin. This can be achieved with RF_ratCapture().
In both cases, the RAT may generate an output signal when being triggered. The signal can be routed to a physical IO pin:
The application can program a TX power level for each RF client with the function RF_setTxPower(). The new value takes immediate effect if the RF core is up and running. Otherwise, it is stored in the RF driver client configuration.
TX power may be stored in a lookup table in ascending order. This table is usually generated and exported from SmartRF Studio together with the rest of the PHY configuration. A typical power table my look as follows:
Given this power table format, the application may program a new power level in multiple ways. It can use convenience functions to search a certain power level in the power table or may access the table index-based:
The current configured power level for a client can be retrieved by RF_getTxPower().
The RF driver improves the accuracy of XOSC_HF by performing temperature dependent compensation. This is commonly done in the BAW/SIP devices where the compensation parameters are already available inside the package.
When temperature compensation is enabled, RF_enableHPOSCTemperatureCompensation() is called during the board initialization(in Board_init()). This function enables the RF driver to update HPOSC_OVERRIDE with the correct frequency offset according to the ambient temperature at radio setup.
The RF driver also subscribes to a temperature notification event that triggers for 3 degree Celsius change in temperature. At every 3 degree Celsius change in temperature, it updates the RF core with the new frequency offset and re-subscribes to the temperature notification with updated thresholds.
When temperature compensation is enabled, but HPOSC_OVERRIDE is not found, then RF_open() returns a NULL handle.
RF_enableHPOSCTemperatureCompensation() returns RF_StatInvalidParamsError if the temperature notification fails to register.
When the temperature notification fails to register, a global callback can be executed by subscribing to the event RF_GlobalEventTempNotifyFail defined in RF_GlobalEvent.
The RF driver simplifies often needed tasks and provides additional functions. For instance, it can read the RSSI while the RF core is in RX mode using the function :tidrivers_api:RF_getRssi
:
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/utils/List.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/devices/cc13x2_26x2/ driverlib/rf_common_cmd.h>
#include <ti/devices/cc13x2_26x2/ driverlib/rf_prop_cmd.h>
#include <ti/devices/cc13x2_26x2/ driverlib/rf_ble_cmd.h>
Go to the source code of this file.
Data Structures | |
struct | RF_TxPowerTable_Value |
PA configuration value for a certain power level. More... | |
struct | RF_TxPowerTable_Entry |
TX power configuration entry in a TX power table. More... | |
struct | RF_Mode |
Specifies a RF core firmware configuration. More... | |
struct | RF_CoexOverride |
Runtime coexistence override parameters. More... | |
struct | RF_CoexOverride_BLEUseCases |
Coexistence override settings for BLE5 application scenarios. More... | |
union | RF_RadioSetup |
A unified type for radio setup commands of different PHYs. More... | |
union | RF_InfoVal |
Stores output parameters for RF_getInfo(). More... | |
struct | RF_ScheduleMapElement |
RF schedule map entry structure. More... | |
struct | RF_ScheduleMap |
RF schedule map structure. More... | |
struct | RF_Params |
RF driver configuration parameters. More... | |
struct | RF_Cmd_s |
struct | RFCC26XX_HWAttrsV2 |
RF Hardware attributes. More... | |
struct | RFCC26XX_SchedulerPolicy |
RF scheduler policy. More... | |
struct | RF_ScheduleCmdParams |
struct | RF_AccessParams |
RF request access parameter struct. More... | |
struct | RF_RatConfigCapture |
RF_ratCapture parameter structure. More... | |
struct | RF_RatConfigCompare |
RF_ratCompare parameter structure. More... | |
struct | RF_RatConfigOutput |
RAT related IO parameter structure. More... | |
Macros | |
#define | RF_convertUsToRatTicks(microseconds) ((microseconds) * (RF_RAT_TICKS_PER_US)) |
Converts a duration given in microseconds into radio timer (RAT) ticks. More... | |
#define | RF_convertMsToRatTicks(milliseconds) ((milliseconds) * 1000 * (RF_RAT_TICKS_PER_US)) |
Converts a duration given in milliseconds into radio timer (RAT) ticks. More... | |
#define | RF_convertRatTicksToUs(ticks) ((ticks) / (RF_RAT_TICKS_PER_US)) |
Converts a duration given in radio timer (RAT) ticks into microseconds. More... | |
#define | RF_convertRatTicksToMs(ticks) ((ticks) / (1000 * (RF_RAT_TICKS_PER_US))) |
Converts a duration given in radio timer (RAT) ticks into milliseconds. More... | |
RF Core Events | |
Events originating on the RF core and caused during command execution. They are aliases for the corresponding interrupt flags. RF Core Events are command-specific and are explained in the Technical Reference Manual.
| |
#define | RF_EventCmdDone (1 << 0) |
A radio operation command in a chain finished. More... | |
#define | RF_EventLastCmdDone (1 << 1) |
A stand-alone radio operation command or the last radio operation command in a chain finished. More... | |
#define | RF_EventFGCmdDone (1 << 2) |
A IEEE-mode radio operation command in a chain finished. More... | |
#define | RF_EventLastFGCmdDone (1 << 3) |
A stand-alone IEEE-mode radio operation command or the last command in a chain finished. More... | |
#define | RF_EventTxDone (1 << 4) |
Packet transmitted. More... | |
#define | RF_EventTXAck (1 << 5) |
ACK packet transmitted. More... | |
#define | RF_EventTxCtrl (1 << 6) |
Control packet transmitted. More... | |
#define | RF_EventTxCtrlAck (1 << 7) |
Acknowledgement received on a transmitted control packet. More... | |
#define | RF_EventTxCtrlAckAck (1 << 8) |
Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet. More... | |
#define | RF_EventTxRetrans (1 << 9) |
Packet retransmitted. More... | |
#define | RF_EventTxEntryDone (1 << 10) |
Tx queue data entry state changed to Finished. More... | |
#define | RF_EventTxBufferChange (1 << 11) |
A buffer change is complete. More... | |
#define | RF_EventPaChanged (1 << 14) |
The PA was reconfigured on the fly. More... | |
#define | RF_EventSamplesEntryDone (1 << 15) |
CTE data has been copied, only valid if autocopy feature is enabled. More... | |
#define | RF_EventRxOk (1 << 16) |
Packet received with CRC OK, payload, and not to be ignored. More... | |
#define | RF_EventRxNOk (1 << 17) |
Packet received with CRC error. More... | |
#define | RF_EventRxIgnored (1 << 18) |
Packet received with CRC OK, but to be ignored. More... | |
#define | RF_EventRxEmpty (1 << 19) |
Packet received with CRC OK, not to be ignored, no payload. More... | |
#define | RF_EventRxCtrl (1 << 20) |
Control packet received with CRC OK, not to be ignored. More... | |
#define | RF_EventRxCtrlAck (1 << 21) |
Control packet received with CRC OK, not to be ignored, then ACK sent. More... | |
#define | RF_EventRxBufFull (1 << 22) |
Packet received that did not fit in the Rx queue. More... | |
#define | RF_EventRxEntryDone (1 << 23) |
Rx queue data entry changing state to Finished. More... | |
#define | RF_EventDataWritten (1 << 24) |
Data written to partial read Rx buffer. More... | |
#define | RF_EventNDataWritten (1 << 25) |
Specified number of bytes written to partial read Rx buffer. More... | |
#define | RF_EventRxAborted (1 << 26) |
Packet reception stopped before packet was done. More... | |
#define | RF_EventRxCollisionDetected (1 << 27) |
A collision was indicated during packet reception. More... | |
#define | RF_EventModulesUnlocked (1 << 29) |
As part of the boot process, the CM0 has opened access to RF core modules and memories. More... | |
#define | RF_EventInternalError (uint32_t)(1 << 31) |
Internal error observed. More... | |
#define | RF_EventMdmSoft 0x0000002000000000 |
Synchronization word detected (MDMSOFT interrupt flag) More... | |
RF Driver Events | |
#define | RF_EventCmdCancelled 0x1000000000000000 |
Command canceled before it was started. More... | |
#define | RF_EventCmdAborted 0x2000000000000000 |
Abrupt command termination caused by RF_cancelCmd() or RF_flushCmd(). More... | |
#define | RF_EventCmdStopped 0x4000000000000000 |
Graceful command termination caused by RF_cancelCmd() or RF_flushCmd(). More... | |
#define | RF_EventRatCh 0x0800000000000000 |
A user-programmable RAT channel triggered an event. More... | |
#define | RF_EventPowerUp 0x0400000000000000 |
RF power up event. More... | |
#define | RF_EventError 0x0200000000000000 |
Event flag used for error callback functions to indicate an error. See RF_Params::pErrCb. More... | |
#define | RF_EventCmdPreempted 0x0100000000000000 |
Command preempted by another command with higher priority. Applies only to multi-client applications. More... | |
Control codes for driver configuration | |
Control codes are used in RF_control(). | |
#define | RF_CTRL_SET_INACTIVITY_TIMEOUT 0 |
Control code used by RF_control to set inactivity timeout. More... | |
#define | RF_CTRL_UPDATE_SETUP_CMD 1 |
Control code used by RF_control to update setup command. More... | |
#define | RF_CTRL_SET_POWERUP_DURATION_MARGIN 2 |
Control code used by RF_control to set powerup duration margin. More... | |
#define | RF_CTRL_SET_PHYSWITCHING_DURATION_MARGIN 3 |
Control code used by RF_control to set the phy switching margin. More... | |
#define | RF_CTRL_SET_RAT_RTC_ERR_TOL_VAL 4 |
Control code used by RF_control to set max error tolerance for RAT/RTC. More... | |
#define | RF_CTRL_SET_POWER_MGMT 5 |
Control code used by RF_control to set power management. More... | |
#define | RF_CTRL_SET_HWI_PRIORITY 6 |
Control code used by RF_control to set the hardware interrupt priority level of the RF driver. More... | |
#define | RF_CTRL_SET_SWI_PRIORITY 7 |
Control code used by RF_control to set the software interrupt priority level of the RF driver. More... | |
#define | RF_CTRL_SET_AVAILABLE_RAT_CHANNELS_MASK 8 |
Control code used by RF_control to mask the available RAT channels manually. More... | |
#define | RF_CTRL_COEX_CONTROL 9 |
Control code used by RF_control to enable or disable the coexistence feature at runtime. More... | |
TX Power Table defines | |
#define | RF_TxPowerTable_MIN_DBM -128 |
#define | RF_TxPowerTable_MAX_DBM 126 |
#define | RF_TxPowerTable_INVALID_DBM 127 |
#define | RF_TxPowerTable_INVALID_VALUE 0x3fffff |
#define | RF_TxPowerTable_TERMINATION_ENTRY { .power = RF_TxPowerTable_INVALID_DBM, .value = { .rawValue = RF_TxPowerTable_INVALID_VALUE, .paType = RF_TxPowerTable_DefaultPA } } |
#define | RF_TxPowerTable_DEFAULT_PA_ENTRY(bias, gain, boost, coefficient) { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9), .paType = RF_TxPowerTable_DefaultPA } |
#define | RF_TxPowerTable_CC13x4Sub1GHz_DEFAULT_PA_ENTRY(bias, gain, boost, coefficient, gain2) { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((gain2) << 16), .paType = RF_TxPowerTable_DefaultPA } |
#define | RF_TxPowerTable_HIGH_PA_ENTRY(bias, ibboost, boost, coefficient, ldotrim) { .rawValue = ((bias) << 0) | ((ibboost) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((ldotrim) << 16), .paType = RF_TxPowerTable_HighPA } |
Other defines | |
#define | RF_GET_RSSI_ERROR_VAL (-128) |
Error return value for RF_getRssi() More... | |
#define | RF_CMDHANDLE_FLUSH_ALL (-1) |
RF command handle to flush all RF commands. More... | |
#define | RF_ALLOC_ERROR (-2) |
RF command or RAT channel allocation error. More... | |
#define | RF_SCHEDULE_CMD_ERROR (-3) |
RF command schedule error. More... | |
#define | RF_ERROR_RAT_PROG (-255) |
A rat channel could not be programmed. More... | |
#define | RF_ERROR_INVALID_RFMODE (-256) |
Invalid RF_Mode. Used in error callback. More... | |
#define | RF_ERROR_CMDFS_SYNTH_PROG (-257) |
Synthesizer error with CMD_FS. Used in error callback. If this error occurred in error callback, user needs to resend CMD_FS to recover. See the device's errata for more details. More... | |
#define | RF_NUM_SCHEDULE_ACCESS_ENTRIES 2 |
Number of access request entries. More... | |
#define | RF_NUM_SCHEDULE_COMMAND_ENTRIES 8 |
Number of scheduled command entries. More... | |
#define | RF_NUM_SCHEDULE_MAP_ENTRIES (RF_NUM_SCHEDULE_ACCESS_ENTRIES + RF_NUM_SCHEDULE_COMMAND_ENTRIES) |
Number of schedule map entries. This is the sum of access request and scheduled command entries. More... | |
#define | RF_SCH_MAP_CURRENT_CMD_OFFSET RF_NUM_SCHEDULE_ACCESS_ENTRIES |
Offset of the current command entry in the schedule map. More... | |
#define | RF_SCH_MAP_PENDING_CMD_OFFSET (RF_SCH_MAP_CURRENT_CMD_OFFSET + 2) |
Offset of the first pending command entry in the schedule map. More... | |
#define | RF_ABORT_PREEMPTION (1<<2) |
Used with RF_cancelCmd() to provoke subscription to RadioFreeCallback. More... | |
#define | RF_ABORT_GRACEFULLY (1<<0) |
Used with RF_cancelCmd() for graceful command termination. More... | |
#define | RF_SCH_CMD_EXECUTION_TIME_UNKNOWN 0 |
For unknown execution time for RF scheduler. More... | |
#define | RF_RAT_ANY_CHANNEL (-1) |
To be used within the channel configuration structure. Allocate any of the available channels. More... | |
#define | RF_RAT_TICKS_PER_US 4 |
Radio timer (RAT) ticks per microsecond. More... | |
#define | RF_LODIVIDER_MASK 0x7F |
Mask to be used to determine the effective value of the setup command's loDivider field. More... | |
Stack ID defines | |
#define | RF_STACK_ID_DEFAULT 0x00000000 |
No value is set. More... | |
#define | RF_STACK_ID_154 0x8000F154 |
ID for TI 15.4 Stack. More... | |
#define | RF_STACK_ID_BLE 0x8000FB1E |
ID for TI BLE Stack. More... | |
#define | RF_STACK_ID_EASYLINK 0x8000FEA2 |
ID for TI EasyLink Stack. More... | |
#define | RF_STACK_ID_THREAD 0x8000FEAD |
ID for TI Thread Stack. More... | |
#define | RF_STACK_ID_TOF 0x8000F00F |
ID for TI TOF Stack. More... | |
#define | RF_STACK_ID_CUSTOM 0x0000FC00 |
ID for Custom Stack. More... | |
Typedefs | |
typedef rfc_radioOp_t | RF_Op |
Base type for all radio operation commands. More... | |
typedef uint64_t | RF_EventMask |
Data type for events during command execution. More... | |
typedef uint32_t | RF_ClientEventMask |
Event mask for combining RF_ClientEvent event flags in RF_Params::nClientEventMask. More... | |
typedef uint32_t | RF_GlobalEventMask |
Event mask for combining RF_GlobalEvent event flags in RFCC26XX_HWAttrsV2::globalEventMask. More... | |
typedef int16_t | RF_CmdHandle |
Command handle that is returned by RF_postCmd(). More... | |
typedef RF_Object * | RF_Handle |
A handle that is returned by to RF_open(). More... | |
typedef int8_t | RF_RatHandle |
RAT handle that is returned by RF_ratCompare() or RF_ratCapture(). More... | |
typedef void(* | RF_Callback) (RF_Handle h, RF_CmdHandle ch, RF_EventMask e) |
Handles events related to RF command execution. More... | |
typedef void(* | RF_RatCallback) (RF_Handle h, RF_RatHandle rh, RF_EventMask e, uint32_t compareCaptureTime) |
Handles events related to the Radio Timer (RAT). More... | |
typedef void(* | RF_ClientCallback) (RF_Handle h, RF_ClientEvent event, void *arg) |
Handles events related to a driver instance. More... | |
typedef void(* | RF_GlobalCallback) (RF_Handle h, RF_GlobalEvent event, void *arg) |
Handles global events as part of PHY configuration. More... | |
typedef struct RF_Cmd_s | RF_Cmd |
typedef RF_ScheduleStatus(* | RF_SubmitHook) (RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue) |
Handles the queue sorting algorithm when a new command is submitted to the driver from any of the active clients. More... | |
typedef RF_ExecuteAction(* | RF_ExecuteHook) (RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd) |
Defines the execution and conflict resolution hook at runtime. More... | |
Functions | |
RF_Handle | RF_open (RF_Object *pObj, RF_Mode *pRfMode, RF_RadioSetup *pRadioSetup, RF_Params *params) |
Creates a a new client instance of the RF driver. More... | |
void | RF_close (RF_Handle h) |
Close client connection to RF driver. More... | |
uint32_t | RF_getCurrentTime (void) |
Return current radio timer value. More... | |
RF_CmdHandle | RF_postCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent) |
Appends RF operation commands to the driver's command queue and returns a command handle. More... | |
RF_ScheduleStatus | RF_defaultSubmitPolicy (RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue) |
Sorts and adds commands to the RF driver internal command queue. More... | |
RF_ExecuteAction | RF_defaultExecutionPolicy (RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd) |
Makes a final decision before dispatching a scheduled command. More... | |
void | RF_ScheduleCmdParams_init (RF_ScheduleCmdParams *pSchParams) |
Initialize the configuration structure to default values to be used with the RF_scheduleCmd() API. More... | |
RF_CmdHandle | RF_scheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent) |
Schedule an RF operation (chain) to the command queue. More... | |
RF_EventMask | RF_pendCmd (RF_Handle h, RF_CmdHandle ch, RF_EventMask bmEvent) |
Synchronizes the calling task to an RF operation command ch and returns accumulated event flags. More... | |
RF_EventMask | RF_runCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent) |
Runs synchronously an RF operation command or a chain of commands and returns the termination reason. More... | |
RF_EventMask | RF_runScheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent) |
Runs synchronously a (chain of) RF operation(s) for dual or single-mode. More... | |
RF_Stat | RF_cancelCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode) |
Abort/stop/cancel single command in command queue. More... | |
RF_Stat | RF_flushCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode) |
Abort/stop/cancel command and any subsequent commands in command queue. More... | |
RF_Stat | RF_runImmediateCmd (RF_Handle h, uint32_t *pCmdStruct) |
Send any Immediate command. More... | |
RF_Stat | RF_runDirectCmd (RF_Handle h, uint32_t cmd) |
Send any Direct command. More... | |
void | RF_yield (RF_Handle h) |
Signal that radio client is not going to issue more commands in a while. More... | |
void | RF_Params_init (RF_Params *params) |
Function to initialize the RF_Params struct to its defaults. More... | |
RF_Stat | RF_getInfo (RF_Handle h, RF_InfoType type, RF_InfoVal *pValue) |
Get value for some RF driver parameters. More... | |
int8_t | RF_getRssi (RF_Handle h) |
Get RSSI value. More... | |
RF_Op * | RF_getCmdOp (RF_Handle h, RF_CmdHandle cmdHnd) |
Get command structure pointer. More... | |
void | RF_RatConfigCompare_init (RF_RatConfigCompare *channelConfig) |
Initialize the configuration structure to be used to set up a RAT compare event. More... | |
void | RF_RatConfigCapture_init (RF_RatConfigCapture *channelConfig) |
Initialize the configuration structure to be used to set up a RAT capture event. More... | |
void | RF_RatConfigOutput_init (RF_RatConfigOutput *ioConfig) |
Initialize the configuration structure to be used to set up a RAT IO. More... | |
RF_RatHandle | RF_ratCompare (RF_Handle rfHandle, RF_RatConfigCompare *channelConfig, RF_RatConfigOutput *ioConfig) |
Setup a Radio Timer (RAT) channel in compare mode. More... | |
RF_RatHandle | RF_ratCapture (RF_Handle rfHandle, RF_RatConfigCapture *channelConfig, RF_RatConfigOutput *ioConfig) |
Setup a Radio Timer (RAT) channel in capture mode. More... | |
RF_Stat | RF_ratDisableChannel (RF_Handle rfHandle, RF_RatHandle ratHandle) |
Disable a RAT channel. More... | |
RF_Stat | RF_control (RF_Handle h, int8_t ctrl, void *args) |
Set RF control parameters. More... | |
RF_Stat | RF_requestAccess (RF_Handle h, RF_AccessParams *pParams) |
Request radio access. More... | |
RF_TxPowerTable_Value | RF_getTxPower (RF_Handle h) |
Returns the currently configured transmit power configuration. More... | |
RF_Stat | RF_setTxPower (RF_Handle h, RF_TxPowerTable_Value value) |
Updates the transmit power configuration of the RF core. More... | |
int8_t | RF_TxPowerTable_findPowerLevel (RF_TxPowerTable_Entry table[], RF_TxPowerTable_Value value) |
Retrieves a power level in dBm for a given power configuration value. More... | |
RF_TxPowerTable_Value | RF_TxPowerTable_findValue (RF_TxPowerTable_Entry table[], int8_t powerLevel) |
Retrieves a power configuration value for a given power level in dBm. More... | |
RF_Stat | RF_enableHPOSCTemperatureCompensation (void) |
Enables temperature monitoring and temperature based drift compensation. More... | |