rflib
Data Fields
RF_RatConfigOutput Struct Reference

RAT related IO parameter structure. More...

#include <RFCC26X2.h>

Data Fields

RF_RatOutputMode mode
 The mode the GPO should operate in. More...
 
RF_RatOutputSelect select
 The signal which shall be connected to the GPO. More...
 

Detailed Description

RAT related IO parameter structure.

These parameters are used with the RF_ratCompare() or RF_ratCapture() calls.

Field Documentation

§ mode

RF_RatOutputMode RF_RatConfigOutput::mode

The mode the GPO should operate in.

§ select

RF_RatOutputSelect RF_RatConfigOutput::select

The signal which shall be connected to the GPO.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale