BLE5-Stack 2.01.00 to BLE5-Stack 2.01.01¶
This section will describe a way to migrate a project from BLE5-Stack 2.01.00 to a BLE5-Stack 2.01.01 project.
The changes you need to address to port your project:
API changes (affecting RTLS example projects
rtls_master/passive/slave
):What is affected How to update RTLSAoa_processAoaResults()
Function arguments: Change input order, add new and delete obsolete rtlsAoaConfigReq_t
Remove struct member antArraySwitch
, and rename memberpAntArray
renamed topAntPattern
RTLSCtrl_aoaResultEvt()
Function arguments: Change input order, add new and delete obsolete RTLSCtrl_connResultEvt()
Function arguments: Add new argument connHandle
RTLSCtrl_initAntenna()
Function arguments: Add new argument pinState
RTLSCtrl_processDataSent()
Function arguments: Add new argument connHandle
RTLSCtrl_sendRtlsRemoteCmd()
Function arguments: Add new argument connHandle
RTLSCtrl_syncEventNotify()
Function arguments: Add new argument connHandle
RTLSCtrl_updateConnStateAndSyncEvt()
Name: Rename to RTLSCtrl_updateConnState()
Function arguments: Add new argumentconnHandle
RTLSSrv_initAntArray()
Function arguments: Only call with argument mainAntenna
New link layer antenna structure
cteAntProp_t
, declared inble_user_config.c
, and is now used to control antenna switching. Edit this structure to run on custom AoA boards. See the Angle of Arrival section of the BLE5 User’s Guide and the Simplelink Academy AoA lab for more information.There are new values to use in the TX power back-off table. This table is declared in the
txPwrBackoffVal_t
structure inble_user_config.c
. The new defined values can be found inhci.h
.The OAD example projects
simple_peripheral_oad_onchip
andsimple_peripheral_oad_offchip
include RCOSC calibration files (rcosc_calibration.c
andrcosc_calibration.h
).The crystal-less BAW wireless MCU, CC2652RB, is now supported by SysConfig in the example projects.
XDCtools updated from version 3.60.00.24_core to 3.60.02.34_core.