![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.01.00
|
Aggregation of ToF structures needed for RTLS Control operation (saved in gRtlsData) More...
Data Fields | |
uint8_t | bSlaveTofEnabled |
Used to determine whether slave is doing ToF or not. | |
uint8_t | bSlaveTofParamPend |
Used to determine whether to send params to slave when a connection is formed. | |
uint8_t | bTofValuesInitialized |
Flag to check if ToF was run at least once. | |
ToF_BurstStat * | pTofAverage |
Array to save average of samples (for each frequency) | |
ToF_BurstStat * | pTofLastRun |
Array to save samples from the last ToF run. | |
rtlsTofCalib_t | tofCalibInfo |
Information about ToF calibration. | |
rtlsTofConfig_t | tofConfig |
Values configured by the user. | |
ToF_Handle | tofHandle |
Handle will be passed to the TOF driver for actions. | |
ToF_Struct | tofStruct |
Struct will be filled by TOF_open. | |
Aggregation of ToF structures needed for RTLS Control operation (saved in gRtlsData)