![]() |
![]() |
| ADC.h | Analog to Digital Conversion (ADC) Input Driver |
| ADCBuf.h | Analog to Digital Conversion Buffer (ADCBuf) Input Driver |
| ADCBufCC26X2.h | ADCBuf driver implementation for a CC26X2 analog-to-digital converter |
| ADCBufCC26XX.h | ADCBuf driver implementation for a CC26XX analog-to-digital converter |
| ADCCC26XX.h | ADC driver implementation for the ADC peripheral on CC26XX |
| AESCBC.h | AESCBC driver header |
| AESCBCCC26XX.h | AESCBC driver implementation for the CC26XX family |
| AESCCM.h | AESCCM driver header |
| AESCCMCC26XX.h | AESCCM driver implementation for the CC26XX family |
| AESCTR.h | AESCTR driver header |
| AESCTRCC26XX.h | AESCTR driver implementation for the CC26XX family |
| AESCTRDRBG.h | AESCTRDRBG driver header |
| AESCTRDRBGXX.h | Generic AESCTRDRBG implementation based on the AESCTR driver |
| AESECB.h | AESECB driver header |
| AESECBCC26XX.h | AESECB driver implementation for the CC26XX family |
| AESGCM.h | AESGCM driver header |
| AESGCMCC26XX.h | AESGCM driver implementation for the CC26XX family |
| AnsiColor.h | |
| Board.h | Portable board-specific symbols |
| Codec1.h | Implementation of TI Codec Type 1 (IMA ADPCM) encoding and decoding |
| CryptoCC26XX.h | Crypto driver implementation for a CC26XX Crypto controller |
| CryptoKey.h | The CryptoKey type is an opaque representation of a cryptographic key |
| CryptoKeyPlaintext.h | |
| CryptoResourceCC26XX.h | Shared resources to arbitrate access to the keyStore, AES, and SHA2 engine |
| Display.h | Generic interface for text output |
| DisplayDogm1286.h | |
| DisplayExt.h | Extention of Display to access GrLib functionality in capable displays |
| DisplayHost.h | Display driver for printf-like output |
| DisplaySharp.h | |
| DisplayUart.h | Display.h implementation for UART output |
| ECCParams.h | |
| ECDH.h | TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme |
| ECDHCC26X2.h | ECDH driver implementation for the CC26X2 family |
| ECDSA.h | TI Driver for Elliptic Curve Digital Signature Algorithm |
| ECDSACC26X2.h | ECDSA driver implementation for the CC26X2 family |
| ECJPAKE.h | TI Driver for Elliptic Curve Password Authenticated Key Exchange by Juggling |
| ECJPAKECC26X2.h | ECJPAKE driver implementation for the CC26X2 family |
| GPIO.h | General Purpose I/O driver interface |
| GPIOCC26XX.h | GPIO driver implementation for CC26xx/CC13xx devices |
| GPTimerCC26XX.h | GPTimer driver implementation for CC26XX/CC13XX |
| I2C.h | Inter-Integrated Circuit (I2C) Driver |
| I2CCC26XX.h | I2C driver implementation for a CC26XX I2C controller |
| I2S.h | Inter-Integrated Circuit Sound (I2S) Bus Driver |
| I2SCC26XX.h | I2S driver implementation for a CC26XX I2S controller |
| LCDDogm1286.h | LCD driver implementation for a DOGM128W-6 LCD display |
| LCDDogm1286_util.h | |
| List.h | Linked List interface for use in drivers |
| NoRTOS.h | NoRTOS framework module |
| NVS.h | Non-Volatile Storage driver interface |
| NVSCC26XX.h | Non-Volatile Storage driver for CC13XX/CC26XX devices |
| NVSRAM.h | RAM implementation of the NVS driver |
| NVSSPI25X.h | Non-Volatile Storage driver implementation for SPI flash peripherals |
| PDMCC26XX.h | PDM driver implementation for a CC26XX PDM controller |
| PDMCC26XX_util.h | PDM utility includes helper functions for configuring the CC26XX I2S controller |
| PIN.h | Generic PIN & GPIO driver |
| PINCC26XX.h | Device-specific pin & GPIO driver for CC26xx family [def] |
| PKAResourceCC26XX.h | Shared resources to arbitrate access to the PKA engine |
| Power.h | Power Manager |
| PowerCC26X2.h | Power manager interface for CC26X2 |
| PowerCC26XX.h | Power manager interface for CC26XX/CC13XX |
| PWM.h | Pulse Width Modulation (PWM) driver |
| PWMTimerCC26XX.h | PWM driver implementation for CC26XX/CC13XX |
| Random.h | Interface to generate pseudo-random numbers |
| RF.h | Radio Frequency (RF) Core Driver for the CC13XX and CC26XX device family |
| RingBuf.h | |
| SD.h | Secure Digital (SD) Driver |
| SDFatFS.h | File Allocation Table File System (FATFS) Driver |
| SDSPI.h | SD driver implementation built on the TI SPI driver |
| SHA2.h | SHA2 driver header |
| SHA2CC26X2.h | SHA2 driver implementation for the CC26X2 family |
| SharpGrLib.h | |
| SPI.h | Serial Peripheral Interface (SPI) Driver Interface |
| SPICC26X2DMA.h | SPI driver implementation for a CC26XX SPI controller using the UDMA controller |
| SPICC26XXDMA.h | SPI driver implementation for a CC26XX SPI controller using the UDMA controller |
| spiffs.h | |
| SPIFFSNVS.h | Module to enable the SPI Flash File System (SPIFFS) on the TI NVS driver |
| TRNG.h | TRNG driver header |
| TRNGCC26XX.h | TRNG driver implementation for the CC26XX family |
| types.h | |
| UART.h | Universal Asynchronous Receiver-Transmitter (UART) Driver |
| UARTCC26X0.h | UART driver implementation for a CC26X0 UART controller |
| UARTCC26X2.h | UART driver implementation for a CC26X2 UART controller |
| UARTCC26XX.h | UART driver implementation for a CC26XX UART controller |
| UDMACC26XX.h | UDMACC26XX driver implementation |
| unistd.h | |
| Watchdog.h | Watchdog driver interface |
| WatchdogCC26XX.h | Watchdog driver implementation for CC13XX/CC26XX |