Data Structures | Macros | Typedefs | Enumerations | Functions
ECDSA.h File Reference

Detailed Description

TI Driver for Elliptic Curve Digital Signature Algorithm.


Overview

The Elliptic Curve Digital Signature Algorithm (ECDSA) is a message authentication scheme between two parties based on operation on elliptic curves over finite fields.

Signing a message with ECDSA proves to the recipient that the sender of the message is in possession of the private key corresponding to the transmitted public key used during verification. For most practical systems, this ensures message authentication and integrity.

Steps involved

Usage

Before starting an ECDSA operation

Before starting an ECDSA operation, the application must do the following:

Signing a message

To sign a message using an agreed upon hash function and elliptic curve, the application must do the following:

Verifying a message

After receiving the message, public key, r, and s, the application should do the following to verify the signature:

General usage

The API expects elliptic curves as defined in ti/drivers/cryptoutils/ecc/ECCParams.h. Several commonly used curves are provided. Check the device-specific ECDSA documentation for curve type (short Weierstrass, Montgomery, Edwards) support for your device. ECDSA support for a curve type on a device does not imply curve-type support for other ECC schemes.

Public keys and shared secrets are points on an elliptic curve. These points can be expressed in several ways. The most common one is in affine coordinates as an X,Y pair. This API uses points expressed in affine coordinates. The point is stored as a concatenated array of X followed by Y in a location described by its CryptoKey.

This API accepts and returns the keying material of public keys according to the following table:

Curve Type Keying Material Array Array Length
Short Weierstrass [X, Y] 2 * Curve Param Length
Montgomery [X, Y] 2 * Curve Param Length
Edwards [X, Y] 2 * Curve Param Length

Synopsis

// Import ECDSA Driver definitions
// Since we are using default ECDSA_Params, we just pass in NULL for that parameter.
ecdsaHandle = ECDSA_open(0, NULL);
if (!ecdsaHandle) {
// Handle error
}
// Initialize myPrivateKey
CryptoKeyPlaintext_initKey(&myPrivateKey, myPrivateKeyingMaterial, sizeof(myPrivateKeyingMaterial));
CryptoKeyPlaintext_initKey(&pmsnKey, pmsn, sizeof(pmsn));
// Initialize the operation
ECDSA_OperationSign_init(&operationSign);
operationSign.curve = &ECCParams_NISTP256;
operationSign.myPrivateKey = &myPrivateKey;
operationSign.pmsn = &pmsnKey;
operationSign.hash = messageHash;
operationSign.r = r;
operationSign.s = s;
// Generate the signature
operationResult = ECDSA_sign(ecdsaHandle, &operationSign);
// Initialize theirPublicKey
CryptoKeyPlaintext_initKey(&theirPublicKey, theirPublicKeyingMaterial, sizeof(theirPublicKeyingMaterial));
ECDSA_OperationVerify_init(&operationVerify);
operationVerify.curve = &ECCParams_NISTP256;
operationVerify.theirPublicKey = &theirPublicKey;
operationVerify.hash = messageHash;
operationVerify.r = r;
operationVerify.s = s;
// Generate the keying material for myPublicKey and store it in myPublicKeyingMaterial
operationResult = ECDSA_verify(ecdsaHandle, &operationVerify);
// Close the driver
ECDSA_close(ecdsaHandle);
@anchor ti_drivers_ECDSA_Examples
# Examples #
## ECDSA sign with plaintext CryotoKeys #
@code
...
// This vector is taken from the NIST ST toolkit examples from ECDSA_Prime.pdf
uint8_t myPrivateKeyingMaterial[32] = {0x96, 0xBF, 0x85, 0x49, 0xC3, 0x79, 0xE4, 0x04,
0xED, 0xA1, 0x08, 0xA5, 0x51, 0xF8, 0x36, 0x23,
0x12, 0xD8, 0xD1, 0xB2, 0xA5, 0xFA, 0x57, 0x06,
0xE2, 0xCC, 0x22, 0x5C, 0xF6, 0xF9, 0x77, 0xC4};
uint8_t messageHashSHA256[32] = {0xC4, 0xA8, 0xC8, 0x99, 0x28, 0xCF, 0x80, 0xB6,
0xE4, 0x42, 0xD5, 0xBD, 0x28, 0x4D, 0xE3, 0xFD,
0x3A, 0x13, 0xD8, 0x65, 0x0C, 0x41, 0x1C, 0x21,
0x48, 0x95, 0x79, 0x2A, 0xA1, 0x41, 0x1A, 0xA4};
uint8_t pmsn[32] = {0xAE, 0x50, 0xEE, 0xFA, 0x27, 0xB4, 0xDB, 0x14,
0x9F, 0xE1, 0xFB, 0x04, 0xF2, 0x4B, 0x50, 0x58,
0x91, 0xE3, 0xAC, 0x4D, 0x2A, 0x5D, 0x43, 0xAA,
0xCA, 0xC8, 0x7F, 0x79, 0x52, 0x7E, 0x1A, 0x7A};
uint8_t r[32] = {0};
uint8_t s[32] = {0};
CryptoKey myPrivateKey;
CryptoKey pmsnKey;
ECDSA_Handle ecdsaHandle;
int_fast16_t operationResult;
// Since we are using default ECDSA_Params, we just pass in NULL for that parameter.
ecdsaHandle = ECDSA_open(0, NULL);
if (!ecdsaHandle) {
// Handle error
}
// Initialize myPrivateKey
CryptoKeyPlaintext_initKey(&myPrivateKey, myPrivateKeyingMaterial, sizeof(myPrivateKeyingMaterial));
CryptoKeyPlaintext_initKey(&pmsnKey, pmsn, sizeof(pmsn));
// Initialize the operation
ECDSA_OperationSign_init(&operationSign);
operationSign.curve = &ECCParams_NISTP256;
operationSign.myPrivateKey = &myPrivateKey;
operationSign.pmsn = &pmsnKey;
operationSign.hash = messageHash;
operationSign.r = r;
operationSign.s = s;
// Generate the signature
operationResult = ECDSA_sign(ecdsaHandle, &operationSign);
if (operationResult != ECDSA_STATUS_SUCCESS) {
// Handle error
}
// Send out signature
// r should be 0x4F, 0x10, 0x46, 0xCA, 0x9A, 0xB6, 0x25, 0x73,
// 0xF5, 0x3E, 0x0B, 0x1F, 0x6F, 0x31, 0x4C, 0xE4,
// 0x81, 0x0F, 0x50, 0xB1, 0xF3, 0xD1, 0x65, 0xFF,
// 0x65, 0x41, 0x7F, 0xD0, 0x76, 0xF5, 0x42, 0x2B
//
// s should be 0xF1, 0xFA, 0x63, 0x6B, 0xDB, 0x9B, 0x32, 0x4B,
// 0x2C, 0x26, 0x9D, 0xE6, 0x6F, 0x88, 0xC1, 0x98,
// 0x81, 0x2A, 0x50, 0x89, 0x3A, 0x99, 0x3A, 0x3E,
// 0xCD, 0x92, 0x63, 0x2D, 0x12, 0xC2, 0x42, 0xDC

ECDSA verify with plaintext CryotoKeys

...
// This vector is taken from the NIST ST toolkit examples from ECDSA_Prime.pdf
uint8_t theirPublicKeyingMaterial[64] = {0x19, 0x7A, 0xBC, 0x89, 0x08, 0xCD, 0x01, 0x82,
0xA3, 0xA2, 0x9E, 0x1E, 0xAD, 0xA0, 0xB3, 0x62,
0x1C, 0xBA, 0x98, 0x47, 0x73, 0x8C, 0xDC, 0xF1,
0xD3, 0xBA, 0x94, 0xFE, 0xFD, 0x8A, 0xE0, 0xB7,
0x09, 0x5E, 0xCC, 0x06, 0xC6, 0xBB, 0x63, 0xB5,
0x61, 0x9E, 0x52, 0x43, 0xAE, 0xC7, 0xAD, 0x63,
0x90, 0x72, 0x28, 0x19, 0xE4, 0x26, 0xB2, 0x4B,
0x7A, 0xBF, 0x9D, 0x95, 0x47, 0xF7, 0x03, 0x36};
uint8_t messageHashSHA256[32] = {0xC4, 0xA8, 0xC8, 0x99, 0x28, 0xCF, 0x80, 0xB6,
0xE4, 0x42, 0xD5, 0xBD, 0x28, 0x4D, 0xE3, 0xFD,
0x3A, 0x13, 0xD8, 0x65, 0x0C, 0x41, 0x1C, 0x21,
0x48, 0x95, 0x79, 0x2A, 0xA1, 0x41, 0x1A, 0xA4};
uint8_t r[32] = {0x4F, 0x10, 0x46, 0xCA, 0x9A, 0xB6, 0x25, 0x73,
0xF5, 0x3E, 0x0B, 0x1F, 0x6F, 0x31, 0x4C, 0xE4,
0x81, 0x0F, 0x50, 0xB1, 0xF3, 0xD1, 0x65, 0xFF,
0x65, 0x41, 0x7F, 0xD0, 0x76, 0xF5, 0x42, 0x2B};
uint8_t s[32] = {0xF1, 0xFA, 0x63, 0x6B, 0xDB, 0x9B, 0x32, 0x4B,
0x2C, 0x26, 0x9D, 0xE6, 0x6F, 0x88, 0xC1, 0x98,
0x81, 0x2A, 0x50, 0x89, 0x3A, 0x99, 0x3A, 0x3E,
0xCD, 0x92, 0x63, 0x2D, 0x12, 0xC2, 0x42, 0xDC};
CryptoKey theirPublicKey;
ECDSA_Handle ecdsaHandle;
int_fast16_t operationResult;
ECDSA_OperationVerify operationVerify;
// Since we are using default ECDSA_Params, we just pass in NULL for that parameter.
ecdsaHandle = ECDSA_open(0, NULL);
if (!ecdsaHandle) {
// Handle error
}
// Initialize theirPublicKey
CryptoKeyPlaintext_initKey(&theirPublicKey, theirPublicKeyingMaterial, sizeof(theirPublicKeyingMaterial));
ECDSA_OperationVerify_init(&operationVerify);
operationVerify.curve = &ECCParams_NISTP256;
operationVerify.theirPublicKey = &theirPublicKey;
operationVerify.hash = messageHash;
operationVerify.r = r;
operationVerify.s = s;
// Generate the keying material for myPublicKey and store it in myPublicKeyingMaterial
operationResult = ECDSA_verify(ecdsaHandle, &operationVerify);
if (operationResult != ECDSA_STATUS_SUCCESS) {
// Handle error
}
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/drivers/cryptoutils/ecc/ECCParams.h>
Include dependency graph for ECDSA.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ECDSA_Config
 ECDSA Global configuration. More...
 
struct  ECDSA_OperationSign
 Struct containing the parameters required for signing a message. More...
 
struct  ECDSA_OperationVerify
 Struct containing the parameters required for verifying a message. More...
 
union  ECDSA_Operation
 Union containing pointers to all supported operation structs. More...
 
struct  ECDSA_Params
 ECDSA Parameters. More...
 

Macros

#define ECDSA_STATUS_RESERVED   (-32)
 
#define ECDSA_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define ECDSA_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define ECDSA_STATUS_RESOURCE_UNAVAILABLE   (-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define ECDSA_STATUS_INVALID_PMSN   (-3)
 The PMSN passed into the the call is invalid. More...
 
#define ECDSA_STATUS_R_LARGER_THAN_ORDER   (-4)
 The r value passed in is larger than the order of the curve. More...
 
#define ECDSA_STATUS_S_LARGER_THAN_ORDER   (-5)
 The s value passed in is larger than the order of the curve. More...
 
#define ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE   (-6)
 The public key of the other party does not lie upon the curve. More...
 
#define ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME   (-7)
 A coordinate of the public key of the other party is too large. More...
 
#define ECDSA_STATUS_POINT_AT_INFINITY   (-8)
 The public key to verify against is the point at infinity. More...
 
#define ECDSA_STATUS_CANCELED   (-9)
 The ongoing operation was canceled. More...
 

Typedefs

typedef struct ECDSA_ConfigECDSA_Handle
 A handle that is returned from an ECDSA_open() call. More...
 
typedef struct ECDSA_Config ECDSA_Config
 ECDSA Global configuration. More...
 
typedef void(* ECDSA_CallbackFxn) (ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
 The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  ECDSA_ReturnBehavior { ECDSA_RETURN_BEHAVIOR_CALLBACK = 1, ECDSA_RETURN_BEHAVIOR_BLOCKING = 2, ECDSA_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation. More...
 
enum  ECDSA_OperationType { ECDSA_OPERATION_TYPE_SIGN = 1, ECDSA_OPERATION_TYPE_VERIFY = 2 }
 Enum for the operation types supported by the driver. More...
 

Functions

void ECDSA_init (void)
 This function initializes the ECDSA module. More...
 
void ECDSA_close (ECDSA_Handle handle)
 Function to close an ECDSA peripheral specified by the ECDSA handle. More...
 
ECDSA_Handle ECDSA_open (uint_least8_t index, ECDSA_Params *params)
 This function opens a given ECDSA peripheral. More...
 
void ECDSA_Params_init (ECDSA_Params *params)
 Function to initialize the ECDSA_Params struct to its defaults. More...
 
void ECDSA_OperationSign_init (ECDSA_OperationSign *operation)
 Function to initialize an ECDSA_OperationSign struct to its defaults. More...
 
void ECDSA_OperationVerify_init (ECDSA_OperationVerify *operation)
 Function to initialize an ECDSA_OperationSign struct to its defaults. More...
 
int_fast16_t ECDSA_sign (ECDSA_Handle handle, ECDSA_OperationSign *operation)
 Signs a hashed message. More...
 
int_fast16_t ECDSA_verify (ECDSA_Handle handle, ECDSA_OperationVerify *operation)
 Verifies a received signature matches a hash and public key. More...
 
int_fast16_t ECDSA_cancelOperation (ECDSA_Handle handle)
 Cancels an ongoing ECDSA operation. More...
 

Macro Definition Documentation

§ ECDSA_STATUS_RESERVED

#define ECDSA_STATUS_RESERVED   (-32)

Common ECDSA status code reservation offset. ECDSA driver implementations should offset status codes with ECDSA_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ECDSAXYZ_STATUS_ERROR0 ECDSA_STATUS_RESERVED - 0
#define ECDSAXYZ_STATUS_ERROR1 ECDSA_STATUS_RESERVED - 1
#define ECDSAXYZ_STATUS_ERROR2 ECDSA_STATUS_RESERVED - 2

§ ECDSA_STATUS_SUCCESS

#define ECDSA_STATUS_SUCCESS   (0)

Successful status code.

Functions return ECDSA_STATUS_SUCCESS if the function was executed successfully.

§ ECDSA_STATUS_ERROR

#define ECDSA_STATUS_ERROR   (-1)

Generic error status code.

Functions return ECDSA_STATUS_ERROR if the function was not executed successfully.

§ ECDSA_STATUS_RESOURCE_UNAVAILABLE

#define ECDSA_STATUS_RESOURCE_UNAVAILABLE   (-2)

An error status code returned if the hardware or software resource is currently unavailable.

ECDSA driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ ECDSA_STATUS_INVALID_PMSN

#define ECDSA_STATUS_INVALID_PMSN   (-3)

The PMSN passed into the the call is invalid.

PMSNs must be integers in the interval [1, n - 1], where n is the order of the curve.

§ ECDSA_STATUS_R_LARGER_THAN_ORDER

#define ECDSA_STATUS_R_LARGER_THAN_ORDER   (-4)

The r value passed in is larger than the order of the curve.

Signature components (r and s) must be integers in the interval [1, n - 1], where n is the order of the curve.

§ ECDSA_STATUS_S_LARGER_THAN_ORDER

#define ECDSA_STATUS_S_LARGER_THAN_ORDER   (-5)

The s value passed in is larger than the order of the curve.

Signature components (r and s) must be integers in the interval [1, n - 1], where n is the order of the curve.

§ ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE

#define ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE   (-6)

The public key of the other party does not lie upon the curve.

The public key received from the other party does not lie upon the agreed upon curve.

§ ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME

#define ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME   (-7)

A coordinate of the public key of the other party is too large.

A coordinate of the public key received from the other party is larger than the prime of the curve. This implies that the point was not correctly generated on that curve.

§ ECDSA_STATUS_POINT_AT_INFINITY

#define ECDSA_STATUS_POINT_AT_INFINITY   (-8)

The public key to verify against is the point at infinity.

The point at infinity is not a valid input.

§ ECDSA_STATUS_CANCELED

#define ECDSA_STATUS_CANCELED   (-9)

The ongoing operation was canceled.

Typedef Documentation

§ ECDSA_Handle

typedef struct ECDSA_Config* ECDSA_Handle

A handle that is returned from an ECDSA_open() call.

§ ECDSA_Config

typedef struct ECDSA_Config ECDSA_Config

ECDSA Global configuration.

The ECDSA_Config structure contains a set of pointers used to characterize the ECDSA driver implementation.

This structure needs to be defined before calling ECDSA_init() and it must not be changed thereafter.

See also
ECDSA_init()

§ ECDSA_CallbackFxn

typedef void(* ECDSA_CallbackFxn) (ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)

The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the ECDSA operation.
returnStatusThe result of the ECDSA operation. May contain an error code if the result is the point at infinity for example.
operationA union of pointers to operation structs. Only one type of pointer is valid per call to the callback function. Which type is currently valid is determined by /c operationType. The union allows easier access to the struct's fields without the need to typecase the result.
operationTypeThis parameter determined which operation the callback refers to and which type to access through /c operation.

Enumeration Type Documentation

§ ECDSA_ReturnBehavior

The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation.

Not all ECDSA operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

ECDSA functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
ECDSA_RETURN_BEHAVIOR_CALLBACK X X X
ECDSA_RETURN_BEHAVIOR_BLOCKING X
ECDSA_RETURN_BEHAVIOR_POLLING X X X
Enumerator
ECDSA_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the ECDSA operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

ECDSA_RETURN_BEHAVIOR_BLOCKING 

The function call will block while ECDSA operation goes on in the background. ECDSA operation results are available after the function returns.

ECDSA_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while ECDSA operation goes on in the background. ECDSA operation results are available after the function returns.

§ ECDSA_OperationType

Enum for the operation types supported by the driver.

Enumerator
ECDSA_OPERATION_TYPE_SIGN 
ECDSA_OPERATION_TYPE_VERIFY 

Function Documentation

§ ECDSA_init()

void ECDSA_init ( void  )

This function initializes the ECDSA module.

Precondition
The ECDSA_config structure must exist and be persistent before this function can be called. This function must also be called before any other ECDSA driver APIs. This function call does not modify any peripheral registers.

§ ECDSA_close()

void ECDSA_close ( ECDSA_Handle  handle)

Function to close an ECDSA peripheral specified by the ECDSA handle.

Precondition
ECDSA_open() has to be called first.
Parameters
handleAn ECDSA handle returned from ECDSA_open()
See also
ECDSA_open()

§ ECDSA_open()

ECDSA_Handle ECDSA_open ( uint_least8_t  index,
ECDSA_Params params 
)

This function opens a given ECDSA peripheral.

Precondition
ECDSA controller has been initialized using ECDSA_init()
Parameters
indexLogical peripheral number for the ECDSA indexed into the ECDSA_config table
paramsPointer to an parameter block, if NULL it will use default values.
Returns
An ECDSA_Handle on success or a NULL on an error or if it has been opened already.
See also
ECDSA_init()
ECDSA_close()

§ ECDSA_Params_init()

void ECDSA_Params_init ( ECDSA_Params params)

Function to initialize the ECDSA_Params struct to its defaults.

Parameters
paramsAn pointer to ECDSA_Params structure for initialization

Defaults values are: returnBehavior = ECDSA_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ ECDSA_OperationSign_init()

void ECDSA_OperationSign_init ( ECDSA_OperationSign operation)

Function to initialize an ECDSA_OperationSign struct to its defaults.

Parameters
operationA pointer to ECDSA_OperationSign structure for initialization

Defaults values are all zeros.

§ ECDSA_OperationVerify_init()

void ECDSA_OperationVerify_init ( ECDSA_OperationVerify operation)

Function to initialize an ECDSA_OperationSign struct to its defaults.

Parameters
operationAn pointer to ECDSA_OperationSign structure for initialization

Defaults values are all zeros.

§ ECDSA_sign()

int_fast16_t ECDSA_sign ( ECDSA_Handle  handle,
ECDSA_OperationSign operation 
)

Signs a hashed message.

ECDSA_sign() generates a signature (r, s) of a hash of a message.

Precondition
ECDSA_OperationSign_init() must be called on operation first. The driver must have been opened by calling ECDSA_open() first.
Parameters
[in]handleAn ECDSA handle returned from ECDSA_open()
[in]operationA struct containing the pointers to the buffers necessary to perform the operation
See also
ECDSA_verify()
Return values
ECDSA_STATUS_SUCCESSThe operation succeeded.
ECDSA_STATUS_ERRORThe operation failed.
ECDSA_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECDSA_STATUS_CANCELEDThe operation was canceled.
ECDSA_STATUS_INVALID_PMSNThe PMSN passed into the the call is invalid.

§ ECDSA_verify()

int_fast16_t ECDSA_verify ( ECDSA_Handle  handle,
ECDSA_OperationVerify operation 
)

Verifies a received signature matches a hash and public key.

Precondition
ECDSA_OperationVerify_init() must be called on operation first. The driver must have been opened by calling ECDSA_open() first.
Parameters
[in]handleAn ECDSA handle returned from ECDSA_open()
[in]operationA struct containing the pointers to the buffers necessary to perform the operation
See also
ECDSA_sign()
Return values
ECDSA_STATUS_SUCCESSThe operation succeeded.
ECDSA_STATUS_ERRORThe operation failed. This is the return status if the signature did not match.
ECDSA_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
ECDSA_STATUS_CANCELEDThe operation was canceled.
ECDSA_STATUS_R_LARGER_THAN_ORDERThe r value passed in is larger than the order of the curve.
ECDSA_STATUS_S_LARGER_THAN_ORDERThe s value passed in is larger than the order of the curve.
ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVEThe public key of the other party does not lie upon the curve.
ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIMEOne of the public key coordinates is larger the the curve's prime.
ECDSA_STATUS_POINT_AT_INFINITYThe public key to verify against is the point at infinity.

§ ECDSA_cancelOperation()

int_fast16_t ECDSA_cancelOperation ( ECDSA_Handle  handle)

Cancels an ongoing ECDSA operation.

Asynchronously cancels an ECDSA operation. Only available when using ECDSA_RETURN_BEHAVIOR_CALLBACK or ECDSA_RETURN_BEHAVIOR_BLOCKING. The operation will terminate as though an error occured. The return status code of the operation will be ECDSA_STATUS_CANCELED.

Parameters
handleHandle of the operation to cancel
Return values
ECDSA_STATUS_SUCCESSThe operation was canceled.
ECDSA_STATUS_ERRORThe operation was not canceled. There may be no operation to cancel.
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale