xWRL6432 MMWAVE-L-SDK  05.05.00.00
trackerproc.h File Reference

Introduction

Implements Tracker processing functionality.

Go to the source code of this file.

Data Structures

struct  DPU_TrackerProc_StaticConfig
 TrackerProc static configuration. More...
 
struct  DPU_TrackerProc_HW_Resources
 TrackerProc DPU Hardware resources. More...
 
struct  DPU_TrackerProc_Config
 Tracking configuration. More...
 
struct  trackerProc_Target
 Structure holds the target features. More...
 
struct  trackerProc_TargetDescrHandle
 
struct  DPU_TrackerProc_OutParams
 TrackerProc output parameter structure. More...
 
struct  trackerProc_Point
 Structure holds the message body for the Point Cloud. More...
 
struct  trackerProcObjType
 TrackerProc DPU Object. More...
 

Macros

#define DPU_TRACKERPROC_POINT_CLOUD_CARTESIAN_BYTE_ALIGNMENT   DPIF_POINT_CLOUD_CARTESIAN_CPU_BYTE_ALIGNMENT
 Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. More...
 
#define DPU_TRACKERPROC_POINT_CLOUD_SIDE_INFO_BYTE_ALIGNMENT   DPIF_POINT_CLOUD_SIDE_INFO_CPU_BYTE_ALIGNMENT
 Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. More...
 
#define DPU_TRACKERPROC_MAX_NUM_TRACKS   TRACKER_MAX_NUM_TR
 Maximum number of tracks. More...
 
#define DP_ERRNO_TRACKER_PROC_BASE   (MMWAVE_ERRNO_DPU_BASE -900)
 
#define DPU_TRACKERPROC_EINVAL   (DP_ERRNO_TRACKER_PROC_BASE-1)
 Error Code: Invalid argument. More...
 
#define DPU_TRACKERPROC_ENOMEM   (DP_ERRNO_TRACKER_PROC_BASE-2)
 Error Code: Out of memory. More...
 
#define DPU_TRACKERPROC_EINTERNAL   (DP_ERRNO_TRACKER_PROC_BASE-3)
 Error Code: Internal error. More...
 
#define DPU_TRACKERPROC_ENOTIMPL   (DP_ERRNO_TRACKER_PROC_BASE-4)
 Error Code: Not implemented. More...
 
#define DPU_TRACKERPROC_EINPROGRESS   (DP_ERRNO_TRACKER_PROC_BASE-5)
 Error Code: In Progress. More...
 
#define DPU_TRACKERPROC_ECMD   (DP_ERRNO_TRACKER_PROC_BASE-6)
 Error Code: Invalid control command. More...
 
#define DPU_TRACKERPROC_EMAX_NUM_TRACKS_EXCEEDED   (DP_ERRNO_TRACKER_PROC_BASE-7)
 Error Code: Maximum number of tracks exceeded. More...
 
#define TRACKERPROC_OUTPUT_TARGET_LIST   7
 
#define TRACKERPROC_OUTPUT_TARGET_INDEX   8
 
#define TRACKERPROC_ACCEL_PARAMS_NUM_ELEMENTS   3
 

Typedefs

typedef uint8_t trackerProc_TargetIndex
 
typedef void * DPU_TrackerProc_Handle
 TrackerProc DPU Handle. More...
 

Enumerations

enum  DPU_TrackerProc_Cmd { DPU_TrackerProc_Cmd_sensorTiltCfg }
 TrackerProc control command. More...
 

Functions

DPU_TrackerProc_Handle DPU_TrackerProc_init (int32_t *errCode)
 
int32_t DPU_TrackerProc_config (DPU_TrackerProc_Handle handle, DPU_TrackerProc_Config *pConfigIn)
 
int32_t DPU_TrackerProc_process (DPU_TrackerProc_Handle handle, uint32_t numObjsIn, DPIF_PointCloudCartesianExt *cfarDetObjList, DPU_TrackerProc_OutParams *outParams)
 
int32_t DPU_TrackerProc_control (DPU_TrackerProc_Handle handle, DPU_TrackerProc_Cmd cmd, void *arg, uint32_t argSize)
 
int32_t DPU_TrackerProc_deinit (DPU_TrackerProc_Handle handle)
 
int32_t DPU_TrackerProc_CartesianToSpherical (uint16_t numPoints, DPIF_PointCloudCartesianExt *objCartExtIn, trackerProc_Point *detObjSphericalOut)
 

Macro Definition Documentation

◆ DPU_TRACKERPROC_POINT_CLOUD_CARTESIAN_BYTE_ALIGNMENT

#define DPU_TRACKERPROC_POINT_CLOUD_CARTESIAN_BYTE_ALIGNMENT   DPIF_POINT_CLOUD_CARTESIAN_CPU_BYTE_ALIGNMENT

Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation.

◆ DPU_TRACKERPROC_POINT_CLOUD_SIDE_INFO_BYTE_ALIGNMENT

#define DPU_TRACKERPROC_POINT_CLOUD_SIDE_INFO_BYTE_ALIGNMENT   DPIF_POINT_CLOUD_SIDE_INFO_CPU_BYTE_ALIGNMENT

Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation.

◆ DPU_TRACKERPROC_MAX_NUM_TRACKS

#define DPU_TRACKERPROC_MAX_NUM_TRACKS   TRACKER_MAX_NUM_TR

Maximum number of tracks.

◆ DP_ERRNO_TRACKER_PROC_BASE

#define DP_ERRNO_TRACKER_PROC_BASE   (MMWAVE_ERRNO_DPU_BASE -900)

◆ TRACKERPROC_OUTPUT_TARGET_LIST

#define TRACKERPROC_OUTPUT_TARGET_LIST   7

◆ TRACKERPROC_OUTPUT_TARGET_INDEX

#define TRACKERPROC_OUTPUT_TARGET_INDEX   8

◆ TRACKERPROC_ACCEL_PARAMS_NUM_ELEMENTS

#define TRACKERPROC_ACCEL_PARAMS_NUM_ELEMENTS   3

Typedef Documentation

◆ trackerProc_TargetIndex

typedef uint8_t trackerProc_TargetIndex

◆ DPU_TrackerProc_Handle

typedef void* DPU_TrackerProc_Handle

TrackerProc DPU Handle.

Enumeration Type Documentation

◆ DPU_TrackerProc_Cmd

TrackerProc control command.

The enum defines the TrackerProc supported run time command

Enumerator
DPU_TrackerProc_Cmd_sensorTiltCfg 

Command to update configuration.

Function Documentation

◆ DPU_TrackerProc_init()

DPU_TrackerProc_Handle DPU_TrackerProc_init ( int32_t *  errCode)

Description
The function is TrackerProc DPU init function. It allocates memory to store its internal data object and returns a handle if it executes successfully.

Parameters
[in]errCodePointer to errCode generates from the API
Return values
Success- valid TrackerProc handle
Error- NULL

◆ DPU_TrackerProc_config()

int32_t DPU_TrackerProc_config ( DPU_TrackerProc_Handle  handle,
DPU_TrackerProc_Config pConfigIn 
)

Description
The function is trackerProc DPU config function.

Precondition
DPU_TrackerProc_init() has been called
Parameters
[in]handletrackerProc DPU handle
[in]pConfigInPointer to trackerProc configuration data structure
Return values
Success- 0
Error- <0

◆ DPU_TrackerProc_process()

int32_t DPU_TrackerProc_process ( DPU_TrackerProc_Handle  handle,
uint32_t  numObjsIn,
DPIF_PointCloudCartesianExt *  cfarDetObjList,
DPU_TrackerProc_OutParams outParams 
)

Description
The function is trackerProc DPU process function.

Precondition
DPU_trackerProc_init() has been called
Parameters
[in]handletrackerProc DPU handle
[in]numObjsInnumber of input points
[in]cfarDetObjListinput point cloud in Cartesian format
[out]outParamsDPU output parameters
Return values
Success- 0
Error- <0

◆ DPU_TrackerProc_control()

int32_t DPU_TrackerProc_control ( DPU_TrackerProc_Handle  handle,
DPU_TrackerProc_Cmd  cmd,
void *  arg,
uint32_t  argSize 
)

Description
The function is the TrackerProc DPU control function.

Precondition
DPU_TrackerProc_init() has been called
Parameters
[in]handleTrackerProc DPU handle
[in]cmdTrackerProc DPU control command
[in]argTrackerProc DPU control argument pointer
[in]argSizeTrackerProc DPU control argument size
Return values
Success- 0
Error- <0

◆ DPU_TrackerProc_deinit()

int32_t DPU_TrackerProc_deinit ( DPU_TrackerProc_Handle  handle)

Description
The function is the TrackerProc DPU deinit function. It frees up the resources allocated during init.

Precondition
DPU_TrackerProc_init() has been called
Parameters
[in]handleTrackerProc DPU handle
Return values
Success- 0
Error- <0

◆ DPU_TrackerProc_CartesianToSpherical()

int32_t DPU_TrackerProc_CartesianToSpherical ( uint16_t  numPoints,
DPIF_PointCloudCartesianExt *  objCartExtIn,
trackerProc_Point detObjSphericalOut 
)

Description
Utility function to convert Cartesian point cloud to Spherical.

Precondition
None
Parameters
[in]numPointsNumber of input points
[in]objCartExtInInput point cloud in Cartesian format
[out]detObjSphericalOutOutput point cloud in spherical format
Return values
Success- 0
Error- <0