AoA DPU HW configuration parameters.
The structure is used to hold the HW configuration parameters for the AoA DPU
Data Fields | |
DPU_AoAProcHWA_EdmaCfg | edmaCfg |
EDMA configuration. More... | |
DPU_AoAProcHWA_HwaCfg | hwaCfg |
HWA configuration. More... | |
DPIF_RadarCube | radar_1D_FFT_Cube |
Radar Cube. More... | |
DPIF_Anglemat | angleMat |
Angle Matrix on which Elevation-Azimuth FFT is to be applied. More... | |
uint32_t * | maxVal_elev_azim |
Matrix where the azimuth-elevation FFT max values is stored (this matrix should be in M4 for ease of computation. More... | |
Edma_IntrObject * | intrObj |
EDMA interrupt object. More... | |
DPU_AoAProcHWA_EdmaCfg DPU_AoAProcHWA_HW_Resources::edmaCfg |
EDMA configuration.
DPU_AoAProcHWA_HwaCfg DPU_AoAProcHWA_HW_Resources::hwaCfg |
HWA configuration.
DPIF_RadarCube DPU_AoAProcHWA_HW_Resources::radar_1D_FFT_Cube |
Radar Cube.
DPIF_Anglemat DPU_AoAProcHWA_HW_Resources::angleMat |
Angle Matrix on which Elevation-Azimuth FFT is to be applied.
uint32_t* DPU_AoAProcHWA_HW_Resources::maxVal_elev_azim |
Matrix where the azimuth-elevation FFT max values is stored (this matrix should be in M4 for ease of computation.
Edma_IntrObject* DPU_AoAProcHWA_HW_Resources::intrObj |
EDMA interrupt object.