Base error code for the cfarProc DPU is defined in the
#define DPU_CFARPROCHWA_EINVAL (DP_ERRNO_CFAR_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_CFARPROCHWA_EINVAL__DET_MATRIX_FORMAT (DP_ERRNO_CFAR_PROC_BASE-2) |
Error Code: Invalid detection matrix format argument.
#define DPU_CFARPROCHWA_EINVAL__NUM_PARAM_SETS (DP_ERRNO_CFAR_PROC_BASE-3) |
Error Code: Invalid number of param sets.
#define DPU_CFARPROCHWA_ENOMEM (DP_ERRNO_CFAR_PROC_BASE-10) |
Error Code: Out of memory when allocating using MemoryP_osal.
#define DPU_CFARPROCHWA_ENOMEM__DET_MATRIX_EXCEEDS_HWA_INP_MEM (DP_ERRNO_CFAR_PROC_BASE-11) |
Error Code: HWA input memory for detection matrix is not sufficient.
#define DPU_CFARPROCHWA_ENOMEMALIGN_DET_MATRIX (DP_ERRNO_CFAR_PROC_BASE-12) |
Error Code: Memory not aligned for detection matrix (detMatrix.data)
#define DPU_CFARPROCHWA_ENOMEMALIGN_HWA_MEM_OUT_RANGE (DP_ERRNO_CFAR_PROC_BASE-15) |
Error Code: Memory not aligned for DPU_CFARProcHWA_HW_Resources::hwaMemOutDetList.
#define DPU_CFARPROCHWA_NUM_RANGE_BINS_EXCEDED_LIMIT (DP_ERRNO_CFAR_PROC_BASE-18) |
Error Code: Memory.
#define DPU_CFARPROCEDMA_ESEMA (DP_ERRNO_CFAR_PROC_BASE-19) |
Error Code: Semaphore.
#define DPU_CFARPROCHWA_EINTERNAL (DP_ERRNO_CFAR_PROC_BASE-20) |
Error Code: Internal error.
#define DPU_CFARPROCHWA_EHWA_PARAM_SAVE_LOC_SIZE (DP_ERRNO_CFAR_PROC_BASE-21) |
Error Code: Insufficient memory to save HWA param sets.
#define DPU_CFARPROCHWA_ENOTIMPL (DP_ERRNO_CFAR_PROC_BASE-30) |
Error Code: Not implemented.
#define DPU_CFARPROCHWA_ESEMA (DP_ERRNO_CFAR_PROC_BASE-40) |
Error Code: Semaphore error.