2. Release Specific¶
2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) provides the core foundation and building blocks that facilitate application software development on TI’s embedded processors. This Release Notes focuses on the Real-time operating system (RTOS).
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
2.1.3. Documentation¶
- Getting Started Guide: Provides information on getting the software and running basic examples/demonstrations bundled in the SDK.
- Migration Guide Provides migration information for applications built on top of the Processor SDK for RTOS.
- Software Developer Guide Provides information on features, functions, delivery package and, compile tools for the Processor SDK RTOS release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
/processor_sdk_rtos_<SOC>_<version>/docsand available to view from the software download page. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 05.00.00¶
Released July 2018.
What’s New
New Features
- AM335x,AM437x,AM57x,K2G
- Uniflash Flash programmer: Available as Early Adopter feature in this release. Includes flashing support through JTAG and UART for following peripherals and EVMs
- SPI: AMIC110 ICE, AM335x EVM, AM335x ICE
- QSPI: AM437x IDK, AM571x IDK,AM572x IDK,AM574x IDK,K2G ICE,K2G EVM
- K2G
- Performance Audio Demo Framework: Demo Audio Application illustrating integration of I/O, auto detection,decoding,audio stream processing and encoding
UART AppLoader: Two stage bootloader support through UART interface
Improved OOB experience for overall Building SDK with introduction of RULES_MAKE based environment. All envrionment variable dependency for processor SDK updates handled during post installation step
Component Version
The following software components and host tools are bundled with the SDK installer. See the Software Developer Guide for more information on each item.
Note
| Component | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| CG_XML | 2.41.0 | X | X | X | X | X | X | X | X | X | X | X |
| CTOOLSLIB | 2.2.0.0 | X | X | X | X | X | X | X | ||||
| DSPLIB | 3.4.0.0 | X | X | X | X | X | X | X | X | X | ||
| EDMA3 LLD | 2.12.5.30 | X | X | X | X | X | X | X | X | X | X | X |
| FC | 3.40.2.7 | X | X | X | X | X | X | X | ||||
| FFTLIB | 3.1.0.0 | X | ||||||||||
| IMGLIB | 3.1.1.0 | X | X | X | X | X | X | X | ||||
| IPC | 3.47.2.0 | X | X | X | X | X | X | X | X | |||
| LIBARCH | 1.0.0.0 | X | ||||||||||
| LINALG | 1.2.0.0 | X | ||||||||||
| MATHLIB | 3.1.1.0 | X | X | X | X | X | X | X | X | X | ||
| MPM | 3.0.4.0 | X | X | X | X | |||||||
| NDK | 2.26.0.0 | X | X | X | X | X | X | X | X | X | X | X |
| OPENMP | 2.6.2 | X | X | X | X | X | X | X | ||||
| PDK | 1.0.11 | 1.0.11 | 1.0.11 | 4.0.10 | 4.0.10 | 4.0.10 | 1.0.10 | 2.0.10 | 2.0.10 | 1.0.5 | 1.0.5 | |
| SYS/BIOS | 6.52.0.12 | X | X | X | X | X | X | X | X | X | X | X |
| UIA | 2.21.2.07 | X | X | X | X | X | X | X | X | X | ||
| XDAIS | 7.24.0.4 | X | X | X | X | X | X | X | X | X | ||
| XDCTOOLS | 3.50.03.33 | X | X | X | X | X | X | X | X | X | X | X |
The following compilers are bundled with the SDK installer:
| Compiler | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| GNU ARM Embedded | 6-2017-q1 | A8 | A9 | A15 | A15 | A15 | A15 | A15 | ||||
| TI ARM CGT | 16.9.3 | M4 | A15(SBL) | ARM9 | ARM9 | |||||||
| TI C6000 CGT | 8.2.2 | C66x | C66x | C66x | C66x | C66x | C66x | C66x | C74x | C74x | ||
| TI PRU CGT | 2.2.1 | PRU | PRU | PRU | PRU |
The SDK uses Code Composer Studio (CCS) as the integrated development environment (IDE) for all devices and EVMs:
| Component | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| CCS | 8.0.0.16 | X | X | X | X | X | X | X | X | X | X | X |
If you need to install CCS, see the CCS installation section in the Getting Started Guide for options to select for Processor-SDK.
Change log
Updated
- CCS 8.0.0.16
- PDK for all platforms
2.1.5. Fixed Issues¶
| Record ID | Platform | Summary |
|---|---|---|
| PRSDK-642 | * | RTOS: SDK components should be signed to avoid Eclipse/CCS warning when importing |
| PRSDK-3718 | AM57x | L3/L4 Interconnect CLKSEL configuration does not take to effect |
| PRSDK-3030 | omap L13x | SPI driver Interrupt mode is not functional |
| PRSDK-3856 | AM335x AM437x | StarterWare build from the PDK starterware folder fails on Windows OS |
| IPC-217 | C667x,k2h,k2e | IPC listMP corruption |
| PRSDK-3859 | am57xx,c665x,c667x omapl13x,keystone2 c674x | Audio benchmark starterkit demo fails to build in Windows with Rules.make environment setup |
| PRSDK-3865 | am57xx,c665x,c667x omapl13x,keystone2 c674x | SPI driver doesn`t support timeout |
| PRSDK-4013 | k2h | Client Socket recv() returns -1 with large stream of data |
| PRSDK-3749 | K2G | USB Spurrious interrupt in device mode config |
| PRSDK-3932 | AMIC110 | DDR Less bootloader support |
| PRSDK-4182 | AM57xx | Global interrupt disabling in EMAC driver breaks real time task |
| PRSDK-4012 | AM335x AM437x | Update to use -Wl, –start-group -Wl, –end-group during linking with GCC compiler |
| PRSDK-3866 | AM57xx | DSP1 image of IPC ex02_messageq example doesn’t work |
| PRSDK-3867 | c674x, omapl13x | MMCSD examples do not detect SD card insertion |
| PRSDK-3933 | AM57x | AM57x Board library sets L3MAIN1 and L4CFG CLKSTCTRL to Reserved_2 |
| PRSDK-4000 | k2g,omapl13x | Aud/CMB loopback test and Audio pre-processing demos failure |
| PRSDK-4048 | k2l | K2L boot loader failure in SPI boot mode |
2.1.6. Supported Platforms¶
2.1.6.1. Devices¶
The following table lists all supported devices for a given installer.
| Installer | Platform/SOC | Supported Devices | |
|---|---|---|---|
| RTOS-AM335X | AM335x | AM3351, AM3352, AM3354, AM3356, AM3357, AM3358, AM3359 | |
| AMIC11x | AMIC110 | ||
| RTOS-AM437X | AM437x | AM4376, AM4377, AM4378, AM4379 | |
| RTOS-AM57X | AM57x | AM5706, AM5708, AM5716, AM5718, AM5726, AM5728, AM5746, AM5748 | |
| RTOS-C665X | C665x | C6652, C6654, C6655, C6657 | |
| RTOS-C667X | C667x | C6671, C6672, C6674, C6678 | |
| RTOS-K2E | K2E | 66AK2E02, 66AK2E05, AM5K2E02, AM5K2E04 | |
| RTOS-K2G | K2G | 66AK2G02 | |
| RTOS-K2HK | K2H | 66AK2H06, 66AK2H12, 66AK2H14 | |
| K2K | TCI6638K2K | ||
| RTOS-K2L | K2L | 66AK2L06 | |
| RTOS-OMAPL137 | OMAP-L1x | OMAP-L137, C6743, C6745, C6747 | |
| RTOS-OMAPL138 | OMAP-L1x | OMAP-L138, C6742, C6746, C6748 | |
2.1.6.2. Evaluation Modules¶
See Processor SDK Supported Platforms page for a list of supported EVMs per platform and links to more information.
2.1.6.3. Demonstrations¶
See Examples and Demonstrations page for a list of demonstrations per platform and EVM.
2.1.6.4. Drivers¶
The following tables show RTOS driver availability per platform and EVM. A shaded box implies that the feature is not applicable for that platform/EVM.
Sitara devices
| Feature | Platform/SOC | AM335x EVM | AM437x EVM | AM57x EVM | ||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| AM335x | AM437x | AM57x | GP | ICE | SK | BBB | GP | IDK | SK | GP | IDK | |
| CSL | X | X | X | X | X | X | X | X | X | X | X | X |
| EMAC | X | X | X | X | X | X | X | X | X | X | X | X |
| EDMA3 | X | X | X | X | X | X | ||||||
| GPIO | X | X | X | X | X | X | X | X | X | |||
| GPMC | X | X | X | X | ||||||||
| I2C | X | X | X | X | X | X | X | X | X | X | X | X |
| PRUSS-I2C f/w | X | X | X | X | X | X | ||||||
| ICSS-EMAC | X | X | X | X | X | X | ||||||
| McASP | X | X | X | X | X | X | ||||||
| McSPI | X | X | X | X | X | X | ||||||
| MMC-SD | X | X | X | X | X | X | X | X | X | X | X | X |
| PCIe | X | X | ||||||||||
| PM | X | X | X | X | ||||||||
| PRUSS | X | X | X | X | X | X | ||||||
| QSPI | X | X | X | X | X | |||||||
| UART | X | X | X | X | X | X | X | X | X | X | X | X |
| USB | X | X | X | X | X | X | X | |||||
| USB Device Audio | X | X | ||||||||||
| USB Device Bulk | X | X | X | X | X | X | ||||||
| VPS | X | X | X | |||||||||
DSP devices - K2x, C66x
| Feature | Platform/SOC | K2 EVM | C66x EVM | ||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| K2H/K2K | K2E | K2L | K2G | C665x | C667x | K2H | K2E | K2L | K2G | K2G-ICE | C665x | C667x | |
| CSL | X | X | X | X | X | X | X | X | X | X | X | X | X |
| AIF2 | X | X | |||||||||||
| BCP | X | X | X | X | |||||||||
| CPPI | X | X | X | X | X | X | X | X | X | X | X | X | X |
| DFE | X | X | |||||||||||
| EDMA3 | X | X | X | X | X | X | X | X | X | X | X | X | X |
| EMAC | X | X | X | X | X | ||||||||
| FFTC | X | X | X | X | |||||||||
| GPIO | X | X | X | X | X | X | X | X | X | X | X | X | X |
| HYPLNK | X | X | X | X | X | X | X | X | |||||
| ICSS-EMAC | X | X | |||||||||||
| I2C | X | X | X | X | X | X | X | X | X | X | X | X | X |
| IQN2 | X | X | |||||||||||
| McASP | X | X | |||||||||||
| McBSP | X | X | X | X | |||||||||
| MMAP | X | X | X | X | |||||||||
| MMC-SD | X | X | X | ||||||||||
| NWAL | X | X | X | X | X | X | X | X | |||||
| PA | X | X | X | X | X | X | X | X | |||||
| PCIe | X | X | X | X | X | X | X | X | X | X | X | X | |
| QMSS | X | X | X | X | X | X | X | X | X | X | X | X | X |
| RM | X | X | X | X | X | X | X | X | X | X | X | X | X |
| SA | X | X | X | X | X | X | X | X | X | X | |||
| SPI | X | X | X | X | X | X | X | X | X | X | X | X | X |
| SRIO | X | X | X | X | X | X | |||||||
| TCP3D | X | X | X | X | X | X | |||||||
| TSIP | X | X | X | X | |||||||||
| UART | X | X | X | X | X | X | X | X | X | X | X | X | X |
| USB | X | X | |||||||||||
| USB Device Audio | |||||||||||||
| USB Device Bulk | X | ||||||||||||
DSP devices - OMAP-L13x, C674x
| Feature | Platform/SOC | OMAP-L137 EVM | OMAP-L138 EVM | ||
|---|---|---|---|---|---|
| OMAP-L137 | OMAP-L138 | 137/6747 SK | LCDK138 | LCDK6748 | |
| CSL | X | X | X | X | X |
| EDMA3 | X | X | X | X | X |
| EMAC | X | X | X | X | X |
| GPIO | X | X | X | X | X |
| I2C | X | X | X | X | X |
| McASP | X | X | X | X | X |
| MMC-SD | X | X | X | X | X |
| SPI | X | X | X | X | X |
| UART | X | X | X | X | X |
| USB | X | X | X | X | X |
| USB Device Audio | X | X | X | X | X |
Unsupported Features
- In general driver support is available across all cores within an SOC with following exceptions
| Feature | Not supported | |
|---|---|---|
| SOC | CPU/Core | |
| McASP | AM57x | M4 |
| USB | AM57x | C66x |
| USB | AM57x | M4 |
| McBSP | K2G | A15 |
| McBSP | OMAP-L13x | ARM9 |
| All Drivers | K2x | A15 |
2.1.6.5. Other Features¶
The following table shows other feature availability per platform and EVM:
Sitara devices
| Feature | Platform/SOC | AM335x EVM | AM437x EVM | AM57x EVM | ||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| AM335x | AM437x | AM57x | GP | ICE | SK | BBB | GP | IDK | SK | GP | IDK | |
| Board Support | X | X | X | X | X | X | X | X | X | X | X | X |
| Boot (SBL) | X | X | X | X | X | X | X | X | X | X | X | X |
| Diagnostics | X | X | X | X | X | X | X | |||||
| FATFS | X | X | X | X | X | X | X | X | X | |||
| NDK-NIMU(CPSW) | X | X | X | X | X | X | X | X | X | X | X | X |
| NDK-NIMU(ICSS) | X | X | X | X | X | X | ||||||
| CC-LINK IE Field Basic(CPSW) | X | X | X | X | X | X | X | X | X | X | X | X |
| CC-Link IE Field Basic(ICSS) | X | X | X | X | X | X | ||||||
DSP devices - K2x, C66x
| Feature | Platform/SOC | K2 EVM | C66x EVM | ||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| K2H/K2K | K2E | K2L | K2G | C665x | C667x | K2H | K2E | K2L | K2G | K2G-ICE | C665x | C667x | |
| Board Support | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Boot (IBL/SBL) | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Diagnostics | X | X | X | ||||||||||
| FATFS | X | X | X | ||||||||||
| Fault Management | X | X | X | X | X | X | |||||||
| IPC Transport (QMSS) | X | X | X | X | X | X | X | X | X | X | |||
| IPC Transport (SRIO) | X | X | X | X | X | X | |||||||
| MAD-UTIL | X | X | X | X | |||||||||
| Network (CPSW) | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Network (ICSS) | X | X | |||||||||||
| CC-Link IE Field Basic(ICSS) | X | X | |||||||||||
| Platform Library (obsolete) | X | X | X | X | X | X | X | X | X | X | |||
| PKTLIB | X | X | X | X | X | X | X | X | |||||
| POST | X | X | X | X | X | X | X | X | X | X | |||
| SERDES Diagnostics | X | X | X | X | X | X | |||||||
| Trace Framework | X | X | X | X | X | X | |||||||
DSP devices - OMAP-L13x, C674x
| Feature | Platform/SOC | OMAP-L137 EVM | OMAP-L138 EVM | ||
|---|---|---|---|---|---|
| OMAP-L137 | OMAP-L138 | 137/6747 SK | LCDK138 | LCDK6748 | |
| Board Support | X | X | X | X | X |
| Boot (SBL) | X | X | X | X | X |
| Diagnostics | X | X | |||
| FATFS | X | X | X | X | X |
| Network (CPSW) | X | X | X | X | X |
2.1.7. Known Issues¶
This section contains the list of known issues at the time of making the release and any known workaround.
| Record ID | Platform | Area | Summary | Workaround |
|---|---|---|---|---|
| PRSDK-642 | * | Processor SDK Installer | RTOS: SDK components should be signed to avoid Eclipse/CCS warning when importing | Ignore the Eclipse/CCS warning |
| PRSDK-335 | AM4X | High-Speed Drivers | USB host MSC fails to re-enumerat e | Re-enumeration support for the case of device unplugged and plugged back currently fails for the example.Workaround is to avoid disconnecting drive while running example. |
| PRSDK-330 | AM4X | High-Speed Drivers | USB device MSC re-enumerat ion fails while disconnecti ng and reconnectin g on a Windows host | Problem not observed with Linux USB Host. |
| PRSDK-1682 | AM5X | Diagnostics | Board diagnostics LCD Touchscreen test does not work with new version of LCD TSC | For LCD/Display checkout example under VPS component could be used |
| PRSDK-2166 | AM5X | High-Speed Drivers | USB3.0 host problem with Sandisk Extreme USB3.0 stick | Start the example without the USB plugged in. Once the example is up and waiting for USB stick, plug the USB stick in and it will enumerateproperly. |
| PRSDK-1975 | * | Board Diagnostics | Timer Diagnostic example does not run on ARM Core 1 | Example can run on ARM Core 0 |
| PRSDK-3344 | am572x-id,a m574x-idk | Board Diagnostics | Diagnostics Baremetal icssEmac_TE ST idkAM57{2/4 }x : LINK IS DOWN, pluggin loopback cable | ICSS-EMAC LLD TI-RTOS example can be used for similar test. |
| PRSDK-3482 | * | CCS | CCSV7.4: Intermitten t issue not able to connect target while using DSS script | Retry for connection failure in DSS script. |
| PRSDK-2336 | am335x-evm, am437x-evm | PM | PM Unit Test failure | Use debug version of PM library for the test. To build from the top-level makefile in pdk.../packages folder run “make BUILD_CONFIG=debug pm” |
| PRSDK-3318 | K2G 1Ghz | EMAC | EMAC_CpswRa teLimit_evm K2G_c66xExa mpleProject failure on 1GHz Flip Chip | Incorrect Core clock config in test. Fix for to set the correct CPU clock |
| PRSDK-4184 | am57x,k2x | Board Diagnostic | Hello_World: Baremetal ARM Cortex-A15 test example failure | Problem observed with using GCC semihosting support Use UART driver for input and output |
| PRSDK-4214 | k2g-hs | Board Diagnostic | create-sdcard script does not boot OOB | Default generated App image is not signed follow the steps mentioned in section 6.2.1.2 of the Processor SDK Secdev Build and Install Guide to sign the app |
| PRSDK-642 | * | Uniflash | Uniflash based flashing is not available through GUI | Command line option can be used. Refer User Guide |
| PRSDK-4325 | * | USB Bulk | USB Bulk Mode Python test script missing in package | Available from External GIT location |
| PRSDK-4108 | omapl13x | USB | USB Audio: Lag when trying to adjust volume | None |
| PRSDK-3383 | am574x-idk | Board Diagnostic | Diagnostic lcdTouchscr een_TEST hangs on AM574x IDK | None |
| PRSDK-3369 | am574x-idk | PCIE-LLD | PCIE board to board ARM test examples hangs on idkAM574x platform | None |
| PRSDK-4304 | am335x | Uniflash Flash Writer | Flash writer prebuilt binaries does not work on AM335x platforms | Rebuilding the flash writer binaries shall fix this issue. Refer the Rebuilding the flash writer |
2.1.8. Installation and Usage¶
The Getting Started Guide provides instructions on how to setup up your development environment, install the SDK and start your development.
To uninstall the SDK, remove the individual component directories from the installed path. This is safe to do even in Windows since these components do not modify the Windows registry.
2.1.9. Host Support¶
The recommended development host is
- Windows: Windows 10 on 64-bit machine
- Linux: Ubuntu 16.04 on 64-bit machine
NOTE
The Windows installer is a 32-bit binary, but is compatibility with 64-bit machine.
2.1.10. Technical Support and Product Updates¶
For further information or to report any problems, contact TI E2E:
- Sitara Processor for AM335x, AM437x, and AM57x
- C6000 Multicore DSP for C665x, C667x, K2E, K2G, K2H, and K2L
- OMAP Processor for OMAP-L13x, C674x
2.2. Supported Platforms and Versions¶
Supported Host Operating Systems
The following operating systems have been validated to work with our SDK.
- Linux SDK
| Operating System | Version |
| Ubuntu | 14.04 (64-bit) |
| Ubuntu | 16.04 (64-bit) |
- RTOS SDK
| Operating System | Version |
| Windows | 7 (64-bit) |
| Ubuntu | 16.04 (64-bit) |
- Android SDK
| Operating System | Version |
| Ubuntu | 14.04 (64-bit) |
Supported Platforms and EVMs
The following platforms and EVMs are supported with Processor SDK
2.3. Migration Guide¶
Overview
This page covers migration information for applications built on top of the last Processor SDK for RTOS release.
Processor SDK RTOS 05.00.00
Build
Migration: TOOLS_INSTALL_PATH macro value changed to SDK_INSTALL_PATH No migration impact if tools and SDK are installed in same location. See additional details
Additional Details: TOOLS_INSTALL_PATH macro value is set to SDK_INSTALL_PATH by default. For accessing the tools from a different path, modify TOOLS_INSTALL_PATH in packages/ti/build/Rules.make file or can be overriden from the build console as shown below.
Windows
set TOOLS_INSTALL_PATH=<Path for the tools root folder>
Linux
TOOLS_INSTALL_PATH=<Path for the tools root folder>
Build Setup
Migration: There is no migration need for components used within processor SDK. Application Software outside processor SDK may require a change if there is a dependency to internal Processor SDK environment variables. See more details below
Additional Details: Rules.make file is used instead of pdksetupenv to setup the build environment variables. Components inside processor SDK are updated to align with this change. Any applications making use of pdksetupenv from processor SDK to setup the build environment variables should include below line in the application makefile.
include $(RULES_MAKE)
Archived
- Processor-SDK RTOS 4.3.0
- Processor-SDK RTOS 4.2.0
- Processor-SDK RTOS 4.1.0
- Processor-SDK RTOS 4.0.0
- Processor-SDK RTOS 3.3.0
- Processor-SDK RTOS 3.2.0
- Processor-SDK RTOS 3.1.0
- Processor-SDK RTOS 3.0.0
- Processor-SDK RTOS 2.0.2
- Processor-SDK RTOS 2.0.1
- Processor-SDK RTOS 2.0.0