2. Release Specific¶
2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) provides the core foundation and building blocks that facilitate application software development on TI’s embedded processors. This Release Notes focuses on the Real-time operating system (RTOS).
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
2.1.3. Documentation¶
- Getting Started Guide: Provides information on getting the software and running basic examples/demonstrations bundled in the SDK.
- Migration Guide Provides migration information for applications built on top of the Processor SDK for RTOS.
- Software Developer Guide Provides information on features, functions, delivery package and, compile tools for the Processor SDK RTOS release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Software Manifest: Provides license information on software included in the SDK release. This document is in the release at /processor_sdk_rtos_<SOC>_<version>/docs and available to view from the software download page.
- EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 04.03.00¶
Released March 2018.
What’s New
New Features
- AM335x,AM437x,AM57x,K2G
- Support for PRUSS based I2C Slave
- I2C Driver extension to support PRUSS I2C Firmware in addition to existing hardware IP instances
- Additional PRUSS LLD API to control IEP clock source
- McASP LLD support for changing channel parameters during run time
- AM335x,AM437x
- Display RTOS Example Support
- AM437x,AM572x
- RTOS Template Application extension for AM437x GP EVM
- RTOS Template Application extension to M4 and C66x cores on AM572x GP EVM
Component Version
The following software components and host tools are bundled with the SDK installer. See the Software Developer Guide for more information on each item.
Note
| Component | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| CG_XML | 2.41.0 | X | X | X | X | X | X | X | X | X | X | X |
| CTOOLSLIB | 2.2.0.0 | X | X | X | X | X | X | X | ||||
| DSPLIB | 3.4.0.0 | X | X | X | X | X | X | X | X | X | ||
| EDMA3 LLD | 2.12.5.30 | X | X | X | X | X | X | X | X | X | X | X |
| FC | 3.40.2.7 | X | X | X | X | X | X | X | ||||
| FFTLIB | 3.1.0.0 | X | ||||||||||
| IMGLIB | 3.1.1.0 | X | X | X | X | X | X | X | ||||
| IPC | 3.47.0.0 | X | X | X | X | X | X | X | X | |||
| LIBARCH | 1.0.0.0 | X | ||||||||||
| LINALG | 1.2.0.0 | X | ||||||||||
| MATHLIB | 3.1.1.0 | X | X | X | X | X | X | X | X | X | ||
| MPM | 3.0.4.0 | X | X | X | X | |||||||
| NDK | 2.26.0.0 | X | X | X | X | X | X | X | X | X | X | X |
| OPENCL | 1.1.14.1 | X | ||||||||||
| OPENMP | Per platform | X | X | X | X | X | X | X | ||||
| PDK | 3.1.1.0 | 1.0.10 | 1.0.10 | 1.0.10 | 4.0.9 | 4.0.9 | 4.0.9 | 1.0.9 | 2.0.9 | 2.0.9 | 1.0.4 | 1.0.4 |
| SYS/BIOS | 6.52.0.12 | X | X | X | X | X | X | X | X | X | X | X |
| UIA | 2.21.2.07 | X | X | X | X | X | X | X | X | X | ||
| XDAIS | 7.24.0.4 | X | X | X | X | X | X | X | X | X | ||
| XDCTOOLS | 3.50.03.33 | X | X | X | X | X | X | X | X | X | X | X |
The following compilers are bundled with the SDK installer:
| Compiler | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| GNU ARM Embedded | 6-2017-q1 | A8 | A9 | A15 | A15 | A15 | A15 | A15 | ||||
| TI ARM CGT | 16.9.3 | M4 | A15(SBL) | ARM9 | ARM9 | |||||||
| TI C6000 CGT | 8.2.2 | C66x | C66x | C66x | C66x | C66x | C66x | C66x | C74x | C74x | ||
| TI PRU CGT | 2.2.1 | PRU | PRU | PRU | PRU |
The SDK uses Code Composer Studio (CCS) as the integrated development environment (IDE) for all devices and EVMs:
| Component | Version | AM335x | AM437x | AM57x | K2H/K2K | K2E | K2L | K2G | C665x | C667x | OMAP-L137 | OMAP-L138 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| CCS | 7.4.0.15 | X | X | X | X | X | X | X | X | X | X | X |
If you need to install CCS, see the CCS installation section in the Getting Started Guide for options to select for Processor-SDK.
Change log
Updated
- TI PRU CGT 2.2.1
- CCS 7.4.0.195
- PDK for all platforms
2.1.5. Fixed Issues¶
| Record ID | Platform | Summary |
|---|---|---|
| PRSDK-415 | AM335x | EDMA3 LLD RM code reserves first 64 parameters which are not available to user app using EDMA3_DRV_requestChan nel |
| PRSDK-1491 | K2G, K2H, K2L, K2K | ARM PLL initialization sequence for K2 SOCs needs to be updated to avoid intermittent hang issue due to glitch observed on PLL clocks |
| PRSDK-2196 | AM57x | DCAN Diag test failed on AM57x IDK Platforms |
| PRSDK-2941 | AM335x | PLL Settings need to be updated for additional optimal values |
| PRSDK-2819 | AM335x | Networking API header files are not compatible with C++ |
| PRSDK-3142 | C667x,k2h,k2e | IPC listMP corruption |
| PRSDK-3382 | AM335x,AM437x,AM57x | UART: API UART_read() reads additional byte from what requested by application and drops in case FIFO has extra bytes |
| PRSDK-3381 | AM335x | Support CPSW port-2 only in NDK/NIMU transport |
| PRSDK-3391 | K2G | EDMA-LLD Sample library: Run time interrupt handling incorrect for EventCombiner APIs. Applicable for C66x/C67x cores |
| PRSDK-3267 | K2G | NIMU_ICSS_CCLinkSlave _idkAM437x_wSoCLib_ar mExampleProject hangs during build on linux |
| PRSDK-3236 | K2E,K2L | PDK: SA_BasicExample hangs on K2E, K2L platforms in nightly |
| PRSDK-3666 | C6657x | cslr_upp.h: Incorrect header file path reference in CSL module |
| PRSDK-3578 | AM57x | QSPI test case fails for higher transfer length and duplicates flash driver files |
| PRSDK-3557 | AMIC110 | PDK Rebuild Failure for LIMIT_BOARDS=iceAMIC1 10 |
| PRSDK-3551 | AM335x | Incorrect interrupt definitions for UART driver instances 1,2,4,5 |
| PRSDK-3549 | K2HK | MLO: Build failure for Windows Host OS |
| PRSDK-3320 | K2HK | Program EVM: No response on UART after programming NOR |
| PRSDK-3540 | AM335x | The Processor SDK RTOS installer doesn’t have UIA package |
| PRSDK-3520 | * | FATFS MMCSD: does not work to save large files |
| PRSDK-3464 | AM57x | SBL doesn`t place pinmux code and data at base of OCMC_RAM1 |
| PRSDK-3391 | AM57x,K2H/K,K2G,C667x ,C6657x | EDMA-LLD Sample library: Run time interrupt handling incorrect for EventCombiner APIs. Applicable for C66x/C67x cores |
| PRSDK-3289 | K2G | Macro inconsistencies for different boards in PDK |
| PRSDK-3267 | AM437x IDK | NIMU_ICSS_CCLinkSlave _idkAM437x_wSoCLib_ar mExampleProject hangs during build on Linux host |
| PRSDK-3083 | K2H | K2HKeystone II Serdes PCIE BER diagnostic doesn’t work |
| PRSDK-2225 | AM335x,AM437x | Button Diag test failed on AM3/4 Platforms |
| PRSDK-2196 | am571x-idk, am572x-idk, am574x-idk | DCAN Diag test failed on AM57x IDK Platforms |
| PRSDK-1932 | am335x-evm, am437x-evm | SORTE firmware: Slave devices report RX_CRC packet errors during Parameterization state |
| PRSDK-1186 | AM57x | SBL fails to read MMCSD card with multiple blocks aligned to 0x200 |
| PRSDK-3387 | C6657 | EMAC_evmc6657_C66Loop back_testProject.out fails on C665x platform |
2.1.6. Supported Platforms¶
2.1.6.1. Devices¶
The following table lists all supported devices for a given installer.
| Installer | Platform/SOC | Supported Devices | |
|---|---|---|---|
| RTOS-AM335X | AM335x | AM3351, AM3352, AM3354, AM3356, AM3357, AM3358, AM3359 | |
| AMIC11x | AMIC110 | ||
| RTOS-AM437X | AM437x | AM4376, AM4377, AM4378, AM4379 | |
| RTOS-AM57X | AM57x | AM5706, AM5708, AM5716, AM5718, AM5726, AM5728,AM5746, AM5748 | |
| RTOS-C665X | C665x | C6652, C6654, C6655, C6657 | |
| RTOS-C667X | C667x | C6671, C6672, C6674, C6678 | |
| RTOS-K2E | K2E | 66AK2E02, 66AK2E05, AM5K2E02, AM5K2E04 | |
| RTOS-K2G | K2G | 66AK2G02 | |
| RTOS-K2HK | K2H | 66AK2H06, 66AK2H12, 66AK2H14 | |
| K2K | TCI6638K2K | ||
| RTOS-K2L | K2L | 66AK2L06 | |
| RTOS-OMAPL137 | OMAP-L1x | OMAP-L137, C6743, C6745, C6747 | |
| RTOS-OMAPL138 | OMAP-L1x | OMAP-L138, C6742, C6746, C6748 | |
2.1.6.2. Evaluation Modules¶
See Processor SDK Supported Platforms page for a list of supported EVMs per platform and links to more information.
2.1.6.3. Demonstrations¶
See Examples and Demonstrations page for a list of demonstrations per platform and EVM.
2.1.6.4. Drivers¶
The following tables show RTOS driver availability per platform and EVM. A shaded box implies that the feature is not applicable for that platform/EVM.
Sitara devices
| Feature | Platform/SOC | AM335x EVM | AM437x EVM | AM57x EVM | ||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| AM335x | AM437x | AM57x | GP | ICE | SK | BBB | GP | IDK | SK | GP | IDK | |
| CSL | X | X | X | X | X | X | X | X | X | X | X | X |
| EMAC | X | X | X | X | X | X | X | X | X | X | X | X |
| EDMA3 | X | X | X | X | X | X | ||||||
| GPIO | X | X | X | X | X | X | X | X | X | |||
| GPMC | X | X | X | X | ||||||||
| I2C | X | X | X | X | X | X | X | X | X | X | X | X |
| PRUSS-I2C f/w | X | X | X | X | X | X | ||||||
| ICSS-EMAC | X | X | X | X | X | X | ||||||
| McASP | X | X | X | X | X | X | ||||||
| McSPI | X | X | X | X | X | X | ||||||
| MMC-SD | X | X | X | X | X | X | X | X | X | X | X | X |
| PCIe | X | X | ||||||||||
| PM | X | X | X | X | ||||||||
| PRUSS | X | X | X | X | X | X | ||||||
| QSPI | X | X | X | X | X | |||||||
| UART | X | X | X | X | X | X | X | X | X | X | X | X |
| USB | X | X | X | X | X | X | X | |||||
| USB Device Audio | X | X | ||||||||||
| VPS | X | X | X | |||||||||
DSP devices - K2x, C66x
| Feature | Platform/SOC | K2 EVM | C66x EVM | ||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| K2H/K2K | K2E | K2L | K2G | C665x | C667x | K2H | K2E | K2L | K2G | K2G-ICE | C665x | C667x | |
| CSL | X | X | X | X | X | X | X | X | X | X | X | X | X |
| AIF2 | X | X | |||||||||||
| BCP | X | X | X | X | |||||||||
| CPPI | X | X | X | X | X | X | X | X | X | X | X | X | X |
| DFE | X | X | |||||||||||
| EDMA3 | X | X | X | X | X | X | X | X | X | X | X | X | X |
| EMAC | X | X | X | X | X | ||||||||
| FFTC | X | X | X | X | |||||||||
| GPIO | X | X | X | X | X | X | X | X | X | X | X | X | X |
| HYPLNK | X | X | X | X | X | X | X | X | |||||
| ICSS-EMAC | X | X | |||||||||||
| I2C | X | X | X | X | X | X | X | X | X | X | X | X | X |
| IQN2 | X | X | |||||||||||
| McASP | X | X | |||||||||||
| McBSP | X | X | X | X | |||||||||
| MMAP | X | X | X | X | |||||||||
| MMC-SD | X | X | X | ||||||||||
| NWAL | X | X | X | X | X | X | X | X | |||||
| PA | X | X | X | X | X | X | X | X | |||||
| PCIe | X | X | X | X | X | X | X | X | X | X | X | X | |
| QMSS | X | X | X | X | X | X | X | X | X | X | X | X | X |
| RM | X | X | X | X | X | X | X | X | X | X | X | X | X |
| SA | X | X | X | X | X | X | X | X | X | X | |||
| SPI | X | X | X | X | X | X | X | X | X | X | X | X | X |
| SRIO | X | X | X | X | X | X | |||||||
| TCP3D | X | X | X | X | X | X | |||||||
| TSIP | X | X | X | X | |||||||||
| UART | X | X | X | X | X | X | X | X | X | X | X | X | X |
| USB | X | X | |||||||||||
| USB Device Audio | |||||||||||||
USB Device Audio
DSP devices - OMAP-L13x, C674x
| Feature | Platform/SOC | OMAP-L137 EVM | OMAP-L138 EVM | ||
|---|---|---|---|---|---|
| OMAP-L137 | OMAP-L138 | 137/6747 SK | LCDK138 | LCDK6748 | |
| CSL | X | X | X | X | X |
| EDMA3 | X | X | X | X | X |
| EMAC | X | X | X | X | X |
| GPIO | X | X | X | X | X |
| I2C | X | X | X | X | X |
| McASP | X | X | X | X | X |
| MMC-SD | X | X | X | X | X |
| SPI | X | X | X | X | X |
| UART | X | X | X | X | X |
| USB | X | X | X | X | X |
| USB Device Audio | X | X | X | X | X |
2.1.6.5. Other Features¶
The following table shows other feature availability per platform and EVM:
Sitara devices
| Feature | Platform/SOC | AM335x EVM | AM437x EVM | AM57x EVM | ||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| AM335x | AM437x | AM57x | GP | ICE | SK | BBB | GP | IDK | SK | GP | IDK | |
| Board Support | X | X | X | X | X | X | X | X | X | X | X | X |
| Boot (SBL) | X | X | X | X | X | X | X | X | X | X | X | X |
| Diagnostics | X | X | X | X | X | X | X | |||||
| FATFS | X | X | X | X | X | X | X | X | X | |||
| NDK-NIMU(CPSW) | X | X | X | X | X | X | X | X | X | X | X | X |
| NDK-NIMU(ICSS) | X | X | X | X | X | X | ||||||
| CC-LINK IE Field Basic(CPSW) | X | X | X | X | X | X | X | X | X | X | X | X |
| CC-Link IE Field Basic(ICSS) | X | X | X | X | X | X | ||||||
DSP devices - K2x, C66x
| Feature | Platform/SOC | K2 EVM | C66x EVM | ||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| K2H/K2K | K2E | K2L | K2G | C665x | C667x | K2H | K2E | K2L | K2G | K2G-ICE | C665x | C667x | |
| Board Support | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Boot (IBL/SBL) | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Diagnostics | X | X | X | ||||||||||
| FATFS | X | X | X | ||||||||||
| Fault Management | X | X | X | X | X | X | |||||||
| IPC Transport (QMSS) | X | X | X | X | X | X | X | X | X | X | |||
| IPC Transport (SRIO) | X | X | X | X | X | X | |||||||
| MAD-UTIL | X | X | X | X | |||||||||
| Network (CPSW) | X | X | X | X | X | X | X | X | X | X | X | X | X |
| Network (ICSS) | X | X | |||||||||||
| CC-Link IE Field Basic(ICSS) | X | X | |||||||||||
| Platform Library (obsolete) | X | X | X | X | X | X | X | X | X | X | |||
| PKTLIB | X | X | X | X | X | X | X | X | |||||
| POST | X | X | X | X | X | X | X | X | X | X | |||
| SERDES Diagnostics | X | X | X | X | X | X | |||||||
| Trace Framework | X | X | X | X | X | X | |||||||
DSP devices - OMAP-L13x, C674x
| Feature | Platform/SOC | OMAP-L137 EVM | OMAP-L138 EVM | ||
|---|---|---|---|---|---|
| OMAP-L137 | OMAP-L138 | 137/6747 SK | LCDK138 | LCDK6748 | |
| Board Support | X | X | X | X | X |
| Boot (SBL) | X | X | X | X | X |
| Diagnostics | X | X | |||
| FATFS | X | X | X | X | X |
| Network (CPSW) | X | X | X | X | X |
2.1.7. Known Issues¶
This section contains the list of known issues at the time of making the release and any known workaround.
| Record ID | Platform | Area | Summary | Workaround |
|---|---|---|---|---|
| PRSDK-335 | AM4X | High-Speed Drivers | USB host MSC fails to re-enumerat e | Re-enumeration support for the case of device unplugged and plugged back currently fails for the example.Workaround is to avoid disconnecting drive while running example. |
| PRSDK-330 | AM4X | High-Speed Drivers | USB device MSC re-enumerat ion fails while disconnecti ng and reconnectin g on a Windows host | Problem not observed with Linux USB Host. |
| PRSDK-1682 | AM5X | Diagnostics | Board diagnostics LCD Touchscreen test does not work with new version of LCD TSC | For LCD/Display checkout example under VPS component could be used |
| PRSDK-2166 | AM5X | High-Speed Drivers | USB3.0 host problem with Sandisk Extreme USB3.0 stick | Start the example without the USB plugged in. Once the example is up and waiting for USB stick, plug the USB stick in and it will enumerateproperly. |
| PRSDK-1975 | * | Board Diagnostics | Timer Diagnostic example does not run on ARM Core 1 | Example can run on ARM Core 0 |
| PRSDK-3344 | am572x-id,a m574x-idk | Board Diagnostics | Diagnostics Baremetal icssEmac_TE ST idkAM57{2/4 }x : LINK IS DOWN, pluggin loopback cable | ICSS-EMAC LLD TI-RTOS example can be used for similar test. |
| PRSDK-642 | * | Processor SDK Installer | RTOS: SDK components should be signed to avoid Eclipse/CCS warning when importing | Ignore the Eclipse/CCS warning |
| PRSDK-3648 | am437x-evm | EMAC | TCP/IP throughput improvement | Use NDK no copy configuration. In addition NIMU driver update for increased number of CPPI descriptors. |
| PRSDK-3718 | All AM57x boards | Board | L3/L4 interconnec t CLKSEL configurati on does not take to effect | Default ROM is setting correct config. For fix modify CLKSEL fields from CM_CLKSEL_DPLL_CORE_REG to CM_CLKSEL_CORE_REG for corePllcParam->l3ClkSel and corePllcParam->l4ClkSel |
| PRSDK-3482 | * | CCS | CCSV7.4: Intermitten t issue not able to connect target while using DSS script | Retry for connection failure in DSS script. |
| PRSDK-2336 | am335x-evm, am437x-evm | PM | PM Unit Test failure | Use debug version of PM library for the test. To build from the top-level makefile in pdk.../packages folder run “make BUILD_CONFIG=debug pm” |
| PRSDK-3030 | omap L13x | SPI | Interrupt mode is not functional | Poll/blocking mode can be used where there is no other task contention |
| PRSDK-3383 | am574x-idk | Board Diagnostic | Diagnostic lcdTouchscr een_TEST hangs on AM574x IDK | None |
| PRSDK-3369 | am574x-idk | PCIE-LLD | PCIE board to board ARM test examples hangs on idkAM574x platform | None |
| PRSDK-3318 | K2G 1Ghz | EMAC | EMAC_CpswRa teLimit_evm K2G_c66xExa mpleProject failure on 1GHz Flip Chip | None |
| PRSDK-3856 | AM335x AM437x | Starterware | StarterWare build from the PDK starterware folder fails on Windows OS | Top-level make command can be used for building starterware on Windows |
| PRSDK-3859 | am57xx, c665x, c667x, omapl13x, keystone2, c674x, | Demo | Audio benchmark starterkit demo fails to build in Windows with Rules.make environment setup | Environment variables in makefile needs to include in double quote for enabling windows build. Makefile under following directories singlePrecision_FFT, singlePrecision_FIR and singlePrecision_IIR will need update for variables: CC_INCS, CC, AR, LD Eg: CC = $(C6X_GEN_INSTALL_PATH)/bin/cl6x needs to be updated to CC = “$(C6X_GEN_INSTALL_PATH)/bin/cl6x” Replace $(SOC) variable in the top level makefile under the folder ‘audio-benchmark-starterkit’ with $(PDK_SOC) Ex: $(MAKE) -C ./src/singlePrecision_FFT SOC=$(SOC) all to $(MAKE) -C ./src/singlePrecision_FFT SOC=$(PDK_SOC) all |
2.1.8. Installation and Usage¶
The Getting Started Guide provides instructions on how to setup up your development environment, install the SDK and start your development.
To uninstall the SDK, remove the individual component directories from the installed path. This is safe to do even in Windows since these components do not modify the Windows registry.
2.1.9. Host Support¶
The recommended development host is
- Windows: Windows 10 on 64-bit machine
- Linux: Ubuntu 16.04 on 64-bit machine
NOTE
The Windows installer is a 32-bit binary, but is compatibility with 64-bit machine.
2.1.10. Technical Support and Product Updates¶
For further information or to report any problems, contact TI E2E:
- Sitara Processor for AM335x, AM437x, and AM57x
- C6000 Multicore DSP for C665x, C667x, K2E, K2G, K2H, and K2L
- OMAP Processor for OMAP-L13x, C674x
2.2. Supported Platforms and Versions¶
Supported Host Operating Systems
The following operating systems have been validated to work with our SDK.
- Linux SDK
| Operating System | Version |
| Ubuntu | 14.04 (64-bit) |
| Ubuntu | 16.04 (64-bit) |
- RTOS SDK
| Operating System | Version |
| Windows | 7 (64-bit) |
| Ubuntu | 16.04 (64-bit) |
- Android SDK
| Operating System | Version |
| Ubuntu | 14.04 (64-bit) |
Supported Platforms and EVMs
The following platforms and EVMs are supported with Processor SDK
All platforms supporting Linux share
- Linux Kernel 4.9
- U-Boot 2017.01
- Linaro GCC 6.2.1 Toolchain
For a full list of components, see the Release Notes for Processor SDK Linux, Processor SDK RTOS, and Processor SDK Android.
2.3. Migration Guide¶
Overview
This page covers migration information for applications built on top of the last Processor SDK for RTOS release.
Processor SDK RTOS 04.03.00
General
OSAL
Migration: No impact expected if Semaphore allocation and HwIP registration from OSAL is not invoked by application.
Additional Details: OSAL module is fine tuned for optimized number of semaphores required internally within drivers. Module provides additional API to application for additional semaphore allocation if required.Application can configure for either default internal static allocation or it can select external memory block that can be provided to create these objects. Note that this decision to go with external memory block or internal memory block need to be done during init configuration of application (near to main) just after Board_init() is called. Below sample code sets SemaphoreP/HwiP to be used from external memory block:
...
...
/* Get the Hw Attrs */
osal_ret = Osal_getHwAttrs(&hwAttrs);
if (osal_ret != osal_OK)
{
return (false);
}
/* This API should set to use external memory block */
hwAttrs.extSemaphorePBlock.base = (uintptr_t) &semPMemBlock[0];
hwAttrs.extSemaphorePBlock.size = SEMP_BLOCK_SIZE;
hwAttrs.extHwiPBlock.size = HWIP_BLOCK_SIZE;
hwAttrs.extHwiPBlock.base = (uintptr_t) &hwiPMemBlock[0];
osal_ret = Osal_setHwAttrs(ctrlBitMap, &hwAttrs);
Board
Migration: Section details applicable only to applications based on DRA7xx SoCs.
Additional Details: DRA7xx board libraries have refactored pad configuration sequence by removing manual pinmux entries and replacing them with a full IODELAY reconfiguration procedure. This was done in order to simplify transition from a standalone application development in CCS to booting the whole device via SBL, ensuring that pad configuration is 100% consistent between the two application loading methods.
The IODELAY and pin control data structures are maintained in each of evmDRA72x and evmDRA75x board library source directories. These structures are also included in the SBL compilation and used in the SBL’s IODELAY reconfiguration. Therefore, changes can be made in one location but reused by both Board and SBL components just through recompilation.
Note that DRA78x does not require IODELAY reconfiguration and pinmux setup is always contained entirely in the application. Hence, there are no corresponding changes to this library.
All of this is done in a transparent manner, so there is no API change and will not affect existing applications. However, there are considerations with respect to memory placement and potential conflicts between the board library and SBL code. These restrictions have always existed but are now more clearly defined and documented. Please refer to Board Support for more details.
I2C
Migration: No migration required for existing user application.
Additional Details: PRUICSS based I2C Firmware have been introduced in this release. This new features increases the number of I2C interface available in the SOC. I2C LLD now depends on PRUSS LLD for compilation of this new feature. All of this is done in a transparent manner, so there is no API change and will not affect existing applications. However, for using the I2C FW feature refer I2C FW for additional details.
Archived
- Processor-SDK RTOS 4.2.0
- Processor-SDK RTOS 4.1.0
- Processor-SDK RTOS 4.0.0
- Processor-SDK RTOS 3.3.0
- Processor-SDK RTOS 3.2.0
- Processor-SDK RTOS 3.1.0
- Processor-SDK RTOS 3.0.0
- Processor-SDK RTOS 2.0.2
- Processor-SDK RTOS 2.0.1
- Processor-SDK RTOS 2.0.0