2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) provides the core foundation and building blocks that facilitate application software development on TI’s embedded processors. This Release Notes focuses on the Real-time operating system (RTOS).
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
2.1.3. Documentation¶
Getting Started Guide: Provides information on getting the software and running basic examples/demonstrations bundled in the SDK.
Migration Guide Provides migration information for applications built on top of the Processor SDK for RTOS.
Software Developer Guide Provides information on features, functions, delivery package and, compile tools for the Processor SDK RTOS release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
Software Manifest: Provides license information on software included in the SDK release. This document is in the release at
/processor_sdk_rtos_<SOC>_<version>/docsand available to view from the software download page.EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Processor SDK v11.01.00¶
Released October 2025
Note
What’s New
Bug Fixes
This release includes only version update to be in sync with the Linux SDK release. No feature updates in the SDK.
Component Version
The following software components and host tools are bundled with the SDK installer. See the Software Developer Guide for more information on each item.
Note
Component |
Version |
|---|---|
CG_XML |
2.61.0 |
CTOOLSLIB |
2.2.0.0 |
DSPLIB |
3.4.0.4 |
EDMA3 LLD |
2.12.5.30 |
FC |
3.40.2.7 |
IMGLIB |
3.1.1.0 |
IPC |
3.52.0 |
MATHLIB |
3.1.2.4 |
NDK |
3.61.1 |
NS |
2.60.1 |
OPENCL |
1.2.0.2 |
OPENMP |
2.6.3.0 |
PDK |
1.0.19 |
SYS/BIOS |
6.76.3.1 |
UIA |
2.30.1.2 |
XDAIS |
7.24.0.4 |
XDCTOOLS |
3.55.02 |
The following compilers are bundled with the SDK installer:
Compiler |
Version |
|---|---|
GNU ARM Embedded |
7-2018-q2 |
TI ARM CGT |
18.12.5 |
TI C6000 CGT |
8.3.2 |
TI PRU CGT |
2.3.3 |
The SDK uses Code Composer Studio (CCS) as the integrated development environment (IDE) for all devices and EVMs:
Component |
Version |
|---|---|
CCS |
12.5.0 |
EMU Pack |
1.4.5 |
Emulators |
8.3.0.0 |
If you need to install CCS, see the CCS installation section in the Getting Started Guide for options to select for Processor-SDK.
2.1.5. Fixed Issues¶
None2.1.6. Known Issues¶
This section contains the list of known issues at the time of making the release and any known workaround.
ID |
Head Line |
Module |
Reported in Release |
Affected Platforms |
Impact |
Workaround in this release |
|---|---|---|---|---|---|---|
PDK-11137 |
Queue overflow count is not returning proper value in poll mode |
ICSS EMAC |
8.01.00 |
am572x-idk, am574x-idk |
Applications will not be able to determine the overflow count |
Use the error count to track over all errors |
2.1.7. Supported Platforms¶
2.1.7.1. Devices¶
The following table lists all supported devices by the release installer.
Installer |
Platform/SOC |
Supported Devices |
|
|---|---|---|---|
AM5706, AM5708, AM5716, AM5718, AM5726, AM5728, AM5746, AM5748 |
|||
2.1.7.2. Evaluation Modules¶
See Processor SDK Supported Platforms page for a list of supported EVMs per platform and links to more information.
2.1.7.3. Demonstrations¶
See Examples and Demonstrations page for a list of demonstrations per platform and EVM.
2.1.7.4. Drivers¶
The following tables show RTOS driver availability per platform and EVM. A shaded box implies that the feature is not applicable for that platform/EVM.
Feature |
SoC |
AM57x EVM |
|
|---|---|---|---|
AM57x |
GP |
IDK |
|
CSL |
X |
X |
X |
EMAC |
X |
X |
X |
EDMA3 |
X |
X |
|
GPIO |
X |
X |
X |
I2C |
X |
X |
X |
PRUSS-I2C f/w |
X |
X |
|
ICSS-EMAC |
X |
X |
|
McASP |
X |
X |
|
McSPI |
X |
X |
|
MMC-SD |
X |
X |
X |
PCIe |
X |
X |
|
PM |
X |
X |
|
PRUSS |
X |
X |
|
QSPI |
X |
X |
|
UART |
X |
X |
X |
USB |
X |
X |
X |
USB Device Bulk |
X |
X |
X |
VPS |
X |
X |
X |
Unsupported Features
In general driver support is available across all cores within an SOC with following exceptions
Feature |
Not supported |
|
|---|---|---|
SOC |
CPU/Core |
|
McASP |
AM57x |
M4 |
USB |
AM57x |
C66x |
USB |
AM57x |
M4 |
2.1.7.5. Other Features¶
The following table shows other feature availability per platform and EVM:
Feature |
SoC |
AM57x EVM |
|
|---|---|---|---|
AM57x |
GP |
IDK |
|
Board Support |
X |
X |
X |
Boot (SBL) |
X |
X |
X |
Diagnostics |
X |
X |
X |
FATFS |
X |
X |
X |
NDK-NIMU(CPSW) |
X |
X |
X |
NDK-NIMU(ICSS) |
X |
X |
|
CC-LINK IE Field Basic(CPSW) |
X |
X |
X |
CC-Link IE Field Basic(ICSS) |
X |
X |
|
2.1.8. Installation and Usage¶
The Getting Started Guide provides instructions on how to setup up your development environment, install the SDK and start your development.
To uninstall the SDK, remove the individual component directories from the installed path. This is safe to do even in Windows since these components do not modify the Windows registry.
2.1.9. Technical Support and Product Updates¶
For further information or to report any problems, contact: - TI E2E Processor Support for all supported platforms
2.1.10. Archived¶
Note: Release Notes prior to 4.3 are not archived. Please see the Migration Guide for information on migration from these releases.