2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) provides the core foundation and building blocks that facilitate application software development on TI’s embedded processors. This Release Notes focuses on the Real-time operating system (RTOS).
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
2.1.3. Documentation¶
- Getting Started Guide: Provides information on getting the software and running basic examples/demonstrations bundled in the SDK.
- Migration Guide Provides migration information for applications built on top of the Processor SDK for RTOS.
- Software Developer Guide Provides information on features, functions, delivery package and, compile tools for the Processor SDK RTOS release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
/processor_sdk_rtos_<SOC>_<version>/docsand available to view from the software download page. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Processor SDK v08.01.00¶
Released March 2022
Note
What’s New
New Features
- SDK
- Naming change for APIs, Macros and Data structures in some of the components. Please refer Migration Guide for more details.
- Board Diagnostics
- 4GB DDR support in memory diagnostic test
- USB driver
- Added USB long run regression test
- PRU
- Upgraded toolchain version to v2.3.3
Other Updates
- Features/Components Removed
- RS485 Diagnostic test support is removed
- Big data IPC and Jailhouse demos
- Bug Fixes
- Bug fixes for USB driver, SPI driver and diagnostic examples. Please refer Fixed Issues section for more details
Component Version
The following software components and host tools are bundled with the SDK installer. See the Software Developer Guide for more information on each item.
Note
| Component | Version |
|---|---|
| CG_XML | 2.61.0 |
| CTOOLSLIB | 2.2.0.0 |
| DSPLIB | 3.4.0.4 |
| EDMA3 LLD | 2.12.5.30 |
| FC | 3.40.2.7 |
| IMGLIB | 3.1.1.0 |
| IPC | 3.50.4 |
| MATHLIB | 3.1.2.4 |
| NDK | 3.61.1 |
| NS | 2.60.1 |
| OPENCL | 1.2.0.2 |
| OPENMP | 2.6.3.0 |
| PDK | 1.0.19 |
| SYS/BIOS | 6.76.3.1 |
| UIA | 2.30.1.2 |
| XDAIS | 7.24.0.4 |
| XDCTOOLS | 3.55.02 |
The following compilers are bundled with the SDK installer:
| Compiler | Version |
|---|---|
| GNU ARM Embedded | 7-2018-q2 |
| TI ARM CGT | 18.12.5 |
| TI C6000 CGT | 8.3.2 |
| TI PRU CGT | 2.3.3 |
The SDK uses Code Composer Studio (CCS) as the integrated development environment (IDE) for all devices and EVMs:
| Component | Version |
|---|---|
| CCS | 9.3.0 |
| EMU Pack | Sitara Device 1.4.5 |
Emulators |
8.3.0.0 |
If you need to install CCS, see the CCS installation section in the Getting Started Guide for options to select for Processor-SDK.
2.1.5. Fixed Issues¶
ID Head Line Module Affected Versions Affected Platforms PDK-9869 McSPI controller peripheral example failures with some HW setups McSPI 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-10870 MCSPI controller peripheral example does not transfer more than 32bytes McSPI 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-10276 False test fail condition reported by diagnostic test framework Diagnostics 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-10285 ICSS EMAC diagnostic test hang after link detection Diagnostics 6.03.02 am574x-idk PDK-10282 CSL timer example hang on DSP core while configuring timer instance 32 CSL examples 6.03.02 am571x-idk, am572x-evm, am572x-idk, am574x-idk PDK-10302 Prebuilt SD images are not included in AM57x processor SDK demos package Demos 6.03.02 am572x-evm, am571x-idk, am572x-idk, am574x-idk PDK-10313 System fails to recover using clearFeature when USB bulk application is made to sleep in different sequences USB 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-11043 ICSS EMAC Example in Poll Mode fails for incorrect overflow count ICSS EMAC 6.03.02 am574x-idk, am572x-idk PDK-10576 UART print hangs on A15_1 core after BIOS_start Demos 6.03.02 am571x-idk, am572x-evm, am572x-idk, am574x-idk PDK-10408 Audio EQ McASP example is not working when equalization is enabled McASP 6.03.02 am572x-evm PDK-10406 QSPI flash block erase & DMA mode write issues QSPI 6.03.02 am572x-idk PDK-11121 Fix for USB bulk write function infinite loop USB 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-10525 PULLUP misspelled as PILLUP (TYPO ERROR) SPI, Board 6.03.02 am571x-idk, am572x-evm, am572x-idk, am574x-idk PDK-10521 RS485 support is wrongly documented for AM57x platform Diagnostics 6.03.02 am571x-idk, am572x-idk, am574x-idk PDK-10398 Documentation improvements Documentation 6.03.02 am571x-idk, am572x-evm, am572x-idk, am574x-idk PDK-10328 Build warnings from hexpru tool while generating PRU firmware loader files ICSS EMAC 8.01.00 am572x-idk, am574x-idk am571x-idk
2.1.6. Known Issues¶
This section contains the list of known issues at the time of making the release and any known workaround.
| ID | Head Line | Module | Reported in Release | Affected Platforms | Impact | Workaround in this release |
|---|---|---|---|---|---|---|
| PDK-11137 | Queue overflow count is not returning proper value in poll mode | ICSS EMAC | 8.01.00 | am572x-idk, am574x-idk | Applications will not be able to determine the overflow count | Use the error count to track over all errors |
2.1.7. Supported Platforms¶
2.1.7.1. Devices¶
The following table lists all supported devices by the release installer.
| Installer | Platform/SOC | Supported Devices | |
|---|---|---|---|
| RTOS-AM57X | AM57x | AM5706, AM5708, AM5716, AM5718, AM5726, AM5728, AM5746, AM5748 | |
2.1.7.2. Evaluation Modules¶
See Processor SDK Supported Platforms page for a list of supported EVMs per platform and links to more information.
2.1.7.3. Demonstrations¶
See Examples and Demonstrations page for a list of demonstrations per platform and EVM.
2.1.7.4. Drivers¶
The following tables show RTOS driver availability per platform and EVM. A shaded box implies that the feature is not applicable for that platform/EVM.
Sitara devices
| Feature | SoC | AM57x EVM | |
|---|---|---|---|
| AM57x | GP | IDK | |
| CSL | X | X | X |
| EMAC | X | X | X |
| EDMA3 | X | X | |
| GPIO | X | X | X |
| I2C | X | X | X |
| PRUSS-I2C f/w | X | X | |
| ICSS-EMAC | X | X | |
| McASP | X | X | |
| McSPI | X | X | |
| MMC-SD | X | X | X |
| PCIe | X | X | |
| PM | X | X | |
| PRUSS | X | X | |
| QSPI | X | X | |
| UART | X | X | X |
| USB | X | X | X |
| USB Device Bulk | X | X | X |
| VPS | X | X | X |
Unsupported Features
- In general driver support is available across all cores within an SOC with following exceptions
| Feature | Not supported | |
|---|---|---|
| SOC | CPU/Core | |
| McASP | AM57x | M4 |
| USB | AM57x | C66x |
| USB | AM57x | M4 |
2.1.7.5. Other Features¶
The following table shows other feature availability per platform and EVM:
Sitara devices
| Feature | SoC | AM57x EVM | |
|---|---|---|---|
| AM57x | GP | IDK | |
| Board Support | X | X | X |
| Boot (SBL) | X | X | X |
| Diagnostics | X | X | X |
| FATFS | X | X | X |
| NDK-NIMU(CPSW) | X | X | X |
| NDK-NIMU(ICSS) | X | X | |
| CC-LINK IE Field Basic(CPSW) | X | X | X |
| CC-Link IE Field Basic(ICSS) | X | X | |
2.1.8. Installation and Usage¶
The Getting Started Guide provides instructions on how to setup up your development environment, install the SDK and start your development.
To uninstall the SDK, remove the individual component directories from the installed path. This is safe to do even in Windows since these components do not modify the Windows registry.
2.1.9. Technical Support and Product Updates¶
For further information or to report any problems, contact: - TI E2E Processor Support for all supported platforms
2.1.10. Archived¶
- Processor-SDK RTOS 6.3.2
- Processor-SDK RTOS 6.3.0
- Processor-SDK RTOS 6.1.0
- Processor-SDK RTOS 6.0.0
- Processor-SDK RTOS 5.3.0
- Processor-SDK RTOS 5.2.0
- Processor-SDK RTOS 5.1.0
- Processor-SDK RTOS 5.0.0
- Processor-SDK RTOS 5.0.0 AM65x EA Release
- Processor-SDK RTOS 4.3.0
Note: Release Notes prior to 4.3 are not archived. Please see the Migration Guide for information on migration from these releases.