Defines the interface to reference generator module (REFGEN)
Go to the source code of this file.
Data Structures | |
struct | dcl_refgen |
Defines the DCL_REFGEN structure. More... | |
Macros | |
#define | DCL_REFGEN_MIN_INC 1.0e-06f |
Defines the minimum normalized increment. More... | |
#define | DCL_REFGEN_DEFAULTS |
Defines default values to initialize the DCL_REFGEN structure. More... | |
Typedefs | |
typedef _DCL_VOLATILE struct dcl_refgen | DCL_REFGEN |
Enumerations | |
enum | DCL_refgen_modes { REFGEN_OFF = 0, REFGEN_STATIC = 1, REFGEN_SINE = 2, REFGEN_SQUARE = 3, REFGEN_SAW = 4, REFGEN_TRIANGLE = 5, REFGEN_PULSE = 6, REFGEN_SINE2 = 7, REFGEN_SINE3 = 8 } |
Defines the REFGEN operating modes. More... | |