Contains direct form 1 3rd order DF13 compensator with its related structures and functions.
- Note
- Due to compatibility reason, this file maintains a copy of legacy function DCL_runDF13_C5(), DCL_runDF13_C6(). It is advised to not use these legacy functions for new development.
|
#define | DF13_SPS_DEFAULTS { 0.25f, 0.25f, 0.25f, 0.25f, 0.0f, 0.0f, 0.0f, 0.0f } |
|
#define | DF13_DEFAULTS |
| Defines default values to initialize DCL_DF13. More...
|
|
#define | DF13_INT_DEFAULTS |
| Macro for internal default values to initialize DCL_DF13 Example: DCL_DF13 df13_ctrl = { .b0 = 0.25f, .b1 = 0.25f, ... .a3 = 0.0f, DF13_INT_DEFAULTS };. More...
|
|
#define | DCL_initDF13() &(DCL_DF13)DF13_DEFAULTS |
| Initialize DCL_DF13 struct with default parameters Example: DCL_DF13* df13_ctrl = DCL_initDF13();. More...
|
|
#define | DCL_initDF13asParam(_b0, _b1, _b2, _b3, _a1, _a2, _a3) |
| Initialize DCL_DF13 struct with input compensator parameters Example: DCL_DF13* DF13_ctrl = DCL_initDF13asParam(0.25f,0.25f,0.25f,0.25f,0.0f,0.0f,0.0f);. More...
|
|
#define | DCL_initDF13asSPS(df_ptr, sps_ptr) |
| Initialize DCL_DF13 struct with sps parameters Example: DCL_DF13_SPS df_sps = { .b0 = , .b1 = , ...}; //initial parameter DCL_DF13 df_ctrl; DCL_initDF13asSPS(&df_ctrl,&df_sps);. More...
|
|
|
_DCL_CODE_ACCESS void | DCL_resetDF13 (DCL_DF13 *df) |
| Resets DF13 internal storage data with interrupt protection Implemented as inline C function. More...
|
|
_DCL_CODE_ACCESS void | DCL_forceUpdateDF13 (DCL_DF13 *df) |
| Loads DF13 tuning parameter from its SPS parameter without interrupt protection. More...
|
|
_DCL_CODE_ACCESS void | DCL_updateDF13NoCheck (DCL_DF13 *df) |
| Loads DF13 tuning parameter from its SPS parameter with interrupt protection. More...
|
|
_DCL_CODE_ACCESS bool | DCL_updateDF13 (DCL_DF13 *df) |
| A conditional update based on the update flag. If the update status is set, the function will update DF13 parameter from its SPS parameter and clear the status flag on completion.. More...
|
|
_DCL_CODE_ACCESS bool | DCL_isStableDF13 (DCL_DF13 *df) |
| Determines stability of the shadow compensator. More...
|
|
_DCL_CODE_ACCESS void | DCL_loadDF13asZPK (DCL_DF13 *df, DCL_ZPK3 *zpk) |
| Loads the DF13 shadow coefficients from a ZPK3 description. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runDF13 (DCL_DF13 *df, float32_t ek) |
| Executes a 3rd order Direct Form 1 controller. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runDF13PartialCompute (DCL_DF13 *df, float32_t ek) |
| Immediate computation to obtain DF13 servo error without updating the controller. More...
|
|
_DCL_CRIT_ACCESS void | DCL_runDF13PartialUpdate (DCL_DF13 *df, float32_t ek, float32_t uk) |
| Update DF13 controller based on pre-computed control effort. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runDF13Clamp (DCL_DF13 *df, float32_t ek, float32_t Umax, float32_t Umin) |
| Executes a 3rd order Direct Form 1 controller with clamp. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runDF13_C5 (DCL_DF13 *p, float32_t ek, float32_t vk) |
| Legacy C28 Function for maintaining backwards compatibility. It Executes an immediate 3rd order Direct Form 1 controller. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runDF13_C6 (DCL_DF13 *p, float32_t ek, float32_t uk) |
| Legacy C28 Function for maintaining backwards compatibility. It executes a partial pre-computed 3rd order Direct Form 1 controller. More...
|
|