SMI General.
Functions | |
IOL_FUNC_DECL void | IOLM_SMI_vGenericReq (IOLM_SMI_SHeader *psuHeader_p, INT8U *pu8ArgBlock_p) |
SMI generic request. | |
IOL_FUNC_DECL void | IOLM_SMI_vSaveNvFinished (void) |
Save configuration finished. | |
void | IOLM_SMI_vExtRsp (IOL_EErrorType eError_p, INT8U *pu8Data_p, INT16U u16Length_p) |
SMI extension response. | |
IOL_FUNC_DECL void | IOLM_SMI_vRun (void) |
SMI Mainloop. | |
IOL_FUNC_DECL void | IOLM_SMI_vInit (IOLM_SMI_SCallbacks *psuCallbacks_p) |
Initialize SMI interface. | |
void IOLM_SMI_vExtRsp | ( | IOL_EErrorType | eError_p, |
INT8U * | pu8Data_p, | ||
INT16U | u16Length_p | ||
) |
SMI extension response.
Responses of extension functions which are proprietary and not included in the IOL/IOLW specification.
[in] | eError_p | Error message as IOL_EErrorType. |
[in] | pu8Data_p | Pointer to the response data. |
[in] | u16Length_p | Length of the response data |
IOL_FUNC_DECL void IOLM_SMI_vGenericReq | ( | IOLM_SMI_SHeader * | psuHeader_p, |
INT8U * | pu8ArgBlock_p | ||
) |
SMI generic request.
The function is used for a generic access of all services of the SMI. The answer to this request is the callback function IOLM_SMI_CBGenericCnf.
[in] | psuHeader_p | Header. |
[in] | pu8ArgBlock_p | Generic ArgBlock. |
IOL_FUNC_DECL void IOLM_SMI_vInit | ( | IOLM_SMI_SCallbacks * | psuCallbacks_p | ) |
Initialize SMI interface.
Initializes the SMI Interface, sets initial values, loads saved configuration (if present), etc. Must be called once before SMI Mainloop (IOLM_SMI_vRun).
[in] | psuCallbacks_p | Set of callback functions. |
IOL_FUNC_DECL void IOLM_SMI_vRun | ( | void | ) |
SMI Mainloop.
Runs periodically to execute the next jobs in the queue, etc. Must be called at least once every millisecond to guarantee a stable stack environment.
IOL_FUNC_DECL void IOLM_SMI_vSaveNvFinished | ( | void | ) |
Save configuration finished.
This service needs to be called by the application code, to inform the stack, that the configuration is successfully written to the non volatile memory function in the application code (which can take a few hundred milliseconds).