IO-Link Masterv2.01.01
 
Loading...
Searching...
No Matches
IOLM_SMI_SVoidArgBlock Struct Reference

This structure is used as general and void ArgBlock. More...

#include <IOLM_SMI_Types.h>

Data Fields

INT16U u16ArgBlockID
 Big endian.
 

Detailed Description

This structure is used as general and void ArgBlock.

The following data and the ArgBlockID(IOLM_SMI_EArgBlockID) depend on the specific use case.