AM263x Digital Power SDK  09.01.00
datalog.h File Reference

Introduction

Contains the public interface to the data logging (DATALOG) module routines.

Go to the source code of this file.

Data Structures

struct  DATALOG_Obj
 Defines the data logging (DATALOG) object. More...
 

Macros

#define IEEE754_TYPES
 
#define DATALOG_DEFAULTS
 Defines the default initialization for the DLOG object. More...
 

Typedefs

typedef float float32_t
 
typedef double float64_t
 
typedef struct _DATALOG_Obj_ * DATALOG_Handle
 Defines the DATALOG handle. More...
 

Enumerations

enum  Trigger_type { manual, auto_trigger }
 

Functions

DATALOG_Handle DATALOG_init (void *pMemory, const size_t numBytes, Trigger_type trigger, float32_t trig_value, int32_t scale)
 Initializes the data logger. More...
 
static void DATALOG_update (DATALOG_Handle handle)
 Updates the data logger. More...
 

Variables

DATALOG_Obj datalog
 Defines the DATALOG object. More...
 
DATALOG_Handle datalogHandle
 the handle for the Datalog object More...
 

Macro Definition Documentation

◆ IEEE754_TYPES

#define IEEE754_TYPES

Typedef Documentation

◆ float32_t

typedef float float32_t

◆ float64_t

typedef double float64_t