Here is the list of APIs used for Digital Control Library
◆ DATALOG_DEFAULTS
Value: { \
NULL, \
NULL, \
NULL}, \
true, \
false, \
0, \
DATA_LOG_BUFF_SIZE \
}
Defines the default initialization for the DLOG object.
◆ DATALOG_Handle
Defines the DATALOG handle.
◆ Trigger_type
Enumerator |
---|
manual | |
auto_trigger | |
◆ DATALOG_init()
Initializes the data logger.
- Parameters
-
[in] | pMemory | The pointer to memory |
[in] | numBytes | size of datalog_obj |
[in] | trigger | manual or auto_triiger |
[in] | trig_value | Trigger value used for Auto triger type to initiate datalog |
[in] | scale | How many datalog update to be skipped |
◆ DATALOG_update()
Updates the data logger.
- Parameters
-
[in] | handle | Datalog handle need to be provided |
◆ datalog
Defines the DATALOG object.
◆ datalogHandle
the handle for the Datalog object