Introduction¶
The Energy Measurement Design Center (EMDC) is a rapid development tool that enables energy measurement using TI MSP430i20xx and MSP430F67xx Flash-based microcontrollers (MCUs). It includes a graphical user interface (GUI), documentation, software library and examples that can simplify development and accelerate designs for power monitoring and energy measurement in smart grid and building automation applications. Start by dragging and dropping a MCU, voltage sensors, and current sensors into the GUI workspace. Configure the MCU and each sensor according to your system configuration. The GUI will check for errors before generating the source code. Import the code into an IDE and program the MCU. The GUI will allow you to easily calibrate the device and view the results.
Dependencies¶
Java JRE 1.7 or later must be installed on the host system. Click here to go to Java Download Page.
HID Bridge requirements:
MSP430F5529 LaunchPad (used as HID bridge for communication)
Isolation Adapter for MSP LaunchPad Development Kits (isolates target from HID bridge)
UniFlash Standalone Tool (used to program LaunchPad with provided HID bridge binary file)
Source code generated by this release requires:
Code Composer Studio (CCS) version 7.1.0 or later
IAR Systems Embedded Workbench for MSP430 version 7.10 or later
Development Kits Support¶
The following development kits are supported in this release :
Device Support¶
The following families of devices are supported in this release of Energy Measurement Design Center:
MSP430i20xx
MSP430F67xx(1)(A)
Software API¶
For more information on the Energy Measurement Software Library and ADC Hardware Abstraction Layer (HAL), see Software Library API Guide.
Technology Guide Overview¶
Each chapter in the Energy Measurement Technology Guide is introduced briefly below.
Energy Measurement Design Center GUI¶
Read the Design Center GUI chapter to get started with the rapid development tool that can simplify development and accelerate designs in a wide range of power monitoring and energy measurement applications, including smart grid and building automation, using MSP430 MCUs with 24-bit Sigma Delta ADCs. Using the Design Center, you can configure, calibrate, and view results without writing a single line of code! This chapter includes the following sections:
Out-Of-Box Experience: This section describes how to program the required tools, make the connections, and quickly view results using the provided EMDC example projects and example firmware images.
Quick Start Guide: This section is intended to provide a very basic and quick overview of how to use the Energy Measurement Design Center (EMDC) to configure a typical energy measurement design (based on the three-phase EVM430-F6779), generate the source code, communicate with the target, and calibrate the system.
User’s Guide: This sections is intended to provide more detailed information about the features of the Energy Measurement Design Center.
Communication Protocol Specification¶
The Communication Protocol Spec chapter introduces the command details and protocol used between EMDC and the target.
Known Limitations¶
Operating Ranges
VRMS: Up to 1000 VAC (max)
IRMS: Up to 500 A (max)
Devices
MSP430i20x0 with 1KB RAM cannot support the native EMDC software library.
GUI
After establishing communication with a supported MSP430 MCU, clicking “Project Save” under the “File” menu automatically disconnects communication. For now, this can be resolved by disconnecting the communication, closing and re-opening the EMDC GUI to the same EMDC project and then restarting the communication. Communication should be re-established (e.g. results in the “Results” tab should start updating).
Revision History¶
The Revision History chapter tracks changes in the Energy Measurement Technology Guide and Energy Measurement Software Library.
For More Information¶
Visit the MSP E2E Forum for support.