Revision History¶
This chapter tracks changes in the Energy Measurement Technology Guide and Energy Measurement Software Library.
Revision History of Energy Measurement Technology Guide Releases¶
Release v1.40.00.00¶
Release Date: 2020-July-31
Software
Fixed an issue where the MSP430i20xx OSR (sampling rate) did not change from the default value.
Removed duplicate hal_system_Init() call.
Re-initialized results after disabling interrupts and writing calibration factors to INFO memory.
Re-calibrated MSP430i20xx EMDC example projects and firmware images.
Technology Guide
Included a flowchart for the EMDC application code including foreground and background processes.
Added a Known Limitations section to the Introduction for more awareness.
Fixed the Result Parameter command values in the Commands from Target to EMDC section and sequence diagrams.
Added more details about the packet structure and checksum calculation in the Communication Protocol Spec section.
Included the default UART communication settings.
Updated the EMDC start-up image to fix a broken pixel in the platform bar.
Fixed some minor formatting issues.
Release v1.30.00.00¶
Release Date: 2018-July-20
Technology Guide
Updated documentation and images to support Rogowski Coil current sensors.
Updated code generation to support both CCS and IAR IDEs.
Added an Out-of-Box Experience section to enable users to view results in EMDC more quickly.
Included a high-level diagram illustrating the communication connections and tools between the PC and EVM.
Updated the tables summarizing the MSP-ISO connections to prevent the target device on the EVM from being back-powered through the UART pins.
Fixed broken links to software API guide and other minor formatting issues.
Renamed EMDC example projects and example firmware examples to include the current sensor type.
Revision History of Energy Measurement Software Library Releases¶
Although Energy Measurement Software Library and Energy Measurement Design Center GUI are delivered together, the Energy Measurement Software Library has its own version tracking and change control. Every major library release comes with change control data in the Software Library API guide that describes any new features that have been added and any changes to existing functionality.