MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
APP_INTERFACE_T Struct Reference

App interface Structure. More...

#include <appInterface.h>

Collaboration diagram for APP_INTERFACE_T:
Collaboration graph
[legend]

Data Fields

USER_INPUTS_T userInputs
 
USER_INPUTS_INTERFACE_T userInputsInterface
 
USER_STATUS_INTERFACE_TpUserOutputs
 
volatile APPINTERFACE_FLAGS_T flags
 
volatile uint16_t servicesCount
 

Detailed Description

App interface Structure.

Field Documentation

§ userInputs

USER_INPUTS_T APP_INTERFACE_T::userInputs

user inputs

§ userInputsInterface

USER_INPUTS_INTERFACE_T APP_INTERFACE_T::userInputsInterface

user input interface

§ pUserOutputs

USER_STATUS_INTERFACE_T* APP_INTERFACE_T::pUserOutputs

user output

§ flags

volatile APPINTERFACE_FLAGS_T APP_INTERFACE_T::flags

App interface flags

§ servicesCount

volatile uint16_t APP_INTERFACE_T::servicesCount

variable is used to count Number of ms the befor service of low priority task


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale