MSPM0G3519SensoredFOCMotorControlLibrary  1.0
Data Fields
userInputMotorStartUp2 Struct Reference

userInputMotorStartUp2 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t thetaErrRampRate: 3
 
uint32_t firstCycFreqSel: 1
 
uint32_t olFirstCycFreq: 4
 
uint32_t reserved: 5
 
uint32_t olMaxSpeed: 5
 
uint32_t reserved1: 1
 
uint32_t olAcc2: 4
 
uint32_t olAcc1: 4
 
uint32_t olILimit: 5
 

Detailed Description

userInputMotorStartUp2 structure

Field Documentation

§ thetaErrRampRate

uint32_t userInputMotorStartUp2::thetaErrRampRate

Ramp rate for reducing difference between estimated theta and open loop theta

§ firstCycFreqSel

uint32_t userInputMotorStartUp2::firstCycFreqSel

First cycle frequency in open loop for align, double align and IPD startup options

Referenced by updateCurrentControlConfigParam().

§ olFirstCycFreq

uint32_t userInputMotorStartUp2::olFirstCycFreq

Frequency of first cycle in OL with fast Startup (% of MAX_SPEED)

Referenced by updateCurrentControlConfigParam().

§ reserved

uint32_t userInputMotorStartUp2::reserved

Align angle

§ olMaxSpeed

uint32_t userInputMotorStartUp2::olMaxSpeed

Open Loop Maximum Speed (% of MAX_SPEED)

Referenced by update_MotorStartUp2Config().

§ reserved1

uint32_t userInputMotorStartUp2::reserved1

Auto handoff enable

§ olAcc2

uint32_t userInputMotorStartUp2::olAcc2

Open loop acceleration coefficient A2

Referenced by update_MotorStartUp2Config().

§ olAcc1

uint32_t userInputMotorStartUp2::olAcc1

Open loop acceleration coefficient A1

Referenced by updateCurrentControlConfigParam().

§ olILimit

uint32_t userInputMotorStartUp2::olILimit

Open loop current limit

Referenced by updateCurrentControlConfigParam().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale