88 #ifndef APPINPUTCTRLINTERFACE_H 89 #define APPINPUTCTRLINTERFACE_H 241 fluxWeakCurrRatio: 3,
243 fluxWeakeningReference: 2,
377 busCurrLimitEnable: 1,
505 forceVQCurrLoopDis: 10,
507 forceVDCurrLoopDis: 10,
536 fluxModeReference: 10,
USER_INPUT_MTR_STARTUP1_T mtrStartUp1
Definition: appInputCtrlInterface.h:438
RAM_SPEED_CTRL_T speedCtrl
Definition: appInputCtrlInterface.h:568
float fluxWeakeningKp
Definition: appInputCtrlInterface.h:425
uint16_t dacEn
Definition: appInputCtrlInterface.h:555
ALGO_DEBUG_2 register.
Definition: appInputCtrlInterface.h:542
float speedLoopKi
Definition: appInputCtrlInterface.h:417
userInputFieldCtrl b
Definition: appInputCtrlInterface.h:254
float maxMotorSpeed
Definition: appInputCtrlInterface.h:411
USER_INPUT_MTR_STARTUP2_T mtrStartUp2
Definition: appInputCtrlInterface.h:440
float currentBase
Definition: appInputCtrlInterface.h:409
int32_t dacScalingFactor
Definition: appInputCtrlInterface.h:559
ramAlgoDebugCtrl3 b
Definition: appInputCtrlInterface.h:545
float fluxWeakeningKi
Definition: appInputCtrlInterface.h:423
DEVICE_CONFIG1 register.
Definition: appInputCtrlInterface.h:565
uint32_t w
Definition: appInputCtrlInterface.h:276
RAM_DAC_CNTRL_T dacCtrl
Definition: appInputCtrlInterface.h:576
SYSTEM_CONFIGURATIONS.
Definition: appInputCtrlInterface.h:396
uint32_t polePairs
Definition: appInputCtrlInterface.h:427
USER_INPUT_MISC_ALGO_T miscAlgo
Definition: appInputCtrlInterface.h:452
ramSpeedCtrl b
Definition: appInputCtrlInterface.h:474
START_UP1_CONFIG register.
Definition: appInputCtrlInterface.h:121
ramAlgoDebugCtrl2 structure
Definition: appInputCtrlInterface.h:532
userInputMotorStartUp2 b
Definition: appInputCtrlInterface.h:159
float voltageBase
Definition: appInputCtrlInterface.h:407
ramAlgoDebugCtrl1 structure
Definition: appInputCtrlInterface.h:480
uint32_t w
Definition: appInputCtrlInterface.h:231
userInputMotorStartUp1 b
Definition: appInputCtrlInterface.h:124
FAULT_CONFIG1 register.
Definition: appInputCtrlInterface.h:271
ALGO_DEBUG_2 register.
Definition: appInputCtrlInterface.h:523
uint32_t w
Definition: appInputCtrlInterface.h:161
userInputPinCfg b
Definition: appInputCtrlInterface.h:363
RAM_ALGO_DEBUG_2_T algoDebugCtrl2
Definition: appInputCtrlInterface.h:572
float mtrSaliency
Definition: appInputCtrlInterface.h:403
SYSTEM_PARAMETERS_T systemParams
Definition: appInputCtrlInterface.h:436
uint32_t w
Definition: appInputCtrlInterface.h:547
userInputFaultCfg1 b
Definition: appInputCtrlInterface.h:274
FAULT_CONFIG2 register.
Definition: appInputCtrlInterface.h:335
DAC_CNTRL register.
Definition: appInputCtrlInterface.h:552
userInputMiscAlgo b
Definition: appInputCtrlInterface.h:338
userInputFieldCtrl structure
Definition: appInputCtrlInterface.h:251
ramAlgoDebugCtrl2 structure
Definition: appInputCtrlInterface.h:499
SPEED_CTRL register.
Definition: appInputCtrlInterface.h:471
uint32_t w
Definition: appInputCtrlInterface.h:528
float currLoopKp
Definition: appInputCtrlInterface.h:419
userInputCloseLoop1 b
Definition: appInputCtrlInterface.h:203
float speedLoopKp
Definition: appInputCtrlInterface.h:415
CLOSELOOP2_CONFIG register.
Definition: appInputCtrlInterface.h:226
USER_INPUT_FAULT_CFG2_T faultCfg2
Definition: appInputCtrlInterface.h:450
USER_INPUT_PIN_CFG_T pinCfg
Definition: appInputCtrlInterface.h:454
uint32_t maxMotorPower
Definition: appInputCtrlInterface.h:413
userInputCloseLoop2 b
Definition: appInputCtrlInterface.h:229
USER_INPUT_FIELD_CTRL_T fieldCtrl
Definition: appInputCtrlInterface.h:446
uint32_t w
Definition: appInputCtrlInterface.h:256
float currLoopKi
Definition: appInputCtrlInterface.h:421
START_UP2_CONFIG register.
Definition: appInputCtrlInterface.h:156
uint32_t w
Definition: appInputCtrlInterface.h:365
ramAlgoDebugCtrl2 b
Definition: appInputCtrlInterface.h:526
userInputFaultCfg2 b
Definition: appInputCtrlInterface.h:313
PERI_CONFIG1 register.
Definition: appInputCtrlInterface.h:387
uint32_t w
Definition: appInputCtrlInterface.h:315
uint32_t w
Definition: appInputCtrlInterface.h:205
uint32_t w
Definition: appInputCtrlInterface.h:392
uint32_t dacOutAddr
Definition: appInputCtrlInterface.h:561
PIN_CONFIG register.
Definition: appInputCtrlInterface.h:360
uint32_t mtrResist
Definition: appInputCtrlInterface.h:399
userInputPeriCfg1 b
Definition: appInputCtrlInterface.h:390
uint32_t w
Definition: appInputCtrlInterface.h:126
uint32_t mtrInductance
Definition: appInputCtrlInterface.h:401
USER_INPUT_FAULT_CFG1_T faultCfg1
Definition: appInputCtrlInterface.h:448
USER_INPUT_CLOSE_LOOP1_T closeLoop1
Definition: appInputCtrlInterface.h:442
uint32_t w
Definition: appInputCtrlInterface.h:476
RAM_ALGO_DEBUG_3_T algoDebugCtrl3
Definition: appInputCtrlInterface.h:574
uint32_t w
Definition: appInputCtrlInterface.h:495
DEVICE_CONFIG1 register.
Definition: appInputCtrlInterface.h:433
FAULT_CONFIG2 register.
Definition: appInputCtrlInterface.h:310
ALGO_DEBUG_1 register.
Definition: appInputCtrlInterface.h:490
USER_INPUT_CLOSE_LOOP2_T closeLoop2
Definition: appInputCtrlInterface.h:444
ramSpeedCtrl structure
Definition: appInputCtrlInterface.h:461
USER_INPUT_PERI_CFG1_T periphCfg1
Definition: appInputCtrlInterface.h:456
RAM_ALGO_DEBUG_1_T algoDebugCtrl1
Definition: appInputCtrlInterface.h:570
int16_t dacShift
Definition: appInputCtrlInterface.h:557
uint32_t mtrBemfConst
Definition: appInputCtrlInterface.h:405
ramAlgoDebugCtrl1 b
Definition: appInputCtrlInterface.h:493
uint32_t w
Definition: appInputCtrlInterface.h:340
CLOSELOOP1_CONFIG register.
Definition: appInputCtrlInterface.h:200