MSPM0G3519SensoredFOCMotorControlLibrary  1.0
Data Fields
userInputCloseLoop2 Struct Reference

userInputCloseLoop2 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t reserved: 14
 
uint32_t leadAngle: 5
 
uint32_t brkCurrThr: 5
 
uint32_t brkSpeedThr: 4
 
uint32_t actSpinThr: 4
 

Detailed Description

userInputCloseLoop2 structure

Field Documentation

§ reserved

uint32_t userInputCloseLoop2::reserved

Reserved

§ leadAngle

uint32_t userInputCloseLoop2::leadAngle

Lead angle for voltage input

Referenced by user_config_faults().

§ brkCurrThr

uint32_t userInputCloseLoop2::brkCurrThr

Brake current threshold

Referenced by updateCurrentControlConfigParam().

§ brkSpeedThr

uint32_t userInputCloseLoop2::brkSpeedThr

Speed threshold for BRAKE pin and motor stop options (low-side braking or high-side braking or align braking) (% of MAX_SPEED)

Referenced by updateCurrentControlConfigParam().

§ actSpinThr

uint32_t userInputCloseLoop2::actSpinThr

Speed threshold for active spin down (% of MAX_SPEED)

Referenced by updateCurrentControlConfigParam().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale