4.11. DIO Module

4.11.1. Acronyms and Definitions

Abbreviation/Term

Explanation

LSB

Least Significant Bit

MSB

Most Significant Bit

DIO

Digital Input Output

ID

Identifier

ADC

Analog to Digital Converter

SPI

Serial Peripheral Interface

PWM

Pulse Width Modulation

ICU

Input Capture Unit

DET

Default Error Tracer

DEM

Diagnostic Event Manager

Definitions

Descriptions

DIO channel

Represents a single general-purpose digital input/output pin

DIO port

Represents several DIO channels that are grouped by hardware

DIO channel group

Represents several adjoining DIO channels represented by a logical group

Physical Level(Input)

Two states possible: LOW/HIGH. A bit value ‘0’ represents a LOW, a bit value ‘1’ represents a HIGH

Physical Level(Output)

Two states possible: LOW/HIGH. A bit value ‘0’ represents a LOW, a bit value ‘1’ represents a HIGH

4.11.2. Introduction

This document describes the functionality, API and configuration of the AUTOSAR BSW module DIO.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Link-time, Pre-compile

Vendor ID

DIO_VENDOR_ID (44)

Module ID

DIO_MODULE_ID (120)

Supported Platform

AM263x

4.11.3. Functional Overview

The DIO driver provides port and channel based read and write access to the internal general purpose I/O ports. The read and write behaviour is unbuffered. The basic behaviour of this driver is synchronous.

The DIO Driver provides services for reading and writing to/from

  1. DIO Channels (Pins)

  2. DIO Ports

  3. DIO Channel Groups

4.11.3.1. DIO Driver Architecture

The DIO driver has architecture as shown in below figure from the AUTOSAR spec

DIO in AUTOSAR architecture

Fig. 4.55 DIO in AUTOSAR architecture

4.11.3.2. Initialization

The DIO module shall not provide an interface for initialization of the hardware. The Port Driver performs this.

4.11.3.3. States

No state is maintained in the DIO driver

4.11.3.4. Assumptions

Below listed are assumed to valid for this design/implementation, exceptions and other deviations are listed for each explicitly. Care should be taken to ensure these assumptions are addressed by an entity outside DIO driver.

1.This module works on pins and ports which must be configured external to this device. Overall configuration and initialization of the port structure which is used in the DIO module.

2.The DIO functions are valid only after the Port Driver has been initialized. If it is not initialized, then DIO behavior is undefined.

3.The functional clock to the DIO module is expected to be ON before calling any DIO module API.

4.Please Note that an entity outside DIO module will take care to configured required voltage level for DIO.

4.11.3.5. Limitations

None

4.11.3.6. Design overview

Please refer SITARA MCU MCAL Architecture Document and AM26x MCAL: DIO Detailed Design Document provided as part of CSP.

4.11.4. Hardware Features

4.11.4.1. IP Supported Features

  • Dedicated general-purpose pins that can be configured as either inputs or outputs

  • Programmable pull up/pull down function

  • Supports GPIO output in push/pull or open-drain modes

  • The GPIO peripheral can produce host CPU interrupts and DMA synchronization events

4.11.4.2. AUTOSAR Supported Features

  • Read/write of individual GPIO pins

  • Read/write of GPIO registers

  • Read/write of GPIO registers with configurable mask

  • Flip the level of a particular GPIO pin

4.11.4.3. Not Supported Features

None

4.11.5. Source files

Static source C Files are defined below in the table.

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Dio
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┗ 📜Dio.h : Contains the API’s of the DIO driver to be used by upper layers
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┗ 📜Dio.c : Implementation of the API’s for DIO driver
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜Dio_Priv.h : Contains data structures and Internal function declarations
┃ ┃ ┃ ┗ 📜Dio_Priv.c : Contains Functions that support the API’s for DIO driver
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt

Plugin files are defined below in the table.

Plugin Structure

Descriptions

Dio_Cfg.h

Contains the base addresses, Precompile switches, Macros for channels, counters etc.

Dio_Lcfg.c

Contains all channels Link time Configuration parameters

Dio_Cfg.c

Contains all channels Pre-Compile Configuration parameters

The below diagram shows the files structure for the DIO driver. The Dio.c and Dio.h are the 2 files that contain the DIO driver’s API’s.

DIO Driver File Structure

Fig. 4.56 DIO Driver File Structure

DIO header file include structure

Fig. 4.57 DIO header file include structure

4.11.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.11.6.1. Memory Mapping

Memory Mapping Sections

DIO_CODE

DIO_CODE_ISR

DIO_VAR_NO_INIT

DIO_VAR_ZERO_INIT

DIO_PBCFG

DIO_PBCFG_ROOT

DIO_START_SEC_VAR_INIT_UNSPECIFIED(.bss)

x

DIO_STOP_SEC_VAR_INIT_UNSPECIFIED

x

DIO_START_SEC_CODE_APPL(.text)

x

DIO_STOP_SEC_CODE_APPL

x

DIO_START_SEC_VAR_UNSPECIFIED(.data)

x

DIO_STOP_SEC_VAR_UNSPECIFIED

x

DIO_START_SEC_CODE(.text)

x

DIO_STOP_SEC_CODE

x

DIO_START_SEC_PBCFG(.data)

x

DIO_STOP_SEC_PBCFG

x

DIO_START_SEC_PBCFG_ROOT(.const)

x

DIO_STOP_SEC_PBCFG_ROOT

x

4.11.6.2. Scheduling

There is no scheduling functions in Dio.

4.11.6.3. Error handling

4.11.6.3.1. Development Error Reporting

By default, development errors are reported to the Development Error Tracer (DET) using the service Det_ReportError() if detection and reporting of development errors is enabled in the configuration tool. If another module is used for development error reporting, the function name for reporting the error can be configured by the integrator, but must have the same signature as the service Det_ReportError().

4.11.6.4. Error Code

4.11.6.4.1. Development Errors

Type of Error

Related Error Code

Value

API parameter checking: Invalid channel requested

DIO_E_PARAM_INVALID_CHANNEL_ID

0x0A

API parameter checking: Invalid port requested

DIO_E_PARAM_INVALID_PORT_ID

0x14

API parameter checking: Invalid channel group requested

DIO_E_PARAM_INVALID_GROUP

0x1F

API service called with a NULL pointer

DIO_E_PARAM_POINTER

0x20

4.11.6.4.2. DEM Errors

The extended production errors reported to DEM module are described in the following table:

Error Code

Description

Assigned by DEM

DIO_WRITE_CHANNEL_EVENT_ID

This error is raised when IO check for the DIO channel fails

Assigned by DEM

DIO_WRITE_PORT_EVENT_ID

This error is raised when DIO write to port fails

Assigned by DEM

DIO_E_HARDWARE_ERROR

This error is raised when register write failure occurs(Hardware Failure)

4.11.7. Used resources

4.11.7.1. Interrupt Handling

The DIO modules doesn’t implement any Interrupt Service Routines.

4.11.7.2. Hardware-Software Mapping

  • GPIO Channels Mapping

AM263x have total 139 GPIO pins available​ which allocated from Bank A(Bank 0) to Bank I(Bank 8).

Each Bank contains 16 channels except Bank I​(Bank 8).

Bank I​ contains 11 channels.

GPIO Banks

GPIO Channels

BankA / Bank0

Channel 0 to channel 15

BankB / Bank1

Channel 16 to channel 31

BankC / Bank2

Channel 32 to channel 47

BankD / Bank3

Channel 48 to channel 63

BankE / Bank4

Channel 64 to channel 79

BankF / Bank5

Channel 80 to channel 95

BankG / Bank6

Channel 96 to channel 111

BankH / Bank7

Channel 112 to channel 127

BankI / Bank8

Channel 128 to channel 138

4.11.8. Integration description

4.11.8.1. Dependent modules

4.11.8.1.1. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF), The switch DIO_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

4.11.8.1.2. DEM

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus ().

Note

Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.

4.11.8.1.3. PORT

The DIO Modules expects that pinmux is set correctly to configure the GPIO pins for GPIO mode. This is done by the PORT driver. The pin direction shall also be set by the PORT driver.

4.11.8.1.4. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that DIO module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.

For DIO Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

Dio Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

DIO_EXCLUSIVE_AREA_0

Dio_WritePort
Dio_WriteChannelGroup
Dio_WriteChannel

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.11.8.1.5. Dio Callback Functions

The DIO driver does not provide any call back functions

4.11.8.2. Multi-core support

Not Supported

4.11.9. Configuration

4.11.9.1. DioConfig

This container contains the configuration parameters and sub containers of the AUTOSAR DIO module. This container is a MultipleConfigurationContainer, i.e. this container and its sub-containers exist once per configuration set.

4.11.9.1.1. DioPort

Configuration of individual DIO ports, consisting of channels and possible channel groups.

4.11.9.1.2. DioPortId

Item

Name

DioPortId

Description

Numeric identifier of the DIO port. Not all MCU ports may be used for DIO, thus there may be “gaps” in the list of all IDs. This value will be

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

4

Min-value

0

4.11.9.1.3. DioChannel

Configuration of an individual DIO channel. Besides a HW specific channel name which is typically fixed for a specific micro controller, additional symbolic names can be defined per channel.

4.11.9.1.4. DioChannelId

Item

Name

DioChannelId

Description

Channel Id of the DIO channel. This value will be assigned to the symbolic names.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

138

Min-value

0

4.11.9.1.5. DioChannelGroup

Definition and configuration of DIO channel groups. A channel group represents several adjoining DIO channels represented by a logical group.

4.11.9.1.6. DioChannelGroupIdentification

Item

Name

DioChannelGroupIdentification

Description

The DIO channel group is identified in DIO API by a pointer to a data structure (of type Dio_ChannelGroupType). That data structure contains the channel group information.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.11.9.1.7. DioPortMask

Item

Name

DioPortMask

Description

This shall be the mask which defines the positions of the channel

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

4294967295

Min-value

0

4.11.9.1.8. DioPortOffset

Item

Name

DioPortOffset

Description

The position of the Channel Group on the port, counted

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

31

Min-value

0

4.11.9.2. DioGeneral

General DIO module configuration parameters.

4.11.9.2.1. DioDevErrorDetect

Item

Name

DioDevErrorDetect

Description

Switches the Development Error Detection and Notification

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.11.9.2.2. DioDemEnable

Item

Name

DioDemEnable

Description

Switches the Diagnostic event manager Notification

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.11.9.2.3. DioFlipChannelApi

Item

Name

DioFlipChannelApi

Description

Adds / removes the service Dio_FlipChannel() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.11.9.2.4. DioVersionInfoApi

Item

Name

DioVersionInfoApi

Description

Adds / removes the service Dio_ GetVersionInfo() from the code.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.11.9.2.5. DioHostCoreId

Item

Name

DioHostCoreId

Description

R5F CPU ownership of GPIO. 0 - R5FSS0 Core0, 1 - R5FSS0 Core1, 2 - R5FSS1 Core0, 3 - R5FSS1 Core1

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

3

Min-value

0

4.11.9.2.6. DioRegisterReadbackApi

Item

Name

DioRegisterReadbackApi

Description

Adds / removes the service Dio_RegisterReadback() from the code.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

Note

GPIO usage for the cores other than R5F0_0 If AUTOSAR MCAL is running on cores other than R5F0_0, user need to take care of following configuration

DioHostCoreId: R5F CPU ownership of GPIO.

0 -> R5FSS0 Core0 
1 -> R5FSS0 Core1 
2 -> R5FSS1 Core0 
3 -> R5FSS1 Core1
../_images/dio_image5.jpg

4.11.10. Examples

4.11.10.1. Overview

  • Dio Example

    • Initialize clock using Mcu_Init()

    • Initialize port using Port_Init()

    • Get Dio Version using Dio_GetVersionInfo()

    • Set Port Pin direction of GPIOGH_128 to PORT_PIN_OUT using Port_SetPinDirection()

    • Read the Port pin channel level using Dio_ReadChannel()

    • Toggle the channel level using Dio_FlipChannel()

    • Change the channel level using Dio_WriteChannel()

    • Set a value to the Port using Dio_WritePort()

    • Read the port level using Dio_ReadPort()

    • Change a subset of the adjoining bits of a port using Dio_WriteChannelGroup()

    • Read a subset of the adjoining bits of a port using Dio_ReadChannelGroup()

    • Verify the read result.

4.11.10.2. Setup required to run example

None

4.11.10.3. How to run examples

1.DIO example application demonstrating the MCAL DIO driver features is in folder <MCAL_ROOT>/examples/Dio.

2.This application can be built from the build folder by giving “gmake –s dio_app PLATFORM=am263” command in command prompt.

3.Once the build is completed we get a binary file, which is loaded in our controller and executed.

4.11.10.3.1. Configuration used to test this example

1.The DIO example app used to verify the port pin (High/Low) functionalities.

2.GPIOI_128(Ball number A15) these pins are configured as a GPIO.

3.Pin Configurations are provided in mcal/example/Config/Port_PBcfg.c File.

4.Read the channel level before and after Dio_FlipChannel

5.Read the Port value before and after Dio_FlipChannel

4.11.10.4. Sample Log

CLANG compiled : DioApp: Sample Application - STARTS !!!
DIO Driver version info:9.1.0
DIO Driver Module/Driver:120.44 
Port Value:1 
Port Value for GPIOGH channel 2 :1 
Dio_FlipChannel - GPIOGH
Port Value:0 
Dio_FlipChannel - GPIOGH
Port Value:1 
Port Value for GPIOGH :1 
Dio_FlipChannel - GPIOGH 
Port Value:0 
Dio_FlipChannel -GPIOGH
Port Value:1 
Dio_WriteChannel -GPIOGH
Port Value:0 
Dio_WriteChannel -GPIOGH
Port Value:1 
Port Value Before Flip:1c1 
After Flip Port Value:0 
Read channel grp Port Value:1 
DIO Test Passed!!!

4.11.10.5. File Structure

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Dio
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜Dioapp.c : Contains Dio test example
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Dio_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Dio_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Dio_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗ 📜Dio_Lcfg.c : contains all Link time configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt

4.11.11. References

AUTOSAR_SWS_DIODriver
Technical Reference Manual