4.3. CDD CMPSS Module
4.3.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
RTE |
Runtime Environment |
BSW |
Basic Software |
MCAL |
Micro Controller Abstraction Layer |
API |
Application Programming Interface |
DET |
Default Error Tracer |
HW |
Hardware |
SW |
Software |
I/O |
Input/Output |
CMPSS |
Comparator Subsystem |
OS |
Operating System |
4.3.2. Introduction
This document describes the functionality and configuration of the Cdd_Cmpss module.
Supported AUTOSAR Release |
4.3.1 |
|---|---|
Supported Configuration Variants |
None |
Vendor ID |
CDD_CMPSS_VENDOR_ID (44) |
Module ID |
CDD_CMPSS_MODULE_ID (255) |
Supported Platform |
AM263x, AM263Px, AM261x |
The CMPSS CDD provides services to configure the Comparator Subsystem (CMPSS) of the SOC.
4.3.3. Functional Overview
CMPSS consists of analog comparators and supporting circuits that are useful for power applications such as peak current mode control, switched-mode power, power factor correction, voltage trip monitoring, and so forth.
4.3.3.1. Initialization
This module doesn’t support any initialization and de-init routines. Hence there is no requirement to support pre-compile and post build configuration options.
The driver provides only compile time configuration options via Cdd_Cmpss_Cfg.h. The user need to edit this file to have different configuration from the current default configurations. Generation of this configuration is not provided via configurator as this module doesn’t have or require init time configurations.
4.3.3.2. States
This driver is stateless.
4.3.3.3. Assumptions
None
4.3.3.4. Limitations
None
4.3.3.5. Design Overview
Please refer SITARA MCU MCAL Architecture Document and MCAL: CDD CMPSS Detailed Design Document provided as part of CSP.
4.3.4. Hardware Features
4.3.4.1. Hardware Features supported
Two analog comparators
Two independently programmable reference 12-bit DACs
One decrementing ramp generator
Two digital filters, max filter clock prescale of 216
Ability to synchronize submodules with EPWMSYNCPER
Ability to extend clear signal with EPWMBLANK
Ability to synchronize output with SYSCLK
Ability to latch output
Ability to invert output
Option to use hysteresis on the input
Option for negative input of comparator to be driven by an external signal or by the reference DAC for COMPH
VDACREF is the DAC reference voltage
Diode emulation support
The system works with EPWM to support the Diode emulation feature
Ramp generator prescaler
4.3.5. Source Files
Static source C Files are defined below
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Cdd_Cmpss
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Cmpss.h : Contains the API’s of the driver to be used by upper layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Cmpss.c : Contains the implementation of the API’s for the driver.
┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┗ 📜Cdd_Cmpss_Soc.h : Contains SOC specific internal data
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt
Plugin files are defined below in the table.
Plugin Files |
Description |
|---|---|
Cdd_Cmpss_Cfg.h |
Contains the Precompile switches, Macros. |
4.3.6. Module Requirements
Please refer Software Product Specification document provided as part of CSP.
4.3.6.1. Memory Mapping
Memory Mapping Sections |
CDD_CMPSS_CODE |
CDD_CMPSS_CONST |
|---|---|---|
CDD_CMPSS_START_SEC_CONST_UNSPECIFIED |
X |
|
CDD_CMPSS_STOP_SEC_CONST_UNSPECIFIED |
X |
|
CDD_CMPSS_START_SEC_CODE |
X |
|
CDD_CMPSS_STOP_SEC_CODE |
X |
4.3.6.2. Scheduling
Not applicable
4.3.6.3. Error Handling
4.3.6.3.1. Development Error Reporting
Development errors are reported to the DET using the service Det_ReportError() when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.
4.3.6.3.1.1. Error Codes
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
API service called will null param pointer |
CDD_CMPSS_E_PARAM_POINTER |
0x01 |
API service called with illegal HW ID |
CDD_CMPSS_E_ILLEGAL_HW_ID |
0x02 |
API service called invalid configuration |
CDD_CMPSS_E_INVALID_CONFIG |
0x03 |
4.3.6.3.1.2. Runtime Error
None
4.3.6.3.2. DEM Error
None
4.3.7. Used Resources
4.3.7.1. Interrupt Handling
None
4.3.8. Integration Description
4.3.8.1. Dependent Modules
4.3.8.1.1. DET
The CMPSS module depends on the DET (by default) to report development errors. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.
4.3.8.2. Multi-core Support
Not Supported
4.3.9. Configuration
The CMPSS Driver implementation supports multiple configuration variants The driver expects Cdd_Cmpss_Cfg.h to be present as input file.
4.3.10. Examples
4.3.10.1. Overview
The CMPSS example enables the CMPSS High comparator and feeds the asynchronous output to GPIO and EPWM. This example enables the CMPSSA1 COMPH comparator and feeds the asynchronous CTRIPOUTH signal to the XBAROUT0 pin and CTRIPH to EPWM0B.
CMPSS is configured to generate trip signals to trip the EPWM signals. CMPIN1P is used to give positive input and internal DAC is configured to provide the negative input. Internal DAC is configured to provide a signal at VDD/2. An EPWM signal is generated at EPWM0B and is configured to be tripped by CTRIPH. This is done via PWM XBAR output 3 configuration.
Note: When no input is provided, the analog input is not fixed and hence the result is not deterministic. Most cases it is seen that the CMPSS trips the PWM when no input is provided.
When a low input(VSS) is provided to CMPIN1P,
Trip signal(XBAROUT0) output is low
EPWM0B gives a PWM signal
When a high input(higher than VDD/2) is provided to CMPIN1P,
Trip signal(XBAROUT0) output turns high
EPWM0B gets tripped and outputs as high
4.3.10.1.1. External Connections
Give input on CMPIN1P (ControlCard HSEC Pin 15)
AM263x and AM263Px
For low input (no trip), connect J6 Pin 9 (0v/GND) to HSEC pin 15
For high input (trips pwm), connect J6 Pin 10 (3.3v/VCC) to HSEC pin 15
AM261x
For low input (no trip), connect any (0v/GND) pin to HSEC pin 15
For high input (trips pwm), connect any (3.3v/VCC) to HSEC pin 15
Outputs can be observed on
XBAROUT0 (SOC pin QSPI0_CSN1. USER_LED1 on ControlCard)
EPWM0B (ControlCard HSEC pin 51) using an oscilloscope
4.3.10.2. Hardware Software Setup and Tools
See example description above
4.3.10.3. Steps to Build and Run Example
CMPSS example application demonstrating the CMPSS features is in folder <MCAL_ROOT>/examples/Cdd_Cmpss.
This application can be built from the build folder by giving “gmake –s cdd_cmpss_app PLATFORM=am263px”
Once the build is completed we get a binary file, which is loaded in our controller and executed.
4.3.10.4. Example Logs
CDD_CMPSS_APP: Asynchronous trip - STARTS !!!
CMPSS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 255
SW Major Version : 1
SW Minor Version : 0
SW Patch Version : 0
CDD_CMPSS_APP: PWM tripped!!!
CDD_CMPSS_APP: PWM one-shot trip event status set!!!
CDD_CMPSS_APP: PWM latched trip interrupt status set!!!
CDD_CMPSS_APP: CMPSS HI and LO filter out status set!!!
CDD_CMPSS_APP: CMPSS HI and LO latched filter out status set!!!
CDD_CMPSS_APP: Output XBAR status set!!!
CDD_CMPSS_APP: Output XBAR latched status set!!!
CDD_CMPSS_APP: Stack Usage: 808 bytes
CDD_CMPSS_APP: Asynchronous trip - DONE (Passed) !!!
CDD_CMPSS_APP: All tests have passed
4.3.10.5. File Structure
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Cdd_Cmpss
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜Cdd_Pwm_PBcfg.c : Contains PWM PB configuration to showcase the PWM trip.
┃ ┃ ┃ ┣ 📜CddCmpssApp.c : Contains test example.
┃ ┃ ┃ ┣ 📜CddCmpssApp.h : Contains test private header containing dependent includes and macro.
┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Cdd_Cmpss_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Cmpss_Cfg.h : Contains the Precompile switches, Macros for CMPSS.
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt
4.3.11. FAQ’s
None