4.19. MCU Module

4.19.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

GPIO

General Purpose Input Output

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

HW

Hardware

SW

Software

I/O

Input/Output

ADC

Analog to Digital Convertor

PWM

Pulse Width Modulation

MCU

Micro Controller Unit

PLL

Phase Locked Loop

OS

Operating System

4.19.2. Introduction

This document describes MCAL MCU Driver functionality and configuration details as per AUTOSAR version 4.3.1 .

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile, Post-build

Vendor ID

MCU_VENDOR_ID (44)

Module ID

MCU_MODULE_ID (101)

Supported Platform

AM261x

The MCU driver provides services for basic microcontroller initialization, reset and microcontroller specific functions required by other MCAL software modules.

The MCU driver provides MCU services for Clock and RAM initialization. In the MCU configuration set, the MCU specific settings for the Clock (i.e. PLL setting) and RAM (i.e. section base address and size) shall be configured.

4.19.3. Functional Overview

4.19.3.1. MCU Driver Architecture

The MCU driver has architecture as shown in below figure from the AUTOSAR spec.

MCU in AUTOSAR architecture

Fig. 4.80 MCU in AUTOSAR architecture

Interface of MCU

Fig. 4.81 Interface of MCU

4.19.3.2. Initialization

Mcu_Init() initializes the MCU driver and does module enable for the configured module ids.

  1. Core_Pll shall be set for 2000MHz and is divided into four HSDIV values such as:

    DPLL_CORE_HSDIV0_CLKOUT0: 400MHz, DPLL_CORE_HSDIV0_CLKOUT1: 500MHz, DPLL_CORE_HSDIV0_CLKOUT2: 400MHz and DPLL_CORE_HSDIV0_CLKOUT3: 133MHz

  2. Per_Pll shall be set for 960MHz and is divided into three HSDIV values such as:

    DPLL_PER_HSDIV0_CLKOUT0: 192MHz, DPLL_PER_HSDIV0_CLKOUT2: 160MHz and DPLL_PER_HSDIV0_CLKOUT3: 120MHz

ADC:

MCU powers the ADC module. The ADC module depends on MCU module for data buffer control and crossbar interrupt mapping of ADC interrupts depending on the Hardware unit being configured. Suppose the Hardware Unit 1 and Hardware Unit 3 are configured for ADC module:

../_images/mcu_image7.png

Then, the MCU module container “McuAdcConfiguration” should be configured as shown in below figure:

../_images/mcu_image8.png
../_images/mcu_image9.png

Interrupt Crossbar(ADC):

MCU is also enabling Interrupt crossbar and Input crossbar in Mcu_Init(). Similarly, the crossbar interrupts also needs to be mapped in MCU module according to HW unit and interrupts being required. The ADC interrupts needs to be mapped to the corresponding cross bar interrupt required. Please refer limitation section of Interrupts to be configured for ADC as per “AdcPriorityImplementation” in ADC user guide.

../_images/mcu_image10.png
../_images/mcu_image11.png

PWM:

MCU also powers the PWM module. The PWM module depends on MCU module to enable PWM Channel and crossbar interrupt mapping of PWM interrupts depending on the Hardware unit being configured. Suppose the PWM channel 0 is configured for PWM module as shown in figure:

../_images/mcu_image12.png

Then, the MCU module container “McuPwmConfiguration” should be configured as shown in below figure:

../_images/mcu_image13.png
../_images/mcu_image14.png

Interrupt Crossbar(PWM):

The crossbar interrupts needs to be mapped in MCU module according to PWM channel configured. The PWM interrupts needs to be mapped to the corresponding cross bar interrupt.

../_images/mcu_image15.png
../_images/mcu_image16.png

The interrupt cross bar generates the functions in “Mcu_IntXbar” in Mcu_PBcfg.c as per the user configuration from configurator as shown in below figure:

../_images/mcu_image17.png

Input Crossbar:

Input Crossbar can be configured from MCU as per following figure:

../_images/mcu_image18.png
../_images/mcu_image19.png

As per user configuration, input crossbars APIs will be generated in Mcu_PBcfg.c as in figure.

../_images/mcu_image20.png

MCU Crossbar Details - AM261x:

McuInterruptChannelXbar

McuInterruptChannelXbarMap

McuInputChannelXbar

McuInputChannelXbarMap

McuGpioIntrXbar

McuGpioXbarOutMap

MCU_INTRXBAR0_OUT_0

MCU_INT_XBAR_EPWM0_INT

MCU_INPUT_XBAR0_OUT_0

MCU_INPUT_XBAR_GPIO0

MCU_GPIO_0

MCU_GPIO_INT_XBAR_ICSS_XBAR_0

MCU_INTRXBAR0_OUT_1

MCU_INT_XBAR_EPWM1_INT

MCU_INPUT_XBAR0_OUT_1

MCU_INPUT_XBAR_GPIO1

MCU_GPIO_1

MCU_GPIO_INT_XBAR_ICSS_XBAR_1

MCU_INTRXBAR0_OUT_2

MCU_INT_XBAR_EPWM2_INT

MCU_INPUT_XBAR0_OUT_2

MCU_INPUT_XBAR_GPIO2

MCU_GPIO_2

MCU_GPIO_INT_XBAR_ICSS_XBAR_2

MCU_INTRXBAR0_OUT_3

MCU_INT_XBAR_EPWM3_INT

MCU_INPUT_XBAR0_OUT_3

MCU_INPUT_XBAR_GPIO3

MCU_GPIO_3

MCU_GPIO_INT_XBAR_ICSS_XBAR_3

MCU_INTRXBAR0_OUT_4

MCU_INT_XBAR_EPWM4_INT

MCU_INPUT_XBAR0_OUT_4

MCU_INPUT_XBAR_GPIO4

MCU_GPIO_4

MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_0

MCU_INTRXBAR0_OUT_5

MCU_INT_XBAR_EPWM5_INT

MCU_INPUT_XBAR0_OUT_5

MCU_INPUT_XBAR_GPIO5

MCU_GPIO_5

MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_1

MCU_INTRXBAR0_OUT_6

MCU_INT_XBAR_EPWM6_INT

MCU_INPUT_XBAR0_OUT_6

MCU_INPUT_XBAR_GPIO6

MCU_GPIO_6

MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_2

MCU_INTRXBAR0_OUT_7

MCU_INT_XBAR_EPWM7_INT

MCU_INPUT_XBAR0_OUT_7

MCU_INPUT_XBAR_GPIO7

MCU_GPIO_7

MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_3

MCU_INTRXBAR0_OUT_8

MCU_INT_XBAR_EPWM8_INT

MCU_INPUT_XBAR0_OUT_8

MCU_INPUT_XBAR_GPIO8

MCU_GPIO_8

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_0

MCU_INTRXBAR0_OUT_9

MCU_INT_XBAR_EPWM9_INT

MCU_INPUT_XBAR0_OUT_9

MCU_INPUT_XBAR_GPIO9

MCU_GPIO_9

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_1

MCU_INTRXBAR0_OUT_10

MCU_INT_XBAR_EPWM0_TZINT

MCU_INPUT_XBAR0_OUT_10

MCU_INPUT_XBAR_GPIO10

MCU_GPIO_10

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_2

MCU_INTRXBAR0_OUT_11

MCU_INT_XBAR_EPWM1_TZINT

MCU_INPUT_XBAR0_OUT_11

MCU_INPUT_XBAR_GPIO11

MCU_GPIO_11

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_3

MCU_INTRXBAR0_OUT_12

MCU_INT_XBAR_EPWM2_TZINT

MCU_INPUT_XBAR0_OUT_12

MCU_INPUT_XBAR_GPIO12

MCU_GPIO_12

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_4

MCU_INTRXBAR0_OUT_13

MCU_INT_XBAR_EPWM3_TZINT

MCU_INPUT_XBAR0_OUT_13

MCU_INPUT_XBAR_GPIO13

MCU_GPIO_13

MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_5

MCU_INTRXBAR0_OUT_14

MCU_INT_XBAR_EPWM4_TZINT

MCU_INPUT_XBAR0_OUT_14

MCU_INPUT_XBAR_GPIO14

MCU_GPIO_14

MCU_GPIO_INT_XBAR_VIM_MODULE0_0

MCU_INTRXBAR0_OUT_15

MCU_INT_XBAR_EPWM5_TZINT

MCU_INPUT_XBAR0_OUT_15

MCU_INPUT_XBAR_GPIO15

MCU_GPIO_15

MCU_GPIO_INT_XBAR_VIM_MODULE0_1

MCU_INTRXBAR0_OUT_16

MCU_INT_XBAR_EPWM6_TZINT

MCU_INPUT_XBAR0_OUT_16

MCU_INPUT_XBAR_GPIO16

MCU_GPIO_16

MCU_GPIO_INT_XBAR_VIM_MODULE0_2

MCU_INTRXBAR0_OUT_17

MCU_INT_XBAR_EPWM7_TZINT

MCU_INPUT_XBAR0_OUT_17

MCU_INPUT_XBAR_GPIO17

MCU_GPIO_17

MCU_GPIO_INT_XBAR_VIM_MODULE0_3

MCU_INTRXBAR0_OUT_18

MCU_INT_XBAR_EPWM8_TZINT

MCU_INPUT_XBAR0_OUT_18

MCU_INPUT_XBAR_GPIO18

MCU_GPIO_18

MCU_GPIO_INT_XBAR_VIM_MODULE1_0

MCU_INTRXBAR0_OUT_19

MCU_INT_XBAR_EPWM9_TZINT

MCU_INPUT_XBAR0_OUT_19

MCU_INPUT_XBAR_GPIO19

MCU_GPIO_19

MCU_GPIO_INT_XBAR_VIM_MODULE1_1

MCU_INTRXBAR0_OUT_20

MCU_INT_XBAR_ADC0_INT1

MCU_INPUT_XBAR0_OUT_20

MCU_INPUT_XBAR_GPIO20

MCU_GPIO_20

MCU_GPIO_INT_XBAR_VIM_MODULE1_2

MCU_INTRXBAR0_OUT_21

MCU_INT_XBAR_ADC0_INT2

MCU_INPUT_XBAR0_OUT_21

MCU_INPUT_XBAR_GPIO21

MCU_GPIO_21

MCU_GPIO_INT_XBAR_VIM_MODULE1_3

MCU_INTRXBAR0_OUT_22

MCU_INT_XBAR_ADC0_INT3

MCU_INPUT_XBAR0_OUT_22

MCU_INPUT_XBAR_GPIO22

MCU_GPIO_22

MCU_GPIO_INT_XBAR_VIM_MODULE2_0

MCU_INTRXBAR0_OUT_23

MCU_INT_XBAR_ADC0_INT4

MCU_INPUT_XBAR0_OUT_23

MCU_INPUT_XBAR_GPIO23

MCU_GPIO_23

MCU_GPIO_INT_XBAR_VIM_MODULE2_1

MCU_INTRXBAR0_OUT_24

MCU_INT_XBAR_ADC0_EVTINT

MCU_INPUT_XBAR0_OUT_24

MCU_INPUT_XBAR_GPIO24

MCU_GPIO_24

MCU_GPIO_INT_XBAR_VIM_MODULE2_2

MCU_INTRXBAR0_OUT_25

MCU_INT_XBAR_ADC1_INT1

MCU_INPUT_XBAR0_OUT_25

MCU_INPUT_XBAR_GPIO25

MCU_GPIO_25

MCU_GPIO_INT_XBAR_VIM_MODULE2_3

MCU_INTRXBAR0_OUT_26

MCU_INT_XBAR_ADC1_INT2

MCU_INPUT_XBAR0_OUT_26

MCU_INPUT_XBAR_GPIO26

MCU_GPIO_26

MCU_GPIO_INT_XBAR_VIM_MODULE3_0

MCU_INTRXBAR0_OUT_27

MCU_INT_XBAR_ADC1_INT3

MCU_INPUT_XBAR0_OUT_27

MCU_INPUT_XBAR_GPIO27

MCU_GPIO_27

MCU_GPIO_INT_XBAR_VIM_MODULE3_1

MCU_INTRXBAR0_OUT_28

MCU_INT_XBAR_ADC1_INT4

MCU_INPUT_XBAR0_OUT_28

MCU_INPUT_XBAR_GPIO28

MCU_GPIO_28

MCU_GPIO_INT_XBAR_VIM_MODULE3_2

MCU_INTRXBAR0_OUT_29

MCU_INT_XBAR_ADC1_EVTINT

MCU_INPUT_XBAR0_OUT_29

MCU_INPUT_XBAR_GPIO29

MCU_GPIO_29

MCU_GPIO_INT_XBAR_VIM_MODULE3_3

MCU_INTRXBAR0_OUT_30

MCU_INT_XBAR_ADC2_INT1

MCU_INPUT_XBAR0_OUT_30

MCU_INPUT_XBAR_GPIO30

MCU_GPIO_30

MCU_INTRXBAR0_OUT_31

MCU_INT_XBAR_ADC2_INT2

MCU_INPUT_XBAR0_OUT_31

MCU_INPUT_XBAR_GPIO31

MCU_GPIO_31

MCU_INT_XBAR_ADC2_INT3

MCU_INPUT_XBAR_GPIO32

MCU_GPIO_32

MCU_INT_XBAR_ADC2_INT4

MCU_INPUT_XBAR_GPIO33

MCU_GPIO_33

MCU_INT_XBAR_ADC2_EVTINT

MCU_INPUT_XBAR_GPIO34

MCU_GPIO_34

MCU_INT_XBAR_FSIRX0_INT1N

MCU_INPUT_XBAR_GPIO35

MCU_GPIO_35

MCU_INT_XBAR_FSIRX0_INT2N

MCU_INPUT_XBAR_GPIO36

MCU_GPIO_36

MCU_INT_XBAR_FSITX0_INT1N

MCU_INPUT_XBAR_GPIO37

MCU_GPIO_37

MCU_INT_XBAR_FSITX0_INT2N

MCU_INPUT_XBAR_GPIO38

MCU_GPIO_38

MCU_INT_XBAR_SD0_ERR

MCU_INPUT_XBAR_GPIO39

MCU_GPIO_39

MCU_INT_XBAR_SD0_FILT0_DRINT

MCU_INPUT_XBAR_GPIO40

MCU_GPIO_40

MCU_INT_XBAR_SD0_FILT1_DRINT

MCU_INPUT_XBAR_GPIO41

MCU_GPIO_41

MCU_INT_XBAR_SD0_FILT2_DRINT

MCU_INPUT_XBAR_GPIO42

MCU_GPIO_42

MCU_INT_XBAR_SD0_FILT3_DRINT

MCU_INPUT_XBAR_GPIO43

MCU_GPIO_43

MCU_INT_XBAR_ECAP0_INT

MCU_INPUT_XBAR_GPIO44

MCU_GPIO_44

MCU_INT_XBAR_ECAP1_INT

MCU_INPUT_XBAR_GPIO45

MCU_GPIO_45

MCU_INT_XBAR_ECAP2_INT

MCU_INPUT_XBAR_GPIO46

MCU_GPIO_46

MCU_INT_XBAR_ECAP3_INT

MCU_INPUT_XBAR_GPIO47

MCU_GPIO_47

MCU_INT_XBAR_ECAP4_INT

MCU_INPUT_XBAR_GPIO48

MCU_GPIO_48

MCU_INT_XBAR_ECAP5_INT

MCU_INPUT_XBAR_GPIO49

MCU_GPIO_49

MCU_INT_XBAR_ECAP6_INT

MCU_INPUT_XBAR_GPIO50

MCU_GPIO_50

MCU_INT_XBAR_ECAP7_INT

MCU_INPUT_XBAR_GPIO51

MCU_GPIO_51

MCU_INT_XBAR_EQEP0_INT

MCU_INPUT_XBAR_GPIO52

MCU_GPIO_52

MCU_INT_XBAR_EQEP1_INT

MCU_INPUT_XBAR_GPIO53

MCU_GPIO_53

MCU_INPUT_XBAR_GPIO54

MCU_GPIO_54

MCU_INPUT_XBAR_GPIO55

MCU_GPIO_55

MCU_INPUT_XBAR_GPIO56

MCU_GPIO_56

MCU_INPUT_XBAR_GPIO57

MCU_GPIO_57

MCU_INPUT_XBAR_GPIO58

MCU_GPIO_58

MCU_INPUT_XBAR_GPIO59

MCU_GPIO_59

MCU_INPUT_XBAR_GPIO60

MCU_GPIO_60

MCU_INPUT_XBAR_GPIO61

MCU_GPIO_61

MCU_INPUT_XBAR_GPIO62

MCU_GPIO_62

MCU_INPUT_XBAR_GPIO63

MCU_GPIO_63

MCU_INPUT_XBAR_GPIO64

MCU_GPIO_64

MCU_INPUT_XBAR_GPIO65

MCU_GPIO_65

MCU_INPUT_XBAR_GPIO66

MCU_GPIO_66

MCU_INPUT_XBAR_GPIO67

MCU_GPIO_67

MCU_INPUT_XBAR_GPIO68

MCU_GPIO_68

MCU_INPUT_XBAR_GPIO69

MCU_GPIO_69

MCU_INPUT_XBAR_GPIO70

MCU_GPIO_70

MCU_INPUT_XBAR_GPIO71

MCU_GPIO_71

MCU_INPUT_XBAR_GPIO72

MCU_GPIO_72

MCU_INPUT_XBAR_GPIO73

MCU_GPIO_73

MCU_INPUT_XBAR_GPIO74

MCU_GPIO_74

MCU_INPUT_XBAR_GPIO75

MCU_GPIO_75

MCU_INPUT_XBAR_GPIO76

MCU_GPIO_76

MCU_INPUT_XBAR_GPIO77

MCU_GPIO_77

MCU_INPUT_XBAR_GPIO78

MCU_GPIO_78

MCU_INPUT_XBAR_GPIO79

MCU_GPIO_79

MCU_INPUT_XBAR_GPIO80

MCU_GPIO_80

MCU_INPUT_XBAR_GPIO81

MCU_GPIO_81

MCU_INPUT_XBAR_GPIO82

MCU_GPIO_82

MCU_INPUT_XBAR_GPIO83

MCU_GPIO_83

MCU_INPUT_XBAR_GPIO84

MCU_GPIO_84

MCU_INPUT_XBAR_GPIO85

MCU_GPIO_85

MCU_INPUT_XBAR_GPIO86

MCU_GPIO_86

MCU_INPUT_XBAR_GPIO87

MCU_GPIO_87

MCU_INPUT_XBAR_GPIO88

MCU_GPIO_88

MCU_INPUT_XBAR_GPIO89

MCU_GPIO_89

MCU_INPUT_XBAR_GPIO90

MCU_GPIO_90

MCU_INPUT_XBAR_GPIO91

MCU_GPIO_91

MCU_INPUT_XBAR_GPIO92

MCU_GPIO_92

MCU_INPUT_XBAR_GPIO93

MCU_GPIO_93

MCU_INPUT_XBAR_GPIO94

MCU_GPIO_94

MCU_INPUT_XBAR_GPIO95

MCU_GPIO_95

MCU_INPUT_XBAR_GPIO96

MCU_GPIO_96

MCU_INPUT_XBAR_GPIO97

MCU_GPIO_97

MCU_INPUT_XBAR_GPIO98

MCU_GPIO_98

MCU_INPUT_XBAR_GPIO99

MCU_GPIO_99

MCU_INPUT_XBAR_GPIO100

MCU_GPIO_100

MCU_INPUT_XBAR_GPIO101

MCU_GPIO_101

MCU_INPUT_XBAR_GPIO102

MCU_GPIO_102

MCU_INPUT_XBAR_GPIO103

MCU_GPIO_103

MCU_INPUT_XBAR_GPIO104

MCU_GPIO_104

MCU_INPUT_XBAR_GPIO105

MCU_GPIO_105

MCU_INPUT_XBAR_GPIO106

MCU_GPIO_106

MCU_INPUT_XBAR_GPIO107

MCU_GPIO_107

MCU_INPUT_XBAR_GPIO108

MCU_GPIO_108

MCU_INPUT_XBAR_GPIO109

MCU_GPIO_109

MCU_INPUT_XBAR_GPIO110

MCU_GPIO_110

MCU_INPUT_XBAR_GPIO111

MCU_GPIO_111

MCU_INPUT_XBAR_GPIO112

MCU_GPIO_112

MCU_INPUT_XBAR_GPIO113

MCU_GPIO_113

MCU_INPUT_XBAR_GPIO114

MCU_GPIO_114

MCU_INPUT_XBAR_GPIO115

MCU_GPIO_115

MCU_INPUT_XBAR_GPIO116

MCU_GPIO_116

MCU_INPUT_XBAR_GPIO117

MCU_GPIO_117

MCU_INPUT_XBAR_GPIO118

MCU_GPIO_118

MCU_INPUT_XBAR_GPIO119

MCU_GPIO_119

MCU_INPUT_XBAR_GPIO120

MCU_GPIO_120

MCU_INPUT_XBAR_GPIO121

MCU_GPIO_121

MCU_INPUT_XBAR_GPIO122

MCU_GPIO_122

MCU_INPUT_XBAR_GPIO123

MCU_GPIO_123

MCU_INPUT_XBAR_GPIO124

MCU_GPIO_124

MCU_INPUT_XBAR_GPIO125

MCU_GPIO_125

MCU_INPUT_XBAR_GPIO126

MCU_GPIO_126

MCU_INPUT_XBAR_GPIO127

MCU_GPIO_127

MCU_INPUT_XBAR_GPIO128

MCU_GPIO_128

MCU_INPUT_XBAR_GPIO129

MCU_GPIO_129

MCU_INPUT_XBAR_GPIO130

MCU_GPIO_130

MCU_INPUT_XBAR_GPIO131

MCU_GPIO_131

MCU_INPUT_XBAR_GPIO132

MCU_GPIO_132

MCU_INPUT_XBAR_GPIO133

MCU_GPIO_133

MCU_INPUT_XBAR_GPIO134

MCU_GPIO_134

MCU_INPUT_XBAR_GPIO135

MCU_GPIO_135

MCU_INPUT_XBAR_GPIO136

MCU_GPIO_136

MCU_INPUT_XBAR_GPIO137

MCU_GPIO_137

MCU_INPUT_XBAR_GPIO138

MCU_GPIO_138

MCU_INPUT_XBAR_GPIO139

MCU_GPIO_139

MCU_INPUT_XBAR_GPIO140

MCU_GPIO_0_BANK_INTR_0

MCU_INPUT_XBAR_GPIO141

MCU_GPIO_0_BANK_INTR_1

MCU_INPUT_XBAR_GPIO142

MCU_GPIO_0_BANK_INTR_2

MCU_INPUT_XBAR_GPIO143

MCU_GPIO_0_BANK_INTR_3

MCU_INPUT_XBAR_ICSSGPO0_PORT0

MCU_GPIO_0_BANK_INTR_4

MCU_INPUT_XBAR_ICSSGPO1_PORT0

MCU_GPIO_0_BANK_INTR_5

MCU_INPUT_XBAR_ICSSGPO2_PORT0

MCU_GPIO_0_BANK_INTR_6

MCU_INPUT_XBAR_ICSSGPO3_PORT0

MCU_GPIO_0_BANK_INTR_7

MCU_INPUT_XBAR_ICSSGPO4_PORT0

MCU_GPIO_0_BANK_INTR_8

MCU_INPUT_XBAR_ICSSGPO5_PORT0

MCU_GPIO_1_BANK_INTR_0

MCU_INPUT_XBAR_ICSSGPO6_PORT0

MCU_GPIO_1_BANK_INTR_1

MCU_INPUT_XBAR_ICSSGPO7_PORT0

MCU_GPIO_1_BANK_INTR_2

MCU_INPUT_XBAR_ICSSGPO8_PORT0

MCU_GPIO_1_BANK_INTR_3

MCU_INPUT_XBAR_ICSSGPO9_PORT0

MCU_GPIO_1_BANK_INTR_4

MCU_INPUT_XBAR_ICSSGPO10_PORT0

MCU_GPIO_1_BANK_INTR_5

MCU_INPUT_XBAR_ICSSGPO11_PORT0

MCU_GPIO_1_BANK_INTR_6

MCU_INPUT_XBAR_ICSSGPO12_PORT0

MCU_GPIO_1_BANK_INTR_7

MCU_INPUT_XBAR_ICSSGPO13_PORT0

MCU_GPIO_1_BANK_INTR_8

MCU_INPUT_XBAR_ICSSGPO14_PORT0

MCU_GPIO_2_BANK_INTR_0

MCU_INPUT_XBAR_ICSSGPO15_PORT0

MCU_GPIO_2_BANK_INTR_1

MCU_INPUT_XBAR_ICSSGPO0_PORT1

MCU_GPIO_2_BANK_INTR_2

MCU_INPUT_XBAR_ICSSGPO1_PORT1

MCU_GPIO_2_BANK_INTR_3

MCU_INPUT_XBAR_ICSSGPO2_PORT1

MCU_GPIO_2_BANK_INTR_4

MCU_INPUT_XBAR_ICSSGPO3_PORT1

MCU_GPIO_2_BANK_INTR_5

MCU_INPUT_XBAR_ICSSGPO4_PORT1

MCU_GPIO_2_BANK_INTR_6

MCU_INPUT_XBAR_ICSSGPO5_PORT1

MCU_GPIO_2_BANK_INTR_7

MCU_INPUT_XBAR_ICSSGPO6_PORT1

MCU_GPIO_2_BANK_INTR_8

MCU_INPUT_XBAR_ICSSGPO7_PORT1

MCU_GPIO_3_BANK_INTR_0

MCU_INPUT_XBAR_ICSSGPO8_PORT1

MCU_GPIO_3_BANK_INTR_1

MCU_INPUT_XBAR_ICSSGPO9_PORT1

MCU_GPIO_3_BANK_INTR_2

MCU_INPUT_XBAR_ICSSGPO10_PORT1

MCU_GPIO_3_BANK_INTR_3

MCU_INPUT_XBAR_ICSSGPO11_PORT1

MCU_GPIO_3_BANK_INTR_4

MCU_INPUT_XBAR_ICSSGPO12_PORT1

MCU_GPIO_3_BANK_INTR_5

MCU_INPUT_XBAR_ICSSGPO13_PORT1

MCU_GPIO_3_BANK_INTR_6

MCU_INPUT_XBAR_ICSSGPO14_PORT1

MCU_GPIO_3_BANK_INTR_7

MCU_INPUT_XBAR_ICSSGPO15_PORT1

MCU_GPIO_3_BANK_INTR_8

4.19.3.3. States

No state is maintained in the MCU driver

4.19.3.4. Assumptions

None

4.19.3.5. Limitations

None

4.19.3.6. Design overview

Will be updated in future release

4.19.4. Hardware Features

4.19.4.1. Hardware Features supported

  • Initialization of Core clock, PLL Clock and peripheral clocks.

  • Initialization of RAM sections.

  • Activation of a µC reset.

  • Provides a service to get the reset reason from hardware.

  • ADC & PWM Enable from MCU.

  • Cross Bar supported: INPUTXBAR, INTXBAR.

4.19.4.2. AUTOSAR Features supported

  • Initialization of MCU clock, PLL, clock prescalers and MCU clock distribution.

  • MCU Reset/Read Reset Reason.

  • Core PLL and Peripheral PLL Supported.

  • Support to get the lock status of the PLL.

4.19.4.3. Not supported Features

  • Support to activate the MCU power modes

  • Cross Bar not supported: PWMXBAR, DMAXBAR, OUTPUTXBAR, PWMSYNCOUTXBAR.

4.19.4.4. Non compliance

4.19.4.4.1. Deviations to requirements (Requirement Traceability)

4.19.4.4.1.1. Deviation of requirements against AUTOSAR specification requirements

Will be updated in next release

4.19.5. Source files

Static source C Files are defined below

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Mcu
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Mcu.h : Contains the API’s of the Mcu driver to be used by upper layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Mcu.c : Contains the implementation of the API’s for Mcu driver.
┃ ┃ ┣ 📂V3
┃ ┃ ┃ ┗ 📜Mcu_Priv.c : Contains Functions that support the API’s for Mcu driver
┃ ┃ ┃ ┣ 📜Mcu_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┗ 📜Mcu_Xbar.h : Contains Macros for Interrupt and Input crossbar and function declarations.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt

Plugin files are defined below in the table.

Plugin Files

Description

Mcu_Cfg.h

Contains the Precompile switches, Symbolic names of McuClockSettingConfig

Mcu_PBcfg.c

Contains all Post-Build Configured parameters

Mcu_Cfg.c

Contains all Pre-Compile Configured parameters

MCU header file include structure

Fig. 4.82 MCU header file include structure

4.19.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.19.6.1. Memory Mapping

Memory Mapping Sections

MCU_CODE

MCU_DATA

MCU_PBCFG

MCU_START_SEC_VAR_INIT_UNSPECIFIED(.bss)

x

MCU_STOP_SEC_VAR_INIT_UNSPECIFIED

x

MCU_START_SEC_CODE(.text)

x

MCU_STOP_SEC_CODE

x

MCU_START_SEC_CONFIG_DATA(.data)

x

MCU_STOP_SEC_CONFIG_DATA

x

4.19.6.2. Scheduling

There are no scheduled functions within the MCU driver.

4.19.6.3. Error handling

4.19.6.3.1. Development Error Reporting (DET)

The errors reported to DET module are described in the following table:

Type of Error

Related Error code

Value (Hex)

API service called with incorrect configuration parameter

MCU_E_PARAM_CONFIG

0x0A

API service called with invalid clock id

MCU_E_PARAM_CLOCK

0x0B

API service called with invalid mode id

MCU_E_PARAM_MODE

0x0C

API service called with invalid ram section parameter

MCU_E_PARAM_RAMSECTION

0x0D

DET error reported when PLL is not locked

MCU_E_PLL_NOT_LOCKED

0x0E

API service used without module initialization

MCU_E_UNINIT

0x0F

API service called with NULL_PTR passed to MCU driver APIs

MCU_E_PARAM_POINTER

0x10

4.19.6.3.2. DEM Errors

The extended production errors reported to DEM module are described in the following table:

Type of Error

Related Error Code

Description

Assigned by DEM

MCU_E_CLOCK_FAILURE

This error is raised when there is an MCU Clock Source Failure

Note: MCU_E_MODE_FAILURE should be always disabled. Since Mcu_SetMode is not supported, MCU_E_MODE_FAILURE should always be disabled.

4.19.7. Used resources

4.19.7.1. Interrupt Handling

The MCU module doesn’t implement any Interrupt Service Routines.

4.19.8. Integration description

4.19.8.1. Dependent modules

4.19.8.1.1. DET

The module MCU depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch MCU_DEV_ERROR_DETECT = STD_ON in the Mcu_Cfg.h

AUTOSAR requires that API functions shall check the validity of their respective parameters. These checks are for development error reporting and can be enabled or disabled.

4.19.8.1.2. DEM

By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().

Note: Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.

4.19.8.1.3. Callback Notification

There are no Callback Notifications.

4.19.8.1.4. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that MCU module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator. For MCU Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

MCU Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

MCU_EXCLUSIVE_AREA_0

Mcu_PerformReset

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.19.8.2. Multi-core support

Not supported

4.19.9. Configuration

4.19.9.1. McuGeneralConfiguration

This container contains the configuration (parameters) of the MCU driver.

4.19.9.1.1. McuDevErrorDetect

Item

Name

McuDevErrorDetect

Description

Pre-processor switch for enabling the development error detection and reporting.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.2. McuIntrCrossbarEnable

Item

Name

McuIntrCrossbarEnable

Description

Pre-processor switch for enabling the Mcu Interrupt Crossbar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.19.9.1.3. McuInputCrossbarEnable

Item

Name

McuInputCrossbarEnable

Description

Pre-processor switch for enabling the Mcu Input Crossbar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.19.9.1.4. McuGetRamStateApi

Item

Name

McuGetRamStateApi

Description

Pre-processor switch to enable/disable the API Mcu_GetRamState.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.5. McuInitClock

Item

Name

McuInitClock

Description

If this parameter is set to FALSE, the clock initialization has to be disabled from the MCU driver. This concept applies when there are some write once clock registers and a bootloader is present. If this parameter is set to TRUE, the MCU driver is responsible of the clock initialization.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.6. McuNoPll

Item

Name

McuNoPll

Description

This parameter shall be set True, if the H/W does not have a PLL or the PLL circuitry is enabled after the power on without S/W intervention. In this case MCU_DistributePllClock has to be disabled and MCU_GetPllStatus has to return MCU_PLL_STATUS_UNDEFINED. Otherwise this parameters has to be set False

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.7. McuPerformResetApi

Item

Name

McuPerformResetApi

Description

Pre-processor switch to enable / disable the use of the function Mcu_PerformReset()

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.19.9.1.8. McuVersionInfoApi

Item

Name

McuVersionInfoApi

Description

Pre-processor switch to enable / disable the API to read out the modules version information.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.9. McuInitRamApi

Item

Name

McuInitRamApi

Description

Pre-processor switch to enable / disable the API to initialize RAM section.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.10. McuRegisterReadbackApi

Item

Name

McuRegisterReadbackApi

Description

Pre-processor switch to enable / disable the API to read MCU registers.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.19.9.1.11. McuDefaultOSCounterId

Item

Name

McuDefaultOSCounterId

Description

Default Os Counter Id if node reference to OsCounter ref McuOsCounterRef is not set

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

16

Min-value

0

4.19.9.1.12. McuTimeoutDuration

Item

Name

McuTimeoutDuration

Description

MCU timeout

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

32000

Max-value

4294967295

Min-value

1

4.19.9.1.13. McuPllTimeoutDuration

Item

Name

McuPllTimeoutDuration

Description

PLL timeout - used in Pll initialization.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

6600

Max-value

4294967295

Min-value

1

4.19.9.1.14. McuOsCounterRef

Item

Name

McuOsCounterRef

Description

This parameter contains a reference to the OsCounter, which is used by the MCU driver.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2. McuModuleConfiguration

This container contains the configuration (parameters) of the MCU driver

4.19.9.2.1. McuClockSrcFailureNotification

Item

Name

McuClockSrcFailureNotification

Description

Enables/Disables clock failure notification. In case this feature is not supported by HW the setting should be disabled.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

DISABLED

Range

DISABLED
ENABLED

4.19.9.2.2. McuNumberOfMcuModes

Item

Name

McuNumberOfMcuModes

Description

This parameter shall represent the number of Modes available for the MCU.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

255

Min-value

1

4.19.9.2.3. McuRamSectors

Item

Name

McuRamSectors

Description

This parameter shall represent the number of RAM sectors available for the MCU.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

4294967295

Min-value

1

4.19.9.2.4. McuResetSetting

Item

Name

McuResetSetting

Description

This parameter relates to the MCU specific reset configuration. This applies to the function Mcu_PerformReset, which performs a microcontroller reset using the hardware feature of the microcontroller.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

5

Max-value

255

Min-value

1

4.19.9.2.5. McuResetMode

Item

Name

McuResetMode

Description

Reset mode enum which can be used in Mcu_PerformReset

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_PERFORM_RESET_MODE_WARM

Range

MCU_PERFORM_RESET_MODE_WARM

4.19.9.2.6. McuClockSettingConfig

This container contains the configuration (parameters) for the Clock settings of the MCU. Please see MCU031 for more information on the MCU clock settings.

4.19.9.2.6.1. McuClockSettingId

Item

Name

McuClockSettingId

Description

The Id of this McuClockSettingConfig to be used as argument for the API call “Mcu_InitClock”.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

200

Max-value

255

Min-value

0

4.19.9.2.6.2. McuClockModuleId

Item

Name

McuClockModuleId

Description

ModuleId for which clock setting to be applied.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_CLKSRC_MODULE_ID_MCAN0

Range

MCU_CLKSRC_MODULE_ID_MCAN0
MCU_CLKSRC_MODULE_ID_MCAN1
MCU_CLKSRC_MODULE_ID_RTI0
MCU_CLKSRC_MODULE_ID_RTI1
MCU_CLKSRC_MODULE_ID_RTI2
MCU_CLKSRC_MODULE_ID_RTI3
MCU_CLKSRC_MODULE_ID_WDT0
MCU_CLKSRC_MODULE_ID_WDT1
MCU_CLKSRC_MODULE_ID_OSPI0
MCU_CLKSRC_MODULE_ID_OSPI1
MCU_CLKSRC_MODULE_ID_MCSPI0
MCU_CLKSRC_MODULE_ID_MCSPI1
MCU_CLKSRC_MODULE_ID_MCSPI2
MCU_CLKSRC_MODULE_ID_MCSPI3
MCU_CLKSRC_MODULE_ID_I2C
MCU_CLKSRC_MODULE_ID_SCI0
MCU_CLKSRC_MODULE_ID_SCI1
MCU_CLKSRC_MODULE_ID_SCI2
MCU_CLKSRC_MODULE_ID_SCI3
MCU_CLKSRC_MODULE_ID_SCI4
MCU_CLKSRC_MODULE_ID_SCI5
MCU_CLKSRC_MODULE_ID_CPTS
MCU_CLKSRC_MODULE_ID_PMIC_CLKOUT
MCU_CLKSRC_MODULE_ID_MCU_CLKOUT0
MCU_CLKSRC_MODULE_ID_MCU_CLKOUT1
MCU_CLKSRC_MODULE_ID_MII100_CLK
MCU_CLKSRC_MODULE_ID_MII10_CLK
MCU_CLKSRC_MODULE_ID_RGMI_CLK
MCU_CLKSRC_MODULE_ID_CONTROLSS_CLK

4.19.9.2.6.3. McuClockSourceId

Item

Name

McuClockSourceId

Description

Clock source Id for selected module

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_CLKSRC_0

Range

MCU_CLKSRC_0
MCU_CLKSRC_1
MCU_CLKSRC_2
MCU_CLKSRC_3
MCU_CLKSRC_4
MCU_CLKSRC_5
MCU_CLKSRC_6
MCU_CLKSRC_7

4.19.9.2.6.4. McuClockDivId

Item

Name

McuClockDivId

Description

McuClockDivider value should be less than or equal to 255 as per hardware limitation for MII10 and it should be less than or equal to 15 for all other modules.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

3

Max-value

255

Min-value

0

4.19.9.2.6.5. McuClockInitializationConfigFlag

Item

Name

McuClockInitializationConfigFlag

Description

Switch for enabling and disabling clock of the modules

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.19.9.2.7. McuClockReferencePoint

This container defines a reference point in the Mcu Clock tree. It defines the frequency which then can be used by other modules as an input value. Lower multiplicity is 1, as even in the simplest case (only one frequency is used), there is one frequency to be defined.

4.19.9.2.7.1. McuClockReferencePointFrequency

Item

Name

McuClockReferencePointFrequency

Description

This is the frequency for the specific instance of the McuClockReferencePoint container. It shall be given in Hz.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1.0

Max-value

INF

Min-value

0.0

4.19.9.2.8. McuXbarChannelTriggerConfiguration

This container contains the Xbar Channel Trigger condition.

4.19.9.2.8.1. McuInterruptChannelXbar

Item

Name

McuInterruptChannelXbar

Description

Cross Bar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_INTRXBAR0_OUT_0

Range

MCU_INTRXBAR0_OUT_0
MCU_INTRXBAR0_OUT_1
MCU_INTRXBAR0_OUT_2
MCU_INTRXBAR0_OUT_3
MCU_INTRXBAR0_OUT_4
MCU_INTRXBAR0_OUT_5
MCU_INTRXBAR0_OUT_6
MCU_INTRXBAR0_OUT_7
MCU_INTRXBAR0_OUT_8
MCU_INTRXBAR0_OUT_9
MCU_INTRXBAR0_OUT_10
MCU_INTRXBAR0_OUT_11
MCU_INTRXBAR0_OUT_12
MCU_INTRXBAR0_OUT_13
MCU_INTRXBAR0_OUT_14
MCU_INTRXBAR0_OUT_15
MCU_INTRXBAR0_OUT_16
MCU_INTRXBAR0_OUT_17
MCU_INTRXBAR0_OUT_18
MCU_INTRXBAR0_OUT_19
MCU_INTRXBAR0_OUT_20
MCU_INTRXBAR0_OUT_21
MCU_INTRXBAR0_OUT_22
MCU_INTRXBAR0_OUT_23
MCU_INTRXBAR0_OUT_24
MCU_INTRXBAR0_OUT_25
MCU_INTRXBAR0_OUT_26
MCU_INTRXBAR0_OUT_27
MCU_INTRXBAR0_OUT_28
MCU_INTRXBAR0_OUT_29
MCU_INTRXBAR0_OUT_30
MCU_INTRXBAR0_OUT_31

4.19.9.2.8.2. McuInterruptChannelXbarMap

Item

Name

McuInterruptChannelXbarMap

Description

Cross Bar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_INT_XBAR_EPWM0_INT

Range

MCU_INT_XBAR_EPWM0_INT
MCU_INT_XBAR_EPWM1_INT
MCU_INT_XBAR_EPWM2_INT
MCU_INT_XBAR_EPWM3_INT
MCU_INT_XBAR_EPWM4_INT
MCU_INT_XBAR_EPWM5_INT
MCU_INT_XBAR_EPWM6_INT
MCU_INT_XBAR_EPWM7_INT
MCU_INT_XBAR_EPWM8_INT
MCU_INT_XBAR_EPWM9_INT
MCU_INT_XBAR_EPWM0_TZINT
MCU_INT_XBAR_EPWM1_TZINT
MCU_INT_XBAR_EPWM2_TZINT
MCU_INT_XBAR_EPWM3_TZINT
MCU_INT_XBAR_EPWM4_TZINT
MCU_INT_XBAR_EPWM5_TZINT
MCU_INT_XBAR_EPWM6_TZINT
MCU_INT_XBAR_EPWM7_TZINT
MCU_INT_XBAR_EPWM8_TZINT
MCU_INT_XBAR_EPWM9_TZINT
MCU_INT_XBAR_ADC0_INT1
MCU_INT_XBAR_ADC0_INT2
MCU_INT_XBAR_ADC0_INT3
MCU_INT_XBAR_ADC0_INT4
MCU_INT_XBAR_ADC0_EVTINT
MCU_INT_XBAR_ADC1_INT1
MCU_INT_XBAR_ADC1_INT2
MCU_INT_XBAR_ADC1_INT3
MCU_INT_XBAR_ADC1_INT4
MCU_INT_XBAR_ADC1_EVTINT
MCU_INT_XBAR_ADC2_INT1
MCU_INT_XBAR_ADC2_INT2
MCU_INT_XBAR_ADC2_INT3
MCU_INT_XBAR_ADC2_INT4
MCU_INT_XBAR_ADC2_EVTINT
MCU_INT_XBAR_FSIRX0_INT1N
MCU_INT_XBAR_FSIRX0_INT2N
MCU_INT_XBAR_FSITX0_INT1N
MCU_INT_XBAR_FSITX0_INT2N
MCU_INT_XBAR_SD0_ERR
MCU_INT_XBAR_SD0_FILT0_DRINT
MCU_INT_XBAR_SD0_FILT1_DRINT
MCU_INT_XBAR_SD0_FILT2_DRINT
MCU_INT_XBAR_SD0_FILT3_DRINT
MCU_INT_XBAR_ECAP0_INT
MCU_INT_XBAR_ECAP1_INT
MCU_INT_XBAR_ECAP2_INT
MCU_INT_XBAR_ECAP3_INT
MCU_INT_XBAR_ECAP4_INT
MCU_INT_XBAR_ECAP5_INT
MCU_INT_XBAR_ECAP6_INT
MCU_INT_XBAR_ECAP7_INT
MCU_INT_XBAR_EQEP0_INT
MCU_INT_XBAR_EQEP1_INT

4.19.9.2.9. McuInputXbarChannelTriggerConfiguration

This container contains the Xbar Channel Trigger condition.

4.19.9.2.9.1. McuInputChannelXbar

Item

Name

McuInputChannelXbar

Description

Cross Bar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_INPUT_XBAR0_OUT_0

Range

MCU_INPUT_XBAR0_OUT_0
MCU_INPUT_XBAR0_OUT_1
MCU_INPUT_XBAR0_OUT_2
MCU_INPUT_XBAR0_OUT_3
MCU_INPUT_XBAR0_OUT_4
MCU_INPUT_XBAR0_OUT_5
MCU_INPUT_XBAR0_OUT_6
MCU_INPUT_XBAR0_OUT_7
MCU_INPUT_XBAR0_OUT_8
MCU_INPUT_XBAR0_OUT_9
MCU_INPUT_XBAR0_OUT_10
MCU_INPUT_XBAR0_OUT_11
MCU_INPUT_XBAR0_OUT_12
MCU_INPUT_XBAR0_OUT_13
MCU_INPUT_XBAR0_OUT_14
MCU_INPUT_XBAR0_OUT_15
MCU_INPUT_XBAR0_OUT_16
MCU_INPUT_XBAR0_OUT_17
MCU_INPUT_XBAR0_OUT_18
MCU_INPUT_XBAR0_OUT_19
MCU_INPUT_XBAR0_OUT_20
MCU_INPUT_XBAR0_OUT_21
MCU_INPUT_XBAR0_OUT_22
MCU_INPUT_XBAR0_OUT_23
MCU_INPUT_XBAR0_OUT_24
MCU_INPUT_XBAR0_OUT_25
MCU_INPUT_XBAR0_OUT_26
MCU_INPUT_XBAR0_OUT_27
MCU_INPUT_XBAR0_OUT_28
MCU_INPUT_XBAR0_OUT_29
MCU_INPUT_XBAR0_OUT_30
MCU_INPUT_XBAR0_OUT_31

4.19.9.2.9.2. McuInputChannelXbarMap

Item

Name

McuInputChannelXbarMap

Description

Cross Bar.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_INPUT_XBAR_GPIO0

Range

MCU_INPUT_XBAR_GPIO0
MCU_INPUT_XBAR_GPIO1
MCU_INPUT_XBAR_GPIO2
MCU_INPUT_XBAR_GPIO3
MCU_INPUT_XBAR_GPIO4
MCU_INPUT_XBAR_GPIO5
MCU_INPUT_XBAR_GPIO6
MCU_INPUT_XBAR_GPIO7
MCU_INPUT_XBAR_GPIO8
MCU_INPUT_XBAR_GPIO9
MCU_INPUT_XBAR_GPIO10
MCU_INPUT_XBAR_GPIO11
MCU_INPUT_XBAR_GPIO12
MCU_INPUT_XBAR_GPIO13
MCU_INPUT_XBAR_GPIO14
MCU_INPUT_XBAR_GPIO15
MCU_INPUT_XBAR_GPIO16
MCU_INPUT_XBAR_GPIO17
MCU_INPUT_XBAR_GPIO18
MCU_INPUT_XBAR_GPIO19
MCU_INPUT_XBAR_GPIO20
MCU_INPUT_XBAR_GPIO21
MCU_INPUT_XBAR_GPIO22
MCU_INPUT_XBAR_GPIO23
MCU_INPUT_XBAR_GPIO24
MCU_INPUT_XBAR_GPIO25
MCU_INPUT_XBAR_GPIO26
MCU_INPUT_XBAR_GPIO27
MCU_INPUT_XBAR_GPIO28
MCU_INPUT_XBAR_GPIO29
MCU_INPUT_XBAR_GPIO30
MCU_INPUT_XBAR_GPIO31
MCU_INPUT_XBAR_GPIO32
MCU_INPUT_XBAR_GPIO33
MCU_INPUT_XBAR_GPIO34
MCU_INPUT_XBAR_GPIO35
MCU_INPUT_XBAR_GPIO36
MCU_INPUT_XBAR_GPIO37
MCU_INPUT_XBAR_GPIO38
MCU_INPUT_XBAR_GPIO39
MCU_INPUT_XBAR_GPIO40
MCU_INPUT_XBAR_GPIO41
MCU_INPUT_XBAR_GPIO42
MCU_INPUT_XBAR_GPIO43
MCU_INPUT_XBAR_GPIO44
MCU_INPUT_XBAR_GPIO45
MCU_INPUT_XBAR_GPIO46
MCU_INPUT_XBAR_GPIO47
MCU_INPUT_XBAR_GPIO48
MCU_INPUT_XBAR_GPIO49
MCU_INPUT_XBAR_GPIO50
MCU_INPUT_XBAR_GPIO51
MCU_INPUT_XBAR_GPIO52
MCU_INPUT_XBAR_GPIO53
MCU_INPUT_XBAR_GPIO54
MCU_INPUT_XBAR_GPIO55
MCU_INPUT_XBAR_GPIO56
MCU_INPUT_XBAR_GPIO57
MCU_INPUT_XBAR_GPIO58
MCU_INPUT_XBAR_GPIO59
MCU_INPUT_XBAR_GPIO60
MCU_INPUT_XBAR_GPIO61
MCU_INPUT_XBAR_GPIO62
MCU_INPUT_XBAR_GPIO63
MCU_INPUT_XBAR_GPIO64
MCU_INPUT_XBAR_GPIO65
MCU_INPUT_XBAR_GPIO66
MCU_INPUT_XBAR_GPIO67
MCU_INPUT_XBAR_GPIO68
MCU_INPUT_XBAR_GPIO69
MCU_INPUT_XBAR_GPIO70
MCU_INPUT_XBAR_GPIO71
MCU_INPUT_XBAR_GPIO72
MCU_INPUT_XBAR_GPIO73
MCU_INPUT_XBAR_GPIO74
MCU_INPUT_XBAR_GPIO75
MCU_INPUT_XBAR_GPIO76
MCU_INPUT_XBAR_GPIO77
MCU_INPUT_XBAR_GPIO78
MCU_INPUT_XBAR_GPIO79
MCU_INPUT_XBAR_GPIO80
MCU_INPUT_XBAR_GPIO81
MCU_INPUT_XBAR_GPIO82
MCU_INPUT_XBAR_GPIO83
MCU_INPUT_XBAR_GPIO84
MCU_INPUT_XBAR_GPIO85
MCU_INPUT_XBAR_GPIO86
MCU_INPUT_XBAR_GPIO87
MCU_INPUT_XBAR_GPIO88
MCU_INPUT_XBAR_GPIO89
MCU_INPUT_XBAR_GPIO90
MCU_INPUT_XBAR_GPIO91
MCU_INPUT_XBAR_GPIO92
MCU_INPUT_XBAR_GPIO93
MCU_INPUT_XBAR_GPIO94
MCU_INPUT_XBAR_GPIO95
MCU_INPUT_XBAR_GPIO96
MCU_INPUT_XBAR_GPIO97
MCU_INPUT_XBAR_GPIO98
MCU_INPUT_XBAR_GPIO99
MCU_INPUT_XBAR_GPIO100
MCU_INPUT_XBAR_GPIO101
MCU_INPUT_XBAR_GPIO102
MCU_INPUT_XBAR_GPIO103
MCU_INPUT_XBAR_GPIO104
MCU_INPUT_XBAR_GPIO105
MCU_INPUT_XBAR_GPIO106
MCU_INPUT_XBAR_GPIO107
MCU_INPUT_XBAR_GPIO108
MCU_INPUT_XBAR_GPIO109
MCU_INPUT_XBAR_GPIO110
MCU_INPUT_XBAR_GPIO111
MCU_INPUT_XBAR_GPIO112
MCU_INPUT_XBAR_GPIO113
MCU_INPUT_XBAR_GPIO114
MCU_INPUT_XBAR_GPIO115
MCU_INPUT_XBAR_GPIO116
MCU_INPUT_XBAR_GPIO117
MCU_INPUT_XBAR_GPIO118
MCU_INPUT_XBAR_GPIO119
MCU_INPUT_XBAR_GPIO120
MCU_INPUT_XBAR_GPIO121
MCU_INPUT_XBAR_GPIO122
MCU_INPUT_XBAR_GPIO123
MCU_INPUT_XBAR_GPIO124
MCU_INPUT_XBAR_GPIO125
MCU_INPUT_XBAR_GPIO126
MCU_INPUT_XBAR_GPIO127
MCU_INPUT_XBAR_GPIO128
MCU_INPUT_XBAR_GPIO129
MCU_INPUT_XBAR_GPIO130
MCU_INPUT_XBAR_GPIO131
MCU_INPUT_XBAR_GPIO132
MCU_INPUT_XBAR_GPIO133
MCU_INPUT_XBAR_GPIO134
MCU_INPUT_XBAR_GPIO135
MCU_INPUT_XBAR_GPIO136
MCU_INPUT_XBAR_GPIO137
MCU_INPUT_XBAR_GPIO138
MCU_INPUT_XBAR_GPIO139
MCU_INPUT_XBAR_GPIO140
MCU_INPUT_XBAR_GPIO141
MCU_INPUT_XBAR_GPIO142
MCU_INPUT_XBAR_GPIO143
MCU_INPUT_XBAR_ICSSGPO0_PORT0
MCU_INPUT_XBAR_ICSSGPO1_PORT0
MCU_INPUT_XBAR_ICSSGPO2_PORT0
MCU_INPUT_XBAR_ICSSGPO3_PORT0
MCU_INPUT_XBAR_ICSSGPO4_PORT0
MCU_INPUT_XBAR_ICSSGPO5_PORT0
MCU_INPUT_XBAR_ICSSGPO6_PORT0
MCU_INPUT_XBAR_ICSSGPO7_PORT0
MCU_INPUT_XBAR_ICSSGPO8_PORT0
MCU_INPUT_XBAR_ICSSGPO9_PORT0
MCU_INPUT_XBAR_ICSSGPO10_PORT0
MCU_INPUT_XBAR_ICSSGPO11_PORT0
MCU_INPUT_XBAR_ICSSGPO12_PORT0
MCU_INPUT_XBAR_ICSSGPO13_PORT0
MCU_INPUT_XBAR_ICSSGPO14_PORT0
MCU_INPUT_XBAR_ICSSGPO15_PORT0
MCU_INPUT_XBAR_ICSSGPO0_PORT1
MCU_INPUT_XBAR_ICSSGPO1_PORT1
MCU_INPUT_XBAR_ICSSGPO2_PORT1
MCU_INPUT_XBAR_ICSSGPO3_PORT1
MCU_INPUT_XBAR_ICSSGPO4_PORT1
MCU_INPUT_XBAR_ICSSGPO5_PORT1
MCU_INPUT_XBAR_ICSSGPO6_PORT1
MCU_INPUT_XBAR_ICSSGPO7_PORT1
MCU_INPUT_XBAR_ICSSGPO8_PORT1
MCU_INPUT_XBAR_ICSSGPO9_PORT1
MCU_INPUT_XBAR_ICSSGPO10_PORT1
MCU_INPUT_XBAR_ICSSGPO11_PORT1
MCU_INPUT_XBAR_ICSSGPO12_PORT1
MCU_INPUT_XBAR_ICSSGPO13_PORT1
MCU_INPUT_XBAR_ICSSGPO14_PORT1
MCU_INPUT_XBAR_ICSSGPO15_PORT1

4.19.9.2.10. McuGpioXbarIntrConfiguration

This container contains channel/bank selection for each output pin of GPIO_XBAR_INTRTR0 routing module

4.19.9.2.10.1. McuGpioIntrXbar

Item

Name

McuGpioIntrXbar

Description

GPIO xbar Intr.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_GPIO_0

Range

MCU_GPIO_0
MCU_GPIO_1
MCU_GPIO_2
MCU_GPIO_3
MCU_GPIO_4
MCU_GPIO_5
MCU_GPIO_6
MCU_GPIO_7
MCU_GPIO_8
MCU_GPIO_9
MCU_GPIO_10
MCU_GPIO_11
MCU_GPIO_12
MCU_GPIO_13
MCU_GPIO_14
MCU_GPIO_15
MCU_GPIO_16
MCU_GPIO_17
MCU_GPIO_18
MCU_GPIO_19
MCU_GPIO_20
MCU_GPIO_21
MCU_GPIO_22
MCU_GPIO_23
MCU_GPIO_24
MCU_GPIO_25
MCU_GPIO_26
MCU_GPIO_27
MCU_GPIO_28
MCU_GPIO_29
MCU_GPIO_30
MCU_GPIO_31
MCU_GPIO_32
MCU_GPIO_33
MCU_GPIO_34
MCU_GPIO_35
MCU_GPIO_36
MCU_GPIO_37
MCU_GPIO_38
MCU_GPIO_39
MCU_GPIO_40
MCU_GPIO_41
MCU_GPIO_42
MCU_GPIO_43
MCU_GPIO_44
MCU_GPIO_45
MCU_GPIO_46
MCU_GPIO_47
MCU_GPIO_48
MCU_GPIO_49
MCU_GPIO_50
MCU_GPIO_51
MCU_GPIO_52
MCU_GPIO_53
MCU_GPIO_54
MCU_GPIO_55
MCU_GPIO_56
MCU_GPIO_57
MCU_GPIO_58
MCU_GPIO_59
MCU_GPIO_60
MCU_GPIO_61
MCU_GPIO_62
MCU_GPIO_63
MCU_GPIO_64
MCU_GPIO_65
MCU_GPIO_66
MCU_GPIO_67
MCU_GPIO_68
MCU_GPIO_69
MCU_GPIO_70
MCU_GPIO_71
MCU_GPIO_72
MCU_GPIO_73
MCU_GPIO_74
MCU_GPIO_75
MCU_GPIO_76
MCU_GPIO_77
MCU_GPIO_78
MCU_GPIO_79
MCU_GPIO_80
MCU_GPIO_81
MCU_GPIO_82
MCU_GPIO_83
MCU_GPIO_84
MCU_GPIO_85
MCU_GPIO_86
MCU_GPIO_87
MCU_GPIO_88
MCU_GPIO_89
MCU_GPIO_90
MCU_GPIO_91
MCU_GPIO_92
MCU_GPIO_93
MCU_GPIO_94
MCU_GPIO_95
MCU_GPIO_96
MCU_GPIO_97
MCU_GPIO_98
MCU_GPIO_99
MCU_GPIO_100
MCU_GPIO_101
MCU_GPIO_102
MCU_GPIO_103
MCU_GPIO_104
MCU_GPIO_105
MCU_GPIO_106
MCU_GPIO_107
MCU_GPIO_108
MCU_GPIO_109
MCU_GPIO_110
MCU_GPIO_111
MCU_GPIO_112
MCU_GPIO_113
MCU_GPIO_114
MCU_GPIO_115
MCU_GPIO_116
MCU_GPIO_117
MCU_GPIO_118
MCU_GPIO_119
MCU_GPIO_120
MCU_GPIO_121
MCU_GPIO_122
MCU_GPIO_123
MCU_GPIO_124
MCU_GPIO_125
MCU_GPIO_126
MCU_GPIO_127
MCU_GPIO_128
MCU_GPIO_129
MCU_GPIO_130
MCU_GPIO_131
MCU_GPIO_132
MCU_GPIO_133
MCU_GPIO_134
MCU_GPIO_135
MCU_GPIO_136
MCU_GPIO_137
MCU_GPIO_138
MCU_GPIO_139
MCU_GPIO_0_BANK_INTR_0
MCU_GPIO_0_BANK_INTR_1
MCU_GPIO_0_BANK_INTR_2
MCU_GPIO_0_BANK_INTR_3
MCU_GPIO_0_BANK_INTR_4
MCU_GPIO_0_BANK_INTR_5
MCU_GPIO_0_BANK_INTR_6
MCU_GPIO_0_BANK_INTR_7
MCU_GPIO_0_BANK_INTR_8
MCU_GPIO_1_BANK_INTR_0
MCU_GPIO_1_BANK_INTR_1
MCU_GPIO_1_BANK_INTR_2
MCU_GPIO_1_BANK_INTR_3
MCU_GPIO_1_BANK_INTR_4
MCU_GPIO_1_BANK_INTR_5
MCU_GPIO_1_BANK_INTR_6
MCU_GPIO_1_BANK_INTR_7
MCU_GPIO_1_BANK_INTR_8
MCU_GPIO_2_BANK_INTR_0
MCU_GPIO_2_BANK_INTR_1
MCU_GPIO_2_BANK_INTR_2
MCU_GPIO_2_BANK_INTR_3
MCU_GPIO_2_BANK_INTR_4
MCU_GPIO_2_BANK_INTR_5
MCU_GPIO_2_BANK_INTR_6
MCU_GPIO_2_BANK_INTR_7
MCU_GPIO_2_BANK_INTR_8
MCU_GPIO_3_BANK_INTR_0
MCU_GPIO_3_BANK_INTR_1
MCU_GPIO_3_BANK_INTR_2
MCU_GPIO_3_BANK_INTR_3
MCU_GPIO_3_BANK_INTR_4
MCU_GPIO_3_BANK_INTR_5
MCU_GPIO_3_BANK_INTR_6
MCU_GPIO_3_BANK_INTR_7
MCU_GPIO_3_BANK_INTR_8

4.19.9.2.10.2. McuGpioXbarOutMap

Item

Name

McuGpioXbarOutMap

Description

Gpio xbar output pin mapping

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MCU_GPIO_INT_XBAR_VIM_MODULE0_0

Range

MCU_GPIO_INT_XBAR_ICSS_XBAR_0
MCU_GPIO_INT_XBAR_ICSS_XBAR_1
MCU_GPIO_INT_XBAR_ICSS_XBAR_2
MCU_GPIO_INT_XBAR_ICSS_XBAR_3
MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_0
MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_1
MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_2
MCU_GPIO_INT_XBAR_DMA_TRIG_XBAR_3
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_0
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_1
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_2
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_3
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_4
MCU_GPIO_INT_XBAR_SOC_TIMESYNC_XBAR1_5
MCU_GPIO_INT_XBAR_VIM_MODULE0_0
MCU_GPIO_INT_XBAR_VIM_MODULE0_1
MCU_GPIO_INT_XBAR_VIM_MODULE0_2
MCU_GPIO_INT_XBAR_VIM_MODULE0_3
MCU_GPIO_INT_XBAR_VIM_MODULE1_0
MCU_GPIO_INT_XBAR_VIM_MODULE1_1
MCU_GPIO_INT_XBAR_VIM_MODULE1_2
MCU_GPIO_INT_XBAR_VIM_MODULE1_3
MCU_GPIO_INT_XBAR_VIM_MODULE2_0
MCU_GPIO_INT_XBAR_VIM_MODULE2_1
MCU_GPIO_INT_XBAR_VIM_MODULE2_2
MCU_GPIO_INT_XBAR_VIM_MODULE2_3
MCU_GPIO_INT_XBAR_VIM_MODULE3_0
MCU_GPIO_INT_XBAR_VIM_MODULE3_1
MCU_GPIO_INT_XBAR_VIM_MODULE3_2
MCU_GPIO_INT_XBAR_VIM_MODULE3_3

4.19.9.2.11. McuPwmConfiguration

This container contains the PWM clock configuration.

4.19.9.2.11.1. McuPwmChannelId

Item

Name

McuPwmChannelId

Description

PwmChannelId

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2.11.2. McuPwmGroupId

Item

Name

McuPwmGroupId

Description

PwmGroupId

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2.12. McuCddPwmConfiguration

This container contains the PWM clock configuration.

4.19.9.2.12.1. McuCddPwmChannelId

Item

Name

McuCddPwmChannelId

Description

CddPwmChannelId

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2.13. McuAdcConfiguration

This container contains the ADC buffer control configuration.

4.19.9.2.13.1. McuAdcHWUnitId

Item

Name

McuAdcHWUnitId

Description

AdcHwUnit

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2.14. McuDemEventParameterRefs

Item

Name

McuDemEventParameterRefs

Description

Reference to the DemEventParameter which shall be issued when the error “Timeout on blocking API call occurs “ has occurred.

Post-build-variant-multiplicity

false

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.19.9.2.15. McuModeSettingConf

This container contains the configuration (parameters) for the Mode setting of the MCU.

4.19.9.2.15.1. McuMode

Item

Name

McuMode

Description

The parameter represents the MCU Mode settings.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

200

Max-value

255

Min-value

0

4.19.9.2.16. McuRamSectorSettingConf

This container contains the configuration (parameters) for the RAM Sector setting. Please see MCU030 for more information on RAM sec-tor settings.

4.19.9.2.16.1. McuRamDefaultValue

Item

Name

McuRamDefaultValue

Description

This parameter shall represent the Data pre-setting to be initialized

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.19.9.2.16.2. McuRamSectionBaseAddress

Item

Name

McuRamSectionBaseAddress

Description

This parameter shall represent the MCU RAM section base address

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1879048192

Max-value

4294967295

Min-value

1

4.19.9.2.16.3. McuRamSectionSize

Item

Name

McuRamSectionSize

Description

This parameter represents the MCU RAM Section size in bytes.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

256

Max-value

4294967295

Min-value

0

4.19.9.2.16.4. McuRamSectionWriteSize

Item

Name

McuRamSectionWriteSize

Description

This parameter shall define the size in bytes of data which can be written into RAM at once.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

8

Max-value

4294967295

Min-value

0

Note: McuPllTimeoutDuration parameter Value should be passed as number of ticks according to clock frequency. The clock source have changed from RTI timers which used 200MHz clock frequency to R5f timers which uses 400MHz clock frequency, so the timeout values need to be configured accordingly.

4.19.9.3. Symbolic Names deviations

None

4.19.10. Examples

4.19.10.1. Overview

  1. Initialize MCU using Mcu_Init() and McuApp_Startup(). MCU module will initialize the clock for configured modules

  2. Do the Port and Platform initialization using Port_Init() and McuApp_PlatformInit()

  3. McuRamSectionBaseAddress is configured with ‘zero’ and reference array is also configured with default value of RAM section.

  4. Mcu_InitRamSection API is invoked in order to set ‘McuRamSectionBaseAddress’ with default value.

  5. Reference array and McuRamSectionBaseAddress is compared with each other to check whether RAM section is initialized properly or not.

  6. It will also check for reset reason.

  7. Mcu_GetResetReason API’s return value is compared with MCU_POWER_ON_RESET to check the wakeup cause.

4.19.10.2. Hardware Software Setup and Tools

None

4.19.10.3. Steps to build and run example

MCU example application demonstrating the MCAL MCU driver features is in folder <MCAL_ROOT>/examples/Mcu.

This application can be built from the root folder by giving gmake –s mcu_app PLATFORM=am261.

Once the build is completed we get a binary file, which is loaded in our controller and executed.

4.19.10.4. Example Logs


Mcu_App: Variant - Post Build being used !!!

McuApp: Sample Application - STARTS !!!
Mcu Driver version info:10.1.0
Mcu Driver Module/Driver:101.44 
RAM section is initialized properly
Wake up from Power ON
All tests have passed!!!
MCU Stack Usage: 808 bytes

4.19.10.5. File Structure

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Mcu
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜Makefile
┃ ┃ ┃ ┣ 📜McuApp.c : Contains MCU test example.
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Mcu_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h : Contains the Precompile switches, Symbolic names of McuClockSettingConfig.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_PBcfg.c : Contains all Post-Build Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt

Note

Mcu_PBcfg.c and Mcu_Cfg.c will be present if Post-Build config variant is selected, only Mcu_Cfg.c will be present if Pre-Compile variant is selected

4.19.11. FAQ’s

None

4.19.12. References

AUTOSAR_SWS_MCUDriver
Technical Reference Manual